This module defines function prototypes for use in defining
callback functions that support device-specific features (e.g.
synchronization with CPU Trace) and support customization and
extensibility of core UIA features (e.g. logging a range of memory values).
| typedef LoggerTypes_InjectIntoTraceFxn |
 |
Callback function that injects syncPoint info into GEM Trace
VALUES
serialNum
the serial number that is to be injected
ctxType
the context type ID to be injected into the trace
DETAILS
This callback function injects correlation info into the trace stream
to enable correlation between software events and hardware trace.
SEE
| typedef LoggerTypes_LogMemoryRangeFxn |
 |
Log an event along with values from a range of memory addresses
typedef Void (*
LoggerTypes_LogMemoryRangeFxn)(
Ptr,
Log_Event,
UInt32,
UInt32,
IArg,
IArg,
IArg,
IArg,
IArg);
VALUES
ptr
module instance object handle
evt
event to be logged
snapshotId
0 = no other snapshot groups, Use value from
LogSnapshot.getSnapshotId() for all snapshots to be
grouped.
fileName
__FILE__ result
lineNum
__LINE__ result
fmt
a printf style format string
startAdrs
value for first format conversion character
lengthInMAUs
value for second format conversion character
DETAILS
Note that this function can support logging of null terminated strings,
arrays of characters and memory mapped registgers as well as blocks of
memory. The LogSnapshot module uses this callback function.
Modules that implement the ILoggerSnapshot interface provide implementations
of this callback function.
SEE
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool LoggerTypes_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LoggerTypes_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 LoggerTypes_Module_getMask();
// Returns the diagnostics mask for this module
Void LoggerTypes_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module