| config Main.usage // module-wide |
 |
Usage for this command
Main.usage = String[] [
' ',
'Usage',
'[-p] [-h] [-m] [-e executable] [-x RTA XML file] [-o output text file] [-c delimter character]',
'[--help]',
' '
];
| Main.exec() // module-wide |
 |
xs script entry point
Main.exec(Any args) returns Any
DETAILS
This function is called from within other XDCscript scripts and
performs the same operations as
main() except that,
rather than output the return value of
inst.run(), this value
is simply returned to the caller of
exec().
| Main.main() // module-wide |
 |
xs shell entry point
Main.main(Any args) returns Any
DETAILS
This function
- creates a no-arg instance, inst, of the module inheriting
this interface;
- parses command line arguments placing all options in the config
params of the inheriting module;
- creates a xdc.tools.Cmdr instance, cmdr;
- calls inst.run() with the cmdr and any command
line command line arguments not parsed as options; and
- outputs the return result from inst.run()
| Instance Config Parameters |
 |
var params = new Main.Params;
// Instance config-params object
params.delimiter = String "|";
// // TODO
[-l output file for load data]
params.executable = String "";
// Path to the executable which was used to generate the data file
params.more = Bool false;
// Wait for the user to press enter before displaying the next packet
params.outputFile = String "";
// Optional path to an output file to write the decoded records to
params.printToScreen = Bool false;
// Whether to print the decoded records to the console
params.rtaXml = String "";
// Optional path to the RTA XML file
params.suppressHeader = Bool false;
// Don't print the header when printing the decoded records
| config Main.Params.delimiter // instance |
 |
// TODO
[-l output file for load data]
var params = new Main.Params;
...
params.delimiter = String "|";
DETAILS
Delimiter character to use when writing out the file.
The character specified here will be inserted between each of the
record fields so that the file can be imported into a spreadsheet
such as excel.
| config Main.Params.executable // instance |
 |
Path to the executable which was used to generate the data file
var params = new Main.Params;
...
params.executable = String "";
| config Main.Params.more // instance |
 |
Wait for the user to press enter before displaying the next packet
var params = new Main.Params;
...
params.more = Bool false;
DETAILS
Without this flag, the tool will simply print all of the records in the
data file to the screen. If this flag is set, then the tool will wait
the user to press enter in between displaying each packet.
| config Main.Params.outputFile // instance |
 |
Optional path to an output file to write the decoded records to
var params = new Main.Params;
...
params.outputFile = String "";
DETAILS
The tool will write the decoded records out as text to the specified
out file. The record properties will be separated with a delimeter
character so that they can be imported into a spreadsheet such as
Excel.
| config Main.Params.printToScreen // instance |
 |
Whether to print the decoded records to the console
var params = new Main.Params;
...
params.printToScreen = Bool false;
DETAILS
You may use this tool to simply print the decoded records, or you
may have them redirected to a file to be processed elsewhere.
| config Main.Params.rtaXml // instance |
 |
Optional path to the RTA XML file
var params = new Main.Params;
...
params.rtaXml = String "";
| config Main.Params.suppressHeader // instance |
 |
Don't print the header when printing the decoded records
var params = new Main.Params;
...
params.suppressHeader = Bool false;
| Main.run() // instance |
 |
Underlying implementation of the command
DETAILS
Since this method is used to support both command line tools and
other XDCscript scripts, it is important to avoid explicit
termination of the JVM via java.lang.System.exit(); doing so
precludes callers from handling failures.
Implementations should instead call