module ti.uia.sysbios.LoggerStreamer

This general purpose logger is useful in situations where the application wants to manage the buffers used to store and transmit events. This includes managing the sending of the buffers to an instrumentation host (e.g. System Analyzer in CCS). The logger is named "LoggerStreamer" because it is designed to enable the application to send a stream of packets containing UIA event data to the instrumentation host

The application is responsible for providing the buffers that LoggerStreamer uses. There are two ways to accomplish this. [ more ... ]
C synopsis target-domain sourced in ti/uia/sysbios/LoggerStreamer.xdc
#include <ti/uia/sysbios/LoggerStreamer.h>
Functions
Void
Void
Void
Void 
macro Void 
Void
Bool 
Void 
Functions common to all ILogger modules
Bool 
Bool 
Void 
Void 
Void 
Void 
Void 
LoggerStreamer_write8// Process a log event with 8 arguments and the calling address(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
Functions common to all IUIATransfer modules
Bool 
UInt16 
SizeT 
Bool 
Void 
Functions common to all IFilterLogger modules
Void 
Functions common to all ILoggerSnapshot modules
Void 
LoggerStreamer_writeMemoryRange// Log an event along with values from a range of memory addresses(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, UInt32 snapshotId, IArg fileName, IArg LineNum, IArg fmt, IArg startAdrs, UInt32 lengthInMAUs);
Functions common to all target instances
LoggerStreamer_handle// Convert this instance structure pointer into an instance handle, LoggerStreamer_Handle_downCast// conditionally move one level down the inheritance hierarchy; NULL upon failure, LoggerStreamer_Handle_downCast2// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure, LoggerStreamer_Handle_downCast3// conditionally move 3 levels down the inheritance hierarchy; NULL upon failure, LoggerStreamer_Handle_downCast4// conditionally move 4 levels down the inheritance hierarchy; NULL upon failure, LoggerStreamer_Handle_label// The label associated with this instance object, LoggerStreamer_Handle_name// The name of this instance object, LoggerStreamer_Handle_upCast// unconditionally move one level up the inheritance hierarchy, LoggerStreamer_Handle_upCast2// unconditionally move 2 levels up the inheritance hierarchy, LoggerStreamer_Handle_upCast3// unconditionally move 3 levels up the inheritance hierarchy, LoggerStreamer_Handle_upCast4// unconditionally move 4 levels up the inheritance hierarchy, LoggerStreamer_Object_count// The number of statically-created instance objects, LoggerStreamer_Object_first// The handle of the first dynamically-created instance object, or NULL, LoggerStreamer_Object_get// The handle of the i-th statically-created instance object (array == NULL), LoggerStreamer_Object_heap// The heap used to allocate dynamically-created instance objects, LoggerStreamer_Object_next// The handle of the next dynamically-created instance object, or NULL, LoggerStreamer_struct// Convert this instance handle into an instance structure pointer
Functions common to all target modules
Typedefs
typedef Ptr 
typedef struct
typedef struct
typedef Ptr 
typedef struct
typedef enum
typedef enum
Constants
extern const SizeT 
extern const String 
extern const Bool 
extern const Bool 
extern const Diags_Mask 
extern const Diags_Mask 
extern const Diags_Mask 
extern const Diags_Mask 
extern const SizeT 
extern const IFilterLogger_Handle 
extern const Bool 
extern const Bool 
 
DETAILS
The application is responsible for providing the buffers that LoggerStreamer uses. There are two ways to accomplish this.
  • Provide a prime callback function via the primeFxn configuration parameter.
  • Call the prime API once.
The logger stores the events in a UIAPacket event packet structure that allows them to be sent directly to System Analyzer (e.g. via UDP), enabling efficient streaming of the data from the target to the host. The first four 32-bit words contain a UIAPacket.Hdr structure. This struct is used by the host (e.g. System Analyzer in CCS) to help decode the data (e.g. endianess, length of data, etc.). The UIAPacket.Hdr structure is initialized via the initBuffer API. All buffers given to LoggerStreamer (via priming or exchange) must be initialized via initBuffer.
The size of buffer -*- includes UIAPacket_Hdr? LoggerStreamer treats the buffer as a UInt32 array. So the application must guarantee the buffers are aligned on word addresses. Alignment on cache line boundaries is recommended for best performance.
When the buffer is filled, LoggerStreamer will hand it off to the application using an application-provided exchange function (exchangeFxn). The exchange function must be of type ExchangeFxnType. The exchange function is called in the context of a log so generally the exchange function should be quick to execute.
The exchange function is called within the context of a Log call, so the exchange function should be designed to be fast. Since the exchange function is called within the context of the Log call, LoggerStreamer guarantees no Log records are dropped (i.e. LoggerStreamer is lossless).
LoggerStreamer was designed to have as minimal impact as possible on an application when calling a Log function. There are several configuration parameters that allow an application to get the optimal performance in exchange for certain restrictions.
Interrupts are disabled during the duration of the log call including when the exchange function is called. LoggerStreamer will ignore any log events generated during the exchangeFxn (e.g. posting a semaphore).
EXAMPLES
The following XDC configuration statements create a logger module, and assign it as the default logger for all modules.
  var Defaults = xdc.useModule('xdc.runtime.Defaults');
  var Diags = xdc.useModule('xdc.runtime.Diags');
  var LoggerStreamer = xdc.useModule('ti.uia.sysbios.LoggerStreamer');

  LoggerStreamer.bufSize = 1024;
  LoggerStreamer.isTimestampEnabled = true;
  LoggerStreamer.primeFxn = '&prime';
  LoggerStreamer.exchangeFxn = '&exchange';
  Defaults.common$.logger = LoggerStreamer.create();
The following C code demonstrates a basic prime and exchange example. A real implementation would send the buffer to an instrumentation host (e.g. System Analyzer in CCS) via a transport such as UDP.
  UInt32 buffer[2][BUFSIZE];

  Ptr prime()
  {
      LoggerStreamer_initBuffer(buffer[0], 0);
      LoggerStreamer_initBuffer(buffer[1], 0);
      return ((Ptr)(buffer[0]));
  }

  Ptr exchange(Ptr *full)
  {
      count++;
      // Ping-pong between the two buffers
      return ((Ptr*)buffer[count & 1]);
  }
 
enum LoggerStreamer_TransferType
C synopsis target-domain
typedef enum LoggerStreamer_TransferType {
    LoggerStreamer_TransferType_RELIABLE,
    LoggerStreamer_TransferType_LOSSY
} LoggerStreamer_TransferType;
 
 
enum LoggerStreamer_TransportType

Used to specify the type of transport to use

C synopsis target-domain
typedef enum LoggerStreamer_TransportType {
    LoggerStreamer_TransportType_UART,
    LoggerStreamer_TransportType_USB,
    LoggerStreamer_TransportType_ETHERNET,
    LoggerStreamer_TransportType_CUSTOM
} LoggerStreamer_TransportType;
 
DETAILS
This enum is used by the instrumentation host to determine what the transport is. It is not used by the target code.
 
typedef LoggerStreamer_ExchangeFxnType

Typedef for the exchange function pointer

C synopsis target-domain
typedef Ptr (*LoggerStreamer_ExchangeFxnType)(Ptr);
 
 
typedef LoggerStreamer_PrimeFxnType

Typedef for the exchange function pointer

C synopsis target-domain
typedef Ptr (*LoggerStreamer_PrimeFxnType)(Void);
 
 
config LoggerStreamer_bufSize  // module-wide

LoggerStreamer buffer size in MAUs (Minimum Addressable Units e.g. Bytes)

C synopsis target-domain
extern const SizeT LoggerStreamer_bufSize;
 
DETAILS
NOTE: the buffer size must contain an integer number of 32b words (e.g. if a MAU = 1 byte, then the buffer size must be a multiple of 4). The buffer size must also be at least maxEventSize + 64.
 
config LoggerStreamer_customTransportType  // module-wide

Custom transport used to send the records to an instrumentation host

C synopsis target-domain
extern const String LoggerStreamer_customTransportType;
 
DETAILS
If the desired transport is not in the TransportType enum, and transportType is set to TransportType_CUSTOM, this parameter must be filled in with the correct transport name.
If transportType is NOT set to TransportType_CUSTOM, this parameter is ignored.
 
config LoggerStreamer_exchangeFxn  // module-wide

Function pointer to the exchange function

C synopsis target-domain
extern const LoggerStreamer_ExchangeFxnType LoggerStreamer_exchangeFxn;
 
DETAILS
exchange function must return a pointer to a buffer that is word aligned, initialized with a UIA header and the correct size. This is called in the context of a log so generally the exchange function should be quick to execute.
 
config LoggerStreamer_filterByLevel  // module-wide

Support filtering of events by event level

C synopsis target-domain
extern const Bool LoggerStreamer_filterByLevel;
 
DETAILS
To improve logging performance, this feature can be disabled by setting filterByLevel to false.
See 'setFilterLevel' for an explanation of level filtering.
 
config LoggerStreamer_isTimestampEnabled  // module-wide

Enable or disable logging the 64b local CPU timestamp at the start of each event

C synopsis target-domain
extern const Bool LoggerStreamer_isTimestampEnabled;
 
DETAILS
Having a timestamp allows an instrumentation host (e.g. System Analyzer) to display events with the correct system time.
 
config LoggerStreamer_level1Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL1

C synopsis target-domain
extern const Diags_Mask LoggerStreamer_level1Mask;
 
DETAILS
See 'level4Mask' for details.
 
config LoggerStreamer_level2Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL2

C synopsis target-domain
extern const Diags_Mask LoggerStreamer_level2Mask;
 
DETAILS
See 'level4Mask' for details.
 
config LoggerStreamer_level3Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL3

C synopsis target-domain
extern const Diags_Mask LoggerStreamer_level3Mask;
 
DETAILS
See 'level4Mask' for details.
 
config LoggerStreamer_level4Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL4

C synopsis target-domain
extern const Diags_Mask LoggerStreamer_level4Mask;
 
DETAILS
If 'filterByLevel' is true, then all LoggerBuf instances will filter incoming events based on their event level.
The LoggerCircBuf module allows for specifying a different filter level for every Diags bit. These filtering levels are module wide; LoggerBuf does not support specifying the levels on a per-instance basis.
The setFilterLevel API can be used to change the filtering levels at runtime.
The default filtering levels are assigned using the 'level1Mask' - 'level4Mask' config parameters. These are used to specify, for each of the four event levels, the set of bits which should filter at that level by default.
The default filtering configuration sets the filter level to Diags.LEVEL4 for all logging-related diags bits so that all events are logged by default.
 
config LoggerStreamer_maxEventSize  // module-wide

The maximum event size (in Maus) that can be written with a single event. Must be less than or equal to bufSize - 64

C synopsis target-domain
extern const SizeT LoggerStreamer_maxEventSize;
 
DETAILS
The writeMemoryRange API checks to see if the event size required to write the block of memory is larger than maxEventSize. If so, it will split the memory range up into a number of smaller blocks and log the blocks using separate events with a common snapshot ID in order to allow the events to be collated and the original memory block to be reconstructed on the host.
 
config LoggerStreamer_primeFxn  // module-wide

Function pointer to the prime function

C synopsis target-domain
extern const LoggerStreamer_PrimeFxnType LoggerStreamer_primeFxn;
 
 
config LoggerStreamer_statusLogger  // module-wide

This configuration option is not supported by this logger and should be left null

C synopsis target-domain
extern const IFilterLogger_Handle LoggerStreamer_statusLogger;
 
 
config LoggerStreamer_supportLoggerDisable  // module-wide

Allow LoggerStreamer to be enabled/disabled during runtime

C synopsis target-domain
extern const Bool LoggerStreamer_supportLoggerDisable;
 
 
config LoggerStreamer_testForNullWrPtr  // module-wide

Protect against log calls during the exchange function

C synopsis target-domain
extern const Bool LoggerStreamer_testForNullWrPtr;
 
 
LoggerStreamer_flush()  // module-wide

Force LoggerStreamer to call the exchange function

C synopsis target-domain
Void LoggerStreamer_flush();
 
DETAILS
This API makes LoggerStreamer call the application provided exchangeFxn function if there are Log events present in the buffer.
The call to the exchangeFxn function is called in the context of the flush call.
 
LoggerStreamer_initBuffer()  // module-wide

Initializes the UIA packet header

C synopsis target-domain
macro Void LoggerStreamer_initBuffer(Ptr buffer, UInt16 src);
 
ARGUMENTS
buffer — Pointer to the buffer that LoggerStreamer will fill with Log events. The first four 32-bit words will contain the UIAPacket_Hdr structure.
src — Used to initialize the UIA source address. For a single core device, this will generally be 0. For multi-core devices, it generally corresponds to the DNUM (on C6xxxx deviecs) or the Ipc MultiProc id. It must be unique for all cores and match the configuration in the System Analyzer endpoint configuration.
DETAILS
This API is used to initialize a buffer before it is given to LoggerStreamer (via priming or exchange). The function initializes the UIAPacket portion of the buffer.
 
LoggerStreamer_prime()  // module-wide

If PrimeFxn is not set the user must call prime with the first buffer

C synopsis target-domain
Bool LoggerStreamer_prime(Ptr buffer);
 
 
LoggerStreamer_setModuleIdToRouteToStatusLogger()  // module-wide

This function is provided for compatibility with the ILoggerSnapshot interface only and simply returns when called

C synopsis target-domain
Void LoggerStreamer_setModuleIdToRouteToStatusLogger(Types_ModuleId mid);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId LoggerStreamer_Module_id();
// Get this module's unique id
 
Bool LoggerStreamer_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle LoggerStreamer_Module_heap();
// The heap from which this module allocates memory
 
Bool LoggerStreamer_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 LoggerStreamer_Module_getMask();
// Returns the diagnostics mask for this module
 
Void LoggerStreamer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct LoggerStreamer_Object LoggerStreamer_Object;
// Opaque internal representation of an instance object
 
typedef LoggerStreamer_Object *LoggerStreamer_Handle;
// Client reference to an instance object
 
typedef struct LoggerStreamer_Struct LoggerStreamer_Struct;
// Opaque client structure large enough to hold an instance object
 
LoggerStreamer_Handle LoggerStreamer_handle(LoggerStreamer_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
LoggerStreamer_Struct *LoggerStreamer_struct(LoggerStreamer_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct LoggerStreamer_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    IUIATransfer_TransferType transferType;
    // 
} LoggerStreamer_Params;
 
Void LoggerStreamer_Params_init(LoggerStreamer_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config LoggerStreamer_Params.transferType  // instance
C synopsis target-domain
      ...
    IUIATransfer_TransferType transferType;
 
Runtime Instance Creation

C synopsis target-domain
LoggerStreamer_Handle LoggerStreamer_create(const LoggerStreamer_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void LoggerStreamer_construct(LoggerStreamer_Struct *structP, const LoggerStreamer_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion

C synopsis target-domain
Void LoggerStreamer_delete(LoggerStreamer_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void LoggerStreamer_destruct(LoggerStreamer_Struct *structP);
// Finalize the instance object inside the provided structure
 
LoggerStreamer_disable()  // instance

Disable a log

C synopsis target-domain
Bool LoggerStreamer_disable(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled, FALSE if disabled) before the call. This return value allows clients to restore the previous state. Note: not thread safe.
 
LoggerStreamer_enable()  // instance

Enable a log

C synopsis target-domain
Bool LoggerStreamer_enable(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
RETURNS
The function returns the state of the log (TRUE if enabled, FALSE if disabled) before the call. This return value allows clients to restore the previous state. Note: not thread safe.
 
LoggerStreamer_getContents()  // instance

Fills buffer that is passed in with unread data, up to size bytes in length

C synopsis target-domain
Bool LoggerStreamer_getContents(LoggerStreamer_Handle handle, Ptr hdrBuf, SizeT size, SizeT *cpSize);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
hdrBuf — Ptr to a buffer that is at least <size> bytes in length
size — The max number of bytes to be read into the buffer
cpSize — The number of bytes actually copied
DETAILS
The logger is responsible for ensuring that no partial event records are stored in the buffer. Bytes are in target endianness.
RETURN
returns false if logger has no more records to read
 
LoggerStreamer_getFilterLevel()  // instance

Returns the mask of diags categories currently set to the specified level

C synopsis target-domain
Diags_Mask LoggerStreamer_getFilterLevel(LoggerStreamer_Handle handle, Diags_EventLevel level);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
See 'setFilterLevel' for an explanation of level filtering.
See 'setFilterLevel' for an explanation of level filtering.
 
LoggerStreamer_getInstanceId()  // instance

Returns an ID value that uniquely identifies this instance of the logger

C synopsis target-domain
UInt16 LoggerStreamer_getInstanceId(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Note that a value of 0 is reserved to indicate that the instance ID has not been initialized yet and a unique value needs to be generated.
 
LoggerStreamer_getMaxLength()  // instance
C synopsis target-domain
SizeT LoggerStreamer_getMaxLength(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
 
LoggerStreamer_getTransferType()  // instance
C synopsis target-domain
IUIATransfer_TransferType LoggerStreamer_getTransferType(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
 
LoggerStreamer_isEmpty()  // instance

Returns true if the transfer buffer has no unread data

C synopsis target-domain
Bool LoggerStreamer_isEmpty(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
RETURN
true if no unread data
 
LoggerStreamer_reset()  // instance

Reset a log to empty state and enable it

C synopsis target-domain
Void LoggerStreamer_reset(LoggerStreamer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
WARNING
This method is not synchronized with other instance methods and, as a result, it must never be called when there is a chance that another instance method is currently in operation or when another method on this instance may preempt this call.
 
LoggerStreamer_setFilterLevel()  // instance

Sets the level of detail that instances will log

C synopsis target-domain
Void LoggerStreamer_setFilterLevel(LoggerStreamer_Handle handle, Diags_Mask mask, Diags_EventLevel filterLevel);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
mask — The diags categories to set the level for
The diags categories to set the level for
filterLevel — The new filtering level for the specified categories
The new filtering level for the specified categories
DETAILS
Events with the specified level or higher will be logged, events below the specified level will be dropped.
Events are filtered first by diags category, then by level. If an event's diags category is disabled in the module's diags mask, then it will be filtered out regardless of level. The event will not even be passed to the logger.
This API allows for setting the filtering level for more than one diags category at a time. The mask parameter can be a single category or multiple categories combined, and the level will be set for all of those categories.
Events with the specified level or higher will be logged, events below the specified level will be dropped.
Events are filtered first by diags category, then by level. If an event's diags category is disabled in the module's diags mask, then it will be filtered out regardless of level. The event will not even be passed to the logger.
This API allows for setting the filtering level for more than one diags category at a time. The mask parameter can be a single category or multiple categories combined, and the level will be set for all of those categories.
 
LoggerStreamer_write0()  // instance

Process a log event with 0 arguments and the calling address

C synopsis target-domain
Void LoggerStreamer_write0(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Same as write4 except with 0 arguments rather than 4.
Same as write4 except with 0 arguments rather than 4.
SEE
 
LoggerStreamer_write1()  // instance

Process a log event with 1 arguments and the calling address

C synopsis target-domain
Void LoggerStreamer_write1(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, IArg a1);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Same as write4 except with 1 arguments rather than 4.
Same as write4 except with 1 arguments rather than 4.
SEE
 
LoggerStreamer_write2()  // instance

Process a log event with 2 arguments and the calling address

C synopsis target-domain
Void LoggerStreamer_write2(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, IArg a1, IArg a2);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Same as write4 except with 2 arguments rather than 4.
Same as write4 except with 2 arguments rather than 4.
SEE
 
LoggerStreamer_write4()  // instance

Process a log event with 4 arguments and the calling address

C synopsis target-domain
Void LoggerStreamer_write4(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, IArg a1, IArg a2, IArg a3, IArg a4);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
evt — event to be logged
mid — module ID of the module which logged the event
a1 — arbitrary argument passed by caller
DETAILS
The evt argument is of type Log.Event, which encodes the Log.EventId, the Diags.Mask, and the Diags.EventLevel of the event. The event ID can be obtained via Types.getEventId(evt), the Diags mask can be obtained via Diags.getMask(evt), and the event level can be obtained via Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the event.
The event information can be used by the logger to handle different events specially. For example, the event ID can be used to compare against other known Log.Events.
      if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
          :
      }
The Diags mask and event level can be used for filtering of events based on event level (see IFilterLogger), or even routing events to separate loggers based on diags category (see, for example, LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but are generally not recorded by the logger because they are not needed in decoding and displaying the event. A more suitable value to record is a Types.Event, which encodes the event ID and module ID. For example, the Log.EventRec type stores a Types.Event in its record definition. A Types.Event can be created using the Types.makeEvent API given the event ID and module ID.
The event ID value of 0 is used to indicate an event triggered by a call to one of the Log_print[0-6] methods. These methods take a format string rather than a Log_Event argument and, as a result, the event ID encoded in evt is 0 and the parameter a1 is the format string.
Non-zero event IDs can also be used to access the msg string associated with the Log.EventDesc that originally defined the Log event.
      Log_EventId id = Log_getEventId(evt));
      if (id != 0) {
          String msg = Text_ropeText(id);
          System_aprintf(msg, a1, a2, a3, a4);
      }
This works because an event's ID is simply an offset into a table of characters (maintained by the Text module) containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted according to the message format string associated with evt.
SEE
 
LoggerStreamer_write8()  // instance

Process a log event with 8 arguments and the calling address

C synopsis target-domain
Void LoggerStreamer_write8(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
DETAILS
Same as write4 except with 8 arguments rather than 4.
Same as write4 except with 8 arguments rather than 4.
SEE
 
LoggerStreamer_writeMemoryRange()  // instance

Log an event along with values from a range of memory addresses

C synopsis target-domain
Void LoggerStreamer_writeMemoryRange(LoggerStreamer_Handle handle, Log_Event evt, Types_ModuleId mid, UInt32 snapshotId, IArg fileName, IArg LineNum, IArg fmt, IArg startAdrs, UInt32 lengthInMAUs);
 
ARGUMENTS
handle — handle of a previously-created LoggerStreamer instance object
evt — event to be logged
snapshotId — 0 = no other snapshot groups, Use value from LogSnapshot.getSnapshotId() for all snapshots to be grouped.
fileName — __FILE__ result
lineNum — __LINE__ result
fmt — a printf style format string
startAdrs — value for first format conversion character
lengthInMAUs — value for second format conversion character
DETAILS
If the mask in the specified LogSnapshot event has any bit set which is also set in the current module's diagnostics mask, then this call to write will "raise" the given LogSnapshot event.
Note that this API supports null terminated strings, arrays of characters and memory mapped registgers as well as blocks of memory. The LogSnapshot module provides macros that map the appropriate values to the writeMemoryRange API's arguments
SEE
Instance Convertors

C synopsis target-domain
ILoggerSnapshot_Handle LoggerStreamer_Handle_upCast(LoggerStreamer_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
LoggerStreamer_Handle LoggerStreamer_Handle_downCast(ILoggerSnapshot_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IUIATransfer_Handle LoggerStreamer_Handle_upCast2(LoggerStreamer_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
LoggerStreamer_Handle LoggerStreamer_Handle_downCast2(IUIATransfer_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
 
IFilterLogger_Handle LoggerStreamer_Handle_upCast3(LoggerStreamer_Handle handle);
// unconditionally move 3 levels up the inheritance hierarchy
 
LoggerStreamer_Handle LoggerStreamer_Handle_downCast3(IFilterLogger_Handle handle);
// conditionally move 3 levels down the inheritance hierarchy; NULL upon failure
 
ILogger_Handle LoggerStreamer_Handle_upCast4(LoggerStreamer_Handle handle);
// unconditionally move 4 levels up the inheritance hierarchy
 
LoggerStreamer_Handle LoggerStreamer_Handle_downCast4(ILogger_Handle handle);
// conditionally move 4 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int LoggerStreamer_Object_count();
// The number of statically-created instance objects
 
LoggerStreamer_Handle LoggerStreamer_Object_get(LoggerStreamer_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
LoggerStreamer_Handle LoggerStreamer_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
LoggerStreamer_Handle LoggerStreamer_Object_next(LoggerStreamer_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle LoggerStreamer_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *LoggerStreamer_Handle_label(LoggerStreamer_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String LoggerStreamer_Handle_name(LoggerStreamer_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/uia/sysbios/LoggerStreamer.xdc
var LoggerStreamer = xdc.useModule('ti.uia.sysbios.LoggerStreamer');
module-wide constants & types
    values of type LoggerStreamer.TransferType// 
        const LoggerStreamer.TransferType_RELIABLE;
        const LoggerStreamer.TransferType_LOSSY;
 
        const LoggerStreamer.TransportType_UART;
        const LoggerStreamer.TransportType_USB;
        const LoggerStreamer.TransportType_ETHERNET;
        const LoggerStreamer.TransportType_CUSTOM;
 
        obj.instanceId = Int  ...
        obj.priority = Int  ...
 
    var obj = new LoggerStreamer.RecordView// ;
        obj.sequence = Int  ...
        obj.timestampRaw = Long  ...
        obj.modName = String  ...
        obj.text = String  ...
        obj.eventId = Int  ...
        obj.eventName = String  ...
        obj.arg0 = IArg  ...
        obj.arg1 = IArg  ...
        obj.arg2 = IArg  ...
        obj.arg3 = IArg  ...
        obj.arg4 = IArg  ...
        obj.arg5 = IArg  ...
        obj.arg6 = IArg  ...
        obj.arg7 = IArg  ...
module-wide config parameters
 
module-wide functions
per-instance config parameters
    var params = new LoggerStreamer.Params// Instance config-params object;
        params.ptrToQueueDescriptorMeta//  = Ptr null;
per-instance creation
    var inst = LoggerStreamer.create// Create an instance-object(params);
 
 
enum LoggerStreamer.TransferType
Configuration settings
values of type LoggerStreamer.TransferType
    const LoggerStreamer.TransferType_RELIABLE;
    const LoggerStreamer.TransferType_LOSSY;
 
C SYNOPSIS
 
enum LoggerStreamer.TransportType

Used to specify the type of transport to use

Configuration settings
values of type LoggerStreamer.TransportType
    const LoggerStreamer.TransportType_UART;
    const LoggerStreamer.TransportType_USB;
    const LoggerStreamer.TransportType_ETHERNET;
    const LoggerStreamer.TransportType_CUSTOM;
 
DETAILS
This enum is used by the instrumentation host to determine what the transport is. It is not used by the target code.
C SYNOPSIS
 
metaonly struct LoggerStreamer.MetaData

This data is added to the RTA MetaData file to support stop mode RTA

Configuration settings
var obj = new LoggerStreamer.MetaData;
 
    obj.instanceId = Int  ...
    obj.priority = Int  ...
 
 
metaonly struct LoggerStreamer.RecordView
Configuration settings
var obj = new LoggerStreamer.RecordView;
 
    obj.sequence = Int  ...
    obj.timestampRaw = Long  ...
    obj.modName = String  ...
    obj.text = String  ...
    obj.eventId = Int  ...
    obj.eventName = String  ...
    obj.arg0 = IArg  ...
    obj.arg1 = IArg  ...
    obj.arg2 = IArg  ...
    obj.arg3 = IArg  ...
    obj.arg4 = IArg  ...
    obj.arg5 = IArg  ...
    obj.arg6 = IArg  ...
    obj.arg7 = IArg  ...
 
 
config LoggerStreamer.bufSize  // module-wide

LoggerStreamer buffer size in MAUs (Minimum Addressable Units e.g. Bytes)

Configuration settings
LoggerStreamer.bufSize = SizeT 1400;
 
DETAILS
NOTE: the buffer size must contain an integer number of 32b words (e.g. if a MAU = 1 byte, then the buffer size must be a multiple of 4). The buffer size must also be at least maxEventSize + 64.
C SYNOPSIS
 
config LoggerStreamer.customTransportType  // module-wide

Custom transport used to send the records to an instrumentation host

Configuration settings
LoggerStreamer.customTransportType = String null;
 
DETAILS
If the desired transport is not in the TransportType enum, and transportType is set to TransportType_CUSTOM, this parameter must be filled in with the correct transport name.
If transportType is NOT set to TransportType_CUSTOM, this parameter is ignored.
C SYNOPSIS
 
config LoggerStreamer.exchangeFxn  // module-wide

Function pointer to the exchange function

Configuration settings
LoggerStreamer.exchangeFxn = Ptr(*)(Ptr) null;
 
DETAILS
exchange function must return a pointer to a buffer that is word aligned, initialized with a UIA header and the correct size. This is called in the context of a log so generally the exchange function should be quick to execute.
C SYNOPSIS
 
config LoggerStreamer.filterByLevel  // module-wide

Support filtering of events by event level

Configuration settings
LoggerStreamer.filterByLevel = Bool false;
 
DETAILS
To improve logging performance, this feature can be disabled by setting filterByLevel to false.
See 'setFilterLevel' for an explanation of level filtering.
C SYNOPSIS
 
config LoggerStreamer.isTimestampEnabled  // module-wide

Enable or disable logging the 64b local CPU timestamp at the start of each event

Configuration settings
LoggerStreamer.isTimestampEnabled = Bool false;
 
DETAILS
Having a timestamp allows an instrumentation host (e.g. System Analyzer) to display events with the correct system time.
C SYNOPSIS
 
config LoggerStreamer.level1Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL1

Configuration settings
LoggerStreamer.level1Mask = Bits16 0;
 
DETAILS
See 'level4Mask' for details.
C SYNOPSIS
 
config LoggerStreamer.level2Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL2

Configuration settings
LoggerStreamer.level2Mask = Bits16 0;
 
DETAILS
See 'level4Mask' for details.
C SYNOPSIS
 
config LoggerStreamer.level3Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL3

Configuration settings
LoggerStreamer.level3Mask = Bits16 0;
 
DETAILS
See 'level4Mask' for details.
C SYNOPSIS
 
config LoggerStreamer.level4Mask  // module-wide

Mask of diags categories whose initial filtering level is Diags.LEVEL4

Configuration settings
LoggerStreamer.level4Mask = Bits16 Diags.ALL_LOGGING;
 
DETAILS
If 'filterByLevel' is true, then all LoggerBuf instances will filter incoming events based on their event level.
The LoggerCircBuf module allows for specifying a different filter level for every Diags bit. These filtering levels are module wide; LoggerBuf does not support specifying the levels on a per-instance basis.
The setFilterLevel API can be used to change the filtering levels at runtime.
The default filtering levels are assigned using the 'level1Mask' - 'level4Mask' config parameters. These are used to specify, for each of the four event levels, the set of bits which should filter at that level by default.
The default filtering configuration sets the filter level to Diags.LEVEL4 for all logging-related diags bits so that all events are logged by default.
C SYNOPSIS
 
config LoggerStreamer.maxEventSize  // module-wide

The maximum event size (in Maus) that can be written with a single event. Must be less than or equal to bufSize - 64

Configuration settings
LoggerStreamer.maxEventSize = SizeT 512;
 
DETAILS
The writeMemoryRange API checks to see if the event size required to write the block of memory is larger than maxEventSize. If so, it will split the memory range up into a number of smaller blocks and log the blocks using separate events with a common snapshot ID in order to allow the events to be collated and the original memory block to be reconstructed on the host.
C SYNOPSIS
 
config LoggerStreamer.primeFxn  // module-wide

Function pointer to the prime function

Configuration settings
LoggerStreamer.primeFxn = Ptr(*)(Void) null;
 
C SYNOPSIS
 
config LoggerStreamer.statusLogger  // module-wide

This configuration option is not supported by this logger and should be left null

Configuration settings
LoggerStreamer.statusLogger = IFilterLogger.Handle null;
 
C SYNOPSIS
 
config LoggerStreamer.supportLoggerDisable  // module-wide

Allow LoggerStreamer to be enabled/disabled during runtime

Configuration settings
LoggerStreamer.supportLoggerDisable = Bool false;
 
C SYNOPSIS
 
config LoggerStreamer.testForNullWrPtr  // module-wide

Protect against log calls during the exchange function

Configuration settings
LoggerStreamer.testForNullWrPtr = Bool true;
 
C SYNOPSIS
 
metaonly config LoggerStreamer.common$  // module-wide

Common module configuration parameters

Configuration settings
LoggerStreamer.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config LoggerStreamer.moduleToRouteToStatusLogger  // module-wide

This configuration option is not supported by this logger and should be left unconfigured

Configuration settings
LoggerStreamer.moduleToRouteToStatusLogger = String undefined;
 
 
metaonly config LoggerStreamer.transportType  // module-wide

Transport used to send the records to an instrumentation host

Configuration settings
 
DETAILS
This parameter is used to specify the transport that the exchangeFxn function will use to send the buffer to an instrumentation host (e.g. System Analyzer in CCS).
This parameter is placed into the generated UIA XML file. The instrumentation host can use the XML file to help it auto-detect as much as possible and act accordingly.
If the desired transport is not in the TransportType enum, select TransportType_CUSTOM and set the customTransportType string with the desired string.
 
metaonly LoggerStreamer.getLoggerInstanceId()  // module-wide

returns the id of this logger instance

Configuration settings
LoggerStreamer.getLoggerInstanceId(Any inst) returns Any
 
 
metaonly LoggerStreamer.getMetaArgs()  // module-wide

Returns any meta data needed to support RTA

Configuration settings
LoggerStreamer.getMetaArgs(Any inst, Any instNum) returns Any
 
DETAILS
This meta data should be returned in the form of a structure which can be converted into XML. This data is added to the RTA XML file during the application's configuration, and can be accessed later through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of the ILogger's static instances.
 
metaonly LoggerStreamer.getPtrToQueueDescriptorMeta()  // module-wide

Each logger instance has a unique queue descriptor address that is stored in the Event Record header to identify itself to the host. This metaonly configuration parameter allows the UIA Metadata to determine what the address is for each statically created logger instance in order to emit XML code to allow the host to look up information about the logger instance (such as its name) based on the queue descriptor address that is stored in the event record header

Configuration settings
LoggerStreamer.getPtrToQueueDescriptorMeta(Any inst) returns Any
 
DETAILS
The pointer is returned per instance of the logger module. The instance object is passed to the function as the first argument.
 
metaonly LoggerStreamer.setPtrToQueueDescriptorMeta()  // module-wide

Sets the queue descriptor address in the logger's object instance data

Configuration settings
LoggerStreamer.setPtrToQueueDescriptorMeta(Any inst, Any queueDescriptorAdrs) returns Any
 
Instance Config Parameters

Configuration settings
var params = new LoggerStreamer.Params;
// Instance config-params object
    params.ptrToQueueDescriptorMeta = Ptr null;
    // 
    // 
 
config LoggerStreamer.Params.transferType  // instance
Configuration settings
var params = new LoggerStreamer.Params;
  ...
 
C SYNOPSIS
 
metaonly config LoggerStreamer.Params.ptrToQueueDescriptorMeta  // instance
Configuration settings
var params = new LoggerStreamer.Params;
  ...
params.ptrToQueueDescriptorMeta = Ptr null;
 
Static Instance Creation

Configuration settings
var params = new LoggerStreamer.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = LoggerStreamer.create(params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
generated on Tue, 17 Oct 2017 18:21:19 GMT