interface xdc.runtime.ITimestampClient

Timestamp Client Interface

This interface defines the methods used by client applications to get timestamp values. It is implemented by the Timestamp module.
XDCspec summary sourced in xdc/runtime/ITimestampClient.xdc
interface ITimestampClient {  ...
// inherits xdc.runtime.IModule
XDCspec declarations sourced in xdc/runtime/ITimestampClient.xdc
package xdc.runtime;
 
interface ITimestampClient {
module-wide config parameters
module-wide functions
}
 
metaonly config ITimestampClient.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in xdc/runtime/ITimestampClient.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
ITimestampClient.get32()  // module-wide

Return a 32-bit timestamp

XDCspec declarations sourced in xdc/runtime/ITimestampClient.xdc
Bits32 get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
ITimestampClient.get64()  // module-wide

Return a 64-bit timestamp

XDCspec declarations sourced in xdc/runtime/ITimestampClient.xdc
Void get64(Types.Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
ITimestampClient.getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

XDCspec declarations sourced in xdc/runtime/ITimestampClient.xdc
Void getFreq(Types.FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
generated on Tue, 17 Oct 2017 18:21:27 GMT