module ti.uiactools.runtime.EventHdr

Module defines the header format to be used when logging an event

Each event's first word includes the type, length of the event and sequence number. The length includes the first word and is in bytes. [ more ... ]
C synopsis target-domain sourced in ti/uiactools/runtime/EventHdr.xdc
#include <ti/uiactools/runtime/EventHdr.h>
Functions
macro UInt32 
macro SizeT 
macro UInt16 
macro Void 
macro Void 
macro Void 
Functions common to all target modules
Typedefs
typedef enum
 
DETAILS
Each event's first word includes the type, length of the event and sequence number. The length includes the first word and is in bytes.
The following is the desciption of the first word.
  EventHdr
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |H H H H H|L L L L L L L L L L L|S S S S S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  H = HdrType         (5-bits)
  L = Event Length    (11-bits)
  S = Sequence Number (16-bits)
There are currently 4 different types of events supported in UIA. The following discusses the format of each one of the types.
  HdrType_Event
    word0: EventHdr
    word1: event Id (top 16 bits) & module Id (bottom 16 bits)

  HdrType_EventWithTimestamp
    word0: EventHdr
    word1: Timestamp lower 32 bits
    word2: Timestamp upper 32 bits
    word3: event Id (top 16 bits) & module Id (bottom 16 bits)

  HdrType_EventWithSnapshotId
    word0: EventHdr
    word1: event Id (top 16 bits) & module Id (bottom 16 bits)
    word2: filename pointer
    word3: linenum
    word4: snapshotId
    word5: address where the data was located
    word6: total length of data (top 16-bits)
           length for this record (bottom 16 bits)
    word7: format pointer
    data:  the rest of the record contains the data

  HdrType_EventWithSnapshotIdAndTimestamp: 
    word0: EventHdr
    word1: Timestamp lower 32 bits
    word2: Timestamp upper 32 bits
    word3: event Id (top 16 bits) & module Id (bottom 16 bits)
    word4: filename pointer
    word5: linenum
    word6: snapshotId
    word7: address where the data was located
    word8: total length of data (top 16-bits)
           length for this record (bottom 16 bits)
    word9: format pointer
    data:  the rest of the record contains the data

  Snapshot events can span multiple records. The snapshotId is used to
  correlate the records when this occurs.
  The length field (word6 or word8) contains two lengths. The bottom 16 bits
  length of data for this record. The top 16 bits is the sum of all 
  lengths for this specific snapshotId. 

  The address field points to the location of the data. When the snapshot
  spans multiple records, the address field is updated accordingly. Therefore
  this field can be used to detect dropped records. Note the snapshot
  event data is contiguous.
For shared, non-packetized event transports that carry events from multiple cores, or for events logged by applications runnning on multiprocess O/Ses, the event header needs to identify which endpoint ID the event was logged from and which process Id logged the event. The following two additional event headers support these situations.
HdrType_EventWithTimestampAndEndpointId word0: EventHdr word1: Timestamp lower 32 bits word2: Timestamp upper 32 bits word3: EndpointId (lower 16 bits) word4: ProcessId word3: event Id (top 16 bits) & module Id (bottom 16 bits)
HdrType_EventWithSnapshotIdAndTimestampAndEndpointId: word0: EventHdr word1: Timestamp lower 32 bits word2: Timestamp upper 32 bits word3: EndpointId (lower 16 bits) word4: ProcessId word5: event Id (top 16 bits) & module Id (bottom 16 bits) word6: filename pointer word7: linenum word8: snapshotId word9: address where the data was located word10: total length of data (top 16-bits) length for this record (bottom 16 bits) word11: format pointer data: the rest of the record contains the data
 
enum EventHdr_HdrType

Enumeration of the various types of events headers

C synopsis target-domain
typedef enum EventHdr_HdrType {
    EventHdr_HdrType_Event,
    // Event with no timestamp or other optional parameters
    EventHdr_HdrType_EventWithTimestamp,
    // Event with 64 bit Timestamp
    EventHdr_HdrType_EventWithSnapshotId,
    // Snapshot event
    EventHdr_HdrType_EventWithSnapshotIdAndTimestamp,
    // Snapshot event with 64 bit Timestamp
    EventHdr_HdrType_Reserved4,
    // reserved for future use
    EventHdr_HdrType_EventWithTimestampAndEndpointId,
    // Event with 64 bit Timestamp, endpoint ID and process Id
    EventHdr_HdrType_Reserved6,
    // reserved for future use
    EventHdr_HdrType_EventWithSnapshotIdAndTimestampAndEndpointId,
    // Snapshot event with 64 bit Timestamp, Endpoint and processId
    EventHdr_HdrType_Reserved8,
    // reserved for future use
    EventHdr_HdrType_Reserved9,
    // reserved for future use
    EventHdr_HdrType_Reserved10,
    // reserved for future use
    EventHdr_HdrType_Reserved11,
    // reserved for future use
    EventHdr_HdrType_Reserved12,
    // reserved for future use
    EventHdr_HdrType_Reserved13,
    // reserved for future use
    EventHdr_HdrType_Reserved14,
    // reserved for future use
    EventHdr_HdrType_Reserved15,
    // reserved for future use
    EventHdr_HdrType_Reserved16,
    // reserved for future use
    EventHdr_HdrType_Reserved17,
    // reserved for future use
    EventHdr_HdrType_Reserved18,
    // reserved for future use
    EventHdr_HdrType_Reserved19,
    // reserved for future use
    EventHdr_HdrType_Reserved20,
    // reserved for future use
    EventHdr_HdrType_Reserved21,
    // reserved for future use
    EventHdr_HdrType_Reserved22,
    // reserved for future use
    EventHdr_HdrType_Reserved23,
    // reserved for future use
    EventHdr_HdrType_Reserved24,
    // reserved for future use
    EventHdr_HdrType_Reserved25,
    // reserved for future use
    EventHdr_HdrType_Reserved26,
    // reserved for future use
    EventHdr_HdrType_Reserved27,
    // reserved for future use
    EventHdr_HdrType_Reserved28,
    // reserved for future use
    EventHdr_HdrType_Reserved29,
    // reserved for future use
    EventHdr_HdrType_Reserved30,
    // reserved for future use
    EventHdr_HdrType_Reserved31
    // reserved for future use
} EventHdr_HdrType;
 
DETAILS
Stored in a 5 bit bitfield (b31-b27) of the first word in the event.
 
EventHdr_genEventHdrWord1()  // module-wide

generates the first word to use in an Event header

C synopsis target-domain
macro UInt32 EventHdr_genEventHdrWord1(SizeT numBytesInEventMsg, UInt16 seqCount, EventHdr_HdrType eventHdrType);
 
ARGUMENTS
numBytesInEventMsg — number of bytes in the event
seqCount — sequence count number to tag the event with
eventHdrType — enum value indicating the format of the event header
 
EventHdr_getHdrType()  // module-wide

Gets the message header type from the first word of the event header

C synopsis target-domain
macro EventHdr_HdrType EventHdr_getHdrType(UInt32 eventWord1);
 
ARGUMENTS
eventWord1 — first word of the event header
RETURNS
HdrType of the event
 
EventHdr_getLength()  // module-wide

gets the event length (in bytes) from the event header

C synopsis target-domain
macro SizeT EventHdr_getLength(UInt32 eventWord1);
 
ARGUMENTS
eventWord1 — first word of the event header
 
EventHdr_getSeqCount()  // module-wide

gets the sequence count from the message header

C synopsis target-domain
macro UInt16 EventHdr_getSeqCount(UInt32 eventWord1);
 
ARGUMENTS
eventWord1 — first word of the event header
 
EventHdr_setHdrType()  // module-wide

Sets the header type in the event header

C synopsis target-domain
macro Void EventHdr_setHdrType(UInt32 eventWord1, EventHdr_HdrType hdrType);
 
ARGUMENTS
eventWord1 — the first word of the event header to be updated
HdrType hdrType — the new header type
 
EventHdr_setLength()  // module-wide

sets the event length (in bytes) in the event header

C synopsis target-domain
macro Void EventHdr_setLength(UInt32 eventWord1, SizeT eventLength);
 
ARGUMENTS
eventWord1 — first word of the event header
eventLength — the new event length
 
EventHdr_setSeqCount()  // module-wide

sets the sequence count in the message header

C synopsis target-domain
macro Void EventHdr_setSeqCount(UInt32 eventWord1, UInt16 seqCount);
 
ARGUMENTS
eventWord1 — first word of the event header
seqCount — the new message sequence count
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId EventHdr_Module_id();
// Get this module's unique id
 
Bool EventHdr_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle EventHdr_Module_heap();
// The heap from which this module allocates memory
 
Bool EventHdr_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 EventHdr_Module_getMask();
// Returns the diagnostics mask for this module
 
Void EventHdr_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/uiactools/runtime/EventHdr.xdc
var EventHdr = xdc.useModule('ti.uiactools.runtime.EventHdr');
module-wide constants & types
module-wide config parameters
 
 
enum EventHdr.HdrType

Enumeration of the various types of events headers

XDCscript usage meta-domain
values of type EventHdr.HdrType
    const EventHdr.HdrType_Event;
    // Event with no timestamp or other optional parameters
    const EventHdr.HdrType_EventWithTimestamp;
    // Event with 64 bit Timestamp
    const EventHdr.HdrType_EventWithSnapshotId;
    // Snapshot event
    const EventHdr.HdrType_EventWithSnapshotIdAndTimestamp;
    // Snapshot event with 64 bit Timestamp
    const EventHdr.HdrType_Reserved4;
    // reserved for future use
    const EventHdr.HdrType_EventWithTimestampAndEndpointId;
    // Event with 64 bit Timestamp, endpoint ID and process Id
    const EventHdr.HdrType_Reserved6;
    // reserved for future use
    const EventHdr.HdrType_EventWithSnapshotIdAndTimestampAndEndpointId;
    // Snapshot event with 64 bit Timestamp, Endpoint and processId
    const EventHdr.HdrType_Reserved8;
    // reserved for future use
    const EventHdr.HdrType_Reserved9;
    // reserved for future use
    const EventHdr.HdrType_Reserved10;
    // reserved for future use
    const EventHdr.HdrType_Reserved11;
    // reserved for future use
    const EventHdr.HdrType_Reserved12;
    // reserved for future use
    const EventHdr.HdrType_Reserved13;
    // reserved for future use
    const EventHdr.HdrType_Reserved14;
    // reserved for future use
    const EventHdr.HdrType_Reserved15;
    // reserved for future use
    const EventHdr.HdrType_Reserved16;
    // reserved for future use
    const EventHdr.HdrType_Reserved17;
    // reserved for future use
    const EventHdr.HdrType_Reserved18;
    // reserved for future use
    const EventHdr.HdrType_Reserved19;
    // reserved for future use
    const EventHdr.HdrType_Reserved20;
    // reserved for future use
    const EventHdr.HdrType_Reserved21;
    // reserved for future use
    const EventHdr.HdrType_Reserved22;
    // reserved for future use
    const EventHdr.HdrType_Reserved23;
    // reserved for future use
    const EventHdr.HdrType_Reserved24;
    // reserved for future use
    const EventHdr.HdrType_Reserved25;
    // reserved for future use
    const EventHdr.HdrType_Reserved26;
    // reserved for future use
    const EventHdr.HdrType_Reserved27;
    // reserved for future use
    const EventHdr.HdrType_Reserved28;
    // reserved for future use
    const EventHdr.HdrType_Reserved29;
    // reserved for future use
    const EventHdr.HdrType_Reserved30;
    // reserved for future use
    const EventHdr.HdrType_Reserved31;
    // reserved for future use
 
DETAILS
Stored in a 5 bit bitfield (b31-b27) of the first word in the event.
C SYNOPSIS
 
metaonly config EventHdr.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
EventHdr.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 27 Jun 2012 04:11:42 GMT