module ti.uiactools.runtime.UIAPacket

Packet format communications between instrumentation clients and instrumentation endpoints

C synopsis target-domain sourced in ti/uiactools/runtime/UIAPacket.xdc
#include <ti/uiactools/runtime/UIAPacket.h>
Functions
macro UInt16 
macro UInt16 
macro UInt16 
macro Int32 
macro Bool 
macro Int32 
Int32 
macro Bits16 
macro Bits16 
macro Int32 
macro Bits32 
macro UInt16 
macro UInt16 
macro UInt16 
macro UInt16 
macro Bits32 
macro UInt16 
macro Void 
UIAPacket_initEventRecHdr// initializes all bitfields in the event packet header(UIAPacket_Hdr *pHdr, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs);
macro Void 
UIAPacket_initEventRecWithPIDHdr// initializes all bitfields in the event packet header(UIAPacket_Hdr5 *pHdr, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs, UInt32 processId);
macro Void 
UIAPacket_initMsgHdr// initializes all bitfields in the message header(UIAPacket_Hdr *pHdr, UIAPacket_PayloadEndian endianness, UIAPacket_MsgType msgType, UInt16 msgLength, UInt16 serviceId, UInt16 seqCount, UInt16 cmdId, UInt32 tag, UInt16 destAdrs, UInt16 senderAdrs);
macro Void 
macro Void 
UIAPacket_initTraceRecHdr// initializes all bitfields in the trace packet header(UIAPacket_Hdr7 *pHdr, UIAPacket_HdrType traceHdrType, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs, UInt32 processId, UInt16 endpointNumber, Bool isFirstPacket, UInt16 tracePktDownCount, UInt16 traceSnapshotNumber);
macro Void 
macro Void 
macro Void 
macro Void 
macro Void 
macro Void 
macro Void 
macro Void 
macro Void 
macro Bits32 
macro Void 
macro Void 
macro Void 
macro Void 
macro Bits32 
macro Bits16 
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
typedef struct
typedef enum
typedef enum
typedef enum
typedef enum
Constants
extern const Int 
 
 
const UIAPacket_BROADCAST

Used to denote a broadcast message

C synopsis target-domain
#define UIAPacket_BROADCAST (UInt16)0xFFFE
 
DETAILS
The broadcast address is always 0xFFFE.
 
const UIAPacket_HOST

The address of the host

C synopsis target-domain
#define UIAPacket_HOST (UInt16)0xFFFF
 
DETAILS
The host address is always 0xFFFF.
 
enum UIAPacket_HdrType

Enumeration of the various types of packet headers

C synopsis target-domain
typedef enum UIAPacket_HdrType {
    UIAPacket_HdrType_InvalidData,
    // Invalid Data packet (1 word header)
    UIAPacket_HdrType_MsgWithPID,
    // Message with Process ID (5 word header)
    UIAPacket_HdrType_EventPktWithPID,
    // Event rec. with Process ID containing multiple events: (5 word hdr)
    UIAPacket_HdrType_Reserved1,
    // reserved for future use
    UIAPacket_HdrType_Reserved2,
    // reserved for future use
    UIAPacket_HdrType_Reserved3,
    // reserved for future use
    UIAPacket_HdrType_Reserved4,
    // reserved for future use
    UIAPacket_HdrType_Reserved5,
    // reserved for future use
    UIAPacket_HdrType_Reserved6,
    // reserved for future use
    UIAPacket_HdrType_Reserved7,
    // reserved for future use
    UIAPacket_HdrType_ChannelizedData,
    // Channelized data stream
    UIAPacket_HdrType_Msg,
    // Message (4 word header)
    UIAPacket_HdrType_EventPkt,
    // Event rec. containing multiple events: (4 word hdr)
    UIAPacket_HdrType_CPUTrace,
    // CPU Trace ETB data (7 word hdr)
    UIAPacket_HdrType_STMTrace,
    // STM Trace ETB data (7 word hdr)
    UIAPacket_HdrType_MemoryBuffer,
    // Memory buffer
    UIAPacket_HdrType_USER2,
    // User defined header type 2
    UIAPacket_HdrType_USER3
    // User defined header type 3
} UIAPacket_HdrType;
 
DETAILS
Stored in a 4 bit bitfield (b31-b28) of the first word in the packet.
The HdrType_InvalidData denotes that following data is invalid. This can used to pad to the end of a buffer. Only the first word of the header is filled in. The length includes the header field.
 
enum UIAPacket_MsgType

Message Types

C synopsis target-domain
typedef enum UIAPacket_MsgType {
    UIAPacket_MsgType_ACK,
    // Reply acknowledging receipt of CMD or DATA packet
    UIAPacket_MsgType_CMD,
    // Command packets
    UIAPacket_MsgType_RESULT,
    // Result reply
    UIAPacket_MsgType_PARTIALRESULT,
    // Partial result reply
    UIAPacket_MsgType_NOTIFY,
    // Notify messaage (equiv. to the EVENT packet in TCF)
    UIAPacket_MsgType_FLOWCTRL,
    // Flow control packet
    UIAPacket_MsgType_DATA,
    // Data packet (used for streaming data to host)
    UIAPacket_MsgType_RESERVED7,
    UIAPacket_MsgType_RESERVED8,
    UIAPacket_MsgType_RESERVED9,
    UIAPacket_MsgType_RESERVED10,
    UIAPacket_MsgType_RESERVED11,
    UIAPacket_MsgType_RESERVED12,
    UIAPacket_MsgType_RESERVED13,
    UIAPacket_MsgType_NACK_BAD_DATA,
    // Negative Acknowledge due to bad data
    UIAPacket_MsgType_NACK_WITH_ERROR_CODE
    // Negative Acknowledge - error code in msg body
} UIAPacket_MsgType;
 
DETAILS
Enumeration of the various types of packets. Stored in a 4 bit bitfield.
MsgType_ACK: Each packet of type CMD or DATA is immediately acknowledged by sending either an ACK reply (if the packet can be processed), a RESULT or PARTIALRESULT reply (if requested data can be provided immediately) or a NACK reply (if the packet cannot be processed). The Service that receives the command is responsible for sending the ACK or NACK. If the requested service is not available, the Endpoint is responsible for sending the NACK packet.
MsgType_CMD: CMD packets are typically sent from the host to the target. The receiving endpoint routes the command to the service identified in the Service Id field.
MsgType_RESULT: RESULT replies are sent along with any requested data. If the Service cannot reply with the requested data immediately, it should return with an ACK packet and send a RESULT packet that echoes the header info of the original command.
MsgType_PARTIALRESULT: PARTIALRESULT replies are sent along with any requested data when the requested action can only be partly fulfilled. Examples are when the service is reporting on some ongoing operation or has been requested to periodically poll some data value.
MsgType_EVENT: EVENT packets are sent to all interested parties in order to notify them about state changes. They can, for example, be used to report an error that has occurred which may impact the ability of the target to continue operating normally.
MsgType_FLOWCTRL FLOWCTRL packets are provided for TCF compliance. They are used to avoid flooding of communication links. In response, endpoints can either increase or decrease rate of packets sent, although this is only loosely defined. TCF services are not directly concerned with flow control. The data passed with FLOWCTRL packets reports the traffic congestion level as an integer between -100 and 100, where 0 = "optimal load"
MsgType_DATA DATA packets are used for sending event log data and other streams of data. Details about how this will be used are being worked out to ensure alignment with BIOS RTA Log Servers.
MsgType_NACK_BAD_DATA: Negative Acknowledge due to bad data. Sent in response to a command that had invalid data in the body of the packet. The original data is echoed in the NACK response.
MsgType_NACK_WITH_ERROR_CODE Negative Acknowledge with Error Code. Sent along with an error code in the first word of the body of the reply that describes the error that was encountered
 
enum UIAPacket_NACKErrorCode

Message Negative Acknowledge Error Codes

C synopsis target-domain
typedef enum UIAPacket_NACKErrorCode {
    UIAPacket_NACKErrorCode_NO_REASON_SPECIFIED,
    // Use this when none of the defined NACK error codes are appropriate
    UIAPacket_NACKErrorCode_SERVICE_NOT_SUPPORTED,
    // A module that handles the requested Service Id could not be found
    UIAPacket_NACKErrorCode_CMD_NOT_SUPPORTED,
    // The service does not support the specified Command Id
    UIAPacket_NACKErrorCode_QUEUE_FULL,
    // Cmd couldn't be passed on to dest. end point due to a queue full condition
    UIAPacket_NACKErrorCode_BAD_ENDPOINT_ADDRESS,
    // The destination end point address does not exists
    UIAPacket_NACKErrorCode_BAD_MESSAGE_LENGTH
    // packet lenght > endpoint max. msg length or not what is required to service the cmd
} UIAPacket_NACKErrorCode;
 
DETAILS
Stored in the first 32b word of the data body of the packet in Network Byte Order
 
enum UIAPacket_PayloadEndian

Enumeration of payload endianness

C synopsis target-domain
typedef enum UIAPacket_PayloadEndian {
    UIAPacket_PayloadEndian_LITTLE,
    UIAPacket_PayloadEndian_BIG
} UIAPacket_PayloadEndian;
 
 
struct UIAPacket_Footer

Packet Footer

C synopsis target-domain
typedef struct UIAPacket_Footer {
    Int32 word1;
    // 16 MSBs contain msg length in Bytes, 16 LSBs contain 0x7777
} UIAPacket_Footer;
 
DETAILS
The packet footer is always in network byte order i.e. big-endian byte ordering
 
struct UIAPacket_Hdr

UIAPacket Header

C synopsis target-domain
typedef struct UIAPacket_Hdr {
    Bits32 word1;
    Bits32 word2;
    Bits32 word3;
    Bits32 word4;
} UIAPacket_Hdr;
 
DETAILS
The following is a breakdown of the packet header based on type packet.
The packet header is always sent in network byte (big endian) order.
The top 4 leftmost bits of word1 denote what type of packet this is: HdrType_Msg or HdrType_EventPkt. The contents of the packet depends on this type.
  HdrType_Msg word1
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |H H H H|E|L L L L L L L L L L L|T T T T|S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  H = HdrType         (4-bits)
  E = Payload endian  (1-bit)
  L = Message Length  (11-bits)
  T = Message Type    (4-bits)
  S = Service Id      (12-bits)

  HdrType_Msg word2
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |S S S S S S S S S S S S S S S S|C C C C C C C C C C C C C C C C|
  |---------------------------------------------------------------|

  S = Sequence Number (16-bits)
  C = Command Id      (16-bits)

  HdrType_Msg word3
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T|
  |---------------------------------------------------------------|

  T - Tag             (32-bits)

  HdrType_Msg word4
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D D D D D D D D D D D D D D D D|S S S S S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  D - Destination Address (16-bits)
  S - Source Address      (16-bits)

  HdrType_EventPkt word1
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |H H H H|E|L L L L L L L L L L L L L L L L L L L L L L L L L L L|
  |---------------------------------------------------------------|

  H = HdrType         (4-bits)
  E = Payload endian   (1-bit)
  L = Event Length   (27-bits)

  HdrType_EventPkt word2
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |S S S S S S S S S S S S S S S S|R R R R R R R R R R R R R R|P P|
  |---------------------------------------------------------------|

  S = Sequence Number              (16-bits)
  R = Reserved                     (14-bits)
  P = Priority: Normal=0, High > 0 (2-bits)

  HdrType_EventPkt word3
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D I I I I I I I I I I I I I I I M M M M M M M M M M M M M M M M|
  |---------------------------------------------------------------|

  D ? wasLoggerDynamicallyCreated  (1-bit:  0 = statically created, 
                                            1 = dynamically created)
  I - Logger Instance ID           (15-bits)
  M - Logger Module ID             (16-bits)

  HdrType_EventPkt word4
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D D D D D D D D D D D D D D D D|S S S S S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  D - Destination Address (16-bits)
  S - Source Address      (16-bits)

For HdrType_EventPktWithPID, HdrType_CPUTrace and HdrType_STMTrace, word 5 holds the 32b process ID of the sender (0 for RTOSes such as SysBIOS) 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P| |---------------------------------------------------------------| P =Process ID (0 if only 1 process) (32-bits)
For STM_trace and CPU_trace hdr types, word 6 is defined as follows: word 6 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |E E E E E E E E E E E E E E E E|F|P P P P P P P P P P P P P P P| |---------------------------------------------------------------|
E = Endpoint Number (16-bits) F = First Packet: 0=first packet, 1=other (1 bit) P = Number of packets left to send in this trace snapshot (15-bits)
For STM_trace and CPU_trace hdr types, word 7 is defined as follows: word 7 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |R R R R R R R R|S S S S S S S S S S S S S S S S S S S S S S S S| |---------------------------------------------------------------|
R = Reserved (8-bits) S = Trace Snapshot Number (24-bits)
 
struct UIAPacket_Hdr5
C synopsis target-domain
typedef struct UIAPacket_Hdr5 {
    Bits32 word1;
    Bits32 word2;
    Bits32 word3;
    Bits32 word4;
    Bits32 word5;
} UIAPacket_Hdr5;
 
 
struct UIAPacket_Hdr7
C synopsis target-domain
typedef struct UIAPacket_Hdr7 {
    Bits32 word1;
    Bits32 word2;
    Bits32 word3;
    Bits32 word4;
    Bits32 word5;
    Bits32 word6;
    Bits32 word7;
} UIAPacket_Hdr7;
 
 
config UIAPacket_maxPktLengthInBytes  // module-wide

maximum number of bytes a packet can contain

C synopsis target-domain
extern const Int UIAPacket_maxPktLengthInBytes;
 
DETAILS
used to limit the amount of memory needed by the packet factories in order to handle a new packet
 
UIAPacket_getCmdId()  // module-wide

gets the packet type from the packet header

C synopsis target-domain
macro UInt16 UIAPacket_getCmdId(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getDestAdrs()  // module-wide

gets the packet destination address from the packet header

C synopsis target-domain
macro UInt16 UIAPacket_getDestAdrs(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
Example1 : Void example1(UIAPacket_Object *obj){ Int16 destAdrs = UIAPacket_getDestAdrs(&obj->hdr); ... } Example2 : Void example2(UIAPacket_Hdr *pHdr){ Int16 destAdrs = UIAPacket_getDestAdrs(pHdr); ... }
 
UIAPacket_getEndpointNumber()  // module-wide

gets the endpoint number from the trace packet header

C synopsis target-domain
macro UInt16 UIAPacket_getEndpointNumber(UIAPacket_Hdr7 *pHdr);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the packet header
DETAILS
Trace Event header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getEventLength()  // module-wide

Gets the packet length (in bytes) from the packet header

C synopsis target-domain
macro Int32 UIAPacket_getEventLength(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Includes the packet header
 
UIAPacket_getFirstPktFlag()  // module-wide

gets the first packet flag from the trace packet header

C synopsis target-domain
macro Bool UIAPacket_getFirstPktFlag(UIAPacket_Hdr7 *pHdr);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the packet header
DETAILS
Trace Event header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getFooter()  // module-wide

returns the integer to use as the packet footer

C synopsis target-domain
macro Int32 UIAPacket_getFooter(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* pHdr) pointer to the packet header
 
UIAPacket_getHdrType()  // module-wide

gets the packet header type from the packet header

C synopsis target-domain
macro UIAPacket_HdrType UIAPacket_getHdrType(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getLength()  // module-wide

Gets the packet length (in bytes) from the packet header

C synopsis target-domain
Int32 UIAPacket_getLength(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Includes the packet header
 
UIAPacket_getLoggerInstanceId()  // module-wide

gets the logger instance ID from the event packet header

C synopsis target-domain
macro Bits16 UIAPacket_getLoggerInstanceId(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getLoggerModuleId()  // module-wide

gets the logger ID from the event packet header

C synopsis target-domain
macro Bits16 UIAPacket_getLoggerModuleId(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getMsgLength()  // module-wide

gets the packet length (in bytes) from the packet header

C synopsis target-domain
macro Int32 UIAPacket_getMsgLength(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getMsgType()  // module-wide

gets the packet type from the packet header

C synopsis target-domain
macro UIAPacket_MsgType UIAPacket_getMsgType(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* pHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getPayloadEndianness()  // module-wide

gets the payload endianness bit from the packet header

C synopsis target-domain
macro Bits32 UIAPacket_getPayloadEndianness(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getSenderAdrs()  // module-wide

gets the packet sender address from the packet header

C synopsis target-domain
macro UInt16 UIAPacket_getSenderAdrs(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getSequenceCount()  // module-wide

gets the sequence count from the packet header

C synopsis target-domain
macro UInt16 UIAPacket_getSequenceCount(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getServiceId()  // module-wide

gets the packet type from the packet header

C synopsis target-domain
macro UInt16 UIAPacket_getServiceId(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getSnapshotNumber()  // module-wide

gets the snapshot number from the trace packet header

C synopsis target-domain
macro UInt16 UIAPacket_getSnapshotNumber(UIAPacket_Hdr7 *pHdr);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the packet header
DETAILS
Trace Event header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_getTag()  // module-wide

gets the 32b tag field from the packet header

C synopsis target-domain
macro Bits32 UIAPacket_getTag(UIAPacket_Hdr *pHdr);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
 
UIAPacket_getTracePktDownCount()  // module-wide

gets the trace packet down count value from the trace packet header

C synopsis target-domain
macro UInt16 UIAPacket_getTracePktDownCount(UIAPacket_Hdr7 *pHdr);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the packet header
DETAILS
Trace Event header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_initEventRecHdr()  // module-wide

initializes all bitfields in the event packet header

C synopsis target-domain
macro Void UIAPacket_initEventRecHdr(UIAPacket_Hdr *pHdr, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs);
 
ARGUMENTS
— (Hdr* pHdr) pointer to the event packet header
endianness — endianness of the payload
eventLength — the number of Bytes in the packet, including the header and footer
seqCount — the sequence number for the packet
priority — the logger's priority
moduleId — the logger's module Id
instanceId — the logger's instanceId
destAdrs — the destination address
senderAdrs — the sender address
 
UIAPacket_initEventRecWithPIDHdr()  // module-wide

initializes all bitfields in the event packet header

C synopsis target-domain
macro Void UIAPacket_initEventRecWithPIDHdr(UIAPacket_Hdr5 *pHdr, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs, UInt32 processId);
 
ARGUMENTS
— (Hdr* pHdr) pointer to the event packet header
endianness — endianness of the payload
eventLength — the number of Bytes in the packet, including the header and footer
seqCount — the sequence number for the packet
priority — the logger's priority
moduleId — the logger's module Id
instanceId — the logger's instanceId
destAdrs — the destination address
senderAdrs — the sender address
processId — the sender process ID
 
UIAPacket_initMsgHdr()  // module-wide

initializes all bitfields in the message header

C synopsis target-domain
macro Void UIAPacket_initMsgHdr(UIAPacket_Hdr *pHdr, UIAPacket_PayloadEndian endianness, UIAPacket_MsgType msgType, UInt16 msgLength, UInt16 serviceId, UInt16 seqCount, UInt16 cmdId, UInt32 tag, UInt16 destAdrs, UInt16 senderAdrs);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
endianness — endianness of the payload
msgType — the packet type
msgLength — the number of Bytes in the packet, including the header and footer
serviceId — the service Id
seqCount — the sequence number for the packet
cmdId — the command Id
tag — the tag value to store in the header
destAdrs — the destination address
senderAdrs — the sender address
 
UIAPacket_initTraceHdrFields()  // module-wide

initializes the hdrType field and bitfields in word5 and word6 of the trace packet header. Call @see initEventRecHdr first to initialize the first 4 words of the trace packet header. Then call this macro to initialize hdr type field and words 5 and 6 of the header

C synopsis target-domain
macro Void UIAPacket_initTraceHdrFields(UIAPacket_Hdr7 *pPktHdr, UIAPacket_HdrType traceHdrType, UInt16 endpointNumber, Bool isFirstPacket, UInt16 tracePktDownCount, UInt32 traceSnapshotNumber);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the 7 word trace packet header
HdrType traceHdrType — the header type to store in word 1 of the trace packet header
endpointNumber — the endpoint number of the ETB that the data is from
isFirstPacket — true for the first packet in the trace snapshot
tracePktDownCount — the number of packets left to send in the trace snapshot
traceSnapshotNumber — the trace snapshot number
 
UIAPacket_initTraceRecHdr()  // module-wide

initializes all bitfields in the trace packet header

C synopsis target-domain
macro Void UIAPacket_initTraceRecHdr(UIAPacket_Hdr7 *pHdr, UIAPacket_HdrType traceHdrType, UIAPacket_PayloadEndian endianness, UInt32 eventLength, UInt16 seqCount, IUIATransfer_Priority priority, UInt16 moduleId, UInt16 instanceId, UInt16 destAdrs, UInt16 senderAdrs, UInt32 processId, UInt16 endpointNumber, Bool isFirstPacket, UInt16 tracePktDownCount, UInt16 traceSnapshotNumber);
 
ARGUMENTS
— (Hdr7* pHdr) pointer to the 6 word trace packet header
HdrType traceHdrType — the header type to store in word 1 of the trace packet header
endianness — endianness of the payload
eventLength — the number of Bytes in the packet, including the header and footer
seqCount — the sequence number for the packet
priority — the logger's priority
moduleId — the logger's module Id
instanceId — the logger's instanceId
destAdrs — the destination address
senderAdrs — the sender address
endpointNumber — the endpoint number of the ETB that the data is from
isFirstPacket — true for the first packet in the trace snapshot
tracePktDownCount — the number of packets left to send in the trace snapshot
traceSnapshotNumber — the trace snapshot number
 
UIAPacket_setCmdId()  // module-wide

sets the command Id in the packet header

C synopsis target-domain
macro Void UIAPacket_setCmdId(UIAPacket_Hdr *pHdr, UInt16 cmdId);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
cmdId — the new command Id
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setDestAdrs()  // module-wide

sets the packet destination address in the packet header

C synopsis target-domain
macro Void UIAPacket_setDestAdrs(UIAPacket_Hdr *pHdr, UInt16 destAdrs);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
destAdrs — the new destination address
DETAILS
The destination address identifies which endpoint (i.e. which CPU or process) the packet should be sent to. 0 is used to broadcast the packet. 1 is used for point-to-point connections. Replies to a packet always use the sender address in the originating packet as the destination address. Destination addresses other than the above can be determined via a discovery process.
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setEventLength()  // module-wide

Sets the packet length (in bytes) from the packet header

C synopsis target-domain
macro Void UIAPacket_setEventLength(UIAPacket_Hdr *pHdr, Bits32 pktLength);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
pktLength — the new packet length
DETAILS
Includes the packet header
 
UIAPacket_setHdrType()  // module-wide

sets the header type in the packet header

C synopsis target-domain
macro Void UIAPacket_setHdrType(UIAPacket_Hdr *pHdr, UIAPacket_HdrType hdrType);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
HdrType hdrType — the new header type
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setInvalidHdr()  // module-wide

Used to set the header type as invalid

C synopsis target-domain
macro Void UIAPacket_setInvalidHdr(UIAPacket_Hdr *pHdr, UInt32 eventLength);
 
ARGUMENTS
— (Hdr* pHdr) pointer to the packet header
eventLength — the number of Bytes in the packet of memory that is invalid (including the first word of the 32-bit hdr)
 
UIAPacket_setLoggerInstanceId()  // module-wide

sets the sequence count in the packet header

C synopsis target-domain
macro Void UIAPacket_setLoggerInstanceId(UIAPacket_Hdr *pHdr, Bits16 loggerInstanceId);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
seqCount — the new packet sequence count
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setLoggerModuleId()  // module-wide

sets the module ID in the event packet header

C synopsis target-domain
macro Void UIAPacket_setLoggerModuleId(UIAPacket_Hdr *pHdr, Bits16 loggerModuleId);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
loggerModuleId — the moduleID of the logger that logged the events
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setMsgLength()  // module-wide

sets the packet length (in bytes) from the packet header

C synopsis target-domain
macro Void UIAPacket_setMsgLength(UIAPacket_Hdr *pHdr, UInt16 pktLength);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
pktLength — the new packet length
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setMsgType()  // module-wide

sets the packet type in the packet header

C synopsis target-domain
macro Void UIAPacket_setMsgType(UIAPacket_Hdr *pHdr, UIAPacket_MsgType msgType);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
msgType — the new packet type
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setPayloadEndianness()  // module-wide

sets the payload endianness bit from the packet header

C synopsis target-domain
macro Bits32 UIAPacket_setPayloadEndianness(UIAPacket_Hdr *pHdr, UIAPacket_PayloadEndian endianess);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header (Hdr* msgHdr) Endianness of the payload
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setSenderAdrs()  // module-wide

sets the packet sender address in the packet header

C synopsis target-domain
macro Void UIAPacket_setSenderAdrs(UIAPacket_Hdr *pHdr, UInt16 senderAdrs);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
senderAdrs — the new destination address
DETAILS
The sender address identifies which endpoint (i.e. which CPU or process) the packet is coming from 1 is used by default. Sender addresses other than 1 can be set via configuration (e.g. to identify which CPU core a packet originated from).
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setSequenceCount()  // module-wide

sets the sequence count in the packet header

C synopsis target-domain
macro Void UIAPacket_setSequenceCount(UIAPacket_Hdr *pHdr, Bits16 seqCount);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
seqCount — the new packet sequence count
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setServiceId()  // module-wide

sets the packet type in the packet header

C synopsis target-domain
macro Void UIAPacket_setServiceId(UIAPacket_Hdr *pHdr, UInt16 serviceId);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
serviceId — the new service Id
DETAILS
Message header is always layed out as big endian (network order). This macro is designed to work on both little endian and big endian targets, since 32b long words are consistently handled for both endianness - it is only when converting from bytes to longs that bit orders get swapped. #ifdef xdc_target__bigEndian can be used if necessary.
 
UIAPacket_setTag()  // module-wide

sets the 32b tag field in the packet header

C synopsis target-domain
macro Void UIAPacket_setTag(UIAPacket_Hdr *pHdr, Bits32 tagValue);
 
ARGUMENTS
— (Hdr* msgHdr) pointer to the packet header
tagValue — the tag value to store in the header
 
UIAPacket_swizzle()  // module-wide

returns the value in big endian format

C synopsis target-domain
macro Bits32 UIAPacket_swizzle(Bits32 value);
 
 
UIAPacket_swizzle16()  // module-wide

returns the value in big endian format

C synopsis target-domain
macro Bits16 UIAPacket_swizzle16(Bits16 value);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId UIAPacket_Module_id();
// Get this module's unique id
 
Bool UIAPacket_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle UIAPacket_Module_heap();
// The heap from which this module allocates memory
 
Bool UIAPacket_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 UIAPacket_Module_getMask();
// Returns the diagnostics mask for this module
 
Void UIAPacket_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/uiactools/runtime/UIAPacket.xdc
var UIAPacket = xdc.useModule('ti.uiactools.runtime.UIAPacket');
module-wide constants & types
 
 
    values of type UIAPacket.MsgType// Message Types
        const UIAPacket.MsgType_RESERVED7;
        const UIAPacket.MsgType_RESERVED8;
        const UIAPacket.MsgType_RESERVED9;
        const UIAPacket.MsgType_RESERVED10;
        const UIAPacket.MsgType_RESERVED11;
        const UIAPacket.MsgType_RESERVED12;
        const UIAPacket.MsgType_RESERVED13;
 
 
        const UIAPacket.PayloadEndian_LITTLE;
        const UIAPacket.PayloadEndian_BIG;
 
    var obj = new UIAPacket.Footer// Packet Footer;
 
    var obj = new UIAPacket.Hdr// UIAPacket Header;
        obj.word1 = Bits32  ...
        obj.word2 = Bits32  ...
        obj.word3 = Bits32  ...
        obj.word4 = Bits32  ...
 
    var obj = new UIAPacket.Hdr5// ;
        obj.word1 = Bits32  ...
        obj.word2 = Bits32  ...
        obj.word3 = Bits32  ...
        obj.word4 = Bits32  ...
        obj.word5 = Bits32  ...
 
    var obj = new UIAPacket.Hdr7// ;
        obj.word1 = Bits32  ...
        obj.word2 = Bits32  ...
        obj.word3 = Bits32  ...
        obj.word4 = Bits32  ...
        obj.word5 = Bits32  ...
        obj.word6 = Bits32  ...
        obj.word7 = Bits32  ...
module-wide config parameters
 
 
 
const UIAPacket.BROADCAST

Used to denote a broadcast message

XDCscript usage meta-domain
const UIAPacket.BROADCAST = 0xFFFE;
 
DETAILS
The broadcast address is always 0xFFFE.
C SYNOPSIS
 
const UIAPacket.HOST

The address of the host

XDCscript usage meta-domain
const UIAPacket.HOST = 0xFFFF;
 
DETAILS
The host address is always 0xFFFF.
C SYNOPSIS
 
enum UIAPacket.HdrType

Enumeration of the various types of packet headers

XDCscript usage meta-domain
values of type UIAPacket.HdrType
    const UIAPacket.HdrType_InvalidData;
    // Invalid Data packet (1 word header)
    const UIAPacket.HdrType_MsgWithPID;
    // Message with Process ID (5 word header)
    const UIAPacket.HdrType_EventPktWithPID;
    // Event rec. with Process ID containing multiple events: (5 word hdr)
    const UIAPacket.HdrType_Reserved1;
    // reserved for future use
    const UIAPacket.HdrType_Reserved2;
    // reserved for future use
    const UIAPacket.HdrType_Reserved3;
    // reserved for future use
    const UIAPacket.HdrType_Reserved4;
    // reserved for future use
    const UIAPacket.HdrType_Reserved5;
    // reserved for future use
    const UIAPacket.HdrType_Reserved6;
    // reserved for future use
    const UIAPacket.HdrType_Reserved7;
    // reserved for future use
    const UIAPacket.HdrType_ChannelizedData;
    // Channelized data stream
    const UIAPacket.HdrType_Msg;
    // Message (4 word header)
    const UIAPacket.HdrType_EventPkt;
    // Event rec. containing multiple events: (4 word hdr)
    const UIAPacket.HdrType_CPUTrace;
    // CPU Trace ETB data (7 word hdr)
    const UIAPacket.HdrType_STMTrace;
    // STM Trace ETB data (7 word hdr)
    const UIAPacket.HdrType_MemoryBuffer;
    // Memory buffer
    const UIAPacket.HdrType_USER2;
    // User defined header type 2
    const UIAPacket.HdrType_USER3;
    // User defined header type 3
 
DETAILS
Stored in a 4 bit bitfield (b31-b28) of the first word in the packet.
The HdrType_InvalidData denotes that following data is invalid. This can used to pad to the end of a buffer. Only the first word of the header is filled in. The length includes the header field.
C SYNOPSIS
 
enum UIAPacket.MsgType

Message Types

XDCscript usage meta-domain
values of type UIAPacket.MsgType
    const UIAPacket.MsgType_ACK;
    // Reply acknowledging receipt of CMD or DATA packet
    const UIAPacket.MsgType_CMD;
    // Command packets
    const UIAPacket.MsgType_RESULT;
    // Result reply
    const UIAPacket.MsgType_PARTIALRESULT;
    // Partial result reply
    const UIAPacket.MsgType_NOTIFY;
    // Notify messaage (equiv. to the EVENT packet in TCF)
    const UIAPacket.MsgType_FLOWCTRL;
    // Flow control packet
    const UIAPacket.MsgType_DATA;
    // Data packet (used for streaming data to host)
    const UIAPacket.MsgType_RESERVED7;
    const UIAPacket.MsgType_RESERVED8;
    const UIAPacket.MsgType_RESERVED9;
    const UIAPacket.MsgType_RESERVED10;
    const UIAPacket.MsgType_RESERVED11;
    const UIAPacket.MsgType_RESERVED12;
    const UIAPacket.MsgType_RESERVED13;
    const UIAPacket.MsgType_NACK_BAD_DATA;
    // Negative Acknowledge due to bad data
    const UIAPacket.MsgType_NACK_WITH_ERROR_CODE;
    // Negative Acknowledge - error code in msg body
 
DETAILS
Enumeration of the various types of packets. Stored in a 4 bit bitfield.
MsgType_ACK: Each packet of type CMD or DATA is immediately acknowledged by sending either an ACK reply (if the packet can be processed), a RESULT or PARTIALRESULT reply (if requested data can be provided immediately) or a NACK reply (if the packet cannot be processed). The Service that receives the command is responsible for sending the ACK or NACK. If the requested service is not available, the Endpoint is responsible for sending the NACK packet.
MsgType_CMD: CMD packets are typically sent from the host to the target. The receiving endpoint routes the command to the service identified in the Service Id field.
MsgType_RESULT: RESULT replies are sent along with any requested data. If the Service cannot reply with the requested data immediately, it should return with an ACK packet and send a RESULT packet that echoes the header info of the original command.
MsgType_PARTIALRESULT: PARTIALRESULT replies are sent along with any requested data when the requested action can only be partly fulfilled. Examples are when the service is reporting on some ongoing operation or has been requested to periodically poll some data value.
MsgType_EVENT: EVENT packets are sent to all interested parties in order to notify them about state changes. They can, for example, be used to report an error that has occurred which may impact the ability of the target to continue operating normally.
MsgType_FLOWCTRL FLOWCTRL packets are provided for TCF compliance. They are used to avoid flooding of communication links. In response, endpoints can either increase or decrease rate of packets sent, although this is only loosely defined. TCF services are not directly concerned with flow control. The data passed with FLOWCTRL packets reports the traffic congestion level as an integer between -100 and 100, where 0 = "optimal load"
MsgType_DATA DATA packets are used for sending event log data and other streams of data. Details about how this will be used are being worked out to ensure alignment with BIOS RTA Log Servers.
MsgType_NACK_BAD_DATA: Negative Acknowledge due to bad data. Sent in response to a command that had invalid data in the body of the packet. The original data is echoed in the NACK response.
MsgType_NACK_WITH_ERROR_CODE Negative Acknowledge with Error Code. Sent along with an error code in the first word of the body of the reply that describes the error that was encountered
C SYNOPSIS
 
enum UIAPacket.NACKErrorCode

Message Negative Acknowledge Error Codes

XDCscript usage meta-domain
values of type UIAPacket.NACKErrorCode
    const UIAPacket.NACKErrorCode_NO_REASON_SPECIFIED;
    // Use this when none of the defined NACK error codes are appropriate
    const UIAPacket.NACKErrorCode_SERVICE_NOT_SUPPORTED;
    // A module that handles the requested Service Id could not be found
    const UIAPacket.NACKErrorCode_CMD_NOT_SUPPORTED;
    // The service does not support the specified Command Id
    const UIAPacket.NACKErrorCode_QUEUE_FULL;
    // Cmd couldn't be passed on to dest. end point due to a queue full condition
    const UIAPacket.NACKErrorCode_BAD_ENDPOINT_ADDRESS;
    // The destination end point address does not exists
    const UIAPacket.NACKErrorCode_BAD_MESSAGE_LENGTH;
    // packet lenght > endpoint max. msg length or not what is required to service the cmd
 
DETAILS
Stored in the first 32b word of the data body of the packet in Network Byte Order
C SYNOPSIS
 
enum UIAPacket.PayloadEndian

Enumeration of payload endianness

XDCscript usage meta-domain
values of type UIAPacket.PayloadEndian
    const UIAPacket.PayloadEndian_LITTLE;
    const UIAPacket.PayloadEndian_BIG;
 
C SYNOPSIS
 
struct UIAPacket.Footer

Packet Footer

XDCscript usage meta-domain
var obj = new UIAPacket.Footer;
 
    obj.word1 = Int32  ...
    // 16 MSBs contain msg length in Bytes, 16 LSBs contain 0x7777
 
DETAILS
The packet footer is always in network byte order i.e. big-endian byte ordering
C SYNOPSIS
 
struct UIAPacket.Hdr

UIAPacket Header

XDCscript usage meta-domain
var obj = new UIAPacket.Hdr;
 
    obj.word1 = Bits32  ...
    obj.word2 = Bits32  ...
    obj.word3 = Bits32  ...
    obj.word4 = Bits32  ...
 
DETAILS
The following is a breakdown of the packet header based on type packet.
The packet header is always sent in network byte (big endian) order.
The top 4 leftmost bits of word1 denote what type of packet this is: HdrType_Msg or HdrType_EventPkt. The contents of the packet depends on this type.
  HdrType_Msg word1
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |H H H H|E|L L L L L L L L L L L|T T T T|S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  H = HdrType         (4-bits)
  E = Payload endian  (1-bit)
  L = Message Length  (11-bits)
  T = Message Type    (4-bits)
  S = Service Id      (12-bits)

  HdrType_Msg word2
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |S S S S S S S S S S S S S S S S|C C C C C C C C C C C C C C C C|
  |---------------------------------------------------------------|

  S = Sequence Number (16-bits)
  C = Command Id      (16-bits)

  HdrType_Msg word3
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T|
  |---------------------------------------------------------------|

  T - Tag             (32-bits)

  HdrType_Msg word4
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D D D D D D D D D D D D D D D D|S S S S S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  D - Destination Address (16-bits)
  S - Source Address      (16-bits)

  HdrType_EventPkt word1
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |H H H H|E|L L L L L L L L L L L L L L L L L L L L L L L L L L L|
  |---------------------------------------------------------------|

  H = HdrType         (4-bits)
  E = Payload endian   (1-bit)
  L = Event Length   (27-bits)

  HdrType_EventPkt word2
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |S S S S S S S S S S S S S S S S|R R R R R R R R R R R R R R|P P|
  |---------------------------------------------------------------|

  S = Sequence Number              (16-bits)
  R = Reserved                     (14-bits)
  P = Priority: Normal=0, High > 0 (2-bits)

  HdrType_EventPkt word3
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D I I I I I I I I I I I I I I I M M M M M M M M M M M M M M M M|
  |---------------------------------------------------------------|

  D ? wasLoggerDynamicallyCreated  (1-bit:  0 = statically created, 
                                            1 = dynamically created)
  I - Logger Instance ID           (15-bits)
  M - Logger Module ID             (16-bits)

  HdrType_EventPkt word4
   3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0
   1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0
  |---------------------------------------------------------------|
  |D D D D D D D D D D D D D D D D|S S S S S S S S S S S S S S S S|
  |---------------------------------------------------------------|

  D - Destination Address (16-bits)
  S - Source Address      (16-bits)

For HdrType_EventPktWithPID, HdrType_CPUTrace and HdrType_STMTrace, word 5 holds the 32b process ID of the sender (0 for RTOSes such as SysBIOS) 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P P| |---------------------------------------------------------------| P =Process ID (0 if only 1 process) (32-bits)
For STM_trace and CPU_trace hdr types, word 6 is defined as follows: word 6 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |E E E E E E E E E E E E E E E E|F|P P P P P P P P P P P P P P P| |---------------------------------------------------------------|
E = Endpoint Number (16-bits) F = First Packet: 0=first packet, 1=other (1 bit) P = Number of packets left to send in this trace snapshot (15-bits)
For STM_trace and CPU_trace hdr types, word 7 is defined as follows: word 7 3 3 2 2 2 2 2 2 2 2 2 2 1 1 1 1 1 1 1 1 1 1 0 0 0 0 0 0 0 0 0 0 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 9 8 7 6 5 4 3 2 1 0 |---------------------------------------------------------------| |R R R R R R R R|S S S S S S S S S S S S S S S S S S S S S S S S| |---------------------------------------------------------------|
R = Reserved (8-bits) S = Trace Snapshot Number (24-bits)
C SYNOPSIS
 
struct UIAPacket.Hdr5
XDCscript usage meta-domain
var obj = new UIAPacket.Hdr5;
 
    obj.word1 = Bits32  ...
    obj.word2 = Bits32  ...
    obj.word3 = Bits32  ...
    obj.word4 = Bits32  ...
    obj.word5 = Bits32  ...
 
C SYNOPSIS
 
struct UIAPacket.Hdr7
XDCscript usage meta-domain
var obj = new UIAPacket.Hdr7;
 
    obj.word1 = Bits32  ...
    obj.word2 = Bits32  ...
    obj.word3 = Bits32  ...
    obj.word4 = Bits32  ...
    obj.word5 = Bits32  ...
    obj.word6 = Bits32  ...
    obj.word7 = Bits32  ...
 
C SYNOPSIS
 
config UIAPacket.maxPktLengthInBytes  // module-wide

maximum number of bytes a packet can contain

XDCscript usage meta-domain
UIAPacket.maxPktLengthInBytes = Int 128;
 
DETAILS
used to limit the amount of memory needed by the packet factories in order to handle a new packet
C SYNOPSIS
 
metaonly config UIAPacket.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
UIAPacket.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 27 Jun 2012 04:11:42 GMT