Texas Instruments Technology for Innovators(tm)

UIACTOOLS 1.00.00.09 Release Notes

This release note is divided into the following sections:
Introduction, Documentation, What's New, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Examples, Version Information, Technical Support.

Introduction

This is a preliminary engineering release of UIACTOOLS 1.00.00.09.

Packages are provided as source code and prebuilt libraries. 

Documentation

The following documentation is available:

Release notes from previous releases are also available in the relnotes_archive directory.


What's New

  • LoggerSTM_writeMemoryRange: Support for logging memory ranges and dynamically allocated strings.(
  • Automatic generation of helper functions for STM Library. (LoggerSTM.isGenerateSTMLibSupportFnsEnabled = true)
  • CDoc documentation for LoggerSTM now included
  • Updated Dependencies: Now depends on UIA_1_01_00_09 or later.
  • Enhancements in UIA_1_00_00.09

    ID Headline
    --Support for C64T
    --Support for logging strings to STM

    Defects Fixed in UIA_1_00_00.09

    ID Headline

    For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory. 

    Upgrade and Compatibility Information

    UIA 1.00.00.09 is not backward compatible with the previous 1.00.00.04_eng release. Changes have been made to the way that LoggerSTM is configured which may require changes to the project's .cfg file. Please see the cdoc for LoggerSTM for details and examples.

    Host Support

    This release requires CCSv5.2.0 or later and System Analyzer 1.1 or later.


    Dependencies

    This release requires the following other software components and tools versions to successfully function: 


    Device Support

    Examples
    uiactools libaries built for

    Validation Information

    This release was validated using the following components:

    Known Issues

    Here are the known issues with this release.

    ID Headline


    Examples

    UIAcTools ships with the following example that interacts with System Analyzer:

    Single-core
    The following example can be built for C66X and ARM CPUs that are on devices that have an STM module. The actual application is the same for all examples. Stairstep varies the Task, Swi and Hwi load every 5 seconds. When viewed on the CPU Load Analysis Feature, it looks like a staircase.

    Version Information

    All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.16_eng or 1.01.00.21-beta).

    This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

    To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. uia_1_00_00_38.

    Subsequent releases of patch upgrades will be identified by the patch number, ex. UIACTOOLS 1.00.00.09 with directory uiactools_1_00_00_09. Typically, these patches only include critical bug fixes.

    Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.


    Technical Support

    For technical support, contact softwaresupport@ti.com


    Last updated: June 27, 2012