[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -r -o -S pathlength -S integrity [Result] -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 512 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 3 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 0 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0xFE03E0F2. Test 3 Word 10: scanned out 0xFE03E0E2 and scanned in 0xFF03E0E2. Test 3 Word 16: scanned out 0xFE03E0E2 and scanned in 0xFE03F0E2. Test 3 Word 21: scanned out 0xFE03E0E2 and scanned in 0x7E03E0E2. Test 3 Word 22: scanned out 0xFE03E0E2 and scanned in 0xFE03E0E3. Test 3 Word 33: scanned out 0xFE03E0E2 and scanned in 0xFE03E062. Test 3 Word 50: scanned out 0xFE03E0E2 and scanned in 0xFE03E0F2. Test 3 Word 55: scanned out 0xFE03E0E2 and scanned in 0xFF03E0E2. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 3, skipped: 0, failed: 1 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 2 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 3 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 4 Some of the values were corrupted - 9.3 percent. The JTAG IR Integrity scan-test has failed. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. [End]