[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -r -o -S pathlength -S integrity [Result] -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 512 32-bit words. The test for the JTAG IR instruction path-length failed. The many-ones then many-zeros tested length was 16384 bits. The many-zeros then many-ones tested length was 0 bits. The test for the JTAG DR bypass path-length failed. The JTAG DR bypass scan-path is stuck-at-ones. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Test 2 Word 0: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 1: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 2: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 3: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 4: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 5: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 6: scanned out 0x00000000 and scanned in 0xFFFFFFFF. Test 2 Word 7: scanned out 0x00000000 and scanned in 0xFFFFFFFF. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 83.3 percent. The JTAG IR Integrity scan-test has failed. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Test 1 Word 0: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 1: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 2: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 3: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 4: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 5: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 6: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 7: scanned out 0xFFFFFFFF and scanned in 0x00000000. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 1, skipped: 0, failed: 1 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 83.3 percent. The JTAG DR Integrity scan-test has failed. [End]