CC1310 SimpleLink LaunchPad Settings & Resources

The CC1310 LaunchPad consists of a LaunchPad board with a CC1310F128 device.

Jumper Settings

Board resources used in driver examples

The following table lists the Board names of the resources used by the driver examples, and their corresponding pins. Note that there may be other resources configured in the board files that are not used by any driver example. Only the example resources are listed in the table.

Board Resource Pin
Board_ADC0 DIO23
Board_ADC1 DIO24
Board_ADCBUF0CHANNEL0 DIO23
Board_GPIO_BUTTON0 DIO13
Board_GPIO_BUTTON1 DIO14
Board_GPIO_LED0 DIO6 (Red - must be jumpered)
Board_GPIO_LED1 DIO7 (Green - must be jumpered)
Board_I2C_TMP DIO4 - SCL, DIO5 - SDA
Board_PIN_LED0 DIO6 (Red - must be jumpered)
Board_PIN_LED1 DIO7 (Green - must be jumpered)
Board_PIN_LED2 DIO6 (Red - must be jumpered)
Board_PIN_BUTTON0 DIO13
Board_PIN_BUTTON1 DIO14
Board_PWM0 DIO6
Board_PWM1 DIO7
Board_SD0 DIO8 - MISO, DIO9 - MOSI, DIO10 - CLK, DIO21 - CS
Board_SPI0 DIO8 - MISO, DIO9 - MOSI, DIO10 - CLK, DIO11 - CS
Board_SPI_MASTER DIO8 - MISO, DIO9 - MOSI, DIO10 - CLK, DIO11 - CS
Board_SPI_SLAVE DIO8 - MISO, DIO9 - MOSI, DIO10 - CLK, DIO11 - CS
Board_SPI_MASTER_READY DIO15
Board_SPI_SLAVE_READY DIO21
Board_UART0 DIO2 - RX, DIO3 - TX

BoosterPacks

The following examples require BoosterPacks.

Example BoosterPack
display BOOSTXL-SHARP128 LCD & SDCard BoosterPack
i2ctmp116 BOOSTXL-BASSENSORS BoosterPack
portable BOOSTXL-BASSENSORS BoosterPack
sdraw BOOSTXL-SHARP128 LCD & SDCard BoosterPack

Peripherals Used

The following list shows which CC1310 LaunchPad peripherals are used by driver and kernel applications. Driver examples control which peripherals (and which ports) are used.