[10/15/2026, 4:37:31 PM] [ERROR] CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information. Microsoft Windows [Version 10.0.19045.6466] (c) Microsoft Corporation. All rights reserved. C:\ti\ccs2050\ccs\ccs_base\common\uscif\xds110>xdsdfu -e USB Device Firmware Upgrade Utility Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved. Scanning USB buses for supported XDS110 devices... <<<< Device 0 >>>> VID: 0x0451 PID: 0xbef3 Device Name: XDS110 Probe with CMSIS-DAP Version: 3.0.0.41 Manufacturer: Texas Instruments Serial Num: 00003110 Mode: Runtime Configuration: Standard Found 1 device. C:\ti\ccs2050\ccs\ccs_base\common\uscif>dbgjtag -f @xds110swd -S integrity -----[Perform the SWD Mode Integrity test]----------------------------------- This test will read the IDCODE register 1 time. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-615' (0xfffffd99). The title is 'SC_ERR_SWD_PROTOCOL'. The explanation is: The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. C:\ti\ccs2050\ccs\ccs_base\common\uscif>