/* ======================================================================
*   Copyright (C) 2023-24 Texas Instruments Incorporated
*
*   All rights reserved. Property of Texas Instruments Incorporated.
*   Restricted rights to use, duplicate or disclose this code are
*   granted through contract.
*
*   The program may not be used without the written permission
*   of Texas Instruments Incorporated or against the terms and conditions
*   stipulated in the agreement under which this program has been
*   supplied.
* ==================================================================== */

/**
 *  \file     Fls_Qspi_Edma.c
 *
 *  \brief    This file contains FLS MCAL driver functions for using EDMA
 *            
 *
 */

/* ========================================================================== */
/*                             Include Files                                  */
/* ========================================================================== */
#include "Fls_Qspi_Edma.h"
#if (FLS_DMA_ENABLE == STD_ON)
#ifdef __cplusplus
extern "C" {
#endif

/* ========================================================================== */
/*                           Macros & Typedefs                                */
/* ========================================================================== */

#define FLS_EDMA_QSPI_A_COUNT           (1U)
/* Max Value for EDMA count */
#define FLS_MAX_EDMA_COUNT              (31U*1024U)
/* Value for C count */
#define FLS_EDMA_QSPI_C_COUNT           (1U)

/* ========================================================================== */
/*                         Structures and Enums                               */
/* ========================================================================== */

/* None */

/* ========================================================================== */
/*                     Function Declarations                                  */
/* ========================================================================== */
void FLS_DmaRxIsrHandler(void* args);
/* ========================================================================== */
/*                            Global Variables                                */
/* ========================================================================== */

/* None */

/* ========================================================================== */
/*                          Function Definitions                              */
/* ========================================================================== */

#define FLS_START_SEC_CODE
#include "Fls_MemMap.h"

/* Requirements : MCAL-____ */
sint32 Fls_Qspi_dmaChInit(Fls_DriverObjType Fls_DrvObj)
{
    sint32              status = MCAL_SystemP_SUCCESS;
    void * appdata = (void*) &Fls_DrvObj;
    status = Cdd_Dma_CbkRegister(FLS_UNIT_EDMA_HANDLER, appdata, &FLS_DmaRxIsrHandler);
    return status;

}


void FLS_edmaTransfer(uint8* dst, uint8* src, uint32 length,
                       QSPI_Handle qspiHandle)
{
    Cdd_Dma_ParamEntry   edmaParam0 , edmaParam1;
    uint32 remaining_size , size, size_adjustment;
 
    /* Dma buffers and length */
    Fls_DrvObj.flsDmaLength = (((((QSPI_Config *)Fls_DrvObj.spiHandle)->object)->transaction)->count);
    Fls_DrvObj.flsDmaDstBuf = (uint8 *)(((((QSPI_Config *)Fls_DrvObj.spiHandle)->object)->transaction)->buf);
    size_adjustment = 0U;    
    /* Chaining is done here fo DMA transfer so length is divided into logical two sizes */
    size = length/FLS_MAX_EDMA_COUNT;
    /* If size is less then 2 times of FLS_MAX_EDMA_COUNT in that case just dividing the length in 2 equal sizes */
    if(size < 2U)
    {
        size = length/2U; 
    }
    else
    {   /* In order to prevent the remaining size to become 0 below implementation is done*/
        if((length % FLS_MAX_EDMA_COUNT) == 0U)
        {
            size = (size-1U)*FLS_MAX_EDMA_COUNT;
        }
        else
        {
            size = size*FLS_MAX_EDMA_COUNT;
        }
    } 
    // To make sure that dma_transfer length for edmaparam0 and edmaparam1 are aligned with 0x04
    if(((size)&(0x3U)) != 0U){
        size_adjustment = 2U;
    }
    // size_adjustment to make size and length as multiple of 0x04
    size = size - size_adjustment;
    remaining_size = length-size;
    uint32 chainOption = (CDD_EDMA_OPT_ITCCHEN_MASK | CDD_EDMA_OPT_TCCHEN_MASK);
    /* edmaParam0 configuration */
    edmaParam0.srcPtr = src;
    edmaParam0.destPtr = dst; 
    if(size > FLS_MAX_EDMA_COUNT)
    {
        edmaParam0.aCnt      = (uint16) FLS_MAX_EDMA_COUNT;
    }
    else
    {
        edmaParam0.aCnt          = (uint16) FLS_EDMA_QSPI_A_COUNT;
    }
    edmaParam0.bCnt          = (uint16) (size/edmaParam0.aCnt);
    edmaParam0.cCnt          = (uint16) FLS_EDMA_QSPI_C_COUNT;
    edmaParam0.bCntReload    = (uint16) (size/edmaParam0.aCnt);
    edmaParam0.srcBIdx       = (sint16) edmaParam0.aCnt;
    edmaParam0.destBIdx      = (sint16) edmaParam0.aCnt;
    edmaParam0.srcCIdx       = (sint16) FLS_EDMA_QSPI_A_COUNT;
    edmaParam0.destCIdx      = (sint16) FLS_EDMA_QSPI_A_COUNT;
    edmaParam0.opt           = (CDD_EDMA_OPT_SYNCDIM_MASK);
    /* edmaParam1 configuration */
    edmaParam1.srcPtr =  (void*)((uint32)(src) + size);
    edmaParam1.destPtr =  (void*)((uint32)(dst) + size);
    edmaParam1.aCnt          = (uint16) FLS_EDMA_QSPI_A_COUNT;
    edmaParam1.bCnt          = (uint16) (remaining_size/edmaParam1.aCnt);
    edmaParam1.cCnt          = (uint16) FLS_EDMA_QSPI_C_COUNT;
    edmaParam1.bCntReload    = (uint16) (remaining_size/edmaParam1.aCnt);
    edmaParam1.srcBIdx       = (sint16) edmaParam1.aCnt;
    edmaParam1.destBIdx      = (sint16) edmaParam1.aCnt;
    edmaParam1.srcCIdx       = (sint16) FLS_EDMA_QSPI_A_COUNT;
    edmaParam1.destCIdx      = (sint16) FLS_EDMA_QSPI_A_COUNT;
    edmaParam1.opt           =
        (CDD_EDMA_OPT_TCINTEN_MASK | CDD_EDMA_OPT_ITCINTEN_MASK | CDD_EDMA_OPT_SYNCDIM_MASK);
    /* Write edmaParam0 param set for fls_read */
    Cdd_Dma_ParamSet(FLS_UNIT_EDMA_HANDLER,0,0,edmaParam0);
    /* Write edmaParam1 param set for fls_read */
    Cdd_Dma_ParamSet(FLS_UNIT_EDMA_HANDLER,1,0,edmaParam1);
    Cdd_Dma_ChainChannel(FLS_UNIT_EDMA_HANDLER,0,0,1,chainOption);
    /* Set manual trigger to start QSPI transfer */
    Cdd_Dma_EnableTransferRegion(FLS_UNIT_EDMA_HANDLER,CDD_EDMA_TRIG_MODE_MANUAL);
    return;
}

void FLS_DmaRxIsrHandler(void *args)
{
    Fls_DrvObj.flsDmaStage = FLS_S_READ_DMA_DONE;
    Mcal_CacheP_inv((void*) Fls_DrvObj.flsDmaDstBuf, Fls_DrvObj.flsDmaLength, Mcal_CacheP_TYPE_ALLD); 
}

#define FLS_STOP_SEC_CODE
#include "Fls_MemMap.h"
#ifdef __cplusplus
}
#endif

#endif//#if (FLS_DMA_ENABLE == STD_ON)