Readme
Example Summary
The following example goes through a set of IQmath operations to showcase the functionality of the module. For this example, we are using the MathACL implementation of IQmath.
Peripherals & Pin Assignments
Peripheral | Pin | Function |
---|---|---|
SYSCTL | ||
MATHACL | ||
DEBUGSS | PA20 | Debug Clock |
DEBUGSS | PA19 | Debug Data In Out |
BoosterPacks, Board Resources & Jumper Settings
Visit LP_MSPM0G3507 for LaunchPad information, including user guide and hardware files.
Pin | Peripheral | Function | LaunchPad Pin | LaunchPad Settings |
---|---|---|---|---|
PA20 | DEBUGSS | SWCLK | N/A |
|
PA19 | DEBUGSS | SWDIO | N/A |
|
Device Migration Recommendations
This project was developed for a superset device included in the LP_MSPM0G3507 LaunchPad. Please visit the CCS User’s Guide for information about migrating to other MSPM0 devices.
Low-Power Recommendations
TI recommends to terminate unused pins by setting the corresponding functions to GPIO and configure the pins to output low or input with internal pullup/pulldown resistor.
SysConfig allows developers to easily configure unused pins by selecting Board→Configure Unused Pins.
For more information about jumper configuration to achieve low-power using the MSPM0 LaunchPad, please visit the LP-MSPM0G3507 User’s Guide.
Example Usage
Compile and load the example. Step through the example and examine the value of result variable (res) as described in the code example.