Readme
Example Summary
ISecondary Bootloader supports programming / verifying data in the memory, with same BSL protocol format as Primary BSL (ROM BSL) in the device. It can be invoked in the same way as the ROM BSL.
It supports the following major functions
- Init
- Receive
- Send
- Deinit
It uses I2C interface to communicate with the Host
This example takes care of secondary Bootloader implementation as well as the registration of it. Hence once this image is loaded to the device, the primary Bootloader in the device can’t be used. Only the secondary Bootloader will be active. To revert the device to use primary Bootloader SWD_Factory_Reset command has to be used.
For more details refer to BSL User Guide.
This example can be used to create custom Bootloader.
NOTE:
- While creating Custom Bootloader make sure that, Flash region in which the custom Bootloader resides is Static write protected in the BCR configuration. Otherwise there are chances for device to get locked during the Bootloading process.
- The default password is given as all ‘0xFFFFFFFF’. It can be changed in secondary_bsl.c
- The values of the defines BSL_SRAM_BUF_START_ADDR, BSL_STACK_SIZE has to be changed according to the SRAM usage.
NOTE: This BSL example uses a provided ti_msp_dl_config.h file that is not generated by SysConfig, and it’s recommended to use this provided file. If it’s necessary to generate Driverlib configuration files (ti_msp_dl_config.h/c), copy the content of the generated ti_msp_dl_config.h file into the provided version.
Peripherals & Pin Assignments
| Peripheral | Pin | Function |
|---|---|---|
| DEBUGSS | PA20 | Debug Clock |
| DEBUGSS | PA19 | Debug Data In Out |
BoosterPacks, Board Resources & Jumper Settings
Visit LP_MSPM0L1306 for LaunchPad information, including user guide and hardware files.
| Pin | Peripheral | Function | LaunchPad Pin | LaunchPad Settings |
|---|---|---|---|---|
| PA20 | DEBUGSS | SWCLK | J2_13 |
|
| PA19 | DEBUGSS | SWDIO | J2_17 |
|
Device Migration Recommendations
This project was developed for a superset device included in the LP_MSPM0L1306 LaunchPad. Please visit the CCS User’s Guide for information about migrating to other MSPM0 devices.
Low-Power Recommendations
TI recommends to terminate unused pins by setting the corresponding functions to GPIO and configure the pins to output low or input with internal pullup/pulldown resistor.
SysConfig allows developers to easily configure unused pins by selecting Board→Configure Unused Pins.
For more information about jumper configuration to achieve low-power using the MSPM0 LaunchPad, please visit the LP-MSPM0L1306 User’s Guide.
Example Usage
Connect I2C_SDA and I2C_SCL with the BSL Host (any microcontroller with I2C).
Compile, load the example.
Create BSL invocation condition using BSL Invoke pin or any other invocation methods. Send Connection command from the host. BSL Acknowledgement should be received. Send GetDeviceInfo command from the host. BSL should respond back with the version information and SRAM buffer space available.
Similarly Send erase, program, verification commands to program data in the memory.