Readme

Example Summary

The following example configures TimerG0 to output a pair of center aligned PWM signals. The device is configured to wait in STOP mode.

Peripherals & Pin Assignments

Peripheral Pin Function
SYSCTL
TIMG0 PA12 Counter Compare Pin 0
TIMG0 PA13 Counter Compare Pin 1
EVENT
DEBUGSS PA20 Debug Clock
DEBUGSS PA19 Debug Data In Out

BoosterPacks, Board Resources & Jumper Settings

Visit LP_MSPM0G3507 for LaunchPad information, including user guide and hardware files.

Pin Peripheral Function LaunchPad Pin LaunchPad Settings
PA12 TIMG0 CCP0 J4_32/J26_1 R64 connects J26_1 (default)
PA13 TIMG0 CCP1 J4_32/J26_3 R65 connects J26_3 (default)
PA20 DEBUGSS SWCLK N/A J101 15:16 ON: Connect to XDS-110 SWCLK (debug)
PA19 DEBUGSS SWDIO N/A J101 13:14 ON: Connect to XDS-110 SWDIO (debug)

Low-Power Recommendations

TI recommends to terminate unused pins by setting the corresponding functions to GPIO and configure the pins to output low or input with internal pullup/pulldown resistor.

SysConfig allows developers to easily configure unused pins by selecting BoardConfigure Unused Pins.

For more information about jumper configuration to achieve low-power using the MSPM0 LaunchPad, please visit the LP-MSPM0G3507 User’s Guide.

Example Usage

Compile, load and run the example. TimerG0 will output a pair of 2.73Hz center aligned PWM signals on PA12 and PA13. PA12 is configured at a 75% duty cycle. PA13 is configured at a 50% duty cycle. Monitor the PWM signals on PA12 and PA13.

Important Note

Early experimental samples have a known issue where the user is unable to reconnect their debugger connection after the device has gone into STOP or STANDBY mode. Please review advisory DEBUGSS_02 to see the steps to regain the ability to connect the device to the debugger. This information is located in the “MSPM0G and MSPM0L Families: Functional Differences With Early Samples” document.