/**
 *  \file   emac.c
 *
 *  \brief  EMAC APIs.
 *
 *   This file contains the device abstraction layer APIs for EMAC.
 */

/* Copyright (C) 2013 Texas Instruments Incorporated - www.ti.com
 * ALL RIGHTS RESERVED
 */

#include "emac.h"
#include "sys_vim.h"



/* Defining interface for all the emac instances */
hdkif_t hdkif_data[MAX_EMAC_INSTANCE];
/*SAFETYMCUSW 25 D MR:8.7 <APPROVED> "Statically allocated memory needs to be available to entire application." */
static uint8_t pbuf_array[MAX_RX_PBUF_ALLOC][MAX_TRANSFER_UNIT];
/*******************************************************************************
*                       INTERNAL MACRO DEFINITIONS
*******************************************************************************/
#define EMAC_CONTROL_RESET             (0x01U)
#define EMAC_SOFT_RESET                (0x01U)
#define EMAC_MAX_HEADER_DESC           (8U)
#define EMAC_UNICAST_DISABLE           (0xFFU)

/*******************************************************************************
*                        API FUNCTION DEFINITIONS
*******************************************************************************/
/**
 * \brief   Enables the TXPULSE Interrupt Generation.
 *
 * \param   emacBase      Base address of the EMAC Module registers.
 * \param   emacCtrlBase  Base address of the EMAC CONTROL module registers
 * \param   ctrlCore      Channel number for which the interrupt to be enabled in EMAC Control module
 * \param   channel       Channel number for which interrupt to be enabled
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_001 */
/* DesignId : ETH_DesignId_001*/
/* Requirements : HL_ETH_SR15 */
void EMACTxIntPulseEnable(uint32_t emacBase, uint32_t emacCtrlBase, uint32_t ctrlCore, uint32_t channel)
{
    HWREG(emacBase + EMAC_TXINTMASKSET) |= ((uint32_t)1U << channel);

    HWREG(emacCtrlBase + EMAC_CTRL_CnTXEN(ctrlCore)) |= ((uint32_t)1U << channel);
}

/**
 * \brief   Disables the TXPULSE Interrupt Generation.
 *
 * \param   emacBase      Base address of the EMAC Module registers.
 * \param   emacCtrlBase  Base address of the EMAC CONTROL module registers
 * \param   ctrlCore      Channel number for which the interrupt to be enabled in EMAC Control module
 * \param   channel       Channel number for which interrupt to be disabled
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_002 */
/* DesignId : ETH_DesignId_002*/
/* Requirements : HL_ETH_SR15 */ 
void EMACTxIntPulseDisable(uint32_t emacBase, uint32_t emacCtrlBase, uint32_t ctrlCore, uint32_t channel)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_TXINTMASKCLEAR) |= (uint32_t)((uint32_t)1U << channel);

    HWREG(emacCtrlBase + EMAC_CTRL_CnTXEN(ctrlCore)) &= (uint32_t)(~((uint32_t)1U << channel));
}

/**
 * \brief   Enables the RXPULSE Interrupt Generation.
 *
 * \param   emacBase      Base address of the EMAC Module registers.
 * \param   emacCtrlBase  Base address of the EMAC CONTROL module registers
 * \param   ctrlCore      Control core for which the interrupt to be enabled.
 * \param   channel       Channel number for which interrupt to be enabled
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_003 */
/* DesignId : ETH_DesignId_003*/
/* Requirements : HL_ETH_SR15 */
void EMACRxIntPulseEnable(uint32_t emacBase, uint32_t emacCtrlBase, uint32_t ctrlCore, uint32_t channel)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_RXINTMASKSET) |= (uint32_t)((uint32_t)1U << channel);

    HWREG(emacCtrlBase + EMAC_CTRL_CnRXEN(ctrlCore)) |= (uint32_t)((uint32_t)1U << channel);
}

/**
 * \brief   Disables the RXPULSE Interrupt Generation.
 *
 * \param   emacBase      Base address of the EMAC Module registers.
 * \param   emacCtrlBase  Base address of the EMAC CONTROL module registers
 * \param   ctrlCore      Control core for which the interrupt to be disabled.
 * \param   channel       Channel number for which interrupt to be disabled
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_004 */
/* DesignId : ETH_DesignId_004*/
/* Requirements : HL_ETH_SR15 */
void EMACRxIntPulseDisable(uint32_t emacBase, uint32_t emacCtrlBase, uint32_t ctrlCore, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXINTMASKCLEAR) |= (uint32_t)((uint32_t)1U << channel);

    HWREG(emacCtrlBase + EMAC_CTRL_CnRXEN(ctrlCore)) &= (uint32_t)(~((uint32_t)1U << channel));
}
/**
 * \brief   This API sets the RMII speed. The RMII Speed can be 10 Mbps or 
 *          100 Mbps
 *
 * \param   emacBase     Base address of the EMAC Module registers.
 * \param   speed        speed for setting.
 *          speed can take the following values. \n
 *                EMAC_RMIISPEED_10MBPS - 10 Mbps \n
 *                EMAC_RMIISPEED_100MBPS - 100 Mbps. 
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_005 */
/* DesignId : ETH_DesignId_005*/
/* Requirements : HL_ETH_SR19 */
void EMACRMIISpeedSet(uint32_t emacBase, uint32_t speed)
{
    HWREG(emacBase + EMAC_MACCONTROL) &= (uint32_t)(~(uint32_t)EMAC_MACCONTROL_RMIISPEED);
    
    HWREG(emacBase + EMAC_MACCONTROL) |= speed;
}
/* SourceId : ETH_SourceId_006 */
/* DesignId : ETH_DesignId_006*/
/* Requirements : HL_ETH_SR18 */
/**
 * \brief   This API enables the MII control block. It also needs to be enabled in the PINMUX module.
 *
 * \param   emacBase     Base address of the EMAC Module registers.
 *
 * \return  None
 *
 **/
void EMACMIIEnable(uint32_t emacBase)
{
    HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_GMIIEN;
}

/**
 * \brief   This API disables the MII module and holds MII Rx and Tx in reset.
 *
 * \param   emacBase     Base address of the EMAC Module registers.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_007 */
/* DesignId : ETH_DesignId_007*/
/* Requirements : HL_ETH_SR18 */
void EMACMIIDisable(uint32_t emacBase)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_MACCONTROL) &= (uint32_t)(~(uint32_t)EMAC_MACCONTROL_GMIIEN);
}

/**
 * \brief   This API sets the duplex mode of operation(full/half) for MAC.
 *
 * \param   emacBase     Base address of the EMAC Module registers.
 * \param   duplexMode   duplex mode of operation.
 *          duplexMode can take the following values. \n
 *                EMAC_DUPLEX_FULL - Full Duplex  \n
 *                EMAC_DUPLEX_HALF - Half Duplex.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_008 */
/* DesignId : ETH_DesignId_008*/
/* Requirements : HL_ETH_SR21 */
void EMACDuplexSet(uint32_t emacBase, uint32_t duplexMode)
{
    HWREG(emacBase + EMAC_MACCONTROL) &= (uint32_t)(~(uint32_t)EMAC_MACCONTROL_FULLDUPLEX);
    
    HWREG(emacBase + EMAC_MACCONTROL) |= duplexMode;
}

/**
 * \brief   API to enable the transmit in the TX Control Register
 *          After the transmit is enabled, any write to TXHDP of
 *          a channel will start transmission
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_009 */
/* DesignId : ETH_DesignId_009*/
/* Requirements : HL_ETH_SR21 */
void EMACTxEnable(uint32_t emacBase)
{
    HWREG(emacBase + EMAC_TXCONTROL) = EMAC_TXCONTROL_TXEN;
}

/**
 * \brief   API to disable the transmit in the TX Control Register
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_010 */
/* DesignId : ETH_DesignId_010*/
/* Requirements : HL_ETH_SR21 */
void EMACTxDisable(uint32_t emacBase)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_TXCONTROL) = EMAC_TXCONTROL_TXDIS;
}

/**
 * \brief   API to enable the receive in the RX Control Register
 *          After the receive is enabled, and write to RXHDP of
 *          a channel, the data can be received in the destination
 *          specified by the corresponding RX buffer descriptor.
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_011*/
/* DesignId : ETH_DesignId_011*/
/* Requirements : HL_ETH_SR21 */
void EMACRxEnable(uint32_t emacBase)
{
    HWREG(emacBase + EMAC_RXCONTROL) = EMAC_RXCONTROL_RXEN;
}

/**
 * \brief   API to disable the receive in the RX Control Register
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_012*/
/* DesignId : ETH_DesignId_012*/
/* Requirements : HL_ETH_SR21 */
void EMACRxDisable(uint32_t emacBase)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_RXCONTROL) = EMAC_RXCONTROL_RXDIS;
}

/**
 * \brief   API to write the TX HDP register. If transmit is enabled,
 *          write to the TX HDP will immediately start transmission.
 *          The data will be taken from the buffer pointer of the TX buffer
 *          descriptor written to the TX HDP
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.\n
 * \param   descHdr       Address of the TX buffer descriptor
 * \param   channel       Channel Number
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_013*/
/* DesignId : ETH_DesignId_013*/
/* Requirements : HL_ETH_SR16 */
void EMACTxHdrDescPtrWrite(uint32_t emacBase, uint32_t descHdr,
                           uint32_t channel)
{
    HWREG(emacBase + EMAC_TXHDP(channel)) = descHdr;
}

/**
 * \brief   API to write the RX HDP register. If receive is enabled,
 *          write to the RX HDP will enable data reception to point to
 *          the corresponding RX buffer descriptor's buffer pointer.
 *
 * \param   emacBase      Base Address of the EMAC Module Registers.\n
 * \param   descHdr       Address of the RX buffer descriptor
 * \param   channel       Channel Number
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_014 */
/* DesignId : ETH_DesignId_014*/
/* Requirements : HL_ETH_SR16 */
void EMACRxHdrDescPtrWrite(uint32_t emacBase, uint32_t descHdr, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXHDP(channel)) = descHdr;
}

/**
 * \brief   This API Initializes the EMAC and EMAC Control modules. The
 *          EMAC Control module is reset, the CPPI RAM is cleared. also,
 *          all the interrupts are disabled. This API does not enable any
 *          interrupt or operation of the EMAC.
 *
 * \param   emacCtrlBase      Base Address of the EMAC Control module
 *                            registers.\n
 * \param   emacBase          Base address of the EMAC module registers
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_015 */
/* DesignId : ETH_DesignId_015*/
/* Requirements : HL_ETH_SR6 */
void EMACInit(uint32_t emacCtrlBase, uint32_t emacBase)
{
    uint32_t cnt;

    /* Reset the EMAC Control Module. This clears the CPPI RAM also */
    HWREG(emacCtrlBase + EMAC_CTRL_SOFTRESET) = EMAC_CONTROL_RESET;

    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while((HWREG(emacCtrlBase + EMAC_CTRL_SOFTRESET) & EMAC_CONTROL_RESET) == EMAC_CONTROL_RESET)
    { 
	} /* Wait */

    /* Reset the EMAC Module. This clears the CPPI RAM also */
    HWREG(emacBase + EMAC_SOFTRESET) = EMAC_SOFT_RESET;

    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while((HWREG(emacBase + EMAC_SOFTRESET) & EMAC_SOFT_RESET) == EMAC_SOFT_RESET )
    { 
	} /* Wait */

    HWREG(emacBase + EMAC_MACCONTROL)= 0U;
    HWREG(emacBase + EMAC_RXCONTROL)= 0U;
    HWREG(emacBase + EMAC_TXCONTROL)= 0U;

    /* Initialize all the header descriptor pointer registers */
    for(cnt =  0U; cnt< EMAC_MAX_HEADER_DESC; cnt++)
    {
        HWREG(emacBase + EMAC_RXHDP(cnt)) = 0U;
        HWREG(emacBase + EMAC_TXHDP(cnt)) = 0U;
        HWREG(emacBase + EMAC_RXCP(cnt)) = 0U;
        HWREG(emacBase + EMAC_TXCP(cnt)) = 0U;
        HWREG(emacBase + EMAC_RXFREEBUFFER(cnt)) = 0xFFU;
    }
    /* Clear the interrupt enable for all the channels */
    HWREG(emacBase + EMAC_TXINTMASKCLEAR) = 0xFFU;
    HWREG(emacBase + EMAC_RXINTMASKCLEAR) = 0xFFU;

    HWREG(emacBase + EMAC_MACHASH1) = 0U;
    HWREG(emacBase + EMAC_MACHASH2) = 0U;

    HWREG(emacBase + EMAC_RXBUFFEROFFSET) = 0U;
}

/**
 * \brief   Sets the MAC Address in MACSRCADDR registers.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   macAddr       Start address of a MAC address array.
 *                        The array[0] shall be the LSB of the MAC address
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_016 */
/* DesignId : ETH_DesignId_016*/
/* Requirements : HL_ETH_SR7 */
void  EMACMACSrcAddrSet(uint32_t emacBase, uint8_t macAddr[6])
{
    HWREG(emacBase + EMAC_MACSRCADDRHI) = ((uint32_t)macAddr[5U] |(uint32_t)((uint32_t)macAddr[4U] << 8U)
                                     |(uint32_t)((uint32_t)macAddr[3U] << 16U) |(uint32_t)((uint32_t)macAddr[2U] << 24U));
    HWREG(emacBase + EMAC_MACSRCADDRLO) = ((uint32_t)macAddr[1U] | (uint32_t)((uint32_t)macAddr[0U] << 8U));
}

/**
 * \brief   Sets the MAC Address in MACADDR registers.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number
 * \param   matchFilt     Match or Filter
 * \param   macAddr       Start address of a MAC address array.
 *                        The array[0] shall be the LSB of the MAC address
 *          matchFilt can take the following values \n
 *          EMAC_MACADDR_NO_MATCH_NO_FILTER - Address is not used to match
 *                                             or filter incoming packet. \n
 *          EMAC_MACADDR_FILTER - Address is used to filter incoming packets \n
 *          EMAC_MACADDR_MATCH - Address is used to match incoming packets \n
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_017 */
/* DesignId : ETH_DesignId_017*/
/* Requirements : HL_ETH_SR7 */
void EMACMACAddrSet(uint32_t emacBase, uint32_t channel, uint8_t macAddr[6], uint32_t matchFilt)
{
    HWREG(emacBase + EMAC_MACINDEX) = channel;

    HWREG(emacBase + EMAC_MACADDRHI) = ((uint32_t)macAddr[5U] |((uint32_t)macAddr[4U] << 8U)
                                     |((uint32_t)macAddr[3U] << 16U) |((uint32_t)macAddr[2U] << 24U));
    HWREG(emacBase + EMAC_MACADDRLO) = ((uint32_t)macAddr[1U] | ((uint32_t)macAddr[0U] << 8U)
                                     | matchFilt | (channel << 16U));
}

/**
 * \brief   Acknowledges an interrupt processed to the EMAC Control Core.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   eoiFlag       Type of interrupt to acknowledge to the EMAC Control
 *                         module.
 *          eoiFlag can take the following values \n
 *             EMAC_INT_CORE0_TX - Core 0 TX Interrupt
 *             EMAC_INT_CORE1_TX - Core 1 TX Interrupt
 *             EMAC_INT_CORE2_TX - Core 2 TX Interrupt
 *             EMAC_INT_CORE0_RX - Core 0 RX Interrupt
 *             EMAC_INT_CORE1_RX - Core 1 RX Interrupt
 *             EMAC_INT_CORE2_RX - Core 2 RX Interrupt
 * \return  None
 * 
 **/
/* SourceId : ETH_SourceId_018 */
/* DesignId : ETH_DesignId_018*/
/* Requirements : HL_ETH_SR15 */
void EMACCoreIntAck(uint32_t emacBase, uint32_t eoiFlag)
{
    /* Acknowledge the EMAC Control Core */
    HWREG(emacBase + EMAC_MACEOIVECTOR) = eoiFlag;
}

/**
 * \brief   Writes the the TX Completion Pointer for a specific channel
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 * \param   comPtr        Completion Pointer Value to be written
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_019 */
/* DesignId : ETH_DesignId_019*/
/* Requirements : HL_ETH_SR27 */
void EMACTxCPWrite(uint32_t emacBase, uint32_t channel, uint32_t comPtr)
{
    HWREG(emacBase + EMAC_TXCP(channel)) = comPtr;
}

/**
 * \brief   Writes the the RX Completion Pointer for a specific channel
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 * \param   comPtr        Completion Pointer Value to be written
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_020 */
/* DesignId : ETH_DesignId_020*/
/* Requirements : HL_ETH_SR27 */
void EMACRxCPWrite(uint32_t emacBase, uint32_t channel, uint32_t comPtr)
{
    HWREG(emacBase + EMAC_RXCP(channel)) = comPtr;
}

/**
 * \brief   Enables a specific channel to receive broadcast frames
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_021 */
/* DesignId : ETH_DesignId_021*/
/* Requirements : HL_ETH_SR28 */
void EMACRxBroadCastEnable(uint32_t emacBase, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXBROADCH);

    HWREG(emacBase + EMAC_RXMBPENABLE) |= ((uint32_t)EMAC_RXMBPENABLE_RXBROADEN | ((uint32_t)channel << (uint32_t)EMAC_RXMBPENABLE_RXBROADCH_SHIFT));
}

/**
 * \brief   Disables a specific channel to receive broadcast frames
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_022 */
/* DesignId : ETH_DesignId_022*/
/* Requirements : HL_ETH_SR28 */
void EMACRxBroadCastDisable(uint32_t emacBase, uint32_t channel)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXBROADCH);
	/* Broadcast Frames are filtered. */
    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXBROADEN);
}

/**
 * \brief   Enables a specific channel to receive multicast frames
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_023 */
/* DesignId : ETH_DesignId_023*/
/* Requirements : HL_ETH_SR28 */
void EMACRxMultiCastEnable(uint32_t emacBase, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXMULTCH);

    HWREG(emacBase + EMAC_RXMBPENABLE) |= ((uint32_t)EMAC_RXMBPENABLE_RXMULTEN |(channel));
}

/**
 * \brief   Disables a specific channel to receive multicast frames
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_024 */
/* DesignId : ETH_DesignId_024*/
/* Requirements : HL_ETH_SR28 */
void EMACRxMultiCastDisable(uint32_t emacBase, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXMULTCH);

    HWREG(emacBase + EMAC_RXMBPENABLE) &= (~(uint32_t)EMAC_RXMBPENABLE_RXMULTEN);
}

/**
 * \brief   Enables unicast for a specific channel
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_025 */
/* DesignId : ETH_DesignId_025*/
/* Requirements : HL_ETH_SR14 */
void EMACRxUnicastSet(uint32_t emacBase, uint32_t channel)
{
    HWREG(emacBase + EMAC_RXUNICASTSET) |= ((uint32_t)1U << channel);
}

/**
 * \brief   Disables unicast for a specific channel
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_026 */
/* DesignId : ETH_DesignId_026*/
/* Requirements : HL_ETH_SR14 */
void EMACRxUnicastClear(uint32_t emacBase, uint32_t channel)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
    HWREG(emacBase + EMAC_RXUNICASTCLEAR) |= ((uint32_t)1U << channel);
}


/**
 * \brief   Set the free buffers for a specific channel
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 * \param   nBuf          Number of free buffers
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_027 */
/* DesignId : ETH_DesignId_027*/
/* Requirements : HL_ETH_SR20 */
void EMACNumFreeBufSet(uint32_t emacBase, uint32_t channel,
                       uint32_t nBuf)
{
    HWREG(emacBase + EMAC_RXFREEBUFFER(channel)) = nBuf;
}

/**
 * \brief   Gets the interrupt vectors of EMAC, which are pending
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 *
 * \return  Vectors
 *
 **/
/* SourceId : ETH_SourceId_028 */
/* DesignId : ETH_DesignId_028*/
/* Requirements : HL_ETH_SR15 */
uint32_t EMACIntVectorGet(uint32_t emacBase)
{
    return (HWREG(emacBase + EMAC_MACINVECTOR));
}



/**
* Function to setup the instance parameters inside the interface
* @param   hdkif Network interface structure
* @return  none.
*/
/* SourceId : ETH_SourceId_029 */
/* DesignId : ETH_DesignId_029*/
/* Requirements : HL_ETH_SR6 */
void EMACInstConfig(hdkif_t *hdkif)
{
    hdkif->emac_base = EMAC_0_BASE;
    hdkif->emac_ctrl_base = EMAC_CTRL_0_BASE;
    hdkif->emac_ctrl_ram = EMAC_CTRL_RAM_0_BASE;
    hdkif->mdio_base = MDIO_BASE;
    hdkif->phy_addr = 1U;
	/* (MISRA-C:2004 10.1/R) MISRA error reported with Code Composer Studio MISRA checker.  */
    hdkif->phy_autoneg = &Dp83640AutoNegotiate;
    hdkif->phy_partnerability = &Dp83640PartnerAbilityGet;
}

/**
* Function to setup the link. AutoNegotiates with the phy for link
* setup and set the EMAC with the result of autonegotiation.
* @param  hdkif Network interface structure.
* @return ERR_OK if everything passed
*         others if not passed
*/
/* SourceId : ETH_SourceId_030 */
/* DesignId : ETH_DesignId_030*/
/* Requirements : HL_ETH_SR6 */
uint32_t EMACLinkSetup(hdkif_t *hdkif) {
  uint32_t linkstat = EMAC_ERR_CONNECT;
  uint16_t partnr_ablty = 0U;
  uint32_t phyduplex = EMAC_DUPLEX_HALF;
  volatile uint32_t delay = 0xFFFFFU;

    if(Dp83640AutoNegotiate((uint32_t)hdkif->mdio_base, (uint32_t)hdkif->phy_addr,
                             (uint16_t)((uint16_t)DP83640_100BTX | (uint16_t)DP83640_100BTX_FD
                              | (uint16_t)DP83640_10BT | (uint16_t)DP83640_10BT_FD)) == TRUE) {
      linkstat = EMAC_ERR_OK;
	  /* (MISRA-C:2004 10.1/R) MISRA error reported with Code Composer Studio MISRA checker (due to use of & ?)  */
      (void)Dp83640PartnerAbilityGet(hdkif->mdio_base, hdkif->phy_addr,
                                &partnr_ablty);

      /* Check for 100 Mbps and duplex capability */
      if((partnr_ablty & DP83640_100BTX_FD) != 0U) {
        phyduplex = EMAC_DUPLEX_FULL;
      }
    }


  else {
    linkstat = EMAC_ERR_CONNECT;
  }

  /* Set the EMAC with the negotiation results if it is successful */
  if(linkstat == EMAC_ERR_OK) {
    EMACDuplexSet(hdkif->emac_base, phyduplex);
  }

  /* Wait for the MII to settle down */
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  while(delay != 0U)
  {
	delay--;
  }

  return linkstat;
}

/**
 * \brief   Perform a transmit queue teardown, that is, transmission is aborted.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_031 */
/* DesignId : ETH_DesignId_031*/
/* Requirements : HL_ETH_SR22 */
void EMACTxTeardown(uint32_t emacBase, uint32_t channel)
{
	HWREG(emacBase + EMAC_TXTEARDOWN) &= (channel);
}

/**
 * \brief   Perform a receive queue teardown, that is, reception is aborted.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel       Channel Number.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_032 */
/* DesignId : ETH_DesignId_032*/
/* Requirements : HL_ETH_SR22 */
void EMACRxTeardown(uint32_t emacBase, uint32_t channel)
{
	HWREG(emacBase + EMAC_RXTEARDOWN) &= (channel);
}


/**
 * \brief   Perform multicast frame filtering using the MAC Hash Registers.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   hashTable     The hash table which specifies which bits are to be accepted.
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_033 */
/* DesignId : ETH_DesignId_033*/
/* Requirements : HL_ETH_SR24 */
void EMACFrameSelect(uint32_t emacBase, uint64 hashTable)
{
	HWREG(emacBase + EMAC_MACHASH1) =  (uint32_t)(hashTable & 0xFFFFFFFFU);
	HWREG(emacBase + EMAC_MACHASH2) = (uint32_t)((uint64)hashTable >> 32U);
}


/**
 * \brief   Sets the Transmit Queue Priority type in the MACCONTROL Register
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   txPType       The Transmit Queue Priority Type.
 * 						  0 results in a round-robin scheme being used to select the next channel, while 1 results
 * 						  in a fixed-priority scheme( channel 7 highest priority).
 *
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_034 */
/* DesignId : ETH_DesignId_034*/
/* Requirements : HL_ETH_SR25 */
void EMACTxPrioritySelect(uint32_t emacBase, uint32_t txPType)
{

	/* 1- The queue uses a fixed-priority (channel 7 highest priority) scheme */
	if(txPType == 1U)
	{
		HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)(EMAC_MACCONTROL_TXPTYPE));
		HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_TXPTYPE;
	}
	else
	{
		HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)(EMAC_MACCONTROL_TXPTYPE));
	}
}


/**
 * \brief   Performs a soft reset of the EMAC and EMAC Control Modules.
 *
 * \param   emacCtrlBase  Base address of the EMAC CONTROL module registers
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_035 */
/* DesignId : ETH_DesignId_035*/
/* Requirements : HL_ETH_SR26 */
void EMACSoftReset(uint32_t emacCtrlBase, uint32_t emacBase)
{
    /* Reset the EMAC Control Module. This clears the CPPI RAM also */
    HWREG(emacCtrlBase + EMAC_CTRL_SOFTRESET) = EMAC_CONTROL_RESET;

    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while((HWREG(emacCtrlBase + EMAC_CTRL_SOFTRESET) & EMAC_CONTROL_RESET) == EMAC_CONTROL_RESET)
    {
		/* Wait for the reset to complete */
	} 

    /* Reset the EMAC Module. */
    HWREG(emacBase + EMAC_SOFTRESET) = EMAC_SOFT_RESET;

    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while((HWREG(emacBase + EMAC_SOFTRESET) & EMAC_SOFT_RESET) == EMAC_SOFT_RESET )
    {
		/* Wait for the Reset to complete */
	} 

}

/**
 * \brief   Enable Idle State of the EMAC Module.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_036 */
/* DesignId : ETH_DesignId_036*/
/* Requirements : HL_ETH_SR32 */
void EMACEnableIdleState(uint32_t emacBase)
{
		HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_CMDIDLE;
}

/**
 * \brief   Disable Idle State of the EMAC Module.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_037 */
/* DesignId : ETH_DesignId_037*/
/* Requirements : HL_ETH_SR32 */
void EMACDisableIdleState(uint32_t emacBase)
{
		HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)(EMAC_MACCONTROL_CMDIDLE));
}

/**
 * \brief   Enables Loopback Mode.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_038 */
/* DesignId : ETH_DesignId_038*/
/* Requirements : HL_ETH_SR50 */
void EMACEnableLoopback(uint32_t emacBase)
/*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "LDRA Tool issue." */
{
	uint32_t GMIIENval=0U;
	/*Store the value of GMIIEN bit before deasserting it */
	GMIIENval = HWREG(emacBase + EMAC_MACCONTROL) & EMAC_MACCONTROL_GMIIEN;
	HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)EMAC_MACCONTROL_GMIIEN);

	/*Enable Loopback */
	HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_LOOPBACK;

	/*Restore the value of GMIIEN bit */
	HWREG(emacBase + EMAC_MACCONTROL) |= GMIIENval;
}

/**
 * \brief   Disables Loopback Mode.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_039 */
/* DesignId : ETH_DesignId_039*/
/* Requirements : HL_ETH_SR50 */
void EMACDisableLoopback(uint32_t emacBase)
{
	uint32_t GMIIENval=0U;

	/*Store the value of GMIIEN bit before deasserting it */
	GMIIENval = HWREG(emacBase + EMAC_MACCONTROL) & EMAC_MACCONTROL_GMIIEN;
	HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)EMAC_MACCONTROL_GMIIEN);

	/*Disable Loopback */
	HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)EMAC_MACCONTROL_LOOPBACK);

	/*Restore the value of GMIIEN bit */
	HWREG(emacBase + EMAC_MACCONTROL) |= GMIIENval;
}

/**
 * \brief   Enable Transmit Flow Control.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_040 */
/* DesignId : ETH_DesignId_040*/
/* Requirements : HL_ETH_SR20 */
void EMACTxFlowControlEnable(uint32_t emacBase)
{
	HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_TXFLOWEN;
}

/**
 * \brief   Disable Transmit Flow Control.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_041 */
/* DesignId : ETH_DesignId_041*/
/* Requirements : HL_ETH_SR20 */
void EMACTxFlowControlDisable(uint32_t emacBase)
{
	HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)EMAC_MACCONTROL_TXFLOWEN);
}

/**
 * \brief   Enable Receive Flow Control.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_042 */
/* DesignId : ETH_DesignId_042*/
/* Requirements : HL_ETH_SR20 */
void EMACRxFlowControlEnable(uint32_t emacBase)
{
	HWREG(emacBase + EMAC_MACCONTROL) |= EMAC_MACCONTROL_RXBUFFERFLOWEN;
}

/**
 * \brief   Disable Receive Flow Control.
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_043 */
/* DesignId : ETH_DesignId_043*/
/* Requirements : HL_ETH_SR20 */
void EMACRxFlowControlDisable(uint32_t emacBase)
{
	HWREG(emacBase + EMAC_MACCONTROL) &= (~(uint32_t)EMAC_MACCONTROL_RXBUFFERFLOWEN);
}

/**
 * \brief   Receive flow threshold. These bits contain the threshold value for issuing flow control on incoming frames for channel n (when enabled).
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel		  Channel Number
 * \param  	threshold	  threshold value for issuing flow control on incoming frames for the given channel
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_044 */
/* DesignId : ETH_DesignId_044*/
/* Requirements : HL_ETH_SR20 */
void EMACRxSetFlowThreshold(uint32_t emacBase, uint32_t channel, uint32_t threshold)
{
	HWREG(emacBase + EMAC_RXFLOWTHRESH(channel)) &= (0x0U);
	HWREG(emacBase + EMAC_RXFLOWTHRESH(channel)) |= threshold;
}

/**
 * \brief				This function reads the contents of the 36 network statistics registers that are present in the module.
 * \param   emacBase    Base Address of the EMAC module registers.
 * \param   statRegNo   The number of the register with RXGOODFRAMES (Offset= 0x200) being 0. Refer the Technical Reference Manual for the list of registers and their contents.
 * \return  uint32_t
 **/
/* SourceId : ETH_SourceId_045 */
/* DesignId : ETH_DesignId_045*/
/* Requirements : HL_ETH_SR29 */
uint32_t EMACReadNetStatRegisters(uint32_t emacBase, uint32_t statRegNo)
{
	return HWREG(emacBase + EMAC_NETSTATREGS(statRegNo));
}


/**
 * \brief   Function to read values of Transmit Interrupt Status registers (TXINTSTATMASKED and TXINTSTATRAW)
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel		  Channel Number
 * \param   txintstat	  pointer to the emac_tx_int_status Structure that will store the register values that have been read
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_046 */
/* DesignId : ETH_DesignId_046*/
/* Requirements : HL_ETH_SR23 */
void EMACTxIntStat(uint32_t emacBase, uint32_t channel, emac_tx_int_status_t *txintstat)
{
	txintstat->intstatmasked = (HWREG(emacBase + EMAC_TXINTSTATMASKED) & (uint32_t)((uint32_t)1U << channel));
	txintstat->intstatraw = (HWREG(emacBase + EMAC_TXINTSTATRAW) & (uint32_t)((uint32_t)1U << channel));
}


/**
 * \brief   Function to read values of Receive Interrupt Status registers (RXINTSTATMASKED, RXINTSTATRAW)
 *
 * \param   emacBase      Base Address of the EMAC module registers.
 * \param   channel		  Channel Number
 * \param  rxintstat	  pointer to the emac_rx_int_status Structure that will store the register values that have been read.
 * \return  None
 **/
/* SourceId : ETH_SourceId_047 */
/* DesignId : ETH_DesignId_047*/
/* Requirements : HL_ETH_SR23 */
void EMACRxIntStat(uint32_t emacBase, uint32_t channel, emac_rx_int_status_t *rxintstat)
{
	rxintstat->intstatmasked_pend = (HWREG(emacBase + EMAC_RXINTSTATMASKED) & ((uint32_t)0x1U << (uint32_t)(channel)));
	rxintstat->intstatmasked_threshpend = (HWREG(emacBase + EMAC_RXINTSTATMASKED) & ((uint32_t)0x1U << ((uint32_t)0x8U + (uint32_t)(channel))));

	rxintstat->intstatraw_pend = (HWREG(emacBase + EMAC_RXINTSTATRAW) & (uint32_t)((uint32_t)0x1U << (uint32_t)(channel)));
	rxintstat->intstatraw_threshpend = (HWREG(emacBase + EMAC_RXINTSTATRAW) & (uint32_t)((uint32_t)0x1U << ((uint32_t)0x8U + (uint32_t)(channel))));
}


/**
 * \brief   Tx and Rx Buffer Descriptors are initialized. Buffer pointers are allocated to the Rx Descriptors.
 *
 * \param   hdkif	network interface structure
 * \return  None
 *
 **/
/* SourceId : ETH_SourceId_048 */
/* DesignId : ETH_DesignId_048*/
/* Requirements : HL_ETH_SR17,HL_ETH_SR30 */
void EMACDMAInit(hdkif_t *hdkif)
{

	  uint32_t num_bd, pbuf_cnt = 0U;
	  volatile emac_tx_bd_t *curr_txbd, *last_txbd;
	  volatile emac_rx_bd_t *curr_bd, *last_bd;
	  txch_t *txch_dma;
	  rxch_t *rxch_dma;
	  uint8_t *p;

	  txch_dma = &(hdkif->txchptr);

	  /**
	  * Initialize the Descriptor Memory For TX and RX
	  * Only single channel is supported for both TX and RX
	  */
	  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  txch_dma->free_head = (volatile emac_tx_bd_t*)(hdkif->emac_ctrl_ram);
	  txch_dma->next_bd_to_process = txch_dma->free_head;
	  txch_dma->active_tail = NULL;

	  /* Set the number of descriptors for the channel */
	  num_bd = (SIZE_EMAC_CTRL_RAM >> 1U) / sizeof(emac_tx_bd_t);

	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  curr_txbd = txch_dma->free_head;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
      last_txbd = curr_txbd;

	  /* Initialize all the TX buffer Descriptors */
	  while(num_bd != 0U) {
        /*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Struct pointer used for linked list is incremented." */
	    curr_txbd->next = curr_txbd + 1U;
	    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
	    curr_txbd->flags_pktlen = 0U;
	    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
		last_txbd = curr_txbd;
	    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
		curr_txbd = curr_txbd->next;
		num_bd--;
	  }
	  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
	  last_txbd->next = txch_dma->free_head;

	  /* Initialize the descriptors for the RX channel */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  rxch_dma = &(hdkif->rxchptr);
      /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  /*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Struct pointer used for linked list is incremented." */
	  curr_txbd++;
	  /*SAFETYMCUSW 94 S MR:11.1,11.2,11.4 <APPROVED> "Linked List pointer needs to be assigned." */
	  /*SAFETYMCUSW 95 S MR:11.1,11.4 <APPROVED> "Linked List pointer needs to be assigned." */
	  /*SAFETYMCUSW 344 S MR:11.5 <APPROVED> "Linked List pointer needs to be assigned to a different structure." */	  
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  rxch_dma->active_head = (volatile emac_rx_bd_t *)curr_txbd;

	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	 
	  rxch_dma->free_head = NULL;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
	  curr_bd = rxch_dma->active_head;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
	  last_bd = curr_bd;


	  /*
	  **  Static allocation of a specific number of packet buffers as specified by MAX_RX_PBUF_ALLOC, whose value is entered by the user in  HALCoGen GUI.
	  */

	  /*Commented part of allocation of pbufs need to check whether its true*/

	  for(pbuf_cnt = 0U;pbuf_cnt < MAX_RX_PBUF_ALLOC;pbuf_cnt++)
		{
	     /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	     p = pbuf_array[pbuf_cnt];
		 /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "RHS is a pointer value required to be stored. - Advisory as per MISRA" */
	     /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		 
	     curr_bd->bufptr = (uint32_t)p;
	     /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
		 curr_bd->bufoff_len = MAX_TRANSFER_UNIT;
	     /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	     
		 curr_bd->flags_pktlen = EMAC_BUF_DESC_OWNER;
	     if (pbuf_cnt == (MAX_RX_PBUF_ALLOC - 1U))
	     {
	         /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
			 curr_bd->next = NULL;
			 /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	    	 
			 last_bd = curr_bd;

	     }
	     else
	     {
             /*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Struct pointer used for linked list is incremented." */
	    	 curr_bd->next = (curr_bd + 1U);
			 /*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Struct pointer used for linked list is incremented." */
	    	 curr_bd++;
			 /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	    	 last_bd = curr_bd;
	     }
	   }
	  
	  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	 
	  last_bd->next = NULL;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
	  rxch_dma->active_tail = last_bd;
}


/**
 * \brief   Initializes the EMAC module for transmission and reception.
 *
 * \param   macaddr    MAC Address of the Module.
 * \param   channel       Channel Number.
 *
 * \return  EMAC_ERR_OK if everything gets initialized
 * 			EMAC_ERR_CONN in case of an error in connecting.
 *
 **/
/* SourceId : ETH_SourceId_049 */
/* DesignId : ETH_DesignId_049*/
/* Requirements : HL_ETH_SR6 */
uint32_t EMACHWInit(uint8_t macaddr[6U])
{
  uint32_t temp, channel;
  volatile uint32_t phyID=0U;
  volatile uint32_t delay = 0xFFFU;
  uint32_t phyIdReadCount = 0xFFFFU;
  volatile uint32_t phyLinkRetries = 0xFFFFU;
  hdkif_t *hdkif;
  rxch_t *rxch;
  uint32_t retVal = EMAC_ERR_OK;
  uint32_t emac_base = 0U;

  hdkif = &hdkif_data[0U];
  EMACInstConfig(hdkif);
  /* set MAC hardware address */
  for(temp = 0U; temp < EMAC_HWADDR_LEN; temp++) {
    hdkif->mac_addr[temp] = macaddr[(EMAC_HWADDR_LEN - 1U) - temp];
  }
  /*Initialize the EMAC, EMAC Control and MDIO modules. */
  EMACInit(hdkif->emac_ctrl_base, hdkif->emac_base);
  MDIOInit(hdkif->mdio_base, MDIO_FREQ_INPUT, MDIO_FREQ_OUTPUT);
  
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  while(delay != 0U)
  {
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	delay--;
  }

  /* Set the MAC Addresses in EMAC hardware */
  emac_base = hdkif->emac_base; /* MISRA Code Fix (12.2) */
  EMACMACSrcAddrSet(emac_base, hdkif->mac_addr);
  for(channel = 0U; channel < 8U; channel++) {
	   emac_base = hdkif->emac_base;
       EMACMACAddrSet(emac_base, channel, hdkif->mac_addr, EMAC_MACADDR_MATCH);
  }

  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  while ((phyID == 0U) && (phyIdReadCount > 0U)) {
	  phyID = Dp83640IDGet(hdkif->mdio_base,hdkif->phy_addr);
	  phyIdReadCount--;
  }

  if (0U == phyID) {
	  retVal = EMAC_ERR_CONNECT;
  } else {

  }

  if((uint32_t)0U == ((MDIOPhyAliveStatusGet(hdkif->mdio_base)
        >> hdkif->phy_addr) & (uint32_t)0x01U )) {
    retVal = EMAC_ERR_CONNECT;
  } else {

  }


  if(!Dp83640LinkStatusGet(hdkif->mdio_base, (uint32_t)EMAC_PHYADDRESS, (uint32_t)phyLinkRetries)) {
      retVal = EMAC_ERR_CONNECT;
  } else {

  }

  if(EMACLinkSetup(hdkif) != EMAC_ERR_OK) {
    retVal = EMAC_ERR_CONNECT;
  } else {

  }

  /* The transmit and receive buffer descriptors are initialized here. 
   * Also, packet buffers are allocated to the receive buffer descriptors.
   */

  EMACDMAInit(hdkif);

  /* Acknowledge receive and transmit interrupts for proper interrupt pulsing*/
  EMACCoreIntAck(hdkif->emac_base, (uint32_t)EMAC_INT_CORE0_RX);
  EMACCoreIntAck(hdkif->emac_base, (uint32_t)EMAC_INT_CORE0_TX);

  /* Enable MII if enabled in the GUI. */
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_MII_ENABLE)
	  EMACMIIEnable(hdkif->emac_base);
#else
      /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */  
      EMACMIIDisable(hdkif->emac_base);
#endif
  

  /* Enable Broadcast if enabled in the GUI. */
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_BROADCAST_ENABLE)
	  EMACRxBroadCastEnable(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER);
#else
   /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */
   /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */
	  EMACRxBroadCastDisable(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER);
#endif
  
  /* Enable Broadcast if enabled in the GUI. */
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_UNICAST_ENABLE)
	  EMACRxUnicastSet(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER);
#else
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */
	  EMACRxUnicastClear(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER);
#endif

  /*Enable Full Duplex or Half-Duplex mode based on GUI Input. */
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if (EMAC_FULL_DUPLEX_ENABLE)
  		EMACDuplexSet(EMAC_0_BASE, (uint32_t)EMAC_DUPLEX_FULL);
#else
	    /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition arameter is taken as input from GUI." */
  		EMACDuplexSet(EMAC_0_BASE, (uint32_t)EMAC_DUPLEX_HALF);
#endif

  /* Enable Loopback based on GUI Input */ 
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_LOOPBACK_ENABLE)
	  EMACEnableLoopback(hdkif->emac_base);
#else
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */  
	  EMACDisableLoopback(hdkif->emac_base);
#endif

  /* Enable Transmit and Transmit Interrupt */ 
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_TX_ENABLE)
	  EMACTxEnable(hdkif->emac_base);
	  EMACTxIntPulseEnable(hdkif->emac_base, hdkif->emac_ctrl_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)EMAC_CHANNELNUMBER);
#else
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */
	  EMACTxDisable(hdkif->emac_base);
	  EMACTxIntPulseDisable(hdkif->emac_base, hdkif->emac_ctrl_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)EMAC_CHANNELNUMBER);	  
#endif

  /* Enable Receive and Receive Interrupt. Then start receiving by writing to the HDP register. */
  /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Parameter is taken as input from GUI." */
#if(EMAC_RX_ENABLE)
	  EMACNumFreeBufSet(hdkif->emac_base,(uint32_t)EMAC_CHANNELNUMBER , (uint32_t)MAX_RX_PBUF_ALLOC);
	  EMACRxEnable(hdkif->emac_base);
	  EMACRxIntPulseEnable(hdkif->emac_base, hdkif->emac_ctrl_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)EMAC_CHANNELNUMBER);
	  rxch = &(hdkif->rxchptr);
	  /* Write to the RX HDP for channel 0 */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  EMACRxHdrDescPtrWrite(hdkif->emac_base, (uint32_t)rxch->active_head, (uint32_t)EMAC_CHANNELNUMBER);
#else
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */    
	  /*SAFETYMCUSW 1 J MR:14.1 <APPROVED> "If condition parameter is taken as input from GUI." */  
	  EMACRxDisable(hdkif->emac_base);
	  EMACRxIntPulseDisable(hdkif->emac_base, hdkif->emac_ctrl_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)EMAC_CHANNELNUMBER);	  
#endif

  return retVal;
}


/**
 * This function should do the actual transmission of the packet. The packet is
 * contained in the pbuf that is passed to the function. This pbuf might be
 * chained. That is, one pbuf can span more than one tx buffer descriptors
 *
 * @param hdkif network interface structure
 * @param pbuf  the pbuf structure which contains the data to be sent using EMAC
 * @return boolean. 
 *		  -Returns FALSE if a Null pointer was passed for transmission
 *		  -Returns TRUE if valid data is sent and is transmitted.
 */
/* SourceId : ETH_SourceId_050 */
/* DesignId : ETH_DesignId_050*/
/* Requirements : HL_ETH_SR31 */
boolean EMACTransmit(hdkif_t *hdkif, pbuf_t *pbuf)
{
	
  txch_t *txch;
  pbuf_t *q;
  volatile emac_tx_bd_t *curr_bd,*active_head, *bd_end;
  boolean retValue = FALSE;
  if((pbuf != NULL) && (hdkif != NULL))
  {
  txch = &(hdkif->txchptr);

  /* Get the buffer descriptor which is free to transmit */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  curr_bd = txch->free_head;
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  bd_end = curr_bd;
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  active_head = curr_bd;

  /* Update the total packet length */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	   
  curr_bd->flags_pktlen &= (uint32_t)(~((uint32_t)0xFFFFU));
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  uint16_t tot_len = pbuf->tot_len;
  curr_bd->flags_pktlen |= (uint32_t)(tot_len);

  /* Indicate the start of the packet */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  curr_bd->flags_pktlen |= (EMAC_BUF_DESC_SOP | EMAC_BUF_DESC_OWNER);


  /* Copy pbuf information into TX buffer descriptors */
	q = pbuf;
	while(q != NULL)
	{
	/* Initialize the buffer pointer and length */
	/*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "RHS is a pointer value required to be stored. - Advisory as per MISRA" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	curr_bd->bufptr = (uint32_t)(q->payload);
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */
	uint16_t len = q->len;
	curr_bd->bufoff_len = (uint32_t)((uint32_t)(len) & 0xFFFFU);
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	bd_end = curr_bd;
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	curr_bd = curr_bd->next;
	q = q->next;
	}


  /* Indicate the start and end of the packet */
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	   
  bd_end->next = NULL;
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  bd_end->flags_pktlen |= EMAC_BUF_DESC_EOP;

  /*SAFETYMCUSW 71 S MR:17.6 <APPROVED> "Assigned pointer value has required scope." */
  txch->free_head = curr_bd;

  /* For the first time, write the HDP with the filled bd */
  if(txch->active_tail == NULL) {
    /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "Address stored in pointer is passed as as an int parameter. - Advisory as per MISRA" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
    EMACTxHdrDescPtrWrite(hdkif->emac_base, (uint32_t)(active_head), (uint32_t)EMAC_CHANNELNUMBER);
  }

  /*
   * Chain the bd's. If the DMA engine, already reached the end of the chain,
   * the EOQ will be set. In that case, the HDP shall be written again.
   */
  else {
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    curr_bd = txch->active_tail;
    /* Wait for the EOQ bit is set */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    while (EMAC_BUF_DESC_EOQ != (curr_bd->flags_pktlen & EMAC_BUF_DESC_EOQ))
	{
	}
    /* Don't write to TXHDP0 until it turns to zero */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  	while (((uint32_t)0U != *((uint32_t *)0xFCF78600U)))
	{
	}
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    curr_bd->next = active_head;
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
    if (EMAC_BUF_DESC_EOQ == (curr_bd->flags_pktlen & EMAC_BUF_DESC_EOQ)) {
      /* Write the Header Descriptor Pointer and start DMA */
      /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "Address stored in pointer is passed as as an int parameter. - Advisory as per MISRA" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
      EMACTxHdrDescPtrWrite(hdkif->emac_base, (uint32_t)(active_head), (uint32_t)EMAC_CHANNELNUMBER);
    }
  }
   
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  txch->active_tail = bd_end;
  retValue = TRUE;
  }
  else
  {
	retValue = FALSE;
  }
  return retValue;
}


/**
 * Function for processing Tx buffer descriptors.
 *
 * @param hdkif interface structure
 * @return none
 */
/* SourceId : ETH_SourceId_051 */
/* DesignId : ETH_DesignId_051*/
/* Requirements : HL_ETH_SR15 */
void EMACTxIntHandler(hdkif_t *hdkif)
{
  txch_t *txch_int;
  volatile emac_tx_bd_t *curr_bd, *next_bd_to_process;

  txch_int = &(hdkif->txchptr);

  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
  next_bd_to_process = txch_int->next_bd_to_process;
  
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
  curr_bd = next_bd_to_process;

  /* Check for correct start of packet */
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
  while(((curr_bd->flags_pktlen) & EMAC_BUF_DESC_SOP) == EMAC_BUF_DESC_SOP) {

    /* Make sure that the transmission is over */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    while(((curr_bd->flags_pktlen) & EMAC_BUF_DESC_OWNER) == EMAC_BUF_DESC_OWNER)
	{
	}

    /* Traverse till the end of packet is reached */
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    while(((curr_bd->flags_pktlen) & EMAC_BUF_DESC_EOP) != EMAC_BUF_DESC_EOP) {
       curr_bd = curr_bd->next;
    }

	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    next_bd_to_process->flags_pktlen &= ~(EMAC_BUF_DESC_SOP);
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	curr_bd->flags_pktlen &= ~(EMAC_BUF_DESC_EOP);

    /**
     * If there are no more data transmitted, the next interrupt
     * shall happen with the pbuf associated with the free_head
     */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    if(curr_bd->next == NULL) {
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
      txch_int->next_bd_to_process = txch_int->free_head;
    }

    else {
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
      txch_int->next_bd_to_process = curr_bd->next;
    }

    /* Acknowledge the EMAC and free the corresponding pbuf */
    /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "Address stored in pointer is passed as as an int parameter. - Advisory as per MISRA" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    /*SAFETYMCUSW 344 S MR:11.5 <APPROVED> "Address stored in pointer is passed as as an int parameter." */
    EMACTxCPWrite(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)curr_bd);
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    next_bd_to_process = txch_int->next_bd_to_process;
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    curr_bd = next_bd_to_process;

  }

}


/**
 * Function for processing received packets.
 *
 * @param hdkif interface structure
 * @return none
 */
/* SourceId : ETH_SourceId_052 */
/* DesignId : ETH_DesignId_052*/
/* Requirements : HL_ETH_SR31 */
void EMACReceive(hdkif_t *hdkif)
{
  rxch_t *rxch_int;
  volatile emac_rx_bd_t *curr_bd, *curr_tail, *last_bd;

  /* The receive structure that holds data about a particular receive channel */
  rxch_int = &(hdkif->rxchptr);

  /* Get the buffer descriptors which contain the earliest filled data */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  curr_bd = rxch_int->active_head;
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  last_bd = rxch_int->active_tail;

  /**
   * Process the descriptors as long as data is available
   * when the DMA is receiving data, SOP flag will be set
  */
  /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
  while((curr_bd->flags_pktlen & EMAC_BUF_DESC_SOP) == EMAC_BUF_DESC_SOP) {


    /* Start processing once the packet is loaded */
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    if((curr_bd->flags_pktlen & EMAC_BUF_DESC_OWNER)
       != EMAC_BUF_DESC_OWNER) {

      /* this bd chain will be freed after processing */
      /*SAFETYMCUSW 71 S MR:17.6 <APPROVED> "Assigned pointer value has required scope." */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */
      rxch_int->free_head = curr_bd;

      /* Get the total length of the packet. curr_bd points to the start
       * of the packet.
       */

      /* 
       * The loop runs till it reaches the end of the packet.
       */
	  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
      while((curr_bd->flags_pktlen & EMAC_BUF_DESC_EOP)!= EMAC_BUF_DESC_EOP)
      {
    	/*Update the flags for the descriptor again and the length of the buffer*/
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
    	curr_bd->flags_pktlen = (uint32_t)EMAC_BUF_DESC_OWNER;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
    	curr_bd->bufoff_len = (uint32_t)MAX_TRANSFER_UNIT;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
        last_bd = curr_bd;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
        curr_bd = curr_bd->next;
      }

      /* Updating the last descriptor (which contained the EOP flag) */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	  
		curr_bd->flags_pktlen = (uint32_t)EMAC_BUF_DESC_OWNER;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
		curr_bd->bufoff_len = (uint32_t)MAX_TRANSFER_UNIT;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
        last_bd = curr_bd;
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
        curr_bd = curr_bd->next;

      /* Acknowledge that this packet is processed */
      /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "Address stored in pointer is passed as as an int parameter. - Advisory as per MISRA" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
      EMACRxCPWrite(hdkif->emac_base, (uint32_t)EMAC_CHANNELNUMBER, (uint32_t)last_bd);

      /* The next buffer descriptor is the new head of the linked list. */
	  /*SAFETYMCUSW 71 S MR:17.6 <APPROVED> "Assigned pointer value has required scope." */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
      rxch_int->active_head = curr_bd;

      /* The processed descriptor is now the tail of the linked list. */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  curr_tail = rxch_int->active_tail;
	/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  curr_tail->next = rxch_int->free_head;

	  /* The last element in the already processed Rx descriptor chain is now the end of list. */
	  /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	  last_bd->next = NULL;


		/**
		 * Check if the reception has ended. If the EOQ flag is set, the NULL
		 * Pointer is taken by the DMA engine. So we need to write the RX HDP
		 * with the next descriptor.
		 */
	    /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */ 
		/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
	  /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		
		if((curr_tail->flags_pktlen & EMAC_BUF_DESC_EOQ) == EMAC_BUF_DESC_EOQ) {
          /*SAFETYMCUSW 439 S MR:11.3 <APPROVED> "Address stored in pointer is passed as as an int parameter. - Advisory as per MISRA" */
	      /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 		 
		  EMACRxHdrDescPtrWrite(hdkif->emac_base, (uint32_t)(rxch_int->free_head), (uint32_t)EMAC_CHANNELNUMBER);
		}

	    /*SAFETYMCUSW 71 S MR:17.6 <APPROVED> "Assigned pointer value has required scope." */
		/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
		rxch_int->free_head  = curr_bd;
		rxch_int->active_tail = last_bd;
	  }
    }
}


/** @fn void EMACGetConfigValue(emac_config_reg_t *config_reg, config_value_type_t type)
*   @brief Get the initial or current values of the configuration registers
*
*	@param[in] *config_reg: pointer to the struct to which the initial or current 
*                           value of the configuration registers need to be stored
*	@param[in] type: 	whether initial or current value of the configuration registers need to be stored
*						- InitialValue: initial value of the configuration registers will be stored 
*                                       in the struct pointed by config_reg
*						- CurrentValue: initial value of the configuration registers will be stored 
*                                       in the struct pointed by config_reg
*
*   This function will copy the initial or current value (depending on the parameter 'type') 
*   of the configuration registers to the struct pointed by config_reg
*
*/
/* SourceId : ETH_SourceId_053 */
/* DesignId : ETH_DesignId_053*/
/* Requirements : HL_ETH_SR52 */
void EMACGetConfigValue(emac_config_reg_t *config_reg, config_value_type_t type)
{
	if (type == InitialValue)
	{
		config_reg->TXCONTROL = EMAC_TXCONTROL_CONFIGVALUE;
		config_reg->RXCONTROL = EMAC_RXCONTROL_CONFIGVALUE;
		config_reg->TXINTMASKSET = EMAC_TXINTMASKSET_CONFIGVALUE;
		config_reg->TXINTMASKCLEAR = EMAC_TXINTMASKCLEAR_CONFIGVALUE;
		config_reg->RXINTMASKSET = EMAC_RXINTMASKSET_CONFIGVALUE;
		config_reg->RXINTMASKCLEAR = EMAC_RXINTMASKCLEAR_CONFIGVALUE;
		config_reg->MACSRCADDRHI = EMAC_MACSRCADDRHI_CONFIGVALUE;
		config_reg->MACSRCADDRLO = EMAC_MACSRCADDRLO_CONFIGVALUE;	
		config_reg->MDIOCONTROL = EMAC_MDIOCONTROL_CONFIGVALUE;
		config_reg->C0RXEN = EMAC_C0RXEN_CONFIGVALUE;
		config_reg->C0TXEN = EMAC_C0TXEN_CONFIGVALUE;
	}
	else
	{
		config_reg->TXCONTROL = HWREG(EMAC_0_BASE + EMAC_TXCONTROL);
		config_reg->RXCONTROL = HWREG(EMAC_0_BASE + EMAC_RXCONTROL);
		config_reg->TXINTMASKSET = HWREG(EMAC_0_BASE + EMAC_TXINTMASKSET);
		config_reg->TXINTMASKCLEAR = HWREG(EMAC_0_BASE + EMAC_TXINTMASKCLEAR);
		config_reg->RXINTMASKSET = HWREG(EMAC_0_BASE + EMAC_RXINTMASKSET);
		config_reg->RXINTMASKCLEAR = HWREG(EMAC_0_BASE + EMAC_RXINTMASKCLEAR);
		config_reg->MACSRCADDRHI = HWREG(EMAC_0_BASE + EMAC_MACSRCADDRHI);
		config_reg->MACSRCADDRLO = HWREG(EMAC_0_BASE + EMAC_MACSRCADDRLO);		
		config_reg->MDIOCONTROL = HWREG(MDIO_0_BASE + MDIO_CONTROL);
		config_reg->C0RXEN = HWREG(EMAC_CTRL_0_BASE + EMAC_CTRL_CnRXEN(0U));
		config_reg->C0TXEN = HWREG(EMAC_CTRL_0_BASE + EMAC_CTRL_CnTXEN(0U));
	}
	
}

/* ISR for EMAC Transmit Interrupt. Calls another handler function for processing the descriptors.
 *
 * @return none
 * */
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> "#pragma required for interrupt handler." */	
#pragma CODE_STATE(EMACTxIntISR, 32)
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> "#pragma required for interrupt handler." */	
#pragma INTERRUPT(EMACTxIntISR, IRQ)
/* SourceId : ETH_SourceId_054 */
/* DesignId : ETH_DesignId_054*/
/* Requirements : HL_ETH_SR15 */
void EMACTxIntISR(void)
{
	hdkif_t *hdkif;
	hdkif= &hdkif_data[0U];
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */		
	emacTxNotification(hdkif);
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	EMACTxIntHandler(hdkif);
	EMACCoreIntAck(hdkif->emac_base, (uint32_t)EMAC_INT_CORE0_TX);
	
}

/**
 * ISR for Receive interrupt.  Calls another function for processing the received packets.
 *
 * @return none
 */
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> "#pragma required for interrupt handler." */	
#pragma CODE_STATE(EMACRxIntISR, 32)
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> "#pragma required for interrupt handler." */	
#pragma INTERRUPT(EMACRxIntISR, IRQ)
/* SourceId : ETH_SourceId_055 */
/* DesignId : ETH_DesignId_055*/
/* Requirements : HL_ETH_SR15 */
void EMACRxIntISR(void)
{
	hdkif_t *hdkif;
	hdkif= &hdkif_data[0U];
	/* The data is received in the allocated receive descriptors starting from (&(hdkif->rxchptr))->active_head */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */		
	emacRxNotification(hdkif);
	/* In this function, the filled receive buffer descriptors are freed for further usage and the receive interrupt is acknowledged. */
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 
	/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are assigned in this driver" */	 	
	EMACReceive(hdkif);


	/* Acknowledge the EMAC Core Rx Interrupts */
	EMACCoreIntAck(hdkif->emac_base, (uint32_t)EMAC_INT_CORE0_RX);
}

/***************************** End Of File ***********************************/