/** @file sys_startup.c 
*   @brief Startup Source File
*   @date 24.Feb.2014
*   @version 03.08.01
*
*   This file contains:
*   - Include Files
*   - Type Definitions
*   - External Functions
*   - VIM RAM Setup
*   - Startup Routine
*   .
*   which are relevant for the Startup.
*/

/* (c) Texas Instruments 2009-2014, All rights reserved. */

/* USER CODE BEGIN (0) */
/* USER CODE END */


/* Include Files */

#include "sys_common.h"
#include "system.h"
#include "sys_vim.h"
#include "sys_core.h"

/* USER CODE BEGIN (1) */
/* USER CODE END */


/* Type Definitions */

typedef void (*handler_fptr)(const uint8_t * in, uint8_t * out);

/* USER CODE BEGIN (2) */
/* USER CODE END */


/* External Functions */
/*SAFETYMCUSW 218 S MR:20.2 <APPROVED> "Functions from library" */
extern void __TI_auto_init(void);
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(main should be declared by the user)" */
extern void main(void);
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(Extern declaration present in the library)" */
extern void exit(void);


/* USER CODE BEGIN (3) */
/* USER CODE END */

/* Startup Routine */
void _c_int00(void);

/* USER CODE BEGIN (4) */
/* USER CODE END */

#pragma CODE_STATE(_c_int00, 32)
#pragma INTERRUPT(_c_int00, RESET)
#pragma WEAK(_c_int00)

/* SourceId : STARTUP_SourceId_001 */
/* DesignId : STARTUP_DesignId_001 */
/* Requirements : HL_SR508 */
void _c_int00(void)
{
    
/* USER CODE BEGIN (5) */
/* USER CODE END */

    /* Initialize Core Registers to avoid CCM Error */
    _coreInitRegisters_();

/* USER CODE BEGIN (6) */
/* USER CODE END */

    /* Initialize Stack Pointers */
    _coreInitStackPointer_();

/* USER CODE BEGIN (7) */
/* USER CODE END */

    /* Work Around for Errata DEVICE#140: ( Only on Rev A silicon) 
     *
     * Errata Description:
     *            The Core Compare Module(CCM-R4) may cause nERROR to be asserted after a cold power-on
     * Workaround:
     *            Clear ESM Group2 Channel 2 error in ESMSR2 and Compare error in CCMSR register */
    if (DEVICE_ID_REV == 0x802AAD05U)
    {
        _esmCcmErrorsClear_();
    }
    
/* USER CODE BEGIN (8) */
/* USER CODE END */

    /* Enable CPU Event Export */
    /* This allows the CPU to signal any single-bit or double-bit errors detected
     * by its ECC logic for accesses to program flash or data RAM.
     */
    _coreEnableEventBusExport_();


/* USER CODE BEGIN (72) */
/* USER CODE END */
    
    /* Enable IRQ offset via Vic controller */
    _coreEnableIrqVicOffset_();
    
    /* Initialize System - Clock, Flash settings with Efuse self check */
    systemInit();

/* USER CODE BEGIN (73) */
/* USER CODE END */

    /* Initialize VIM table */
    vimInit();    

/* USER CODE BEGIN (74) */
    _copyAPI2RAM_();
/* USER CODE END */

    /* Configure system response to error conditions signaled to the ESM group1 */
    /* This function can be configured from the ESM tab of HALCoGen */
//    esmInit();
    /* initialize copy table */
    __TI_auto_init();

/* USER CODE BEGIN (75) */
/* USER CODE END */
    
    /* call the application */
/*SAFETYMCUSW 296 S MR:8.6 <APPROVED> "Startup code(library functions at block scope)" */
/*SAFETYMCUSW 326 S MR:8.2 <APPROVED> "Startup code(Declaration for main in library)" */
/*SAFETYMCUSW 60 D MR:8.8 <APPROVED> "Startup code(Declaration for main in library;Only doing an extern for the same)" */
    main();

/* USER CODE BEGIN (76) */
/* USER CODE END */
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
    exit();

/* USER CODE BEGIN (77) */
/* USER CODE END */
}

/* USER CODE BEGIN (78) */
/* USER CODE END */