UsbTreeView V3.8.2 - Shows the USB Device Tree Freeware by Uwe Sieber - www.uwe-sieber.de Works under Windows 2000, XP, Windows 7, 8, 10, 11 and Server 2000 to 2022 Usage: Without parameters it starts with a GUI. Params: UsbTreeView [/R=filename] [/X=filename] [/O=filename] [/L[n]=logfile] /R=filename write (silently) a text report to filename /X=filename write (silently) an XML report to filename /O=filename open an XML report from filename /L[n]=logfile write a logfile for debugging, helpful in case of crash or hang (causes slowdown); n is the optional loglevel, 0..5, default is 3; sample: /L4=C:\temp\UsbTreeView.log UsbTreeView is based upon the USBView sample from the Microsoft Windows Driver Kit for Windows Server 2003. Improvements: - refresh on device change performed asynchronously, per device and selected item stays selected - shows additional information gathered from the Windows device management - shows drive letters/mountpoints and COM ports - can perform safe removal, device restart and port restart - shows open handles on failed safe removal - TreeView highlighting of arrived and removed devices - better icons in the treeview - custom font and color for the right pane - toolbar with jump-lists for easily finding devices in complex trees - search to find device IDs, device names etc - nodes of empty hubs kept closed by default - nodes can be renamed by pressing F2 or by clicking it when already selected (needs admin privileges) - additional descriptors are decoded as Audio 2.0, UVC 1.5 - write and read a report in XML format (not compatible with USBview's) - copy a screenshot of the tree-view to the Windows clipboard History since V2.5.0, for old history see UsbTreeView.txt in here: http://www.uwe-sieber.de/files/usbtreeview261.zip V3.8.2 - Bugfix: Since V3.7.7 no more new devices where detected after removing a hub until a full refresh - New: Billboard Capability Descriptor decoded V3.8.1 - Bugfix: Starting Regedit did not work mostly V3.8.0 - New: Context menu item "Regedit..." to open certain device specific registry keys in the Windows Registry Editor. Needs admin privileges. - Rewind: A bcdUSB value if 0x200 is no more blamed as "wrong" for low and full speed devices because an additional spec doc says that it's ok in contrast to the main spec V3.7.8 - Bugfix: V3.7.7 did no show a Windows when started under XP thru the Windows Explorer - Bugfix: V3.7.7 crashed when a hub did not deliver its USB_HUB_INFORMATION V3.7.7 - Workaround: Some ASMedia host controllers fail to deliver their root-hub's symlink by means of IOCTL_USB_GET_ROOT_HUB_NAME. Same problem when requesting the symlink of a standard hub (IOCTL_USB_GET_NODE_CONNECTION_NAME). Both calls may fail with ERROR_NOT_SUPPORTED when the ASMedia drivers asmtxhci.sys and asmthub3.sys are used. Both cases are resolved now by devices' parent-child relation. - New: For /R and /X a 'magic' file name of "stdout" makes it write the text- or XML-report to stdout instead of an actual file. If not redirected it attaches to parent process' console or creates a new one. V3.7.6 - Bugfix: wChannelConfig of Audio 1.0 descriptors decoded wrong, possible crash - Bugfix: Other Speed Configuration Descriptor not shown since V3.4 V3.7.5 - Bugfix: x64 Release did not save settings when it has no write access to the INI file because Windows does VirtualStore redirection for 32 bit apps only. Without write access the INI is now saved to %ALLUSERSPROFILE%\Uwe Sieber (under Windows 2000, XP and 2003 to %APPDATA%) V3.7.4 - Bugfix: Option "Read Msft String Descriptor 0xEE" was read inverted from INI since V3.4.0, so it switched between on and off every start - Bugfix: bInterval of endpoint descriptors decoded wrong - New: Drop-down lists as wide as the longest item V3.7.3 - New: Some fine-tuning for smart node naming V3.7.2 - Bugfix: When renaming a USB dev's node the default name was always the device description from the Device Manager, even another source was selected V3.7.1 - Bugfix: V3.7.0 had no valid default for the new source of display names resultung in showing device IDs until a valid source was selected V3.7.0 - New: Tree nodes of USB devices can show now either names from the Device Manager (as USBview and UsbTreeView before V3.7) or names build from USB string descriptors or (new default) a smart choice of the available strings - Bugfix: V3.6.0 reported an error for a trailing NULL character in string descriptors even there is none V3.6.0 - New: Support for high-DPI screens - no more bitmap scaling under Windows 8 and 10 V3.5.4 - Bugfix: String descriptor might shown wrong for multiple languages V3.5.3 - Bugfix: Wrong font color when highlighting selected node while not focused V3.5.2 - Bugfix: Port maximum speed shown wrong on pre-Win8 systems - Bugfix: Comboboxs with old content after loading an XML report V3.5.1 - Bugfix: Minor fixes V3.5.0 - Bugfix: Crash on Windows 8, 8.1, Server 2008 when dealing with companion ports - New: Highlight for companion ports (Win8+) - New: Right-click -> Copy Tree from here can copy a full treeview screenshot V3.4.4 - Bugfix: since V3.4.0 copy tree to clipboard did not work - Bugfix: since V3.4.1 possible crash when restarting a hub V3.4.3 - Bugfix: since V3.4.1 SuperSpeed ports got no 'S' icon and max speed shown as SuperSpeedPlus V3.4.2 - Bugfix: V3.4.1 crashed on pre-Win8 systems V3.4.1 - Bugfix: Child devices sorted by device id instead of kernel name, at least for devices the author came across with this leads to better sorting, e.g. for COM ports - Bugfix: TreeView's context menu did not work on negative mouse coordinates - New: Shows a summary with the most interesting information - New: Can shows sum of used endpoints of all devices attached to a root-hub in the tree-view - New: Remembers which ports have ever operated at SuperSpeedPlus (because so far there is no way to request the capability) V3.4.0 - Bugfix: Crash with failed USB hub - Bugfix: Focus of active app stolen when silently creating a report file - New: UVC 1.5 H.264 descriptors are decoded - New: More device class and device interface GUIDs are resolved - New: Reporting a USB version of 2.0 is blamed as an error if the device does not deliver an "other_speed" device_qualifier descriptor, see below V3.3.8 - New: USB vendor names from https://cms.usb.org/usb/api/usbif.json which seems to contain all vendors ever registered at usb.org (about 12000). The former used 'usb.if' contained current members only (about 1000). This results in a 70 KB larger exe file. - New: Option to allow only one instance of the same UsbTreeView.exe running - New: tree items with an error or a problem show a tool-tip on mouse-over - Bugfix: More than one companion port can be shown V3.3.7 - Bugfix: Renamed tree items not shown with the customized name on startup V3.3.6 - New: Shows Registry flags under HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\usbstor\VVVVPPPP V3.3.5 - New: Sum of used endpoints shown for root-hubs - New: Option to show the number of used endpoints in the tree - Bugfix: Crashs on device removal V3.3.4 - Bugfix: Sometimes truncated XML report - New: A selected tree node can be renamed by pressing F2 or single left-click it (needs admin privileges) V3.3.3 - New: Finds root hubs which are not the child device of their host controller (often seen on virtual USB over LAN) V3.3.2 - Bugfix: Text report by command-line did not work since V3.3.0 V3.3.1 - Bugfix: Device arrivals not detected when registry contains wrong device path for a USB hub V3.3.0 - New: Can write and read a report in XML format V3.2.4 - Bugfix: Crash when showing open handle after failed safe removal of a device with a COM port - Bugfix: guidExtensionCode in 'Video Control Extension Unit Descriptor' was not shown - Bugfix: MessageBox was shown after writing a report by command-line - New: Name of guidExtensionCode (e.g. 'YUY2') is extracted from the first four bytes of the GUID V3.2.3 - Bugfix: Some strings for Smart Card Functional Descriptor where shown as question marks - Bugfix: UVC frame intervals where shown without fraction of milliseconds for continuous frame type V3.2.2 - Bugfix: UVC frame intervals where shown without fraction of milliseconds for discrete frame type V3.2.1 - Bugfix: Under XP the UsbTreeView process did not end after using "Safely Remove" - New: Highlight color of selected item darker V3.2.0 - New: TreeView highlighting as known from the SysInternals ProcessExplorer - New: On failed 'safe removal' it shows open handles found for the device ID Windows returns as VetoName - New: Shows global registry USB flags under HKLM\SYSTEM\CurrentControlSet\Control\UsbFlags and HKLM\SYSTEM\CurrentControlSet\Services\usbhub\hubg V3.1.8 - New: Shows for each USB device registry USB flags under HKLM\SYSTEM\CurrentControlSet\Control\UsbFlags V3.1.7 - New: Detects arrival of USB devices even its driver fails to start, e.g. if no driver is installed yet - New: Detects childs of USB devices even they don't generate device notifications nor they are enumerated by SetupDiGetClassDevs (seen on Arduino Micro) V3.1.6 - Bugfix: Device Qualifier Descriptor was requested even the device is running at SuperSpeed V3.1.5 - New: Option to show the port chain instead the port number in the tree - Bugfix: Some hexdumps where missing - Bugfix: Device Qualifier Descriptor was requested for USB 1.x devices V3.1.4 - New: Copy tree to clipboard function - New: Text copied to clipboard as HTML fragment enclosed in
tags to get a monospaced font offhand
- New: SmartCard Reader Feature Descriptor decoded
- Bugfix: Volume of CDROM drives not recognized on arrival
V3.1.3 - Bugfix: Wrong value shown for Clock Selector in Audio Control Clock Selector Unit Descriptor 2.0
- New: Full enumeration when missing USB device notifcation is detected (workaround for SILEX USB Device Servers)
V3.1.2 - Bugfix: Occasional crash on safe removal
- Bugfix: Since V3.0.6 no device information for UHCI controllers under Windows 2000
- Bugfix: wPacketSize decoded wrong if SuperSpeed device reported a Device Bus Speed of 0x02
V3.1.1 - New: Can show multiple Configuration and Other-Speed-Configuration Descriptors
- New: TreeView sub-menu to copy some id strings to clipboard
- New: Basic check for DLL hijacking
V3.1.0 - Bugfix: Removal of storage volumes not handled correctly
- New: Project is UNICODE now, so non-ASCII string descriptors are shown correctly even the Windows ANSI codepage cannot
- New: Improved robustness when decoding invalid descriptors
- New: Option "Always On Top"
V3.0.8 - Bugfix: No more font change in the text pane when hitting some special charaters
V3.0.7 - New: Improved detection of arrival/removal of child devices
- New: Devices in low power state but no problem code get a 'D1', 'D2' etc icon instead of an exclamation mark
- New: Workaround for a strange phenomenon: On some Windows device notifications come with wide strings
even RegisterDeviceNotificationA was used; This is dealt with now.
V3.0.6 - New: Support for virtual USB Controllers where Hostcontroller and Root-Hub are one and the same device
V3.0.5 - New: New port property PortConnectorIsTypeC (Win10 only)
V3.0.4 - New: Device Manager problem numbers shown in the treeview icons
V3.0.3 - New: Search hits get highlighted in the text pane (which is a Richedit control now)
V3.0.2 - Bugfix: Dropdown lists not refreshed on device arrival and removal
V3.0.1 - Bugfix: Crash on full refresh
V3.0.0 - New: No more enumeration of all devices on arrival and removal of a USB device
- New: Search function (not full text, only things like device ID, drive letter, volume name etc)
- New: Toolbar controls shrink if required
- New: Some new Keyboard shortcuts (Alt+D to open the drives list, Alt+O the Others list, Alt+S to focus the
search edit, Alt+Left/Right to cycle thru the search hits
- New: options not to expand empty hubs or hub with only empty hubs attached
- New: options to jump to arrived and removed devices
- New: option to expand tree items to make selected arrived and removed devices visible
- New: Uses Windows visual theme with option to turn it off
V2.6.1 - Bugfix: Limit of 32 root hubs removed
- Bugfix: Other Speed Configuration' descriptors were not read
- New: Shows progress information in the status bar, when stuck giving a hint where
- New: Getting Microsoft String Descritor 0xEE can be deactivated because it causes some devices to freeze.
If in the Registry under HKLM\SYSTEM\CurrentControlSet\Control\UsbFlags\VVVVPPPPRRRR there is a
osvc value != 0 then UsbTreeView reads it anyway because Windows already read it successfully.
VVVVPPPPRRRR is a 12 digit hex value containing idVendor, idProduct and bcdDevice from the USB Device Descriptor
V2.6.0 - Bugfix: bRefresh field in endpoint descriptors of Audio 1.0 devices was not shown
V2.5.9 - Bugfix: Wrong warning about characters below 0x20 in some string descriptors
- Bugfix: Delay on opening a Windows Device Manager device properties dialog removed
- New: Decoding of Microsoft string descriptor 0xEE
V2.5.8 - Bugfix: Decoding of SuperSpeedPlus descriptor and some others fixed
V2.5.7 - New: Display SuperSpeedPlus in Connection Information V2 under Windows 10
V2.5.6 - Bugfix: String descriptors containing invalid characters where not shown at all
- Bugfix: Crash when more than 64 ports per hub
- New: On Windows 8 and 10 the Microsoft USB stack returns for USB devices running at SuperSpeed a
Device Bus Speed of 0x02 (High-Speed). So far UsbTreeView faked it to 0x03 (SuperSpeed) as Microsoft's USBview does.
Now the truely returned value is shown with a hint if it is not the true speed.
V2.5.5 - Bugfix: Occasional crash after device safe removal or reactivation
V2.5.4 - Bugfix: Crash on H.264 WebCams
- Bugfix: Crash when more than 127 USB devices
- New: Reading of the Microsoft specific string descriptor 0xEE
V2.5.3 - New/Bugfix: USB Attached SCSI drives (UASPStor) shown with drive letter in the tree and in the drives combobox
V2.5.2 - New: Option to show the drive numbers in the tree, e.g. Disk3, CdRom1 etc.
V2.5.1 - Bugfix: Since V2.5.0 possible crash when getting a string descriptor
V2.5.0 - New: Audio 2.0 descriptors
New: Can write a text report to a file or copy it to the Windows Clipboard
About the icons
Computer : Computer
blue USB : empty port, with Letters L, F, H, S for Low, Full, High and SuperSpeed
blue+red USB : port with a device connected (no error, no problem), with Letters L, F, H, S for Low, Full, High and SuperSpeed
Controller Card: USB host controller
Root : USB root hub
Hub white : Standard Full-Speed hub
Hub green : Standard High-Speed hub
Hub blue : Standard SuperSpeed hub
Green Number : Problem code from Windows device manager (safely removed: 21, 24, 47)
Yellow Number : Problem code from Windows device manager (all others)
D1..D4 : Power state from Windows device manager if not D0 and no problem code
Red E : Unexpected error
Red OC : Over-current error
Exclamation : Device Connection Status is neither NoDeviceConnected nor DeviceConnected or
error when reading the USB configuration descriptor or
the 'Current Config Value' is 0
Keyboard shortcuts:
F5 re-enumeration of all information
Ctrl+S save XML report
Ctrl+O open a XML report
Alt+D open the drives list
Alt+O open the "Others" list
Alt+S focus the search edit
Alt+Left/Right cycle thru the search hits
About maximum port speeds
Requesting a USB ports maximum speed is supported by Windows 8 and higher. On older
system there is no way to determine which ports of an xHCI root hub supports SuperSpeed,
therefore the icons have no letter indicating the speed. Ports of High-Speed hubs are
assumed to handle High-Speed, ports of SuperSpeed standard hubs to handle SuperSpeed.
About SuperSpeedPlus maximum Port Speed
So far the Win32 USB API does not support requesting a USB port's max supported
SuperSpeedPlus speed or a USB version higher than 3.0, see enum USB_PROTOCOLS in
usbioctl.h:
https://docs.microsoft.com/en-us/windows-hardware/drivers/ddi/usbioctl/ns-usbioctl-_usb_protocols
Workaround:
If a device is running at SuperSpeedPlus then the UsbTreeView remembers that the
used port obviously supports that speed.
About SuperSpeedPlus > 10 GBits/s
The Win32 USB API does not provide any more information than "SuperSpeedPlus capable or higher"
and "operating at SuperSpeedPlus or higher", so UsbTreeView cannot show more than that.
The only data struct which seem to support to report more than 10 GBits/s is the
"SuperSpeedPlus USB Device Capability Descriptor" (see USB 3.2 spec 9.6.2.5).
But so far this descriptor looks identical for all ever seen devices, including those
which are running at 20 GBits/s speed: Length of 20 Bytes, reporting exactly one RX and TX
sub-link at a speed of 10 GBits/s. No idea if this is a limitation of the Windows USB API
or if this really comes from the devices. But even this would report as expeced, it still
is the device's capability only, not the actual connection speed.
About the "Port Chain"
Originally I introduced the port chain as "UsbPortName" criteria in USBDLM
when users asked for a way to have drive letters depending on the USB port.
The only uncertain part is the first digit: A SetupDi enumeration for
GUID_DEVINTERFACE_USB_HOST_CONTROLLER is performed and the first digit is
just the index in this enumeration starting with 1. So when a USB host
controller is added or removed this digit might change!
The other digits are safe, they are just the port numbers from the USB API
as shown in the treeview of UsbTreeView.
About the "Device Qualifier Descriptor"
USB 2.0 High-Speed devices must support High- and Full-Speed. In the "Device Qualifier Descriptor"
they report their capabilities for the other speed which for instance is different
for web-cams which support lower resolutions and frame-rates at Full-Speed.
The USB 2.0 make contradictorily claims about the USB version:
9.2.6.6:
"Devices that are high-speed capable must set the version number in the bcdUSB field of
their descriptors to 0200H. This indicates that such devices support the other_speed
requests defined by USB 2.0."
9.6.1
Full speed and low speed only devices designed to this specification should also use version
number 2.0 (0200H). If the device is full-speed or low-speed only this version number indicates
that it will respond correctly to a request for the device_qualifier descriptor (i.e., it will
respond with a request error).
So, for USB 2.0 devices UsbTreeView requests the "Device Qualifier Descriptor".
For non-High-Speed devices this leads to ERROR_GEN_FAILURE.
If this causes trouble it can be skipped for Low-Speed devices by setting
SkipDeviceQualiDescForLowSpeedDevs=1
in the UsbTreeView.ini (while it is not running).
About Unknown Descriptors
There are two reasons why decriptors cannot be decoded and therefore
shown as "Unknown":
- decoding is not implemented
- the device's InterfaceClass is 0xFF (vendor specific), so class specific
descriptors cannot be decoded since their class is unknown
So, if you have an unknown descriptor and the interface class is not 0xFF
then please let me know, maybe I find the right specification document
and can add the decoding for it.
About HID descriptors
HID descriptors usually cannot be read. Probably this is because they
must be requested from the interface rather than the device but the
IOCTL_USB_GET_DESCRIPTOR_FROM_NODE_CONNECTION call doesn't offer the
choice. The parameters are ignored and filled by the USB stack:
MSDN says: "the USB stack ignores the value of bmRequest and inserts
a value of 0x80 which indicates standard USB device request".
https://msdn.microsoft.com/en-us/library/windows/hardware/ff539272%28v=vs.85%29.aspx
For most devices the result is an ERROR_GEN_FAILURE or ERROR_INVALID_PARAMETER.
But some devices return the HID descriptor anyway.
About ERROR_INVALID_FUNCTION
3rd party USB controller and hub drivers usually do no support all the
requests the Microsoft standard drivers do. They fail with ERROR_INVALID_FUNCTION.
For instance that's the case for several USB hub information request, here you
get five ERROR_INVALID_FUNCTION in a row. That's not a problem, just some missing
information.
About Endpoints / USB Controller Resources
Each USB device uses a bidirectional control endpoint 0 to which the
"Default Control Pipe" is attached thru which the device is controlled.
Further endpoints are unidirectional and usually at least one is used.
For instance a simple mouse has one IN data endpoint of type "interupt"
thru which the mouse reports movement and click events.
UsbTreeView counts 1 endpoint for the Default Control Pipe if the configuration
descriptor can be read plus the number of open pipes to data endpoints which
are reported by Windows in the "Connection Information".
Intel Series 8 xHCI (USB3) controllers are known for having a limitited number of
64 endpoints. The Windows error message is "Not Enough USB Controller Resources"
when attaching a new device.
To save used endpoints it does not help to disable a USB devices's
child device. Only deactivating (or safely removing) the USB device itself
does the trick (even the USB API still reports the endpoints as open when
the device is safely removed - UsbTreeView counts 1 endpoint then).
If a USB2 host controller is availlable then moving non-SuperSpeed devices
there helps safing endpoints on the xHCI controller. Last resort is disabling
xHCI in the BIOS setup which doubles the number of allocatable endpoints
according to Intel's guy Adolfo her:
https://community.intel.com/t5/Embedded-Intel-Core-Processors/Hardware-limitations-on-USB-endpoints-XHCI/td-p/264556
UsbTreeView can show the used andpoionts in the tree-view: Options -> Endpoints in Tree.
About "Safe Removal" and "Restart"
On Safe Removal UsbTreeView first calls the configuration management call
CM_Query_And_Remove_SubTree. On success the device has the problem code
21 which is CM_PROB_WILL_BE_REMOVED. A code 21 device can be reactivated
by performing a DIF_PROPERTYCHANGE class installer call. This is what
UsbTreeView does if you select "Restart device".
But CM_Query_And_Remove_SubTree needs admin privileges, otherwise it fails
with CR_ACCESS_DENIED. In this case CM_Request_Device_Eject is called
which works without admin privileges but leads to problem code 47 which
is CM_PROB_HELD_FOR_EJECT. Such a device cannot be reactivated alone by
means of the device manager.
A reactivation is possible by restarting the port or the whole hub it is
attached to. But the latter of course restarts all devices attached to
the hub. Under XP and again since Windows 8 a USB port reset restarts the
device too.
In all cases UsbTreeView just performs the system call and shows a
message-box if Windows returns an error. But Windows does not always
return an error, even there was one, so sometimes nothing happens at all.
About "Restart Port"
This calls IOCTL_USB_HUB_CYCLE_PORT which simulates a disconnect and
reconnect of the attached device.
It is available under XP but usually only for hubs which run with the
Microsoft standard driver. 3rd party drivers usually return
ERROR_UNKNOWN_FUNCTION.
Under Vista and Windows 7 it is no more supported by the Windows standard
drivers, it always fails with ERROR_NOT_SUPPORTED.
Since Windows 8 it works again but in contrast to XP admin privileges
are required. Without admin privileges it fails as under Vista and Win7
with ERROR_NOT_SUPPORTED or since Win10 version 1903 with ERROR_GEN_FAILURE,
which both are quite missleading here since it's a privilege issue.
About the Debug-Port
In Microsoft's USBView sample there is a list of USB host controllers
and their debug port. I've put the table into UsbTreeView, it shows
then in the properties of the host controller a line like so:
DebugPort (from List): 1
Windows 8 has extended USB information, it reports for each port if it
is debug capable and this works indeed (seen on a i945G Chipset with ICH7).
USB Mouses
If a USB mouse is moved while the tool requests its USB properties there
is usually an error because the mouse just has more important things to
do than answering descriptor requests. UsbTreeView tries then for some
seconds to get this information.
You might see the yellow question mark at the mouse's tree node for a
moment which disappears as soon as you stop moving the mouse.
This retry mechanism is done for all type of devices but usually its a
mouse where it helps.
Information shown in the tree-view
UsbTreeView is optimized for speed, therefore USB string descriptors are
not gathered before a device is selected in the tree-view. So, information
which come from USB string descriptors cannot be shown in the tree-view, it
all comes from the Windows device manager.
This is also why creating a full report takes a moment.
Always On Top
By default the state of the "Always On Top" option is persistent (written
to and read from the INI). If you find this annoying then add the line
TopmostPersistent=0
to section [Settings] in the UsbTreeView.ini, then "Always On Top" is
no more written to the INI, so you can set Topmost=0 or Topmost=1 and
keep this as startup default.
Hints
A similar tool for drives is "USB Drive Info":
https://www.uwe-sieber.de/usbdriveinfo_e.html
A similar tool for serial COM ports is "COM Port Info":
https://www.uwe-sieber.de/comportinfo_e.html
A command-line tool to reset a USB port is "RestartUsbPort":
https://www.uwe-sieber.de/misc_tools_e.html#restartusbport
UsbTreeView is Freeware.
Allowed:
- usage in any environment, including commercial
- include in software products, including commercial
- include on CD/DVD of computer magazines
- distribution by means of packet managers
Not allowed:
- modify any of the files
- offer for download by means of a "downloader" software
Uwe Sieber, mail@uwe-sieber.de
Nov 2022