###################################################
#File version="1.0.0.0" Copyright="Copyright (c) 2005-2007 Texas Instruments"
###################################################
#
#
#
# The client reads this property to create the reference to the
# "ChannelServer" object in the server.
#
ChannelServer.Proxy=ChannelServer:tcp -p 6501:udp -p 6501

#
# The server creates one single object adapter with the name
# "ChannelServer". The following line sets the endpoints for this
# adapter.
#
ChannelServer.Endpoints=tcp -p 6501:udp -p 6501


#
# The Target Adapter channel ctools-> trace server
#
TargetAdapterFactory.Proxy=TargetAdapterFactory:tcp -p 6502:udp -p 6502

TargetAdapterFactory.Endpoints=tcp -p 6502:udp -p 6502


#
# The Target Event Broker trace server-> ctools/ICETargetAdapter
#
TargetEventBroker.Proxy=TargetEventBroker:tcp -p 6503:udp -p 6503

TargetEventBroker.Endpoints=tcp -p 6503:udp -p 6503

#
# Warn about connection exceptions
#
Ice.Warn.Connections=0

#
#Disable Active Connection Management
#
Ice.ConnectionIdleTime=0

#
# Network Tracing
#
# 0 = no network tracing
# 1 = trace connection establishment and closure
# 2 = like 1, but more detailed
# 3 = like 2, but also trace data transfer
#
Ice.Trace.Network=0

#
# Protocol Tracing
#
# 0 = no protocol tracing
# 1 = trace protocol messages
#
Ice.Trace.Protocol=0

#
# Security Tracing
#
# 0 = no security tracing
# 1 = trace warning messages
# 2 = config file parsing warnings
#
IceSSL.Trace.Security=0

#
# SSL Configuration File
#
# An XML based file that specifies the certificates, keys, SSL version
# and other pertinent information for creating an SSL connection.
#
#Ice.Plugin.IceSSL=IceSSL:create
#IceSSL.Client.CertPath=../../../certs
#IceSSL.Client.Config=sslconfig.xml
#IceSSL.Server.CertPath=../../../certs
#IceSSL.Server.Config=sslconfig.xml

#
# Glacier settings
#
Glacier.Router.Endpoints=default -p 6504
Glacier.Router.Client.Endpoints=tcp:udp:ssl
Glacier.Router.Trace.Client=0
Glacier.Router.Trace.RoutingTable=1

#
# IcePack registry settings (assumes that a db directory exists in the 
# current working directory).
# 
IcePack.Registry.Client.Endpoints=default -p 6505
IcePack.Registry.Server.Endpoints=default
IcePack.Registry.Admin.Endpoints=default
IcePack.Registry.Data=db
IcePack.Registry.DynamicRegistration=1


#
# This property is used to configure the endpoints of the clock
# subscriber adapter.
#
ChannelListener.Subscriber.Endpoints=tcp

#
# This property is used by the clients to connect to IceStorm.
#
IceStorm.TopicManager.Proxy=IceStorm/TopicManager:default -p 6506

#
# This property defines the endpoints on which the IceStorm
# TopicManager listens.
#
IceStorm.TopicManager.Endpoints=default -p 6506

#
# This property defines the endpoints on which the topic
# publisher objects listen.
#
IceStorm.Publish.Endpoints=default

#
# TopicManager Tracing
#
# 0 = no tracing
# 1 = trace topic creation, subscription, unsubscription
# 2 = like 1, but with more detailed subscription information
#
IceStorm.Trace.TopicManager=0

#
# Topic Tracing
#
# 0 = no tracing
# 1 = trace unsubscription diagnostics
#
IceStorm.Trace.Topic=0

#
# Subscriber Tracing
#
# 0 = no tracing
# 1 = subscriber diagnostics (subscription, unsubscription, event
#     propagation failures)
#
IceStorm.Trace.Subscriber=0

#
# Flush Tracing (for batch mode transfer flushing)
#
# 0 = no tracing
# 1 = trace activity of flusher thread
#
IceStorm.Trace.Flush=0

#
# Amount of time in milliseconds between flushes for batch mode
# transfer. The minimum allowable value is 100ms.
#
IceStorm.Flush.Timeout = 0