Description Resource Path Location Type
gmake: Target 'all' not remade because of errors. REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [tm4c1290ncpdt_startup_ccs.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/usb_serial_structs.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/usb_dev_serial.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/Sensor_Interface.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/Printhead_Interface.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/Printhead_Control.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/Motor_Common.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/Memory_Utils.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/main.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/I2CInterface.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/cpu_usage.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/arcsend.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/ARCNET_MessageProcessor.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/ARCmain.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [drivers/pinout.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [drivers/exosite_hal_lwip.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [drivers/eth_client_lwip.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
#80 expected a type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#760 variable "page" is not a type name arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#68 expected a "}" I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1553 C/C++ Problem
#68 expected a "}" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 52 C/C++ Problem
#66 expected a ";" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 59 C/C++ Problem
#41 expected an identifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 102 C/C++ Problem
#41 expected an identifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#20 identifier "xPortSysTickHandler" is undefined tm4c1290ncpdt_startup_ccs.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT line 112 C/C++ Problem
#20 identifier "X_MID_TROuint8_tLE" is undefined ARCmain.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 639 C/C++ Problem
#20 identifier "vPortSVCHandler" is undefined tm4c1290ncpdt_startup_ccs.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT line 108 C/C++ Problem
#20 identifier "UsageFault_Handler" is undefined tm4c1290ncpdt_startup_ccs.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT line 103 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 141 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 143 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 144 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 146 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 147 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 149 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 160 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 161 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 163 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 164 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 165 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 166 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 167 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 168 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 169 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 170 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 171 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 172 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 173 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 174 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 175 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 176 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 177 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 178 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 179 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 180 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 181 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 182 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 183 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 184 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 185 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 186 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 187 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 188 C/C++ Problem
#20 identifier "uint8_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 190 C/C++ Problem
#20 identifier "uint8_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 526 C/C++ Problem
#20 identifier "uint8_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 528 C/C++ Problem
#20 identifier "uint32_t" is undefined debug.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 49 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 141 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 142 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 143 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 144 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 145 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 146 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 147 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 148 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 149 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 150 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 151 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 152 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 153 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 154 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 155 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 156 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 157 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 159 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 160 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 161 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 162 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 163 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 164 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 165 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 166 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 167 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 168 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 169 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 170 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 171 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 172 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 173 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 174 C/C++ Problem
#148 declaration is incompatible with "uint8_t Arc_Txd_Mode" (declared at line 30) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 114 C/C++ Problem
#148 declaration is incompatible with "uint8_t snd_seq_no" (declared at line 29) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 59 C/C++ Problem
#148 declaration is incompatible with "void ARCNET_DisableInterupt(void)" (declared at line 26) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 110 C/C++ Problem
#148 declaration is incompatible with "void ARCNET_EnableInterupt(void)" (declared at line 25) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 118 C/C++ Problem
#148 declaration is incompatible with "void c19_clear_flags(void)" (declared at line 22) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#148 declaration is incompatible with "void c19_interrupts_enableTA(void)" (declared at line 24) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 115 C/C++ Problem
#148 declaration is incompatible with "void c19_set_tx_page(uint8_t, uint8_t)" (declared at line 23) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#148 declaration is incompatible with "void c19_write_data(uint8_t, uint16_t, uint16_t, uint8_t, uint8_t *)" (declared at line 21) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 102 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 121 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 71 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 69 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 60 C/C++ Problem
#18 expected a ")" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#1965 cannot open source file "reent.h" Memory_Utils.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 4 C/C++ Problem
#1965 cannot open source file "REPMTFA_Source/globals.h" pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 36 C/C++ Problem
#1965 cannot open source file "utils/cpu_usage.h" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 12 C/C++ Problem
#1965 cannot open source file "utils/lwiplib.h" eth_client_lwip.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 34 C/C++ Problem
#1965 cannot open source file "utils/ringbuf.h" exosite_hal_lwip.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 38 C/C++ Problem
#20 identifier "bool" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 559 C/C++ Problem
#20 identifier "bool" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 511 C/C++ Problem
#20 identifier "bool" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 255 C/C++ Problem
#20 identifier "bool" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 253 C/C++ Problem
#20 identifier "bool" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 249 C/C++ Problem
#20 identifier "bool" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 247 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 645 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 628 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 627 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 626 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 602 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 596 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 586 C/C++ Problem
#20 identifier "bool" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 585 C/C++ Problem
#20 identifier "bool" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 153 C/C++ Problem
#20 identifier "g_bSecond_Ticket_Flag" is undefined I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 313 C/C++ Problem
#20 identifier "g_ui32SysClock" is undefined I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 407 C/C++ Problem
#20 identifier "GPIO_PORTG_DATA_R" is undefined Printhead_Control.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 268 C/C++ Problem
#20 identifier "int32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 529 C/C++ Problem
#20 identifier "int32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 527 C/C++ Problem
#20 identifier "int32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 525 C/C++ Problem
#20 identifier "int32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 160 C/C++ Problem
#20 identifier "MemManage_Handler" is undefined tm4c1290ncpdt_startup_ccs.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT line 101 C/C++ Problem
#20 identifier "SENSOR_ADC_Sample_ISR" is undefined tm4c1290ncpdt_startup_ccs.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT line 127 C/C++ Problem
#20 identifier "TIMER_CFG_16_BIT_PAIR" is undefined Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1131 C/C++ Problem
#20 identifier "TIMER_CFG_16_BIT_PAIR" is undefined Motor_Common.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 147 C/C++ Problem
#20 identifier "TIMER_CFG_16_BIT_PAIR" is undefined Motor_Common.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 128 C/C++ Problem
#20 identifier "TIMER_CFG_32_BIT_OS" is undefined Sensor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 405 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 584 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 583 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 582 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 191 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 190 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 189 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 188 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 187 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 186 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 185 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 184 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 183 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 182 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 181 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 180 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 606 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 607 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 608 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 612 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 613 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 614 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 615 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 616 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 617 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 618 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 619 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 620 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 621 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 622 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 623 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 624 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 625 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 605 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 604 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 603 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 630 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 631 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 634 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 635 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 636 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 637 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 638 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 639 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 640 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 641 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 642 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 643 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 644 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 602 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 645 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 248 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 601 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 250 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 251 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 252 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 600 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 254 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 599 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 256 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 257 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 258 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 259 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 260 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 261 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 262 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 263 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 243 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 244 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 245 C/C++ Problem
#20 identifier "uint32_t" is undefined timer.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 246 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 595 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 548 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 549 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 550 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 551 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 552 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 553 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 554 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 555 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 556 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 557 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 558 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 594 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 559 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 560 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 500 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 501 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 502 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 503 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 504 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 505 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 506 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 507 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 508 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 509 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 510 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 593 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 512 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 513 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 514 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 515 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 516 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 517 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 518 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 519 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 520 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 521 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 522 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 523 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 524 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 592 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 525 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 179 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 526 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 591 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 527 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 178 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 528 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 590 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 529 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 530 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 531 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 532 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 533 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 534 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 535 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 536 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 537 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 538 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 539 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 540 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 541 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 542 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 543 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 544 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 545 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 546 C/C++ Problem
#20 identifier "uint32_t" is undefined usb.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 547 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 589 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 588 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 587 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 177 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 586 C/C++ Problem
#20 identifier "uint32_t" is undefined sysctl.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 585 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 176 C/C++ Problem
#20 identifier "uint32_t" is undefined gpio.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/driverlib line 175 C/C++ Problem
#225-D function "SetPrintAndMoveCommandLockStatus" declared implicitly I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 311 C/C++ Problem
#225-D function "ROM_SysCtlPeripheralEnable" declared implicitly buttons.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 166 C/C++ Problem
#225-D function "ROM_GPIOPinRead" declared implicitly buttons.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 96 C/C++ Problem
#225-D function "ROM_GPIOPinRead" declared implicitly buttons.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 179 C/C++ Problem
#225-D function "ROM_GPIOIntRegister" declared implicitly I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 197 C/C++ Problem
#225-D function "ROM_GPIODirModeSet" declared implicitly buttons.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 171 C/C++ Problem
#225-D function "REPM_ExecuteMovement" declared implicitly I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 315 C/C++ Problem
#225-D function "REPM_ExecuteMovement" declared implicitly I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 321 C/C++ Problem
#225-D function "GPIOPortIntRegister" declared implicitly ARCNET_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 87 C/C++ Problem
#225-D function "GPIOPortIntRegister" declared implicitly FeedDetect_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 95 C/C++ Problem
#93-D identifier-list parameters may only be used in a function definition arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 102 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 59 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 102 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 110 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 114 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 115 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 118 C/C++ Problem
#552-D variable "m_uiTicks" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#552-D variable "m_uiNumCharactersToPrint" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 81 C/C++ Problem
#552-D variable "m_uiCont4TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 93 C/C++ Problem
#552-D variable "m_uiCont3TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 94 C/C++ Problem
#552-D variable "m_uiCont2TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 95 C/C++ Problem
#552-D variable "m_uiCont1TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 96 C/C++ Problem
#552-D variable "m_ucSensorInputsToUseForMoving" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 18 C/C++ Problem
#552-D variable "m_ucSensorInputMatters" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 19 C/C++ Problem
#552-D variable "m_ucSensor2ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 28 C/C++ Problem
#552-D variable "m_ucSensor1ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 27 C/C++ Problem
#552-D variable "m_ucSensor0ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 26 C/C++ Problem
#552-D variable "m_ucChip1PortInputData" was set but never used I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#552-D variable "dummyVal" was set but never used arccom19.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 87 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 190 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 288 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 387 C/C++ Problem
#48-D incompatible redefinition of macro "INT_WATCHDOG" (declared at line 66 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 462 C/C++ Problem
#48-D incompatible redefinition of macro "INT_USB0" (declared at line 89 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 461 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UDMAERR" (declared at line 92 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 460 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UDMA" (declared at line 91 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 459 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART7" (declared at line 107 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 458 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART6" (declared at line 106 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 457 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART5" (declared at line 105 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 456 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART4" (declared at line 104 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 455 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART3" (declared at line 103 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 454 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART2" (declared at line 81 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 453 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART1" (declared at line 54 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 452 C/C++ Problem
#48-D incompatible redefinition of macro "INT_UART0" (declared at line 53 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 451 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER7B" (declared at line 140 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 450 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER7A" (declared at line 139 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 449 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER6B" (declared at line 138 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 448 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER6A" (declared at line 137 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 447 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER5B" (declared at line 113 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 446 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER5A" (declared at line 112 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 445 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER4B" (declared at line 111 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 444 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER4A" (declared at line 110 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 443 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER3B" (declared at line 84 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 442 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER3A" (declared at line 83 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 441 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER2B" (declared at line 72 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 440 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER2A" (declared at line 71 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 439 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER1B" (declared at line 70 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 438 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER1A" (declared at line 69 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 437 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER0B" (declared at line 68 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 436 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TIMER0A" (declared at line 67 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 435 C/C++ Problem
#48-D incompatible redefinition of macro "INT_TAMPER0" (declared at line 120 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 434 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SYSEXC" (declared at line 114 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 433 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SYSCTL" (declared at line 76 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 432 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SSI3" (declared at line 102 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 431 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SSI2" (declared at line 101 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 430 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SSI1" (declared at line 82 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 429 C/C++ Problem
#48-D incompatible redefinition of macro "INT_SSI0" (declared at line 55 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 428 C/C++ Problem
#48-D incompatible redefinition of macro "INT_QEI0" (declared at line 61 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 425 C/C++ Problem
#48-D incompatible redefinition of macro "INT_PWM0_FAULT" (declared at line 57 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 419 C/C++ Problem
#48-D incompatible redefinition of macro "INT_PWM0_3" (declared at line 90 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 418 C/C++ Problem
#48-D incompatible redefinition of macro "INT_PWM0_2" (declared at line 60 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 417 C/C++ Problem
#48-D incompatible redefinition of macro "INT_PWM0_1" (declared at line 59 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 416 C/C++ Problem
#48-D incompatible redefinition of macro "INT_PWM0_0" (declared at line 58 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 415 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C9" (declared at line 144 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 412 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C8" (declared at line 143 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 411 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C7" (declared at line 142 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 410 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C6" (declared at line 141 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 409 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C5" (declared at line 117 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 408 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C4" (declared at line 116 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 407 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C3" (declared at line 109 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 406 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C2" (declared at line 108 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 405 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C1" (declared at line 85 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 404 C/C++ Problem
#48-D incompatible redefinition of macro "INT_I2C0" (declared at line 56 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 403 C/C++ Problem
#48-D incompatible redefinition of macro "INT_HIBERNATE" (declared at line 88 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 402 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ7" (declared at line 136 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 398 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ6" (declared at line 135 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 397 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ5" (declared at line 134 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 396 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ4" (declared at line 133 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 395 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ3" (declared at line 132 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 394 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ2" (declared at line 131 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 393 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ1" (declared at line 130 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 392 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOQ0" (declared at line 129 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 391 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP7" (declared at line 128 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 390 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP6" (declared at line 127 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 389 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP5" (declared at line 126 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 388 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP4" (declared at line 125 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 387 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP3" (declared at line 124 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 386 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP2" (declared at line 123 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 385 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP1" (declared at line 122 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 384 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOP0" (declared at line 121 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 383 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPION" (declared at line 119 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 382 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOM" (declared at line 118 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 381 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOL" (declared at line 100 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 380 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOK" (declared at line 99 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 379 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOJ" (declared at line 98 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 378 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOH" (declared at line 80 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 377 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOG" (declared at line 79 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 376 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOF" (declared at line 78 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 375 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOE" (declared at line 52 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 374 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOD" (declared at line 51 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 373 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOC" (declared at line 50 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 372 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOB" (declared at line 49 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 371 C/C++ Problem
#48-D incompatible redefinition of macro "INT_GPIOA" (declared at line 48 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 370 C/C++ Problem
#48-D incompatible redefinition of macro "INT_FLASH" (declared at line 77 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 369 C/C++ Problem
#48-D incompatible redefinition of macro "INT_EPI0" (declared at line 97 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 368 C/C++ Problem
#48-D incompatible redefinition of macro "INT_COMP2" (declared at line 75 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 365 C/C++ Problem
#48-D incompatible redefinition of macro "INT_COMP1" (declared at line 74 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 364 C/C++ Problem
#48-D incompatible redefinition of macro "INT_COMP0" (declared at line 73 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 363 C/C++ Problem
#48-D incompatible redefinition of macro "INT_CAN1" (declared at line 87 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 362 C/C++ Problem
#48-D incompatible redefinition of macro "INT_CAN0" (declared at line 86 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 361 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC1SS3" (declared at line 96 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 359 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC1SS2" (declared at line 95 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 358 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC1SS1" (declared at line 94 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 357 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC1SS0" (declared at line 93 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 356 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC0SS3" (declared at line 65 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 355 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC0SS2" (declared at line 64 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 354 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC0SS1" (declared at line 63 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 353 C/C++ Problem
#48-D incompatible redefinition of macro "INT_ADC0SS0" (declared at line 62 of "C:/TFS/RD_10_SOURCE/REPM/05_REPM_FIRMWARE_SOURCE_CODE/TI_Code_Composer_BulkValidatorFirmware-TM4C1290NCPDT/REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc/tm4c1290ncpdt.h") hw_ints.h /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/inc line 352 C/C++ Problem
#179-D variable "m_ucFirmwareVer" was declared but never referenced LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 16 C/C++ Problem
#179-D variable "m_bReadRequest" was declared but never referenced I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 85 C/C++ Problem
#179-D variable "iSendPortCountDevice2" was declared but never referenced I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 98 C/C++ Problem
#179-D variable "iSendPortCountDevice1" was declared but never referenced I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 97 C/C++ Problem
#179-D variable "dummy" was declared but never referenced xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 244 C/C++ Problem
#179-D variable "dummy" was declared but never referenced xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 340 C/C++ Problem
#169-D argument of type "unsigned long *" is incompatible with parameter of type "uint32_t *" Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 244 C/C++ Problem
#169-D argument of type "unsigned long *" is incompatible with parameter of type "uint32_t *" Sensor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 313 C/C++ Problem
#129-D loop is not reachable ARCmain.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 215 C/C++ Problem
#12-D parsing restarts here after previous syntax error arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 68 C/C++ Problem
#12-D parsing restarts here after previous syntax error arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 99 C/C++ Problem