Example Summary
---------------
This application demonstrates how to use TCP.

Peripherals Exercised
---------------------
Board_LED0      Indicates that the board was initialized within main()
Board_EMAC      Connection to network

Resources & Jumper Settings
---------------------------
Please refer to the development board's specific "Settings and Resources"
section in the Getting Started Guide. For convenience, a short summary is also
shown below.

| Development board | Notes                                                  |
| ================= | ====================================================== |
| DK-TM4C129X       | N/A                                                    |
| EK-TM4C1294XL     |                                                        |
| EK-TM4C129EXL     |                                                        |
| ----------------- | ------------------------------------------------------ |
| TMDXDOCK28M36     | The MAC address in the TMDXDOCK28M36 needs to be       |
|                   | updated from {0xff, 0xff, 0xff, 0xff, 0xff, 0xff} to a |
|                   | valid and unique address.                              |
| ----------------- | ------------------------------------------------------ |
| TMDXDOCKH52C1     | The MAC address in the TMDXDOCKH52C1 needs to be       |
|                   | updated from {0xff, 0xff, 0xff, 0xff, 0xff, 0xff} to a |
|                   | valid and unique address. Also, update jumpers on      |
|                   | Connectivity Back 01-15: B-C position (Ethernet)       |
| ----------------- | ------------------------------------------------------ |

Example Usage
-------------
The device must be connected to a network with a DHCP server to run this
example successfully.

The example turns ON Board_LED0 and starts the network stack. When the stack
receives an IP address from the DHCP server, the IP address is written to the
console.

Run the tcpSendReceive Linux or Windows executable that is shipped with TI-RTOS.
The executable is found in:

  <tirtos_install_dir>\packages\examples\tools\tcpSendReceive

  Usage: ./tcpSendReceive <IP-addr> <port> <id> -l[length] -s[sleep in uS]

  <IP-addr> is the IP address
  <port>    is the TCP port being listened to (1000)
  <id>      is a unique id for the executable. Printed out when 1000 packets are
            transmitted. It allows the user to run multiple instances
            of tcpSendReceive.

  Optional:
    -l[length]      size of the packet in bytes. Default is 1024 bytes.
    -s[sleep in uS] usleep time to between sends. Default is 1000 uSecs.

  Example:
        tcpSendReceive 192.168.1.100 1000 1 -s100

Messages such as the following will begin to appear on the terminal window when
a TCP packet has been echoed back:

        Starting test with a 1000 uSec delay between transmits
        [id 1] count = 1000, time = 12
        [id 1] count = 2000, time = 24
        [id 1] count = 3000, time = 36

Application Design Details
--------------------------
This application uses two types of task:

tcpHandler  Creates a socket and accepts incoming connections.  When a
            connection is established a tcpWorker task is dynamically
            created to send or receive data.
tcpWorker   Echoes TCP packages back to the client.

  'tcpHandler' performs the following actions:
      Create a socket and bind it to a port (1000 for this example).

      Wait for incoming requests.

      Once a request is received, a new tcpWorker task is dynamically created to
      manage the communication (echo TCP packets).

      Waiting for new requests.

  'tcpWorker' performs the following actions:
      Allocate memory to serve as a TCP packet buffer.

      Receive data from socket client.

      Echo the TCP packet back to the client.

      When client closes the socket, close server socket, free TCP buffer memory
      and exit the task.

For GNU and IAR users, please read the following website for details about
semi-hosting:
    http://processors.wiki.ti.com/index.php/TI-RTOS_Examples_SemiHosting