U-Boot SPL 2015.01-00001-gb2412df (Jan 29 2015 - 15:01:06) U-Boot 2015.01-00001-gb2412df (Jan 29 2015 - 15:01:06), Build: jenkins-github_Bootloader-Builder-105 Watchdog enabled I2C: ready DRAM: 512 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Net: not set. Validating first E-fuse MAC cpsw Hit any key to stop autoboot: 0 gpio: pin 53 (gpio 53) value is 1 Card did not respond to voltage select! Card did not respond to voltage select! gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 switch to partitions #0, OK mmc1(part 0) is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... Checking for: /boot.scr ... Checking for: /boot/boot.scr ... Checking for: /boot/uEnv.txt ... gpio: pin 55 (gpio 55) value is 1 818 bytes read in 28 ms (28.3 KiB/s) Loaded environment from /boot/uEnv.txt Checking if uname_r is set in /boot/uEnv.txt... gpio: pin 56 (gpio 56) value is 1 Running uname_boot ... loading /boot/vmlinuz-3.8.13-bone70 ... 5617184 bytes read in 344 ms (15.6 MiB/s) loading /boot/dtbs/3.8.13-bone70/am335x-boneblack.dtb ... 26098 bytes read in 37 ms (688.5 KiB/s) loading /boot/initrd.img-3.8.13-bone70 ... 2867606 bytes read in 190 ms (14.4 MiB/s) debug: [console=ttyO0,115200n8 root=UUID=a5db3a2d-e6df-4c53-9bf9-4a110221662a ro rootfstype=ext4 rootwait fixrtc quiet init=/lib/systemd/systemd] ... debug: [bootz 0x82000000 0x88080000:2bc196 0x88000000] ... Kernel image @ 0x82000000 [ 0x000000 - 0x55b620 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Ramdisk to 8fd43000, end 8ffff196 ... OK Loading Device Tree to 8fd39000, end 8fd425f1 ... OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.372795] omap2_mbox_probe: platform not supported [ 0.527720] tps65217-bl tps65217-bl: no platform data provided [ 0.591116] bone-capemgr bone_capemgr.9: slot #0: No cape found [ 0.628224] bone-capemgr bone_capemgr.9: slot #1: No cape found [ 0.665332] bone-capemgr bone_capemgr.9: slot #2: No cape found [ 0.702441] bone-capemgr bone_capemgr.9: slot #3: No cape found [ 0.718134] bone-capemgr bone_capemgr.9: slot #6: BB-BONELT-HDMIN conflict P8.45 (#5:BB-BONELT-HDMI) [ 0.727680] bone-capemgr bone_capemgr.9: slot #6: Failed verification [ 0.734407] bone-capemgr bone_capemgr.9: loader: failed to load slot-6 BB-BONELT-HDMIN:00A0 (prio 2) [ 0.750909] omap_hsmmc mmc.5: of_parse_phandle_with_args of 'reset' failed [ 0.814045] pinctrl-single 44e10800.pinmux: pin 44e10854 already requested by 44e10800.pinmux; cannot claim for gpio-leds.8 [ 0.825734] pinctrl-single 44e10800.pinmux: pin-21 (gpio-leds.8) status -22 [ 0.833003] pinctrl-single 44e10800.pinmux: could not request pin 21 on device pinctrl-single Loading, please wait... systemd-fsck[202]: rootfs: clean, 84851/233856 files, 487942/933632 blocks Debian GNU/Linux 7 beaglebone ttyO0 BeagleBoard.org Debian Image 2015-03-01 Support/FAQ: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian default username:password is [debian:temppwd] The IP Address for usb0 is: 192.168.7.2 beaglebone login: