README
gpiointerrupt
Example Summary
Application that toggles an LED(s) using a GPIO pin interrupt.
Peripherals Exercised
Board_GPIO_LED0
- Indicates that the board was initialized withinmainThread()
also toggled byBoard_GPIO_BUTTON0
Board_GPIO_LED1
- Toggled byBoard_GPIO_BUTTON1
Board_GPIO_BUTTON0
- TogglesBoard_GPIO_LED0
Board_GPIO_BUTTON1
- TogglesBoard_GPIO_LED1
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
Run the example.
Board_GPIO_LED0
turns ON to indicate driver initialization is complete.Board_GPIO_LED0
is toggled by pushingBoard_GPIO_BUTTON0
.Board_GPIO_LED1
is toggled by pushingBoard_GPIO_BUTTON1
.
Application Design Details
The
gpioButtonFxn0/1
functions are configured in the Board.c file. These functions are called in the context of the GPIO interrupt.Not all boards have more than one button, so
Board_GPIO_LED1
may not be toggled.There is no button de-bounce logic in the example.
TI-RTOS:
- When building in Code Composer Studio, the configuration project will be imported along with the example. These projects can be found under \
\/kernel/tirtos/builds/\ /(release|debug)/(ccs|gcc). The configuration project is referenced by the example, so it will be built first. The “release” configuration has many debug features disabled. These features include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” configurations, please refer to the TI-RTOS Kernel User’s Guide.
FreeRTOS:
- Please view the
FreeRTOSConfig.h
header file for example configuration information.