Http Get
Table of Contents
Example Summary
This application demonstrates how to perform an HTTP GET request.
Example Usage
Configure the AP parameters in platform.c:
#define SSID_NAME
#define SECURITY_TYPE
#define SECURITY_KEY
Configure the HTTP parameters in httpget.c
#define HOSTNAME “http://www.example.com”
#define REQUEST_URI “/”
#define USER_AGENT “HTTPClient (ARM; TI-RTOS)”
Build the project, flash it by using the Uniflash tool for cc32xx,
Or equivalently, run debug session on the IDE of your choice.Open a serial port session (e.g. ‘HyperTerminal’,‘puTTY’, ‘Tera Term’ etc.) to the appropriate COM port -
listed as ‘User UART’. The COM port can be determined via Device Manager in Windows or vials /dev/tty*in Linux.
The connection should have the following connection settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example by pressing the reset button or by running debug session through your IDE.
The example then makes an HTTP GET call to “www.example.com” and prints the HTTP response status and the number of bytes of data received.
Application Design Details
- This application uses a task for HTTP communication:
httpTask - is waiting for ip to be acquired and then creates a connection to the HTTP server. When a connection is established, the application makes an HTTP GET method call using the request URI. The response status code, header fields and body from the HTTP server are processed to get response status code and data. The connection is closed and resources are freed before the task exits.
References
For further information please refer to the user programmers guide: CC3X20 Programmer’s Guide