testUser Cleartext-Password := "pass123"

#
# 	Configuration file for the rlm_files module.
# 	Please see rlm_files(5) manpage for more information.
#
# 	This file contains authentication security and configuration
#	information for each user.  Accounting requests are NOT processed
#	through this file.  Instead, see 'accounting', in this directory.
#
#	The first field is the user's name and can be up to
#	253 characters in length.  This is followed (on the same line) with
#	the list of authentication requirements for that user.  This can
#	include password, comm server name, comm server port number, protocol
#	type (perhaps set by the "hints" file), and huntgroup name (set by
#	the "huntgroups" file).
#
#	If you are not sure why a particular reply is being sent by the
#	server, then run the server in debugging mode (radiusd -X), and
#	you will see which entries in this file are matched.
#
#	When an authentication request is received from the comm server,
#	these values are tested. Only the first match is used unless the
#	"Fall-Through" variable is set to "Yes".
#
#	A special user named "DEFAULT" matches on all usernames.
#	You can have several DEFAULT entries. All entries are processed
#	in the order they appear in this file. The first entry that
#	matches the login-request will stop processing unless you use
#	the Fall-Through variable.
#
#	Indented (with the tab character) lines following the first
#	line indicate the configuration values to be passed back to
#	the comm server to allow the initiation of a user session.
#	This can include things like the PPP configuration values
#	or the host to log the user onto.
#
#	You can include another `users' file with `$INCLUDE users.other'

#
#	For a list of RADIUS attributes, and links to their definitions,
#	see: http://www.freeradius.org/rfc/attributes.html
#
#	Entries below this point are examples included in the server for
#	educational purposes. They may be deleted from the deployed
#	configuration without impacting the operation of the server.
#

#
# Deny access for a specific user.  Note that this entry MUST
# be before any other 'Auth-Type' attribute which results in the user
# being authenticated.
#
# Note that there is NO 'Fall-Through' attribute, so the user will not
# be given any additional resources.
#
#lameuser	Auth-Type := Reject
#		Reply-Message = "Your account has been disabled."

#
# Deny access for a group of users.
#
# Note that there is NO 'Fall-Through' attribute, so the user will not
# be given any additional resources.
#
#DEFAULT	Group == "disabled", Auth-Type := Reject
#		Reply-Message = "Your account has been disabled."
#

#
# This is a complete entry for "steve". Note that there is no Fall-Through
# entry so that no DEFAULT entry will be used, and the user will NOT
# get any attributes in addition to the ones listed here.
#
#steve	Cleartext-Password := "testing"
#	Service-Type = Framed-User,
#	Framed-Protocol = PPP,
#	Framed-IP-Address = 172.16.3.33,
#	Framed-IP-Netmask = 255.255.255.0,
#	Framed-Routing = Broadcast-Listen,
#	Framed-Filter-Id = "std.ppp",
#	Framed-MTU = 1500,
#	Framed-Compression = Van-Jacobsen-TCP-IP

#
# The canonical testing user which is in most of the
# examples.
#
#bob	Cleartext-Password := "hello"
#	Reply-Message := "Hello, %{User-Name}"
#

#
# This is an entry for a user with a space in their name.
# Note the double quotes surrounding the name.  If you have
# users with spaces in their names, you must also change
# the "filter_username" policy to allow spaces.
#
# See raddb/policy.d/filter, filter_username {} section.
#
#"John Doe"	Cleartext-Password := "hello"
#		Reply-Message = "Hello, %{User-Name}"

#
# Dial user back and telnet to the default host for that port
#
#Deg	Cleartext-Password := "ge55ged"
#	Service-Type = Callback-Login-User,
#	Login-IP-Host = 0.0.0.0,
#	Callback-Number = "9,5551212",
#	Login-Service = Telnet,
#	Login-TCP-Port = Telnet

#
# Another complete entry. After the user "dialbk" has logged in, the
# connection will be broken and the user will be dialed back after which
# he will get a connection to the host "timeshare1".
#
#dialbk	Cleartext-Password := "callme"
#	Service-Type = Callback-Login-User,
#	Login-IP-Host = timeshare1,
#	Login-Service = PortMaster,
#	Callback-Number = "9,1-800-555-1212"

#
# user "swilson" will only get a static IP number if he logs in with
# a framed protocol on a terminal server in Alphen (see the huntgroups file).
#
# Note that by setting "Fall-Through", other attributes will be added from
# the following DEFAULT entries
#
#swilson	Service-Type == Framed-User, Huntgroup-Name == "alphen"
#		Framed-IP-Address = 192.0.2.65,
#		Fall-Through = Yes

#
# If the user logs in as 'username.shell', then authenticate them
# using the default method, give them shell access, and stop processing
# the rest of the file.
#
#DEFAULT	Suffix == ".shell"
#		Service-Type = Login-User,
#		Login-Service = Telnet,
#		Login-IP-Host = your.shell.machine


#
# The rest of this file contains the several DEFAULT entries.
# DEFAULT entries match with all login names.
# Note that DEFAULT entries can also Fall-Through (see first entry).
# A name-value pair from a DEFAULT entry will _NEVER_ override
# an already existing name-value pair.
#

#
# Set up different IP address pools for the terminal servers.
# Note that the "+" behind the IP address means that this is the "base"
# IP address. The Port-Id (S0, S1 etc) will be added to it.
#
#DEFAULT	Service-Type == Framed-User, Huntgroup-Name == "alphen"
#		Framed-IP-Address = 192.0.2.32+,
#		Fall-Through = Yes

#DEFAULT	Service-Type == Framed-User, Huntgroup-Name == "delft"
#		Framed-IP-Address = 198.51.100.32+,
#		Fall-Through = Yes

#
# Sample defaults for all framed connections.
#
#DEFAULT	Service-Type == Framed-User
#	Framed-IP-Address = 255.255.255.254,
#	Framed-MTU = 576,
#	Service-Type = Framed-User,
#	Fall-Through = Yes

#
# Default for PPP: dynamic IP address, PPP mode, VJ-compression.
# NOTE: we do not use Hint = "PPP", since PPP might also be auto-detected
#	by the terminal server in which case there may not be a "P" suffix.
#	The terminal server sends "Framed-Protocol = PPP" for auto PPP.
#
DEFAULT	Framed-Protocol == PPP
	Framed-Protocol = PPP,
	Framed-Compression = Van-Jacobson-TCP-IP

#
# Default for CSLIP: dynamic IP address, SLIP mode, VJ-compression.
#
DEFAULT	Hint == "CSLIP"
	Framed-Protocol = SLIP,
	Framed-Compression = Van-Jacobson-TCP-IP

#
# Default for SLIP: dynamic IP address, SLIP mode.
#
DEFAULT	Hint == "SLIP"
	Framed-Protocol = SLIP

#
# Last default: rlogin to our main server.
#
#DEFAULT
#	Service-Type = Login-User,
#	Login-Service = Rlogin,
#	Login-IP-Host = shellbox.ispdomain.com

# #
# # Last default: shell on the local terminal server.
# #
# DEFAULT
# 	Service-Type = Administrative-User


# On no match, the user is denied access.


#########################################################
# You should add test accounts to the TOP of this file! #
# See the example user "bob" above.                     #
#########################################################