=== AUGENTIX SPL v0.0.10 === DDR = Generic DDR3, 1600 MT/s, DDR3, 128 MB DRAM INIT PASS, ret: 0x00000640 [PLL INFO] CPU Fvco 1008000000 port3(N/A ): -1 port4(N/A ): -1 port5(N/A ): -1 DRAM Fvco 1596000000 port3(N/A ): -1 port4(AXI DRAMC): 399000000 port5(N/A ): -1 Cascade Fvco 1350000000 port3(N/A ): -1 port4(25M ): 25000000 port5(27M ): 27000000 EMAC Fvco 1500000000 port3(EMAC ): 250000000 port4(QSPI ): 150000000 port5(ISP, VP ): 375000000 Sensor Fvco 891000000 port3(N/A ): -1 port4(IS, DISP ): 445500000 port5(SENIF ): 297000000 VENC Fvco 1000000000 port3(SDC 0 ): 200000000 port4(SDC 1 ): 200000000 port5(ENC ): 333333333 Audio Fvco 460800000 port3(PWM ): 46080000 port4(Audio in ): 61440000 port5(Audio out): 256000 MIPI TX Fvco 600000000 port4(MIPI TX ): 25000000 [Start FM] Cascade(P5) PASS Freq : 27000000 CPU(FB) PASS Freq : 24000000 EMAC(P3) PASS Freq : 250000000 Sensor(P4) PASS Freq : 445500000 Venc(P5) PASS Freq : 333325000 DDR(P4) PASS Freq : 399000000 Audio(P4) PASS Freq : 61450000 MIPI_TX(P4) PASS Freq : 25000000 NOR Quad lane, 3 byte mode NOR:Load u-boot from part=0x00007900 to 0x00008000 size 0x00042a14 SEC Uboot...OK U-Boot 2016.03-00007-g8f1214a8 (Jun 03 2025 - 14:49:41 +0800) I2C: ready DRAM: 128 MiB MMC: Synopsys Mobile storage: 0 Using default environment *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Net: eqos_eth Saving Environment to SPI Flash... Erasing SPI flash...Writing to SPI flash...done device 0 offset 0x100000, size 0x600000 SF: 6291456 bytes @ 0x100000 Read: OK ## Executing script at 01000000 sha256,rsa2048:key3+ ## Loading kernel from FIT Image at 01000000 ... Using 'conf-1' configuration Verifying Hash Integrity ... OK Trying 'kernel-1' kernel subimage Verifying Hash Integrity ... sha256,rsa2048:key3+ OK XIP Kernel Image ... OK Starting kernel ... ** 20 printk messages dropped ** CLK: clk add provider finish OF: /soc@80000000/usbc@A0000000: #phy-cells = 1 found 0 SCSI subsystem initialized run auge_spi_setup done m25p80 spi0.0: found w25q256, expected m25p80 5 cmdlinepart partitions found on MTD device nor_flash Creating 5 MTD partitions on "nor_flash": 0x000000000000-0x0000000f0000 : "boot" 0x0000000f0000-0x000000100000 : "bootenv" 0x000000100000-0x000000700000 : "linux" 0x000000700000-0x000001b00000 : "rootfs" 0x000001b00000-0x000002000000 : "usrdata" Import GPIO_HIGH_AT_PROBE solution clk: Not disabling unused clocks platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 dw_mmc SDC1P0: card claims to support voltages below defined range Kernel memory protection not selected by kernel config. random: crng init done mount: mounting devpts on /dev/pts failed: No such device overlayfs: upper fs does not support tmpfile. overlayfs: upper fs does not support RENAME_WHITEOUT. overlayfs: failed to set xattr on upper overlayfs: upper fs does not support tmpfile. overlayfs: upper fs does not support RENAME_WHITEOUT. overlayfs: failed to set xattr on upper Starting logging: OK Starting mdev... Current system mode: factory Initializing random number generator... done. cc33xx_sdio mmc1:0001:2: sdio read failed (-84) wlcore: ERROR IO error during core status read wlcore: ERROR Fatal error during driver init, cannot recover ifdown: interface wlan0 not configured cat: can't open '/sys/class/net/eth0/address': No such file or directory sh: 02:00:00:00:00:00: unknown operand Starting crond: OK [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# lsmod Module Size Used by Not tainted cc33xx_sdio 3889 0 cc33xx 90836 1 [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# [root@Augentix:/root]# dmesg 0x000000000000-0x0000000f0000 : "boot" 0x0000000f0000-0x000000100000 : "bootenv" 0x000000100000-0x000000700000 : "linux" 0x000000700000-0x000001b00000 : "rootfs" 0x000001b00000-0x000002000000 : "usrdata" dwc2 a0000000.usbc: DWC OTG Controller dwc2 a0000000.usbc: new USB bus registered, assigned bus number 1 dwc2 a0000000.usbc: irq 25, io mem 0xa0000000 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.01 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: DWC OTG Controller usb usb1: Manufacturer: Linux 6.1.102 dwc2_hsotg usb usb1: SerialNumber: a0000000.usbc hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected augentix-i2c: probing 80070000.i2c, <0x80070000 0xff>, irq 26. i2c_dev: i2c /dev entries driver Augentix AON WDT driver probed. device-mapper: ioctl: 4.47.0-ioctl (2022-07-28) initialised: dm-devel@redhat.com dw_mmc SDC0: fifo-depth property not found, using value of FIFOTH register as default dw_mmc SDC0: IDMAC supports 32-bit address mode. dw_mmc SDC0: Using internal DMA controller. dw_mmc SDC0: Version ID is 290a dw_mmc SDC0: DW MMC controller at irq 28,32 bit host data width,256 deep fifo Initializing XFRM netlink socket NET: Registered PF_PACKET protocol family NET: Registered PF_KEY protocol family Import GPIO_HIGH_AT_PROBE solution dw_mmc SDC1P0: fifo-depth property not found, using value of FIFOTH register as default dw_mmc SDC1P0: IDMAC supports 32-bit address mode. dw_mmc SDC1P0: Using internal DMA controller. dw_mmc SDC1P0: Version ID is 290a dw_mmc SDC1P0: DW MMC controller at irq 29,32 bit host data width,256 deep fifo mmc_host mmc1: card is non-removable. device-mapper: init: waiting for all devices to be available before creating mapped devices mmc_host mmc0: Bus speed (slot 0) = 100000000Hz (slot req 400000Hz, actual 400000HZ div = 125) mmc_host mmc1: Bus speed (slot 0) = 250000000Hz (slot req 400000Hz, actual 399361HZ div = 313) device-mapper: verity: sha256 using implementation "sha256-asm" device-mapper: ioctl: dm-0 (rootfs) is ready clk: Not disabling unused clocks ALSA device list: No soundcards found. platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 cfg80211: failed to load regulatory.db dw_mmc SDC1P0: card claims to support voltages below defined range VFS: Mounted root (squashfs filesystem) readonly on device 254:0. mmc_host mmc1: Bus speed (slot 0) = 250000000Hz (slot req 25000000Hz, actual 25000000HZ div = 5) devtmpfs: mounted Freeing unused kernel image (initmem) memory: 116K Kernel memory protection not selected by kernel config. Run /sbin/init as init process with arguments: /sbin/init with environment: HOME=/ TERM=linux ethaddr=02:00:00:00:00:00 mmc1: new SDIO card at address 0001 random: crng init done overlayfs: upper fs does not support tmpfile. overlayfs: upper fs does not support RENAME_WHITEOUT. overlayfs: failed to set xattr on upper overlayfs: upper fs does not support tmpfile. overlayfs: upper fs does not support RENAME_WHITEOUT. overlayfs: failed to set xattr on upper cc33xx_sdio mmc1:0001:2: Using SDIO in-band IRQ wlcore: cc33xx_probe :: Start wlcore: Wireless Driver Version 1.7.0.208 wlcore: WLAN CC33xx platform device probe done wlcore: Chip wakeup wlcore: Set BLKsize to 128 cc33xx_sdio mmc1:0001:2: sdio read failed (-84) wlcore: ERROR IO error during core status read wlcore: ERROR Fatal error during driver init, cannot recover [root@Augentix:/root]#