#include #include #include #include #include #include #include #include #include // TI-Driver includes #include #include // Simplelink includes #include // SlNetSock includes #include // MQTT Library includes #include "network_if.h" // Common interface includes #include "uart_term.h" #include "Board.h" // Application includes #include "client_cbs.h" #include "mqueue.h" #include "time.h" #include #include #include //***************************************************************************** // LOCAL DEFINES //***************************************************************************** #define CLIENT_INIT_STATE (0x01) #define MQTT_INIT_STATE (0x04) #define APPLICATION_VERSION "1.1.1" #define APPLICATION_NAME "MQTT client" #define SLNET_IF_WIFI_PRIO (5) #define MQTT_3_1_1 false // Operate Lib in MQTT 3.1 mode. #define MQTT_3_1 true #define WILL_TOPIC "Client" #define WILL_MSG "Client Stopped" #define WILL_QOS MQTT_QOS_2 #define WILL_RETAIN false //#define SERVER_ADDRESS "messagesight.demos.ibm.com" // Defining Broker IP address and port Number #define SERVER_ADDRESS "m2m.eclipse.org" #define SERVER_IP_ADDRESS "192.168.100.215" #define PORT_NUMBER 1883 #define SECURED_PORT_NUMBER 8883 #define LOOPBACK_PORT 1882 #define CLEAN_SESSION true // Clean session flag #define RETAIN_ENABLE 1 // Retain Flag. Used in publish message. #define TASKSTACKSIZE 2048 // Spawn task priority and Task and Thread Stack Size #define RXTASKSIZE 4096 #define MQTTTHREADSIZE 2048 #define SPAWN_TASK_PRIORITY 9 // secured client requires time configuration, in order to verify server certificate validity (date). #define DAY 1 // Day of month (DD format) range 1-31 #define MONTH 5 // Month (MM format) in the range of 1-12 #define YEAR 2017 // Year (YYYY format) #define HOUR 12 // Hours in the range of 0-23 #define MINUTES 33 // Minutes in the range of 0-59 #define SEC 21 // Seconds in the range of 0-59 /* Number of files used for secure connection */ #define CLIENT_NUM_SECURE_FILES 1 /* Expiration value for the timer that is being used to toggle the Led. */ #define TIMER_EXPIRATION_VALUE 100 * 1000000 //***************************************************************************** // LOCAL FUNCTION PROTOTYPES //***************************************************************************** void pushButtonInterruptHandler2(uint_least8_t index); void pushButtonInterruptHandler3(uint_least8_t index); void cycleStartInterruptHandler(uint_least8_t index); void cycleStopInterruptHandler(uint_least8_t index); void materialShortInterruptHandler(uint_least8_t index); void dieChangeInterruptHandler(uint_least8_t index); void alarmInterruptHandler(uint_least8_t index); void TimerPeriodicIntHandler(sigval val); void LedTimerConfigNStart(); void LedTimerDeinitStop(); static void DisplayBanner(char * AppName); void *MqttClient(void *pvParameters); void Mqtt_ClientStop(uint8_t disconnect); void Mqtt_ServerStop(); void Mqtt_Stop(); void Mqtt_start(); int32_t Mqtt_IF_Connect(); int32_t MqttServer_start(); int32_t MqttClient_start(); int32_t MQTT_SendMsgToQueue(struct msgQueue *queueElement); //***************************************************************************** // GLOBAL VARIABLES //***************************************************************************** /* Connection state: (0) - connected, (negative) - disconnected */ int32_t gApConnectionState = -1; uint32_t gInitState = 0; uint32_t memPtrCounterfree = 0; bool gResetApplication = false; static MQTTClient_Handle gMqttClient; MQTTClient_Params MqttClientExmple_params; unsigned short g_usTimerInts; /* Receive task handle */ pthread_t g_rx_task_hndl = (pthread_t) NULL; uint32_t gUiConnFlag = 0; /* AP Security Parameters */ SlWlanSecParams_t SecurityParams = { 0 }; /* Client ID */ /* If ClientId isn't set, the MAC address of the device will be copied into the ClientID parameter. */ char ClientId[13] = {'\0'}; /* Client User Name and Password */ const char *ClientUsername = "user1234567"; const char *ClientPassword = "pwd123"; unsigned char qos = MQTT_QOS_2; /* Subscription topics and qos values */ char *topic = "cc32xx/TimeSync" ; /* Publishing topics and messages */ const char *publish_topic0 = "cc32xx/ButtonPressEvtSw2"; const char *publish_CycleStart = "2"; // "cc32xx/CycleStart" ; const char *publish_CycleStop = "3"; // "cc32xx/CycleStop"; const char *publish_MaterialShort = "4"; // "cc32xx/MaterialShort"; const char *publish_MaterialAvailable = "5"; // "cc32xx/MaterialAvailable"; const char *publish_DieChange_Begin = "6"; // "cc32xx/DieChange"; const char *publish_DieChange_End = "7"; // "cc32xx/DieChange"; const char *publish_OilLevel_Low = "8"; // cc32xx/OilLevel"; const char *publish_OilLevel_High = "9"; // cc32xx/OilLevel"; const char *publish_Alarm = "11"; // "cc32xx/Alarm"; const char *publish_ConnStatus = "cc32xx/ConnStatus"; /* Message Queue */ mqd_t g_PBQueue; pthread_t mqttThread = (pthread_t) NULL; pthread_t appThread = (pthread_t) NULL; timer_t g_timer; /* Printing new line */ char lineBreak[] = "\n\r"; SlDateTime_t ReaddateTime = {0}; int TimeValue[6]; char *tok; char str0[5], str1[3], str2[3], str3[3], str4[3], str5[3]; char *str, *dateTimeValue ; int intrCount[5] = { 0,0,0,0,0 }, countVal[5] = { 0,0,0,0,0 }; uint32_t cycle_TimeCount[2], material_TimeCount[2], die_TimeCount[2], oil_TimeCount[2], alarm_TimeCount[2] ; //***************************************************************************** // Banner VARIABLES //***************************************************************************** #ifdef SECURE_CLIENT char *Mqtt_Client_secure_files[CLIENT_NUM_SECURE_FILES] = {"ca-cert.pem"}; MQTTClient_ConnParams Mqtt_ClientCtx = { MQTTCLIENT_NETCONN_IP4 | MQTTCLIENT_NETCONN_SEC, SERVER_IP_ADDRESS, //SERVER_ADDRESS, SECURED_PORT_NUMBER,// PORT_NUMBER SLNETSOCK_SEC_METHOD_SSLv3_TLSV1_2, SLNETSOCK_SEC_CIPHER_FULL_LIST, CLIENT_NUM_SECURE_FILES, Mqtt_Client_secure_files }; void setTime() { SlDateTime_t dateTime = {0}; dateTime.tm_day = (uint32_t)DAY; dateTime.tm_mon = (uint32_t)MONTH; dateTime.tm_year = (uint32_t)YEAR; dateTime.tm_hour = (uint32_t)HOUR; dateTime.tm_min = (uint32_t)MINUTES; dateTime.tm_sec = (uint32_t)SEC; sl_DeviceSet(SL_DEVICE_GENERAL, SL_DEVICE_GENERAL_DATE_TIME, sizeof(SlDateTime_t), (uint8_t *)(&dateTime)); } #else MQTTClient_ConnParams Mqtt_ClientCtx = { MQTTCLIENT_NETCONN_URL, SERVER_IP_ADDRESS, PORT_NUMBER, 0, 0, 0, NULL }; #endif MQTTClient_Will will_param = // Initialize the will_param structure to the default will parameters { WILL_TOPIC, WILL_MSG, WILL_QOS, WILL_RETAIN }; int32_t MQTT_SendMsgToQueue(struct msgQueue *queueElement) { struct timespec abstime = {0}; clock_gettime(CLOCK_REALTIME, &abstime); if(g_PBQueue) { if (mq_timedsend(g_PBQueue, (char *) queueElement, sizeof(struct msgQueue), 0, &abstime) == 0) // send message to the queue { return 0; } } return -1; } struct subMsgHeader { uint32_t stopicLen; uint32_t spayLen; bool sretain; bool sdup; unsigned char sqos; }; void TimeSync() { SlDateTime_t TSdateTime = {0}; TSdateTime.tm_year = (uint32_t)TimeValue[0]; TSdateTime.tm_mon = (uint32_t)TimeValue[1]; TSdateTime.tm_day = (uint32_t)TimeValue[2]; TSdateTime.tm_hour = (uint32_t)TimeValue[3]; TSdateTime.tm_min = (uint32_t)TimeValue[4]; TSdateTime.tm_sec = (uint32_t)TimeValue[5]; sl_DeviceSet(SL_DEVICE_GENERAL, SL_DEVICE_GENERAL_DATE_TIME, sizeof(SlDateTime_t), (uint8_t *)(&TSdateTime)); /* UART_PRINT("Year %d,Mon %d,Day %d,Hour %d,Min %d,Sec %d\n",TSdateTime.tm_year,TSdateTime.tm_mon,TSdateTime.tm_day, TSdateTime.tm_hour,TSdateTime.tm_min,TSdateTime.tm_sec); */ } char* readDateandTime() { SlDateTime_t dateTime = {0}; _u16 configLen = sizeof (SlDateTime_t); _u8 configOpt = SL_DEVICE_GENERAL_DATE_TIME; sl_DeviceGet(SL_DEVICE_GENERAL,&configOpt, &configLen,(_u8 *)(&dateTime)); str = (char *) malloc (15*sizeof(char)); sprintf (str0, "%04d-", dateTime.tm_year); sprintf (str1, "%02d-", dateTime.tm_mon); sprintf (str2, "%02d ", dateTime.tm_day); sprintf (str3, "%02d:", dateTime.tm_hour); sprintf (str4, "%02d:", dateTime.tm_min); sprintf (str5, "%02d ", dateTime.tm_sec); strcpy (str, str0); strcat (str, str1); strcat (str, str2); strcat (str, str3); strcat (str, str4); strcat (str, str5); return str; } void pushButtonInterruptHandler2(uint_least8_t index) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_BUTTON0); // SW2 queueElement.event = PUBLISH_PUSH_BUTTON_PRESSED; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } void cycleInterruptHandler(uint_least8_t index) { if ( !intrCount[0] && ( GPIO_read ( Board_GPIO_Cycle ) == 1 ) ) { cycle_TimeCount[0] = Clock_getTicks(); if ( countVal[0] == 0 || ( cycle_TimeCount[0] - cycle_TimeCount[1] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_Cycle); queueElement.event = PUBLISH_CYCLE_START; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[0] = !intrCount[0]; } else if ( intrCount[0] && ( GPIO_read ( Board_GPIO_Cycle ) == 0 ) ) { cycle_TimeCount[1] = Clock_getTicks(); if ( ( cycle_TimeCount[1] - cycle_TimeCount[0] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_Cycle); queueElement.event = PUBLISH_CYCLE_STOP; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[0] = !intrCount[0]; countVal[0] ++; } } void materialShortInterruptHandler(uint_least8_t index) { if ( !intrCount[1] && ( GPIO_read ( Board_GPIO_Material ) == 1 ) ) { material_TimeCount[0] = Clock_getTicks(); if ( countVal[1] == 0 || ( material_TimeCount[0] - material_TimeCount[1] ) >= 100 ) { struct msgQueue queueElement; queueElement.event = PUBLISH_MATERIAL_SHORT; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[1] = !intrCount[1]; } else if ( intrCount[1] && ( GPIO_read ( Board_GPIO_Material ) == 0 ) ) { material_TimeCount[1] = Clock_getTicks(); if ( ( material_TimeCount[1] - material_TimeCount[0] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_Material); queueElement.event = PUBLISH_MATERIAL_AVAILABLE; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[1] = !intrCount[1]; countVal[1] ++; } } void dieChangeInterruptHandler(uint_least8_t index) { if ( !intrCount[2] && ( GPIO_read ( Board_GPIO_DiaChange ) == 1 ) ) { die_TimeCount[0] = Clock_getTicks(); if ( countVal[2] == 0 || ( die_TimeCount[0] - die_TimeCount[1] ) >= 100 ) { struct msgQueue queueElement; queueElement.event = PUBLISH_DIA_CHANGE_BEGIN; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[2] = !intrCount[2]; } else if ( intrCount[2] && ( GPIO_read ( Board_GPIO_DiaChange ) == 0 ) ) { die_TimeCount[1] = Clock_getTicks(); if ( ( die_TimeCount[1] - die_TimeCount[0] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_DiaChange); queueElement.event = PUBLISH_DIA_CHANGE_END; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[2] = !intrCount[2]; countVal[2]++ ; } } void oilLevelInterruptHandler(uint_least8_t index) { if ( !intrCount[3] && ( GPIO_read ( Board_GPIO_OilLevel ) == 1 ) ) { oil_TimeCount[0] = Clock_getTicks(); if ( countVal[3] == 0 || ( oil_TimeCount [0] - oil_TimeCount [1] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_OilLevel); queueElement.event = PUBLISH_MACHINE_OILLEVEL_LOW; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[3] = !intrCount[3]; } else if ( intrCount[3] && ( GPIO_read ( Board_GPIO_OilLevel ) == 0 ) ) { oil_TimeCount[1] = Clock_getTicks(); if ( ( oil_TimeCount[1] - oil_TimeCount[0] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_OilLevel); queueElement.event = PUBLISH_MACHINE_OILLEVEL_HIGH; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[3] = !intrCount[3]; countVal[3]++ ; } } void alarmInterruptHandler(uint_least8_t index) { if ( !intrCount[4] && ( GPIO_read ( Board_GPIO_Alarm ) == 1 ) ) { alarm_TimeCount[0] = Clock_getTicks(); if ( countVal[4] == 0 || ( alarm_TimeCount[0] - alarm_TimeCount[1] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_Alarm); queueElement.event = PUBLISH_MACHINE_ALARM; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[3] = !intrCount[3]; } else if ( intrCount[4] && ( GPIO_read ( Board_GPIO_Alarm ) == 0 ) ) { alarm_TimeCount[1] = Clock_getTicks(); if ( ( alarm_TimeCount[1] - alarm_TimeCount[0] ) >= 100 ) { struct msgQueue queueElement; GPIO_disableInt(Board_GPIO_Alarm); queueElement.event = PUBLISH_MACHINE_ALARM; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full\n\n\r"); } } intrCount[4] = !intrCount[4]; countVal[4]++ ; } } void pushButtonInterruptHandler3(uint_least8_t index) { struct msgQueue queueElement; struct msgQueue queueElemRecv; queueElement.event = DISC_PUSH_BUTTON_PRESSED; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating disconnect push button pressed message { UART_PRINT("\n\n\rQueue is full, throw first msg and send the new one\n\n\r"); mq_receive(g_PBQueue, (char*) &queueElemRecv, sizeof(struct msgQueue), NULL); MQTT_SendMsgToQueue(&queueElement); } } void TimerPeriodicIntHandler(sigval val) { g_usTimerInts++; // Increment our interrupt counter. if (!(g_usTimerInts & 0x1)) { GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_OFF); // Turn Led Off } else { GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON); // Turn Led On } } void LedTimerConfigNStart() { struct itimerspec value; sigevent sev; sev.sigev_notify = SIGEV_SIGNAL; // Create Timer sev.sigev_notify_function = &TimerPeriodicIntHandler; timer_create(2, &sev, &g_timer); value.it_interval.tv_sec = 0; // start timer value.it_interval.tv_nsec = TIMER_EXPIRATION_VALUE; value.it_value.tv_sec = 0; value.it_value.tv_nsec = TIMER_EXPIRATION_VALUE; timer_settime(g_timer, 0, &value, NULL); } void LedTimerDeinitStop() { /* Disable the LED blinking Timer as Device is connected to AP. */ timer_delete(g_timer); } static void DisplayBanner(char * AppName) { UART_PRINT("\n\n\n\r"); UART_PRINT("\t\t *************************************************\n\r"); UART_PRINT("\t\t CC3220 %s Application \n\r", AppName); UART_PRINT("\t\t *************************************************\n\r"); UART_PRINT("\n\n\n\r"); } void *MqttClientThread(void * pvParameters) { struct msgQueue queueElement; struct msgQueue queueElemRecv; MQTTClient_run((MQTTClient_Handle)pvParameters); queueElement.event = LOCAL_CLIENT_DISCONNECTION; queueElement.msgPtr = NULL; /* write message indicating disconnect Broker message. */ if (MQTT_SendMsgToQueue(&queueElement)) { UART_PRINT("\n\n\rQueue is full, throw first msg and send the new one\n\n\r"); mq_receive(g_PBQueue, (char*) &queueElemRecv, sizeof(struct msgQueue), NULL); MQTT_SendMsgToQueue(&queueElement); } pthread_exit(0); return NULL; } void * MqttClient(void *pvParameters) { struct msgQueue queueElemRecv; long lRetVal = -1; struct publishMsgHeader *publishMsgHeaderptr; uint32_t topicLen, payLen; char *topic, *payload, *messagePtr; int m; /* Initializing Client and Subscribing to the Broker. */ if (gApConnectionState >= 0) { lRetVal = MqttClient_start(); if (lRetVal == -1) { UART_PRINT("MQTT Client lib initialization failed\n\r"); pthread_exit(0); return NULL; } } for (;;) { /* waiting for signals */ mq_receive(g_PBQueue, (char*) &queueElemRecv, sizeof(struct msgQueue), NULL); switch (queueElemRecv.event) { case PUBLISH_CYCLE_START: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_CycleStart, strlen((char*) publish_CycleStart), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_CycleStart); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Cycle); GPIO_enableInt(Board_GPIO_Cycle); break; case PUBLISH_CYCLE_STOP: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_CycleStop, strlen((char*) publish_CycleStop), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_CycleStop); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Cycle); GPIO_enableInt(Board_GPIO_Cycle); break; case PUBLISH_MATERIAL_SHORT: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_MaterialShort, strlen((char*) publish_MaterialShort), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_MaterialShort); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Material); GPIO_enableInt(Board_GPIO_Material); break; case PUBLISH_MATERIAL_AVAILABLE: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_MaterialAvailable, strlen((char*) publish_MaterialAvailable), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_MaterialAvailable); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Material); GPIO_enableInt(Board_GPIO_Material); break; case PUBLISH_DIA_CHANGE_BEGIN: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_DieChange_Begin, strlen((char*) publish_DieChange_Begin), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_DieChange_Begin); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_DiaChange); GPIO_enableInt(Board_GPIO_DiaChange); break; case PUBLISH_DIA_CHANGE_END: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_DieChange_End, strlen((char*) publish_DieChange_End), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_DieChange_End); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_DiaChange); GPIO_enableInt(Board_GPIO_DiaChange); break; case PUBLISH_MACHINE_OILLEVEL_LOW: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_OilLevel_Low, strlen((char*) publish_OilLevel_Low), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_OilLevel_Low); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_OilLevel); GPIO_enableInt(Board_GPIO_OilLevel); break; case PUBLISH_MACHINE_OILLEVEL_HIGH: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_OilLevel_High, strlen((char*) publish_OilLevel_High), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_OilLevel_High); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_OilLevel); GPIO_enableInt(Board_GPIO_OilLevel); break; case PUBLISH_MACHINE_ALARM: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_Alarm, strlen((char*) publish_Alarm), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_Alarm); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Alarm); GPIO_enableInt(Board_GPIO_Alarm); break; case PUBLISH_MACHINE_CONNSTATUS: dateTimeValue = readDateandTime(); lRetVal = MQTTClient_publish(gMqttClient, (char*) publish_ConnStatus, strlen((char*) publish_ConnStatus), (char*) dateTimeValue, strlen((char*) dateTimeValue), MQTT_QOS_2 | ((RETAIN_ENABLE)?MQTT_PUBLISH_RETAIN:0) ); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); // send publish message UART_PRINT("Topic: %s\n\r", publish_ConnStatus); UART_PRINT("Data: %s\n\r", dateTimeValue); GPIO_clearInt(Board_GPIO_Alarm); GPIO_enableInt(Board_GPIO_Alarm); break; case MSG_RECV_BY_CLIENT: messagePtr = (char *) queueElemRecv.msgPtr; publishMsgHeaderptr = malloc(sizeof(struct publishMsgHeader)); memcpy((void *) publishMsgHeaderptr, (const void *) messagePtr, sizeof(struct publishMsgHeader)); topicLen = publishMsgHeaderptr->topicLen; payLen = publishMsgHeaderptr->payLen; topic = malloc(topicLen); memcpy((void*) topic, ((const void*) (messagePtr + sizeof(struct publishMsgHeader))), topicLen); payload = malloc(payLen); memcpy((void*) payload, (const void*) (messagePtr + sizeof(struct publishMsgHeader) + topicLen + 1), payLen); if(strcmp(topic, "cc32xx/TimeSync") == 0) { tok = strtok (payload, ","); for (m = 0; tok != NULL; m++) { TimeValue[m] = atoi(tok); tok = strtok (NULL, ","); } TimeSync(); } free(queueElemRecv.msgPtr); free(publishMsgHeaderptr); free(topic); free(payload); break; case LOCAL_CLIENT_DISCONNECTION: UART_PRINT("\n\rOn-board Client Disconnected\n\r\r\n"); gUiConnFlag = 0; break; /* Push button for full restart check */ case DISC_PUSH_BUTTON_PRESSED: gResetApplication = true; break; case THREAD_TERMINATE_REQ: gUiConnFlag = 0; pthread_exit(0); return NULL; default: sleep(1); break; } } } int32_t Mqtt_IF_Connect() { int32_t lRetVal; char SSID_Remote_Name[32]; int8_t Str_Length; memset(SSID_Remote_Name, '\0', sizeof(SSID_Remote_Name)); Str_Length = strlen(SSID_NAME); if (Str_Length) { /* Copy the Default SSID to the local variable */ strncpy(SSID_Remote_Name, SSID_NAME, Str_Length); } /* Display Application Banner */ DisplayBanner(APPLICATION_NAME); GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_OFF); GPIO_write(Board_GPIO_LED1, Board_GPIO_LED_OFF); GPIO_write(Board_GPIO_LED2, Board_GPIO_LED_OFF); /* Reset The state of the machine */ Network_IF_ResetMCUStateMachine(); /* Start the driver */ lRetVal = Network_IF_InitDriver(ROLE_STA); if (lRetVal < 0) { UART_PRINT("Failed to start SimpleLink Device\n\r", lRetVal); return -1; } /* switch on Green LED to indicate Simplelink is properly up. */ GPIO_write(Board_GPIO_LED2, Board_GPIO_LED_ON); /* Start Timer to blink Red LED till AP connection */ LedTimerConfigNStart(); /* Initialize AP security params */ SecurityParams.Key = (signed char *) SECURITY_KEY; SecurityParams.KeyLen = strlen(SECURITY_KEY); SecurityParams.Type = SECURITY_TYPE; /* Connect to the Access Point */ lRetVal = Network_IF_ConnectAP(SSID_Remote_Name, SecurityParams); if (lRetVal < 0) { UART_PRINT("Connection to an AP failed\n\r"); return -1; } /* Disable the LED blinking Timer as Device is connected to AP. */ LedTimerDeinitStop(); /* Switch ON RED LED to indicate that Device acquired an IP. */ GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON); sleep(1); GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_OFF); GPIO_write(Board_GPIO_LED1, Board_GPIO_LED_OFF); GPIO_write(Board_GPIO_LED2, Board_GPIO_LED_OFF); return 0; } void Mqtt_start() { int32_t threadArg = 100; pthread_attr_t pAttrs; struct sched_param priParam; int32_t retc = 0; mq_attr attr; unsigned mode = 0; /* sync object for inter thread communication */ attr.mq_maxmsg = 10; attr.mq_msgsize = sizeof(struct msgQueue); g_PBQueue = mq_open("g_PBQueue", O_CREAT, mode, &attr); if (g_PBQueue == NULL) { UART_PRINT("MQTT Message Queue create fail\n\r"); gInitState &= ~MQTT_INIT_STATE; return; } /* Set priority and stack size attributes */ pthread_attr_init(&pAttrs); priParam.sched_priority = 2; retc = pthread_attr_setschedparam(&pAttrs, &priParam); retc |= pthread_attr_setstacksize(&pAttrs, MQTTTHREADSIZE); retc |= pthread_attr_setdetachstate(&pAttrs, PTHREAD_CREATE_DETACHED); if (retc != 0) { gInitState &= ~MQTT_INIT_STATE; UART_PRINT("MQTT thread create fail\n\r"); return; } retc = pthread_create(&mqttThread, &pAttrs, MqttClient, (void *) &threadArg); if (retc != 0) { gInitState &= ~MQTT_INIT_STATE; UART_PRINT("MQTT thread create fail\n\r"); return; } GPIO_setCallback(Board_GPIO_Cycle, cycleInterruptHandler); GPIO_enableInt(Board_GPIO_Cycle); GPIO_setCallback(Board_GPIO_Material, materialShortInterruptHandler); GPIO_enableInt(Board_GPIO_Material); GPIO_setCallback(Board_GPIO_DiaChange, dieChangeInterruptHandler); GPIO_enableInt(Board_GPIO_DiaChange); GPIO_setCallback(Board_GPIO_OilLevel, oilLevelInterruptHandler); GPIO_enableInt(Board_GPIO_OilLevel); GPIO_setCallback(Board_GPIO_Alarm, alarmInterruptHandler); GPIO_enableInt(Board_GPIO_Alarm); gInitState &= ~MQTT_INIT_STATE; } void Mqtt_Stop() { struct msgQueue queueElement; struct msgQueue queueElemRecv; if (gApConnectionState >= 0) { Mqtt_ClientStop(1); } queueElement.event = THREAD_TERMINATE_REQ; queueElement.msgPtr = NULL; if (MQTT_SendMsgToQueue(&queueElement)) // write message indicating publish message { UART_PRINT("\n\n\rQueue is full, throw first msg and send the new one\n\n\r"); mq_receive(g_PBQueue, (char*) &queueElemRecv, sizeof(struct msgQueue), NULL); MQTT_SendMsgToQueue(&queueElement); } sleep(2); mq_close(g_PBQueue); g_PBQueue = NULL; sl_Stop(SL_STOP_TIMEOUT); UART_PRINT("\n\r Client Stop completed\r\n"); GPIO_disableInt(Board_GPIO_Cycle); // GPIO_disableInt(Board_GPIO_Material); // GPIO_disableInt(Board_GPIO_DiaChange); // GPIO_disableInt(Board_GPIO_OilLevel); // GPIO_disableInt(Board_GPIO_Alarm); } int32_t MqttClient_start() { int32_t lRetVal = -1; int32_t threadArg = 100; pthread_attr_t pAttrs; struct sched_param priParam; MqttClientExmple_params.clientId = ClientId; MqttClientExmple_params.connParams = &Mqtt_ClientCtx; MqttClientExmple_params.mqttMode31 = MQTT_3_1; MqttClientExmple_params.blockingSend = true; gInitState |= CLIENT_INIT_STATE; gMqttClient = MQTTClient_create(MqttClientCallback, &MqttClientExmple_params); // Initialize MQTT client lib if( gMqttClient == NULL ) { gInitState &= ~CLIENT_INIT_STATE; // lib initialization failed return -1; } /* Open Client Receive Thread start the receive task. Set priority and stack size attributes */ pthread_attr_init(&pAttrs); priParam.sched_priority = 2; lRetVal = pthread_attr_setschedparam(&pAttrs, &priParam); lRetVal |= pthread_attr_setstacksize(&pAttrs, RXTASKSIZE); lRetVal |= pthread_attr_setdetachstate(&pAttrs, PTHREAD_CREATE_DETACHED); lRetVal |= pthread_create(&g_rx_task_hndl, &pAttrs, MqttClientThread, (void *) &threadArg); if (lRetVal != 0) { UART_PRINT("Client Thread Create Failed failed\n\r"); gInitState &= ~CLIENT_INIT_STATE; return -1; } #ifdef SECURE_CLIENT setTime(); #endif MQTTClient_set(gMqttClient, MQTTClient_WILL_PARAM, &will_param, sizeof(will_param)); // setting will parameters #ifdef CLNT_USR_PWD MQTTClient_set(gMqttClient, MQTTClient_USER_NAME, (void *)ClientUsername, strlen((char*)ClientUsername)); // Set user name for client connection MQTTClient_set(gMqttClient, MQTTClient_PASSWORD, (void *)ClientPassword, strlen((char*)ClientPassword)); // Set password #endif if (gApConnectionState >= 0) // Initiate MQTT Connect { #if CLEAN_SESSION == false bool clean = CLEAN_SESSION; MQTTClient_set(gMqttClient, MQTTClient_CLEAN_CONNECT, (void *)&clean, sizeof(bool)); #endif /* The return code of MQTTClient_connect is the ConnACK value that returns from the server */ lRetVal = MQTTClient_connect(gMqttClient); /* negative lRetVal means error, 0 means connection successful without session stored by the server, greater than 0 means successful connection with session stored by the server */ if (0 > lRetVal) { UART_PRINT("Connection to broker failed, Error code: %d\n\r", lRetVal); // lib initialization failed gUiConnFlag = 0; } else { gUiConnFlag = 1; } /* Subscribe to topics when session is not stored by the server */ if ( (gUiConnFlag == 1) && (0 == lRetVal) ) { MQTTClient_SubscribeParams subscriptionInfo[1]; subscriptionInfo[0].topic = topic; subscriptionInfo[0].qos = qos; if (MQTTClient_subscribe(gMqttClient , subscriptionInfo, 1) < 0) { UART_PRINT("\n\r Subscription Error \n\r"); MQTTClient_disconnect(gMqttClient); gUiConnFlag = 0; } else { UART_PRINT("Client subscribed on %s\n\r,", topic); MQTTClient_publish(gMqttClient, (char*) publish_ConnStatus, strlen((char*)publish_ConnStatus), (char*) "1", 1, MQTT_QOS_2 | MQTT_PUBLISH_RETAIN ); } } } gInitState &= ~CLIENT_INIT_STATE; return 0; } void Mqtt_ClientStop(uint8_t disconnect) { MQTTClient_UnsubscribeParams subscriptionInfo[1]; subscriptionInfo[0].topic = topic; MQTTClient_unsubscribe(gMqttClient , subscriptionInfo, 1); UART_PRINT("Unsubscribed from the topic %s\r\n", topic); MQTTClient_publish(gMqttClient, (char*) publish_ConnStatus, strlen((char*)publish_ConnStatus), (char*) "0", 1, MQTT_QOS_2 | MQTT_PUBLISH_RETAIN ); gUiConnFlag = 0; MQTTClient_delete(gMqttClient); // exiting the Client library } void printBorder(char ch, int n) { int i = 0; for(i=0; i> 4) & 0xf; /* Copy the 4 LSB - the least significant character */ Client_Mac_Name[1] = macAddress[Index] & 0xf; if (Client_Mac_Name[0] > 9) { /* Converts and copies from number that is greater than 9 in */ /* hexadecimal representation (a to f) into ascii character */ ClientId[2 * Index] = Client_Mac_Name[0] + 'a' - 10; } else { /* Converts and copies from number 0 - 9 in hexadecimal */ /* representation into ascii character */ ClientId[2 * Index] = Client_Mac_Name[0] + '0'; } if (Client_Mac_Name[1] > 9) { /* Converts and copies from number that is greater than 9 in */ /* hexadecimal representation (a to f) into ascii character */ ClientId[2 * Index + 1] = Client_Mac_Name[1] + 'a' - 10; } else { /* Converts and copies from number 0 - 9 in hexadecimal */ /* representation into ascii character */ ClientId[2 * Index + 1] = Client_Mac_Name[1] + '0'; } } } } int32_t DisplayAppBanner(char* appName, char* appVersion) { int32_t ret = 0; uint8_t macAddress[SL_MAC_ADDR_LEN]; uint16_t macAddressLen = SL_MAC_ADDR_LEN; uint16_t ConfigSize = 0; uint8_t ConfigOpt = SL_DEVICE_GENERAL_VERSION; SlDeviceVersion_t ver = {0}; ConfigSize = sizeof(SlDeviceVersion_t); ret = sl_DeviceGet(SL_DEVICE_GENERAL, &ConfigOpt, &ConfigSize, (uint8_t*)(&ver)); /* Print device version info. */ ret = sl_NetCfgGet(SL_NETCFG_MAC_ADDRESS_GET, 0, &macAddressLen, &macAddress[0]); /* Print device Mac address */ UART_PRINT(lineBreak); UART_PRINT("\t"); printBorder('=', 44); UART_PRINT(lineBreak); UART_PRINT("\t %s Example Ver: %s",appName, appVersion); UART_PRINT(lineBreak); UART_PRINT("\t"); printBorder('=', 44); UART_PRINT(lineBreak); UART_PRINT(lineBreak); UART_PRINT("\t CHIP: 0x%x",ver.ChipId); UART_PRINT(lineBreak); UART_PRINT("\t MAC: %d.%d.%d.%d",ver.FwVersion[0],ver.FwVersion[1],ver.FwVersion[2],ver.FwVersion[3]); UART_PRINT(lineBreak); UART_PRINT("\t PHY: %d.%d.%d.%d",ver.PhyVersion[0],ver.PhyVersion[1],ver.PhyVersion[2],ver.PhyVersion[3]); UART_PRINT(lineBreak); UART_PRINT("\t NWP: %d.%d.%d.%d",ver.NwpVersion[0],ver.NwpVersion[1],ver.NwpVersion[2],ver.NwpVersion[3]); UART_PRINT(lineBreak); UART_PRINT("\t ROM: %d",ver.RomVersion); UART_PRINT(lineBreak); UART_PRINT("\t HOST: %s", SL_DRIVER_VERSION); UART_PRINT(lineBreak); UART_PRINT("\t MAC address: %02x:%02x:%02x:%02x:%02x:%02x", macAddress[0], macAddress[1], macAddress[2], macAddress[3], macAddress[4], macAddress[5]); UART_PRINT(lineBreak); UART_PRINT(lineBreak); UART_PRINT("\t"); printBorder('=', 44); UART_PRINT(lineBreak); UART_PRINT(lineBreak); SetClientIdNamefromMacAddress(macAddress); return ret; } void mainThread(void * args) { uint32_t count = 0; pthread_t spawn_thread = (pthread_t) NULL; pthread_attr_t pAttrs_spawn; struct sched_param priParam; int32_t retc = 0; UART_Handle tUartHndl; SlNetIf_init(0); /* Initialize SlNetSock layer with CC3x20 interface */ SlNetIf_add(SLNETIF_ID_1, "CC3220", (const SlNetIf_Config_t *)&SlNetIfConfigWifi, SLNET_IF_WIFI_PRIO); SlNetSock_init(0); SlNetUtil_init(0); GPIO_init(); SPI_init(); tUartHndl = InitTerm(); // Configure the UART UART_control(tUartHndl, UART_CMD_RXDISABLE, NULL); //remove uart receive from LPDS dependency /* Create the sl_Task */ pthread_attr_init(&pAttrs_spawn); priParam.sched_priority = SPAWN_TASK_PRIORITY; retc = pthread_attr_setschedparam(&pAttrs_spawn, &priParam); retc |= pthread_attr_setstacksize(&pAttrs_spawn, TASKSTACKSIZE); retc |= pthread_attr_setdetachstate(&pAttrs_spawn, PTHREAD_CREATE_DETACHED); retc = pthread_create(&spawn_thread, &pAttrs_spawn, sl_Task, NULL); if (retc != 0) { UART_PRINT("could not create simplelink task\n\r"); while (1); } retc = sl_Start(0, 0, 0); if (retc < 0) { UART_PRINT("\n sl_Start failed\n"); /* Handle Error */ while(1); } retc = DisplayAppBanner(APPLICATION_NAME, APPLICATION_VERSION); /* Output device information to the UART terminal */ retc = sl_Stop(SL_STOP_TIMEOUT ); if (retc < 0) { UART_PRINT("\n sl_Stop failed\n"); /* Handle Error */ while(1); } if(retc < 0) { UART_PRINT("mqtt_client - Unable to retrieve device information \n"); /* Handle Error */ while (1); } while (1) { gResetApplication = false; gInitState = 0; gApConnectionState = Mqtt_IF_Connect(); gInitState |= MQTT_INIT_STATE; Mqtt_start(); while (gInitState != 0) { UART_PRINT("."); sleep(1); } UART_PRINT(".\r\n"); while (gResetApplication == false); UART_PRINT("TO Complete - Closing all threads and resources\r\n"); Mqtt_Stop(); UART_PRINT("reopen MQTT # %d \r\n", ++count); } }