# # reboot # Stopping iptables: /etc/init.d/S99NAT: line 110: arithmetic syntax error Stopping udhcpd: OK Stopping IPsec... Stopping stunnel: FAIL Stopping ProFTPD: done Stopping dropbear sshd: OK Stopping ntpd: FAIL Stopping network...Saving random seed... done. Stopping logging: OK umount: /dev/mmcblk0p1 busy - remounted read-only umount: sysfs busy - remounted read-only umount: tmpfs busy - remounted read-only umount: can't remount tmpfs read-only umount: devtmpfs busy - remounted read-only umount: can't remount /dev/root read-only umount: can't remount rootfs read-only The system is going down NOW! wlan1: interface state ENABLED->DISABLED wlan1: AP-DISABLED rmdir[ctrl_interface=/var/run/hostapd]: Read-only file system nl80211: deinit ifname=wlan1 disabled_11b_rates=0 Sent SIGTERM to all processes nl80211: Failed to open /proc/sys/net/ipv4/conf/[ 379.770515] wlcore: down mesh0/drop_unicast_in_l2_multicast: No such file or directory nl80211: Failed to set IPv4 unica[ 379.781667] wlcore: down st in multicast filter nl80211: deinit ifname=mesh0 disabled_11b_rates=0 Sent SIGKILL to all processes Requesting system reboot [ 381.757301] musb-hdrc musb-hdrc.1.auto: remove, state 4 [ 381.762868] usb usb2: USB disconnect, device number 1 [ 381.768780] musb-hdrc musb-hdrc.1.auto: USB bus 2 deregistered [ 381.775025] musb-hdrc musb-hdrc.0.auto: remove, state 4 [ 381.780541] usb usb1: USB disconnect, device number 1 [ 381.786307] musb-hdrc musb-hdrc.0.auto: USB bus 1 deregistered [ 381.792935] reboot: Restarting system U-Boot SPL 2014.07 (Sep 12 2018 - 13:21:36) [enable_pin_mux] Using default environment U-Boot 2014.07 (Sep 12 2018 - 13:21:36) I2C: ready DRAM: 512 MiB [board_init ] enable watchdog [board_init] gpio init BUZZER setbuzzer set111 [board_init]GPMC init done [board_init] cs eth init MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Net: [board_eth_init] start [board_eth_init] atop init phy [board_eth_init] cpsw_register [board_eth_init] FIBER CONFIG [board_eth_init] Select RMII2_CRS_DV on GPMC_A9 pin. [board_eth_init] Set eth1 Isolate. [board_eth_init] ***Set eth0 basic control reg. cpsw [main_loop] boot Hit ESC to execute ATOP menu: switch to partitions #0, OK mmc1(part 0) is current device MMC read: dev # 1, block # 2816, count 1280 ... 1280 blocks read: OK Wait ... 0 MMC read: dev # 1, block # 4096, count 20480 ... 20480 blocks read: OK MMC read: dev # 1, block # 24576, count 40960 ... 40960 blocks read: OK Booting from ramdisk ... Kernel image @ 0x82000000 [ 0x000000 - 0x3d2540 ] ## Loading init Ramdisk from Legacy Image at 84080000 ... Image Name: RootFS Created: 2018-09-28 2:58:46 UTC Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 15801599 Bytes = 15.1 MiB Load Address: 00000000 Entry Point: 00000000 Verifying Checksum ... OK ## Flattened Device Tree blob at 84000000 Booting using the fdt blob at 0x84000000 Loading Ramdisk to 870ee000, end 87fffcff ... OK Loading Device Tree to 870e2000, end 870ed0b4 ... OK [ARM announce]Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 3.14.26-svn1801 (jove@jove-VirtualBox) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #15 Fri Sep 28 10:54:35 CST 2018 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x EVM [ 0.000000] cma: CMA: reserved 16 MiB at 9e800000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129792 [ 0.000000] Kernel command line: console=ttyO0,115200n8 ramdisk_size=800000 root=/dev/ram0 rw bootloader_ver=1.3 rootfstype=ext2 [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 478444K/523264K available (5367K kernel code, 293K rwdata, 1940K rodata, 292K init, 401K bss, 44820K reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc072b1c0 (7309 kB) [ 0.000000] .init : 0xc072c000 - 0xc077527c ( 293 kB) [ 0.000000] .data : 0xc0776000 - 0xc07bf778 ( 294 kB) [ 0.000000] .bss : 0xc07bf778 - 0xc0823dc0 ( 402 kB) [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns [ 0.000031] OMAP clocksource: timer1 at 24000000 Hz [ 0.000303] Console: colour dummy device 80x30 [ 0.000329] Calibrating delay loop... 794.62 BogoMIPS (lpj=397312) [ 0.006481] pid_max: default: 32768 minimum: 301 [ 0.006576] Security Framework initialized [ 0.006630] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.006640] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.013275] CPU: Testing write buffer coherency: ok [ 0.013709] Setting up static identity map for 0x805148b0 - 0x80514920 [ 0.014904] devtmpfs: initialized [ 0.016679] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.022872] omap_hwmod: tptc0 using broken dt data from edma [ 0.022944] omap_hwmod: tptc1 using broken dt data from edma [ 0.023008] omap_hwmod: tptc2 using broken dt data from edma [ 0.026970] omap_hwmod: debugss: _wait_target_disable failed [ 0.080747] pinctrl core: initialized pinctrl subsystem [ 0.081851] regulator-dummy: no parameters [ 0.083661] NET: Registered protocol family 16 [ 0.085616] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.087190] cpuidle: using governor ladder [ 0.087203] cpuidle: using governor menu [ 0.095732] platform 49000000.edma: alias fck already exists [ 0.095759] platform 49000000.edma: alias fck already exists [ 0.095772] platform 49000000.edma: alias fck already exists [ 0.096903] OMAP GPIO hardware version 0.1 [ 0.110028] No ATAGs? [ 0.110049] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.129045] bio: create slab at 0 [ 0.142446] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.143419] vmmcsd_fixed: 3300 mV [ 0.143969] wlan-en-regulator: 3300 mV [ 0.145330] usbcore: registered new interface driver usbfs [ 0.145521] usbcore: registered new interface driver hub [ 0.145745] usbcore: registered new device driver usb [ 0.146609] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins_default, deferring probe [ 0.146634] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral [ 0.148582] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.150768] Switched to clocksource timer1 [ 0.186522] NET: Registered protocol family 2 [ 0.187373] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.187430] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.187476] TCP: Hash tables configured (established 4096 bind 4096) [ 0.187545] TCP: reno registered [ 0.187556] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.187573] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.187755] NET: Registered protocol family 1 [ 0.188127] RPC: Registered named UNIX socket transport module. [ 0.188140] RPC: Registered udp transport module. [ 0.188146] RPC: Registered tcp transport module. [ 0.188152] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.189043] Trying to unpack rootfs image as initramfs... [ 0.190333] rootfs image is not initramfs (no cpio magic); looks like an initrd [ 0.274683] Freeing initrd memory: 15428K (c70ee000 - c7fff000) [ 0.275040] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available [ 0.278143] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.432247] NFS: Registering the id_resolver key type [ 0.432340] Key type id_resolver registered [ 0.432348] Key type id_legacy registered [ 0.432389] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.432573] msgmni has been set to 996 [ 0.434142] io scheduler noop registered [ 0.434156] io scheduler deadline registered [ 0.434179] io scheduler cfq registered (default) [ 0.435884] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.437237] Serial: 8250/16550 driver, 48 ports, IRQ sharing enabled [ 0.454447] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.454604] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0 [ 1.051896] console [ttyO0] enabled [ 1.056399] omap_uart 48022000.serial: no wakeirq for uart0 [ 1.062411] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a OMAP UART1 [ 1.073039] omap_uart 48024000.serial: no wakeirq for uart0 [ 1.079017] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 90, base_baud = 3000000) is a OMAP UART2 [ 1.090357] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 1.107891] brd: module loaded [ 1.116588] loop: module loaded [ 1.120276] (hci_tty): inside hci_tty_init [ 1.125058] (hci_tty): allocated 251, 0 [ 1.130721] Atop update device initialize success. [ 1.136487] atop_relay.8: [ 1.139187] Register atop_relay0 success. [ 1.145491] ATOP Do Driver Install [ 1.150603] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.157895] bonding: Ethernet Channel Bonding Driver: v3.7.1 (April 27, 2011) [ 1.171439] PPP generic driver version 2.4.2 [ 1.176446] PPP MPPE Compression module registered [ 1.181508] NET: Registered protocol family 24 [ 1.186218] PPTP driver version 0.8.5 [ 1.190607] usbcore: registered new interface driver cdc_ether [ 1.196957] usbcore: registered new interface driver smsc95xx [ 1.203170] usbcore: registered new interface driver rndis_host [ 1.209616] usbcore: registered new interface driver cdc_ncm [ 1.215579] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.222446] ehci-omap: OMAP-EHCI Host Controller driver [ 1.228218] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 1.234748] ohci-platform: OHCI generic platform driver [ 1.240818] usbcore: registered new interface driver usbserial [ 1.247100] usbcore: registered new interface driver option [ 1.253113] usbserial: USB Serial support registered for GSM modem (1-port) [ 1.262469] 47401300.usb-phy supply vcc not found, using dummy regulator [ 1.272037] musb-hdrc musb-hdrc.0.auto: Failed to request rx1. [ 1.278255] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.286438] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.294856] 47401b00.usb-phy supply vcc not found, using dummy regulator [ 1.304290] musb-hdrc musb-hdrc.1.auto: Failed to request rx1. [ 1.310481] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 1.318657] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 1.340557] input: beeper.9 as /devices/beeper.9/input/input0 [ 1.348334] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.355817] 44e3e000.rtc: already running [ 1.360505] i2c /dev entries driver [ 1.470452] omap_hsmmc 48060000.mmc: card claims to support voltages below defined range [ 1.489413] mmc0: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.497832] oprofile: using arm/armv7 [ 1.501805] Netfilter messages via NETLINK v0.30. [ 1.506781] nf_conntrack version 0.5.0 (7972 buckets, 31888 max) [ 1.513354] ctnetlink v0.93: registering with nfnetlink. [ 1.519153] gre: GRE over IPv4 demultiplexor driver [ 1.524288] ip_gre: GRE over IPv4 tunneling driver [ 1.531648] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.537377] TCP: cubic registered [ 1.540875] Initializing XFRM netlink socket [ 1.545440] NET: Registered protocol family 10 [ 1.551467] sit: IPv6 over IPv4 tunneling driver [ 1.558757] NET: Registered protocol family 17 [ 1.563519] NET: Registered protocol family 15 [ 1.568252] Bridge firewalling registered [ 1.572539] 8021q: 802.1Q VLAN Support v1.8 [ 1.576995] Key type dns_resolver registered [ 1.582492] ondemand governor failed, too long transition latency of HW, fallback to performance governor [ 1.593352] PM: bootloader does not support rtc-only! [ 1.598737] ThumbEE CPU extension supported. [ 1.603276] Registering SWP/SWPB emulation handler [ 1.610139] regulator-dummy: disabling [ 1.614882] mmc0: new high speed SDIO card at address 0001 [ 1.623071] at24 0-0057: 8192 byte 24c64 EEPROM, writable, 1 bytes/write [ 1.679583] mmc1: BKOPS_EN bit is not set [ 1.686168] mmc1: new high speed MMC card at address 0001 [ 1.692533] mmcblk0: mmc1:0001 SEM08G 7.28 GiB [ 1.697479] mmcblk0boot0: mmc1:0001 SEM08G partition 1 2.00 MiB [ 1.704065] mmcblk0boot1: mmc1:0001 SEM08G partition 2 2.00 MiB [ 1.714760] mmcblk0: p1 [ 1.719561] mmcblk0boot1: unknown partition table [ 1.726337] mmcblk0boot0: unknown partition table [ 1.861918] rtc-pcf8563 0-0051: chip found, driver version 0.4.3 [ 1.869143] rtc-pcf8563 0-0051: rtc core: registered rtc-pcf8563 as rtc1 [ 1.876247] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.885608] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver [ 1.891689] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1 [ 1.900163] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 1.907320] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 1.914921] usb usb1: Product: MUSB HDRC host driver [ 1.920144] usb usb1: Manufacturer: Linux 3.14.26-svn1801 musb-hcd [ 1.926646] usb usb1: SerialNumber: musb-hdrc.0.auto [ 1.933004] hub 1-0:1.0: USB hub found [ 1.937004] hub 1-0:1.0: 1 port detected [ 1.944919] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver [ 1.950998] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2 [ 1.959410] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 1.966568] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 1.974166] usb usb2: Product: MUSB HDRC host driver [ 1.979393] usb usb2: Manufacturer: Linux 3.14.26-svn1801 musb-hcd [ 1.985890] usb usb2: SerialNumber: musb-hdrc.1.auto [ 1.992216] hub 2-0:1.0: USB hub found [ 1.996239] hub 2-0:1.0: 1 port detected [ 2.048808] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6 [ 2.055253] davinci_mdio 4a101000.mdio: detected phy mask fffffff4 [ 2.063630] libphy: 4a101000.mdio: probed [ 2.067876] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver unknown [ 2.076299] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver unknown [ 2.084717] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver unknown [ 2.093914] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT. [ 2.100703] cpsw 4a100000.ethernet: Using 1 as Reserved VLAN for 0 slave [ 2.107779] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT. [ 2.114552] cpsw 4a100000.ethernet: Using 2 as Reserved VLAN for 1 slave [ 2.121601] cpsw 4a100000.ethernet: Detected MACID = fc:69:47:bd:ef:06 [ 2.130193] cpsw 4a100000.ethernet: cpsw: Detected MACID = fc:69:47:bd:ef:08 [ 2.140062] input: gpio_keys.10 as /devices/gpio_keys.10/input/input1 [ 2.148108] rtc-pcf8563 0-0051: setting system clock to 2018-10-05 01:28:15 UTC (1538702895) [ 2.160714] RAMDISK: gzip image found at block 0 [ 2.551047] musb-hdrc musb-hdrc.0.auto: VBUS_ERROR in a_wait_vrise (80, [ 7.564648] bonding: bond0: Setting MII monitoring interval to 100. [ 7.571499] bonding: bond0: Setting fail_over_mac to active (1). [ 7.646715] net eth0: initializing cpsw version 1.12 (0) [ 7.708121] net eth0: phy found : id is : 0x221513 [ 7.720363] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 7.726505] 8021q: adding VLAN 0 to HW filter on device eth0 [ 7.744952] Unhandled fault: external abort on non-linefetch (0x1818) at 0xb6cf5050 Bus error [ 7.766487] net eth1: initializing cpsw version 1.12 (0) [ 7.828178] net eth1: phy found : id is : 0x221513 [ 7.840365] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 7.846507] 8021q: adding VLAN 0 to HW filter on device eth1 [ 7.864727] Unhandled fault: external abort on non-linefetch (0x1818) at 0xb6c31050 Bus error nameif: /etc/mactab: No such file or directory [ 7.911274] net eth0: initializing cpsw version 1.12 (0) [ 7.972153] net eth0: phy found : id is : 0x221513 [ 7.981857] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 7.988000] 8021q: adding VLAN 0 to HW filter on device eth0 [ 8.038538] net eth1: initializing cpsw version 1.12 (0) [ 8.100138] net eth1: phy found : id is : 0x221513 [ 8.109820] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 8.115978] 8021q: adding VLAN 0 to HW filter on device eth1 New Monit id: b262b200f3404dc112424aa8b5067e42 Stored in '//.monit.id' Starting Monit 5.18 daemon Monit start delay set -- pause for 10s Starting network... [ 8.597728] device eth0 entered promiscuous mode [ 8.630808] net eth0: initializing cpsw version 1.12 (0) [ 8.692158] net eth0: phy found : id is : 0x221513 [ 8.699483] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 8.705637] 8021q: adding VLAN 0 to HW filter on device eth0 net.ipv6.conf.eth0.accept_ra = 1 [ 8.757649] device eth1 entered promiscuous mode [ 8.789914] net eth1: initializing cpsw version 1.12 (0) [ 8.850172] net eth1: phy found : id is : 0x221513 [ 8.855511] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 8.861659] 8021q: adding VLAN 0 to HW filter on device eth1 net.ipv6.conf.eth1.accept_ra = 1 Starting WIFI ... lrwxrwxrwx 1 root root 10 Oct [ 8.909500] random: nonblocking pool is initialized 5 01:28 /jffs2 -> /mnt/jffs2
MESHssid=ATOP_Mesh3,MESHpsk=atop1234,dhcp_server=1,dhcpd_start=10,dhcpd_end=60 channel=1
wifi cmd=/jffs2/WifiMesh.sh 1 ATOP_AP1 atop5678 ATOP_Mesh3 2412 atop1234 1 192.168.3.100 255.255.255.0 192.168.4.200 255.255.255.0 192.168.4.254 1 & Segmentation fault [Mode] = 1 Starting ntpd: [AP SSID] = ATOP_AP1 [AP PSK]= atop5678 [Mesh SSID] = ATOP_Mesh3 [Mesh Freq] = 2412 [Mesh PSK] = atop1234 [Dhcpd] = 1 [IP] = 192.168.3.100 [Mask] = 255.255.255.0 [WAN IP] = 192.168.4.200 [WAN MASK] = 255.255.255.0 [WAN GATEWAY] = 192.168.4.254 [DHCPC] = 1 OK Starting dropbear sshd: OK Starting ProFTPD: [ 9.164275] warning: `proftpd' uses 32-bit capabilities (legacy support in use) done Starting stunnel: [.] stunnel 5.09 on arm-buildroot-linux-gnueabihf platform [.] Compiled/running with OpenSSL 1.0.2 22 Jan 2015 [.] Threading:FORK Sockets:POLL,IPv6 TLS:ENGINE,FIPS,OCSP,PSK,SNI [ ] errno: (*__errno_location ()) [.] Reading configuration from file /etc/stunnel/stunnel.conf [.] UTF-8 byte order mark detected [ ] Enabling support for engine "capi" [!] error queue: 2606A074: error:2606A074:engine routines:ENGINE_by_id:no such engine [!] ENGINE_by_id: 260B606D: error:260B606D:engine routines:DYNAMIC_LOAD:init failed [!] Line 18: "engine = capi": Failed to open the engine FAIL Starting IPsec... Mount debugfs [ 10.164861] Loading modules backported from Linux version R8.7_SP3-0-g8cbba96 [ 10.172398] Backport generated by backports.git R8.7_SP3-0-gd4777ef [ 10.703282] libphy: 4a101000.mdio:01 - Link is Up - 100/Full [ 10.709302] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 10.755347] libphy: 4a101000.mdio:03 - Link is Up - 100/Full [ 10.762052] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11) [ 10.769064] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready [ 10.810560] wlcore: loaded [ 10.813496] wlcore: driver version: R8.7_SP3 ################# driver done ################# adding mesh0 interface Successfully initialized wpa_supplicant [ 11.934039] wlcore: PHY firmware version: Rev 8.2.0.0.242 [ 12.025500] wlcore: firmware booted (Rev 8.9.0.0.79) [ 12.038790] IPv6: ADDRCONF(NETDEV_UP): mesh0: link is not ready Starting udhcpd: OK Starting PPTP... [ 12.497713] usbcore: deregistering interface driver GobiNet [ 12.542307] usbcore: deregistering interface driver cdc_xr_usb_serial Starting iptables: OK Welcome to ATOP system ATOP login: ################# mesh start ################# netid=0 ========================= OK OK OK OK OK OK mesh0: CTRL-EVENT-REGDOM-CHANGE init=BEACON_HINT type=UNKNOWN Using interface mesh0 with hwaddr 40:bd:32:89:3d[ 18.954593] wlcore: down :02 and ssid "" mesh0: interface state UNINITIALIZED->ENABLED AP-ENABLED [ 19.352209] wlcore: PHY firmware version: Rev 8.2.0.0.242 [ 19.490509] wlcore: firmware booted (Rev 8.9.0.0.79) [ 19.504670] IPv6: ADDRCONF(NETDEV_UP): mesh0: link is not ready random: Only 12/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool for secure operations - update keys later when the first station connects mesh0: joining mesh ATOP_Mesh3 [ 19.583861] IPv6: ADDRCONF(NETDEV_CHANGE): mesh0: link becomes ready mesh0: CTRL-EVENT-CONNECTED - Connection to 00:00:00:00:00:00 completed [id=0 id_str=] mesh0: MESH-GROUP-STARTED ssid="ATOP_Mesh3" id=0 mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 ################# mesh join done ################# adding wlan1 interface Configuration file: /jffs2/hostapd.conf [ 22.897828] IPv6: ADDRCONF(NETDEV_UP): wlan1: link is not ready wlan1: interface state UNINITIALIZED->COUNTRY_UPDATE mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 ################# AP Start ################# mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 ################# wlan0 down ################# Using interface wlan1 with hwaddr 42:bd:32:89:3d:01 and ssid "ATOP_AP1" [ 27.949683] device mesh0 entered promiscuous mode [ 27.983591] device wlan1 entered promiscuous mode random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 0/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool for secure operations - update[ 28.100750] IPv6: ADDRCONF(NETDEV_CHANGE): wlan1: link becomes ready keys later when the first station connects wlan1: interface state COUNTRY_UPDATE->ENABLED wlan1: AP-ENABLED mesh0: CTRL-EVENT-SCAN-FAILED ret=-16 retry=1 mesh0: mesh plink with 40:bd:32:89:33:35 established mesh0: ===> PLINKS NUMBER: 1 mesh0: MESH-PEER-CONNECTED 40:bd:32:89:33:35 ################# PrimaryAP bridge eth1 mesh0 wlan1 ################# ################# udhcp done ################# mesh0: CTRL-EVENT-REGDOM-CHANGE init=BEACON_HINT type=UNKNOWN [ 33.079428] net eth0: initializing cpsw version 1.12 (0) [ 33.138139] net eth0: phy found : id is : 0x221513 [ 33.143544] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 33.149716] 8021q: adding VLAN 0 to HW filter on device eth0 udhcpc (v1.23.1) started Sending discover... [ 35.038302] libphy: 4a101000.mdio:01 - Link is Up - 100/Full [ 35.044323] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready Sending discover... Sending select for 192.168.4.231... Lease of 192.168.4.231 obtained, lease time 86400 deleting routers adding dns 168.95.1.1 adding dns 8.8.8.8 ################# Set up WAN IP address done ################# ################# NAT done ################# wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: authenticated wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: associated (aid 1) random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 0/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool to proceed - reject first 4-way handshake wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: authenticated wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: associated (aid 1) random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 0/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool to proceed - reject first 4-way handshake wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: authenticated wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: associated (aid 1) random: Only 4/20 bytes of strong random data available from /dev/random random: Allow operation to proceed based on internal entropy wlan1: AP-STA-CONNECTED ac:fd:ce:89:e4:dc wlan1: STA ac:fd:ce:89:e4:dc WPA: pairwise key handshake completed (RSN) Welcome to ATOP system ATOP login: root Password: # ifconfig br0 Link encap:Ethernet HWaddr 40:BD:32:89:3D:02 inet addr:192.168.3.100 Bcast:192.168.3.255 Mask:255.255.255.0 inet6 addr: fe80::42bd:32ff:fe89:3d02/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:1157 errors:0 dropped:0 overruns:0 frame:0 TX packets:139 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:158226 (154.5 KiB) TX bytes:20910 (20.4 KiB) eth0 Link encap:Ethernet HWaddr 00:60:E9:15:18:17 inet addr:192.168.4.231 Bcast:192.168.4.255 Mask:255.255.255.0 inet6 addr: fe80::260:e9ff:fe15:1817/64 Scope:Link UP BROADCAST RUNNING PROMISC MULTICAST MTU:1500 Metric:1 RX packets:5937 errors:0 dropped:6 overruns:0 frame:0 TX packets:128 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:898058 (877.0 KiB) TX bytes:19987 (19.5 KiB) Interrupt:56 eth1 Link encap:Ethernet HWaddr 00:60:E9:15:18:18 inet6 addr: fe80::260:e9ff:fe15:1818/64 Scope:Link UP BROADCAST RUNNING PROMISC MULTICAST MTU:1500 Metric:1 RX packets:863 errors:0 dropped:0 overruns:0 frame:0 TX packets:705 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:93128 (90.9 KiB) TX bytes:149606 (146.0 KiB) lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:2 errors:0 dropped:0 overruns:0 frame:0 TX packets:2 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:196 (196.0 B) TX bytes:196 (196.0 B) mesh0 Link encap:Ethernet HWaddr 40:BD:32:89:3D:02 inet6 addr: fe80::42bd:32ff:fe89:3d02/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:5 errors:0 dropped:0 overruns:0 frame:0 TX packets:1132 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:732 (732.0 B) TX bytes:213999 (208.9 KiB) wlan1 Link encap:Ethernet HWaddr 42:BD:32:89:3D:01 inet6 addr: fe80::40bd:32ff:fe89:3d01/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:549 errors:0 dropped:0 overruns:0 frame:0 TX packets:1162 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:126624 (123.6 KiB) TX bytes:203562 (198.7 KiB) # wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: authenticated wlan1: STA ac:fd:ce:89:e4:dc IEEE 802.11: associated (aid 1) wlan1: STA ac:fd:ce:89:e4:dc WPA: pairwise key handshake completed (RSN) # cat /jffs2/user_pre.sh #!/bin/sh cp -f /jffs2/wlcore_sdio.ko /lib/modules/3.14.26-svn1801/updates/drivers/net/wireless/ti/wlcore/wlcore_sdio.ko cp -f /jffs2/wl18xx.ko /lib/modules/3.14.26-svn1801/updates/drivers/net/wireless/ti/wl18xx/wl18xx.ko cp -f /jffs2/wlcore.ko /lib/modules/3.14.26-svn1801/updates/drivers/net/wireless/ti/wlcore/wlcore.ko cp -f /jffs2/mac80211.ko /lib/modules/3.14.26-svn1801/updates/net/mac80211/mac80211.ko cp -f /jffs2/cfg80211.ko /lib/modules/3.14.26-svn1801/updates/net/wireless/cfg80211.ko cp -f /jffs2/compat.ko /lib/modules/3.14.26-svn1801/updates/compat/compat.ko # mesh0: mesh plink with 40:bd:32:89:33:35 closed with reason 55 mesh0: MESH-PEER-DISCONNECTED 40:bd:32:89:33:35 [ 820.554845] Unable to handle kernel NULL pointer dereference at virtual address 0000005d [ 820.563373] pgd = dcb6c000 [ 820.566217] [0000005d] *pgd=9717d831, *pte=00000000, *ppte=00000000 [ 820.572867] Internal error: Oops: 17 [#1] ARM [ 820.577439] Modules linked in: wlcore_sdio(O) wl18xx(O) wlcore(O) mac80211(O) cfg80211(O) compat(O) [last unloaded: xr] [ 820.588794] CPU: 0 PID: 1111 Comm: wpa_supplicant Tainted: G O 3.14.26-svn1801 #15 [ 820.597650] task: d715c080 ti: d9c1c000 task.ti: d9c1c000 [ 820.603867] PC is at mesh_get_low_signal_link+0x24/0x6c [mac80211] [ 820.610516] LR is at ieee80211_get_low_signal_mesh+0x10/0x34 [mac80211] [ 820.617457] pc : [] lr : [] psr: 800f0013 [ 820.617457] sp : d9c1dca8 ip : dcb44fb0 fp : 00000000 [ 820.629496] r10: dcb44000 r9 : de1dab90 r8 : d71894e8 [ 820.634980] r7 : d9c1dcf4 r6 : dcb44160 r5 : d7189000 r4 : d9c1dcc2 [ 820.641826] r3 : d7098000 r2 : 00000000 r1 : d7189000 r0 : 00000000 [ 820.648679] Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user [ 820.656160] Control: 10c5387d Table: 9cb6c019 DAC: 00000015 [ 820.662193] Process wpa_supplicant (pid: 1111, stack limit = 0xd9c1c238) [ 820.669222] Stack: (0xd9c1dca8 to 0xd9c1e000) [ 820.673785] dca0: bf0727a4 d7098000 bf07e2f4 bf043f58 bf072dcc d9c1dcf4 [ 820.682365] dcc0: 00000001 d7317680 de1dab80 bf07e2f4 dcb60800 bf072dcc d7317680 de1dab80 [ 820.690950] dce0: 00000000 c041a724 bf0727a4 c0417354 00000002 5bb6bec3 65800457 de1dab80 [ 820.699529] dd00: de1dab90 de1dab94 dcb60800 dcb44000 d7189000 de129800 de1dab80 d7317680 [ 820.708107] dd20: c041a518 d7317680 d9c1dd5c 00000000 00000000 c0419c18 c07b303c d7317680 [ 820.716702] dd40: d718ac00 c0419da8 c0419d88 de129800 0000001c c04195e0 0000001c 7fffffff [ 820.725290] dd60: d9c1de90 d9c1df7c d9c1de10 d718ac00 0000001c 00000000 00000000 c0419994 [ 820.733857] dd80: 00000000 c03f5998 d718a400 d7317680 00000008 00000000 00000001 de0696c0 [ 820.742444] dda0: 00000000 00000457 00000000 00000000 00000000 c04196ec d715c080 d9c1de88 [ 820.751032] ddc0: 00000000 dd9f16c0 00000000 00000000 d9c1de88 c03e8144 00000000 00000000 [ 820.759614] dde0: 00000000 d9c1de10 d715c080 00000000 00000000 00000000 00000000 00000000 [ 820.768197] de00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 0000001c [ 820.776785] de20: dd9f16c0 d9c1dec8 d9c1dd9c d9c1df7c d9c1de88 d9c1de88 00000008 00000000 [ 820.785362] de40: d9c1df7c c03f4998 00000000 bef0b1f4 d9c1de88 d9c1df7c 0000001c c03e8d54 [ 820.793943] de60: d9c1de68 d9c1de68 00000040 d9c1de80 bef0bb24 c03e8a68 c078f890 00000000 [ 820.802531] de80: 001c398c 00003ea4 001cabc4 00000000 00000000 00000000 c078da20 c0074730 [ 820.811112] dea0: 00000000 d9c1c000 bef0b1a8 bef0b1ac ddb1aac0 bef0b1a8 00000004 00000000 [ 820.819692] dec0: 00000004 c03ed7e8 00000010 00000000 00000000 00000000 0ca69fc0 000000bf [ 820.828270] dee0: c07c0a80 c07c0904 00000002 c003dda8 c07a6a20 00015200 00005411 c03e9278 [ 820.836842] df00: 00005452 0000000d 00000000 c00ef91c 95cfe133 00000004 ffffffff 00000000 [ 820.845430] df20: 00000001 d9c1df78 d9c1c000 bef0bc40 00000001 bef0bc40 00000008 bef0bb24 [ 820.854019] df40: 00000000 bef0b1f4 00000000 dd9f16c0 bef0b1f4 00000000 00000128 c000e524 [ 820.862602] df60: d9c1c000 00000000 00000032 c03ea1a4 bef0b1a4 00000000 fffffff7 d9c1dec8 [ 820.871196] df80: 0000000c d9c1de88 00000001 00000000 00000000 00000000 001b2398 001b2320 [ 820.879785] dfa0: 001b83c0 c000e3a0 001b2398 001b2320 00000005 bef0b1f4 00000000 00000000 [ 820.888365] dfc0: 001b2398 001b2320 001b83c0 00000128 bef0b1f4 00000033 00000089 00000032 [ 820.896937] dfe0: 00000000 bef0b1b4 b6db6d5d b6ddf9fc 600f0010 00000005 5f767264 5f746573 [ 820.905880] [] (mesh_get_low_signal_link [mac80211]) from [] (ieee80211_get_low_signal_mesh+0x10/0x34 [mac80211]) [ 820.918889] [] (ieee80211_get_low_signal_mesh [mac80211]) from [] (nl80211_get_low_signal_mesh+0x6c/0x1d0 [cfg80211]) [ 820.931983] [] (nl80211_get_low_signal_mesh [cfg80211]) from [] (genl_rcv_msg+0x20c/0x368) [ 820.942492] [] (genl_rcv_msg) from [] (netlink_rcv_skb+0xac/0xc0) [ 820.950723] [] (netlink_rcv_skb) from [] (genl_rcv+0x20/0x34) [ 820.958582] [] (genl_rcv) from [] (netlink_unicast+0x178/0x1e0) [ 820.966616] [] (netlink_unicast) from [] (netlink_sendmsg+0x2a8/0x388) [ 820.975306] [] (netlink_sendmsg) from [] (sock_sendmsg+0x84/0xa4) [ 820.983539] [] (sock_sendmsg) from [] (___sys_sendmsg.part.25+0x268/0x278) [ 820.992567] [] (___sys_sendmsg.part.25) from [] (__sys_sendmsg+0x4c/0x78) [ 821.001523] [] (__sys_sendmsg) from [] (ret_fast_syscall+0x0/0x30) [ 821.009838] Code: e59d3004 e153000c 0a000010 e5932064 (e5d2105d) [ 821.016473] ---[ end trace df2f0bd9b9957bcc ]---