=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2014.05.05 16:30:46 =~=~=~=~=~=~=~=~=~=~=~= CCCCCCCC U-Boot SPL 2011.09 (Feb 09 2012 - 15:38:59) Texas Instruments Revision detection unimplemented OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Feb 09 2012 - 15:11:31) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled Found a daughter card connected NAND: HW ECC Hamming Code selected 256 MiB MMC: OMAP SD/MMC: 0 Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed NAND read from offset 260000 failed -74 *** Warning - readenv() failed, using default environment Net: cpsw Hit any key to stop autoboot: 3  2  1  0 SD/MMC found on device 0 reading uEnv.txt ** Unable to read "uEnv.txt" from mmc 0:1 ** reading uImage 2922160 bytes read ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Arago/3.1.0-psp04.06.00.03.sdk/a Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2922096 Bytes = 2.8 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.1.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Feb 9 14:58:49 CST 2012 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f [ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253724k/253724k available, 8420k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] DMA : 0xffa00000 - 0xffe00000 ( 4 MB) [ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc0534000 (5296 kB) [ 0.000000] .init : 0xc0534000 - 0xc056d000 ( 228 kB) [ 0.000000] .data : 0xc056e000 - 0xc05c2d80 ( 340 kB) [ 0.000000] .bss : 0xc05c2da4 - 0xc05fd320 ( 234 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz [ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000199] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.059022] pid_max: default: 32768 minimum: 301 [ 0.059146] Security Framework initialized [ 0.059250] Mount-cache hash table entries: 512 [ 0.059619] CPU: Testing write buffer coherency: ok [ 0.064165] print_constraints: dummy: [ 0.064539] NET: Registered protocol family 16 [ 0.064885] GPMC revision 6.0 [ 0.066887] OMAP GPIO hardware version 0.1 [ 0.069006] omap_l3_smx omap_l3_smx.0: couldn't find resource [ 0.069770] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.072754] omap_i2c.1: alias fck already exists [ 0.074209] omap2_mcspi.1: alias fck already exists [ 0.074422] omap2_mcspi.2: alias fck already exists [ 0.096899] bio: create slab at 0 [ 0.098622] SCSI subsystem initialized [ 0.101037] usbcore: registered new interface driver usbfs [ 0.101371] usbcore: registered new interface driver hub [ 0.101584] usbcore: registered new device driver usb [ 0.119148] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz [ 0.121140] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.122180] Switching to clocksource gp timer [ 0.129107] Switched to NOHz mode on CPU #0 [ 0.137539] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.137728] musb-hdrc musb-hdrc.0: dma type: pio [ 0.138568] musb-hdrc musb-hdrc.0: USB OTG mode controller at d080a000 using PIO, IRQ 18 [ 0.138749] musb-hdrc musb-hdrc.1: dma type: pio [ 0.139451] musb-hdrc musb-hdrc.1: USB OTG mode controller at d080c800 using PIO, IRQ 19 [ 0.139854] NET: Registered protocol family 2 [ 0.140051] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.140342] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.140503] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.140598] TCP: Hash tables configured (established 8192 bind 8192) [ 0.140610] TCP reno registered [ 0.140623] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.140645] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.140829] NET: Registered protocol family 1 [ 0.141125] RPC: Registered named UNIX socket transport module. [ 0.141140] RPC: Registered udp transport module. [ 0.141149] RPC: Registered tcp transport module. [ 0.141158] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.141383] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.154353] VFS: Disk quotas dquot_6.5.2 [ 0.154423] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.154966] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.155251] msgmni has been set to 495 [ 0.156019] io scheduler noop registered [ 0.156033] io scheduler deadline registered [ 0.156107] io scheduler cfq registered (default) [ 0.159496] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.161166] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.632249] console [ttyO0] enabled [ 0.636455] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.644232] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.651879] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.659574] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.667257] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.683632] brd: module loaded [ 0.691399] loop: module loaded [ 0.695135] i2c-core: driver [tsl2550] using legacy suspend method [ 0.701578] i2c-core: driver [tsl2550] using legacy resume method [ 0.708028] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.715930] Detected a daughter card on AM335x EVM.. [ 0.720960] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.736351] Board name: A33515BB [ 0.739712] Board version: 1.2A [ 0.742993] SKU: SKU#01 [ 0.746088] The board is general purpose EVM in profile 0 [ 0.751713] Found invalid GP EVM revision, falling back to Rev1.1A [ 0.758856] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 0.779681] Console: switching to colour frame buffer device 100x30 [ 0.792131] TSC connected to beta GP EVM [ 0.797332] omap_i2c.2: alias fck already exists [ 0.822266] omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz [ 0.828609] tsl2550 2-0039: standard operating mode [ 0.834408] tsl2550 2-0039: support ver. 1.2 enabled [ 0.840319] omap_hsmmc.0: alias fck already exists [ 0.845776] omap_hsmmc.2: alias fck already exists [ 0.851122] Configure Bluetooth Enable pin... [ 0.855753] _omap_mux_get_by_name: Could not find signal gpmc_a8.gpio1_22 [ 0.864462] lis3lv02d: 8 bits 3DLH sensor found [ 0.942611] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 0.953513] mtdoops: mtd device (mtddev=name/number) must be supplied [ 0.960424] omap2-nand driver initializing [ 0.965118] ONFI flash detected [ 0.968513] ONFI param page 0 valid [ 0.972159] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 0.980552] Creating 8 MTD partitions on "omap2-nand.0": [ 0.986109] 0x000000000000-0x000000020000 : "SPL" [ 0.992787] 0x000000020000-0x000000040000 : "SPL.backup1" [ 0.999680] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.006675] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.013620] 0x000000080000-0x000000260000 : "U-Boot" [ 1.020805] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.027679] 0x000000280000-0x000000780000 : "Kernel" [ 1.036119] 0x000000780000-0x000010000000 : "File System" [ 1.145339] OneNAND driver initializing [ 1.192242] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.198697] davinci_mdio davinci_mdio.0: detected phy mask fffffffe [ 1.205950] davinci_mdio.0: probed [ 1.209501] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.217043] CAN device driver interface [ 1.221038] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.227412] usbcore: registered new interface driver cdc_ether [ 1.233721] usbcore: registered new interface driver cdc_subset [ 1.239937] Initializing USB Mass Storage driver... [ 1.245226] usbcore: registered new interface driver usb-storage [ 1.251489] USB Mass Storage support registered. [ 1.256369] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 1.261977] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 1.269818] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 1.276913] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 1.284453] usb usb1: Product: MUSB HDRC host driver [ 1.289624] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd [ 1.295167] usb usb1: SerialNumber: musb-hdrc.1 [ 1.300690] hub 1-0:1.0: USB hub found [ 1.304664] hub 1-0:1.0: 1 port detected [ 1.309832] mousedev: PS/2 mouse device common for all mice [ 1.316658] input: matrix-keypad as /devices/platform/matrix-keypad/input/input1 [ 1.325812] input: ti-tsc-adcc as /devices/platform/tsc/input/input2 [ 1.333937] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.340768] i2c /dev entries driver [ 1.346032] lm75 2-0048: hwmon0: sensor 'tmp275' [ 1.384502] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.391234] cpuidle: using governor ladder [ 1.396027] cpuidle: using governor menu [ 1.474181] usbcore: registered new interface driver usbhid [ 1.479996] usbhid: USB HID core driver [ 1.485050] usbcore: registered new interface driver snd-usb-audio [ 1.493608] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator [ 1.501383] _regulator_get: 2-001b supply DVDD not found, using dummy regulator [ 1.509094] _regulator_get: 2-001b supply AVDD not found, using dummy regulator [ 1.516758] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator [ 1.530147] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 1.549741] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.556589] mmc1: new SDIO card at address 0001 [ 1.583230] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.590734] ALSA device list: [ 1.593877] #0: AM335X EVM [ 1.596874] oprofile: hardware counters not available [ 1.602133] oprofile: using timer interrupt. [ 1.606622] nf_conntrack version 0.5.0 (3964 buckets, 15856 max) [ 1.613421] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.619072] TCP cubic registered [ 1.622470] NET: Registered protocol family 17 [ 1.627111] can: controller area network core (rev 20090105 abi 8) [ 1.633649] NET: Registered protocol family 29 [ 1.638284] can: raw protocol (rev 20090105) [ 1.642745] can: broadcast manager protocol (rev 20090105 t) [ 1.648680] Registering the dns_resolver key type [ 1.653677] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.661668] ThumbEE CPU extension supported. [ 1.666927] _regulator_get: mpu.0 supply mpu not found, using dummy regulator [ 1.674516] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=720000000 v=1260000)on vddmpu [ 1.683692] omap2_set_init_voltage: unable to set vdd_mpu [ 1.691306] Detected MACID=0:18:31:e0:8d:4a [ 1.697776] input: gpio-keys as /devices/platform/gpio-keys/input/input3 [ 1.705539] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 1.714761] Waiting for root device /dev/mmcblk0p2...