/* * MTD SPI driver for ST M25Pxx (and similar) serial flash chips * * Author: Mike Lavender, mike@steroidmicros.com * * Copyright (c) 2005, Intec Automation Inc. * * Some parts are based on lart.c by Abraham Van Der Merwe * * Cleaned up and generalized based on mtd_dataflash.c * * This code is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #include #include #include #include #include #include #include #include #include #include #define FLASH_PAGESIZE 256 /* Flash opcodes. */ #define OPCODE_WREN 0x06 /* Write enable */ #define OPCODE_RDSR 0x05 /* Read status register */ #define OPCODE_NORM_READ 0x03 /* Read data bytes (low frequency) */ #define OPCODE_FAST_READ 0x0b /* Read data bytes (high frequency) */ #define OPCODE_PP 0x02 /* Page program (up to 256 bytes) */ #define OPCODE_BE_4K 0x20 /* Erase 4K block */ #define OPCODE_BE_32K 0x52 /* Erase 32K block */ #define OPCODE_CHIP_ERASE 0xc7 /* Erase whole flash chip */ #define OPCODE_SE 0xd8 /* Sector erase (usually 64K) */ #define OPCODE_RDID 0x9f /* Read JEDEC ID */ /* Status Register bits. */ #define SR_WIP 1 /* Write in progress */ #define SR_WEL 2 /* Write enable latch */ /* meaning of other SR_* bits may differ between vendors */ #define SR_BP0 4 /* Block protect 0 */ #define SR_BP1 8 /* Block protect 1 */ #define SR_BP2 0x10 /* Block protect 2 */ #define SR_SRWD 0x80 /* SR write protect */ /* Define max times to check status register before we give up. */ #define MAX_READY_WAIT_COUNT 1000000 #define MAX_READY_WAIT_JIFFIES (10 * HZ) /* eg. M25P128 specs 6s max sector erase */ #define CMD_SIZE 4 #ifdef CONFIG_M25PXX_USE_FAST_READ #define OPCODE_READ OPCODE_FAST_READ #define FAST_READ_DUMMY_BYTE 1 #else #define OPCODE_READ OPCODE_NORM_READ #define FAST_READ_DUMMY_BYTE 0 #endif #ifdef CONFIG_MTD_PARTITIONS #define mtd_has_partitions() (1) #else #define mtd_has_partitions() (0) #endif /****************************************************************************/ struct m25p { struct spi_device *spi; struct semaphore lock; struct mtd_info mtd; unsigned partitioned:1; u8 erase_opcode; u8 command[CMD_SIZE + FAST_READ_DUMMY_BYTE ]; }; static inline struct m25p *mtd_to_m25p(struct mtd_info *mtd) { return container_of(mtd, struct m25p, mtd); } /****************************************************************************/ /* * Internal helper functions */ /* * Read the status register, returning its value in the location * Return the status register value. * Returns negative if error occurred. */ static int read_sr(struct m25p *flash) { ssize_t retval; u8 code = OPCODE_RDSR; u8 val; retval = spi_write_then_read(flash->spi, &code, 1, &val, 1); if (retval < 0) { dev_err(&flash->spi->dev, "error %d reading SR\n", (int) retval); return retval; } return val; } /* * Set write enable latch with Write Enable command. * Returns negative if error occurred. */ static inline int write_enable(struct m25p *flash) { u8 code = OPCODE_WREN; return spi_write_then_read(flash->spi, &code, 1, NULL, 0); } /* * Service routine to read status register until ready, or timeout occurs. * Returns non-zero if error. */ static int wait_till_ready(struct m25p *flash) { unsigned long deadline; int sr; deadline = jiffies + MAX_READY_WAIT_JIFFIES; do { if ((sr = read_sr(flash)) < 0) break; else if (!(sr & SR_WIP)) return 0; cond_resched(); } while (!time_after_eq(jiffies, deadline)); return 1; } /* * Erase the whole flash memory * * Returns 0 if successful, non-zero otherwise. */ static int erase_chip(struct m25p *flash) { DEBUG(MTD_DEBUG_LEVEL3, "%s: %s %dKiB\n", flash->spi->dev.bus_id, __func__, flash->mtd.size / 1024); /* Wait until finished previous write command. */ if (wait_till_ready(flash)) return 1; /* Send write enable, then erase commands. */ write_enable(flash); /* Set up command buffer. */ flash->command[0] = OPCODE_CHIP_ERASE; spi_write(flash->spi, flash->command, 1); return 0; } /* * Erase one sector of flash memory at offset ``offset'' which is any * address within the sector which should be erased. * * Returns 0 if successful, non-zero otherwise. */ static int erase_sector(struct m25p *flash, u32 offset) { DEBUG(MTD_DEBUG_LEVEL3, "%s: %s %dK at 0x%08x\n", flash->spi->dev.bus_id, __FUNCTION__, flash->mtd.erasesize / 1024, offset); /* Wait until finished previous write command. */ if (wait_till_ready(flash)) return 1; /* Send write enable, then erase commands. */ write_enable(flash); /* Set up command buffer. */ flash->command[0] = flash->erase_opcode; flash->command[1] = offset >> 16; flash->command[2] = offset >> 8; flash->command[3] = offset; spi_write(flash->spi, flash->command, sizeof(flash->command)); return 0; } /****************************************************************************/ /* * MTD implementation */ /* * Erase an address range on the flash chip. The address range may extend * one or more erase sectors. Return an error is there is a problem erasing. */ static int m25p80_erase(struct mtd_info *mtd, struct erase_info *instr) { struct m25p *flash = mtd_to_m25p(mtd); u32 addr,len; DEBUG(MTD_DEBUG_LEVEL2, "%s: %s %s 0x%08x, len %d\n", flash->spi->dev.bus_id, __FUNCTION__, "at", (u32)instr->addr, instr->len); /* sanity checks */ if (instr->addr + instr->len > flash->mtd.size) return -EINVAL; if ((instr->addr % mtd->erasesize) != 0 || (instr->len % mtd->erasesize) != 0) { return -EINVAL; } addr = instr->addr; len = instr->len; down(&flash->lock); /* whole-chip erase? */ if (len == flash->mtd.size) { if (erase_chip(flash)) { instr->state = MTD_ERASE_FAILED; up(&flash->lock); return -EIO; } /* REVISIT in some cases we could speed up erasing large regions * by using OPCODE_SE instead of OPCODE_BE_4K. We may have set up * to use "small sector erase", but that's not always optimal. */ /* "sector"-at-a-time erase */ } else { while (len) { if (erase_sector(flash, addr)) { instr->state = MTD_ERASE_FAILED; up(&flash->lock); return -EIO; } addr += mtd->erasesize; len -= mtd->erasesize; } } up(&flash->lock); instr->state = MTD_ERASE_DONE; mtd_erase_callback(instr); return 0; } /* * Read an address range from the flash chip. The address range * may be any size provided it is within the physical boundaries. */ static int m25p80_read(struct mtd_info *mtd, loff_t from, size_t len, size_t *retlen, u_char *buf) { struct m25p *flash = mtd_to_m25p(mtd); struct spi_transfer t[2]; struct spi_message m; DEBUG(MTD_DEBUG_LEVEL2, "%s: %s %s 0x%08x, len %zd\n", flash->spi->dev.bus_id, __FUNCTION__, "from", (u32)from, len); /* sanity checks */ if (!len) return 0; if (from + len > flash->mtd.size) return -EINVAL; spi_message_init(&m); memset(t, 0, (sizeof t)); /* NOTE: * OPCODE_FAST_READ (if available) is faster. * Should add 1 byte DUMMY_BYTE. */ t[0].tx_buf = flash->command; t[0].len = CMD_SIZE + FAST_READ_DUMMY_BYTE; spi_message_add_tail(&t[0], &m); t[1].rx_buf = buf; t[1].len = len; spi_message_add_tail(&t[1], &m); /* Byte count starts at zero. */ if (retlen) *retlen = 0; down(&flash->lock); /* Wait till previous write/erase is done. */ if (wait_till_ready(flash)) { /* REVISIT status return?? */ up(&flash->lock); return 1; } /* FIXME switch to OPCODE_FAST_READ. It's required for higher * clocks; and at this writing, every chip this driver handles * supports that opcode. */ /* Set up the write data buffer. */ flash->command[0] = OPCODE_READ; flash->command[1] = from >> 16; flash->command[2] = from >> 8; flash->command[3] = from; spi_sync(flash->spi, &m); *retlen = m.actual_length - CMD_SIZE - FAST_READ_DUMMY_BYTE; up(&flash->lock); return 0; } /* * Write an address range to the flash chip. Data must be written in * FLASH_PAGESIZE chunks. The address range may be any size provided * it is within the physical boundaries. */ static int m25p80_write(struct mtd_info *mtd, loff_t to, size_t len, size_t *retlen, const u_char *buf) { struct m25p *flash = mtd_to_m25p(mtd); u32 page_offset, page_size; struct spi_transfer t[2]; struct spi_message m; DEBUG(MTD_DEBUG_LEVEL2, "%s: %s %s 0x%08x, len %zd\n", flash->spi->dev.bus_id, __FUNCTION__, "to", (u32)to, len); if (retlen) *retlen = 0; /* sanity checks */ if (!len) return(0); if (to + len > flash->mtd.size) return -EINVAL; spi_message_init(&m); memset(t, 0, (sizeof t)); t[0].tx_buf = flash->command; t[0].len = CMD_SIZE; spi_message_add_tail(&t[0], &m); t[1].tx_buf = buf; spi_message_add_tail(&t[1], &m); down(&flash->lock); /* Wait until finished previous write command. */ if (wait_till_ready(flash)) return 1; write_enable(flash); /* Set up the opcode in the write buffer. */ flash->command[0] = OPCODE_PP; flash->command[1] = to >> 16; flash->command[2] = to >> 8; flash->command[3] = to; /* what page do we start with? */ page_offset = to % FLASH_PAGESIZE; /* do all the bytes fit onto one page? */ if (page_offset + len <= FLASH_PAGESIZE) { t[1].len = len; spi_sync(flash->spi, &m); *retlen = m.actual_length - CMD_SIZE; } else { u32 i; /* the size of data remaining on the first page */ page_size = FLASH_PAGESIZE - page_offset; t[1].len = page_size; spi_sync(flash->spi, &m); *retlen = m.actual_length - CMD_SIZE; /* write everything in PAGESIZE chunks */ for (i = page_size; i < len; i += page_size) { page_size = len - i; if (page_size > FLASH_PAGESIZE) page_size = FLASH_PAGESIZE; /* write the next page to flash */ flash->command[1] = (to + i) >> 16; flash->command[2] = (to + i) >> 8; flash->command[3] = (to + i); t[1].tx_buf = buf + i; t[1].len = page_size; wait_till_ready(flash); write_enable(flash); spi_sync(flash->spi, &m); if (retlen) *retlen += m.actual_length - CMD_SIZE; } } up(&flash->lock); return 0; } /****************************************************************************/ /* * SPI device driver setup and teardown */ struct flash_info { char *name; /* JEDEC id zero means "no ID" (most older chips); otherwise it has * a high byte of zero plus three data bytes: the manufacturer id, * then a two byte device id. */ u32 jedec_id; u16 ext_id; /* The size listed here is what works with OPCODE_SE, which isn't * necessarily called a "sector" by the vendor. */ unsigned sector_size; u16 n_sectors; u16 flags; #define SECT_4K 0x01 /* OPCODE_BE_4K works uniformly */ }; /* NOTE: double check command sets and memory organization when you add * more flash chips. This current list focusses on newer chips, which * have been converging on command sets which including JEDEC ID. */ static struct flash_info __devinitdata m25p_data [] = { /* Atmel -- some are (confusingly) marketed as "DataFlash" */ { "at25fs010", 0x1f6601, 0, 32 * 1024, 4, SECT_4K, }, { "at25fs040", 0x1f6604, 0, 64 * 1024, 8, SECT_4K, }, { "at25df041a", 0x1f4401, 0, 64 * 1024, 8, SECT_4K, }, { "at25df641", 0x1f4800, 0, 64 * 1024, 128, SECT_4K, }, { "at26f004", 0x1f0400, 0, 64 * 1024, 8, SECT_4K, }, { "at26df081a", 0x1f4501, 0, 64 * 1024, 16, SECT_4K, }, { "at26df161a", 0x1f4601, 0, 64 * 1024, 32, SECT_4K, }, { "at26df321", 0x1f4701, 0, 64 * 1024, 64, SECT_4K, }, /* Spansion -- single (large) sector size only, at least * for the chips listed here (without boot sectors). */ { "s25sl004a", 0x010212, 0, 64 * 1024, 8, }, { "s25sl008a", 0x010213, 0, 64 * 1024, 16, }, { "s25sl016a", 0x010214, 0, 64 * 1024, 32, }, { "s25sl032a", 0x010215, 0, 64 * 1024, 64, }, { "s25sl064a", 0x010216, 0, 64 * 1024, 128, }, { "s25sl12800", 0x012018, 0x0300, 256 * 1024, 64, }, { "s25sl12801", 0x012018, 0x0301, 64 * 1024, 256, }, /* SST -- large erase sizes are "overlays", "sectors" are 4K */ { "sst25vf040b", 0xbf258d, 0, 64 * 1024, 8, SECT_4K, }, { "sst25vf080b", 0xbf258e, 0, 64 * 1024, 16, SECT_4K, }, { "sst25vf016b", 0xbf2541, 0, 64 * 1024, 32, SECT_4K, }, { "sst25vf032b", 0xbf254a, 0, 64 * 1024, 64, SECT_4K, }, /* ST Microelectronics -- newer production may have feature updates */ { "m25p05", 0x202010, 0, 32 * 1024, 2, }, { "m25p10", 0x202011, 0, 32 * 1024, 4, }, { "m25p20", 0x202012, 0, 64 * 1024, 4, }, { "m25p40", 0x202013, 0, 64 * 1024, 8, }, { "m25p80", 0, 0, 64 * 1024, 16, }, { "m25p16", 0x202015, 0, 64 * 1024, 32, }, { "m25p32", 0x202016, 0, 64 * 1024, 64, }, { "m25p64", 0x202017, 0, 64 * 1024, 128, }, { "m25p128", 0x202018, 0, 256 * 1024, 64, }, { "m45pe80", 0x204014, 0, 64 * 1024, 16, }, { "m45pe16", 0x204015, 0, 64 * 1024, 32, }, { "m25pe80", 0x208014, 0, 64 * 1024, 16, }, { "m25pe16", 0x208015, 0, 64 * 1024, 32, SECT_4K, }, /* Winbond -- w25x "blocks" are 64K, "sectors" are 4KiB */ { "w25x10", 0xef3011, 0, 64 * 1024, 2, SECT_4K, }, { "w25x20", 0xef3012, 0, 64 * 1024, 4, SECT_4K, }, { "w25x40", 0xef3013, 0, 64 * 1024, 8, SECT_4K, }, { "w25x80", 0xef3014, 0, 64 * 1024, 16, SECT_4K, }, { "w25x16", 0xef3015, 0, 64 * 1024, 32, SECT_4K, }, { "w25x32", 0xef3016, 0, 64 * 1024, 64, SECT_4K, }, { "w25x64", 0xef3017, 0, 64 * 1024, 128, SECT_4K, }, }; static struct flash_info *__devinit jedec_probe(struct spi_device *spi) { int tmp; u8 code = OPCODE_RDID; u8 id[5]; u32 jedec; u16 ext_jedec; struct flash_info *info; /* JEDEC also defines an optional "extended device information" * string for after vendor-specific data, after the three bytes * we use here. Supporting some chips might require using it. */ tmp = spi_write_then_read(spi, &code, 1, id, 5); if (tmp < 0) { DEBUG(MTD_DEBUG_LEVEL0, "%s: error %d reading JEDEC ID\n", spi->dev.bus_id, tmp); return NULL; } jedec = id[0]; jedec = jedec << 8; jedec |= id[1]; jedec = jedec << 8; jedec |= id[2]; ext_jedec = id[3] << 8 | id[4]; for (tmp = 0, info = m25p_data; tmp < ARRAY_SIZE(m25p_data); tmp++, info++) { if (info->jedec_id == jedec) { if (info->ext_id != 0 && info->ext_id != ext_jedec) continue; return info; } } dev_err(&spi->dev, "unrecognized JEDEC id %06x\n", jedec); return NULL; } /* * board specific setup should have ensured the SPI clock used here * matches what the READ command supports, at least until this driver * understands FAST_READ (for clocks over 25 MHz). */ static int __devinit m25p_probe(struct spi_device *spi) { struct flash_platform_data *data; struct m25p *flash; struct flash_info *info; unsigned i; /* Platform data helps sort out which chip type we have, as * well as how this board partitions it. If we don't have * a chip ID, try the JEDEC id commands; they'll work for most * newer chips, even if we don't recognize the particular chip. */ data = spi->dev.platform_data; if (data && data->type) { for (i = 0, info = m25p_data; i < ARRAY_SIZE(m25p_data); i++, info++) { if (strcmp(data->type, info->name) == 0) break; } /* unrecognized chip? */ if (i == ARRAY_SIZE(m25p_data)) { DEBUG(MTD_DEBUG_LEVEL0, "%s: unrecognized id %s\n", spi->dev.bus_id, data->type); info = NULL; /* recognized; is that chip really what's there? */ } else if (info->jedec_id) { struct flash_info *chip = jedec_probe(spi); if (!chip || chip != info) { dev_warn(&spi->dev, "found %s, expected %s\n", chip ? chip->name : "UNKNOWN", info->name); info = NULL; } } } else info = jedec_probe(spi); if (!info) return -ENODEV; flash = kzalloc(sizeof *flash, SLAB_KERNEL); if (!flash) return -ENOMEM; flash->spi = spi; init_MUTEX(&flash->lock); dev_set_drvdata(&spi->dev, flash); if (data && data->name) flash->mtd.name = data->name; else flash->mtd.name = spi->dev.bus_id; flash->mtd.type = MTD_NORFLASH; flash->mtd.writesize = 1; flash->mtd.flags = MTD_CAP_NORFLASH; flash->mtd.size = info->sector_size * info->n_sectors; flash->mtd.erase = m25p80_erase; flash->mtd.read = m25p80_read; flash->mtd.write = m25p80_write; /* prefer "small sector" erase if possible */ if (info->flags & SECT_4K) { flash->erase_opcode = OPCODE_BE_4K; flash->mtd.erasesize = 4096; } else { flash->erase_opcode = OPCODE_SE; flash->mtd.erasesize = info->sector_size; } dev_info(&spi->dev, "%s (%d Kbytes)\n", info->name, flash->mtd.size / 1024); DEBUG(MTD_DEBUG_LEVEL2, "mtd .name = %s, .size = 0x%.8x (%uM) " ".erasesize = 0x%.8x (%uK) .numeraseregions = %d\n", flash->mtd.name, flash->mtd.size, flash->mtd.size / (1024*1024), flash->mtd.erasesize, flash->mtd.erasesize / 1024, flash->mtd.numeraseregions); if (flash->mtd.numeraseregions) for (i = 0; i < flash->mtd.numeraseregions; i++) DEBUG(MTD_DEBUG_LEVEL2, "mtd.eraseregions[%d] = { .offset = 0x%.8x, " ".erasesize = 0x%.8x (%uK), " ".numblocks = %d }\n", i, flash->mtd.eraseregions[i].offset, flash->mtd.eraseregions[i].erasesize, flash->mtd.eraseregions[i].erasesize / 1024, flash->mtd.eraseregions[i].numblocks); /* partitions should match sector boundaries; and it may be good to * use readonly partitions for writeprotected sectors (BP2..BP0). */ if (mtd_has_partitions()) { struct mtd_partition *parts = NULL; int nr_parts = 0; #ifdef CONFIG_MTD_CMDLINE_PARTS static const char *part_probes[] = { "cmdlinepart", NULL, }; nr_parts = parse_mtd_partitions(&flash->mtd, part_probes, &parts, 0); #endif if (nr_parts <= 0 && data && data->parts) { parts = data->parts; nr_parts = data->nr_parts; } if (nr_parts > 0) { for (i = 0; i < nr_parts; i++) { DEBUG(MTD_DEBUG_LEVEL2, "partitions[%d] = " "{.name = %s, .offset = 0x%.8x, " ".size = 0x%.8x (%uK) }\n", i, parts[i].name, parts[i].offset, parts[i].size, parts[i].size / 1024); } flash->partitioned = 1; return add_mtd_partitions(&flash->mtd, parts, nr_parts); } } else if (data->nr_parts) dev_warn(&spi->dev, "ignoring %d default partitions on %s\n", data->nr_parts, data->name); return add_mtd_device(&flash->mtd) == 1 ? -ENODEV : 0; } static int __devexit m25p_remove(struct spi_device *spi) { struct m25p *flash = dev_get_drvdata(&spi->dev); int status; /* Clean up MTD stuff. */ if (mtd_has_partitions() && flash->partitioned) status = del_mtd_partitions(&flash->mtd); else status = del_mtd_device(&flash->mtd); if (status == 0) kfree(flash); return 0; } static struct spi_driver m25p80_driver = { .driver = { .name = "m25p80", .bus = &spi_bus_type, .owner = THIS_MODULE, }, .probe = m25p_probe, .remove = __devexit_p(m25p_remove), /* REVISIT: many of these chips have deep power-down modes, which * should clearly be entered on suspend() to minimize power use. * And also when they're otherwise idle... */ }; static int m25p80_init(void) { return spi_register_driver(&m25p80_driver); } static void m25p80_exit(void) { spi_unregister_driver(&m25p80_driver); } module_init(m25p80_init); module_exit(m25p80_exit); MODULE_LICENSE("GPL"); MODULE_AUTHOR("Mike Lavender"); MODULE_DESCRIPTION("MTD SPI driver for ST M25Pxx flash chips");