Data Structures | |
| struct | EDMA3_DRV_ParamentryRegs |
| EDMA3 PaRAM Set. More... | |
| struct | EDMA3_DRV_PaRAMRegs |
| EDMA3 Parameter RAM Set in User Configurable format. More... | |
| struct | EDMA3_DRV_EvtQuePriority |
| Event queue priorities setup. More... | |
Enumerations | |
| enum | EDMA3_DRV_PaRAMEntry { EDMA3_DRV_PARAM_ENTRY_OPT = 0, EDMA3_DRV_PARAM_ENTRY_SRC = 1, EDMA3_DRV_PARAM_ENTRY_ACNT_BCNT = 2, EDMA3_DRV_PARAM_ENTRY_DST = 3, EDMA3_DRV_PARAM_ENTRY_SRC_DST_BIDX = 4, EDMA3_DRV_PARAM_ENTRY_LINK_BCNTRLD = 5, EDMA3_DRV_PARAM_ENTRY_SRC_DST_CIDX = 6, EDMA3_DRV_PARAM_ENTRY_CCNT = 7 } |
| PaRAM Set Entry type. More... | |
| enum | EDMA3_DRV_PaRAMField { EDMA3_DRV_PARAM_FIELD_OPT = 0, EDMA3_DRV_PARAM_FIELD_SRCADDR = 1, EDMA3_DRV_PARAM_FIELD_ACNT = 2, EDMA3_DRV_PARAM_FIELD_BCNT = 3, EDMA3_DRV_PARAM_FIELD_DESTADDR = 4, EDMA3_DRV_PARAM_FIELD_SRCBIDX = 5, EDMA3_DRV_PARAM_FIELD_DESTBIDX = 6, EDMA3_DRV_PARAM_FIELD_LINKADDR = 7, EDMA3_DRV_PARAM_FIELD_BCNTRELOAD = 8, EDMA3_DRV_PARAM_FIELD_SRCCIDX = 9, EDMA3_DRV_PARAM_FIELD_DESTCIDX = 10, EDMA3_DRV_PARAM_FIELD_CCNT = 11 } |
| PaRAM Set Field type. More... | |
| enum | EDMA3_DRV_IoctlCmd { EDMA3_DRV_IOCTL_MIN_IOCTL = 0, EDMA3_DRV_IOCTL_SET_PARAM_CLEAR_OPTION, EDMA3_DRV_IOCTL_GET_PARAM_CLEAR_OPTION, EDMA3_DRV_IOCTL_MAX_IOCTL } |
| EDMA3 Driver IOCTL commands. More... | |
Functions | |
| EDMA3_DRV_Result | EDMA3_DRV_setQdmaTrigWord (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_RM_QdmaTrigWord trigWord) |
| Assign a Trigger Word to the specified QDMA channel. | |
| EDMA3_DRV_Result | EDMA3_DRV_setPaRAM (EDMA3_DRV_Handle hEdma, unsigned int lCh, const EDMA3_DRV_PaRAMRegs *newPaRAM) |
| Copy the user specified PaRAM Set onto the PaRAM Set associated with the logical channel (DMA/QDMA/Link). | |
| EDMA3_DRV_Result | EDMA3_DRV_getPaRAM (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_DRV_PaRAMRegs *currPaRAM) |
| Retrieve existing PaRAM set associated with specified logical channel (DMA/QDMA/Link). | |
| EDMA3_DRV_Result | EDMA3_DRV_setPaRAMEntry (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_DRV_PaRAMEntry paRAMEntry, unsigned int newPaRAMEntryVal) |
| Set a particular PaRAM set entry of the specified PaRAM set. | |
| EDMA3_DRV_Result | EDMA3_DRV_getPaRAMEntry (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_DRV_PaRAMEntry paRAMEntry, unsigned int *paRAMEntryVal) |
| Get a particular PaRAM set entry of the specified PaRAM set. | |
| EDMA3_DRV_Result | EDMA3_DRV_setPaRAMField (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_DRV_PaRAMField paRAMField, unsigned int newPaRAMFieldVal) |
| Set a particular PaRAM set field of the specified PaRAM set. | |
| EDMA3_DRV_Result | EDMA3_DRV_getPaRAMField (EDMA3_DRV_Handle hEdma, unsigned int lCh, EDMA3_DRV_PaRAMField paRAMField, unsigned int *currPaRAMFieldVal) |
| Get a particular PaRAM set field of the specified PaRAM set. | |
| EDMA3_DRV_Result | EDMA3_DRV_setEvtQPriority (EDMA3_DRV_Handle hEdma, const EDMA3_DRV_EvtQuePriority *evtQPriObj) |
| Sets EDMA TC priority. | |
| EDMA3_DRV_Result | EDMA3_DRV_mapChToEvtQ (EDMA3_DRV_Handle hEdma, unsigned int channelId, EDMA3_RM_EventQueue eventQ) |
| Associate Channel to Event Queue. | |
| EDMA3_DRV_Result | EDMA3_DRV_getMapChToEvtQ (EDMA3_DRV_Handle hEdma, unsigned int channelId, unsigned int *mappedEvtQ) |
| Get the Event Queue mapped to the specified DMA/QDMA channel. | |
| EDMA3_DRV_Result | EDMA3_DRV_setCCRegister (EDMA3_DRV_Handle hEdma, unsigned int regOffset, unsigned int newRegValue) |
| Set the Channel Controller (CC) Register value. | |
| EDMA3_DRV_Result | EDMA3_DRV_getCCRegister (EDMA3_DRV_Handle hEdma, unsigned int regOffset, unsigned int *regValue) |
| Get the Channel Controller (CC) Register value. | |
| EDMA3_DRV_Result | EDMA3_DRV_waitAndClearTcc (EDMA3_DRV_Handle hEdma, unsigned int tccNo) |
| Wait for a transfer completion interrupt to occur and clear it. | |
| EDMA3_DRV_Result | EDMA3_DRV_checkAndClearTcc (EDMA3_DRV_Handle hEdma, unsigned int tccNo, unsigned short *tccStatus) |
| Returns the status of a previously initiated transfer. | |
| EDMA3_DRV_Result | EDMA3_DRV_getPaRAMPhyAddr (EDMA3_DRV_Handle hEdma, unsigned int lCh, unsigned int *paramPhyAddr) |
| Get the PaRAM Set Physical Address associated with a logical channel. | |
| EDMA3_DRV_Result | EDMA3_DRV_Ioctl (EDMA3_DRV_Handle hEdma, EDMA3_DRV_IoctlCmd cmd, void *cmdArg, void *param) |
| EDMA3 Driver IOCTL. | |
| EDMA3_DRV_Handle | EDMA3_DRV_getInstHandle (unsigned int phyCtrllerInstId, EDMA3_RM_RegionId regionId, EDMA3_DRV_Result *errorCode) |
| Return the previously opened EDMA3 Driver Instance handle. | |
The Optional EDMA transfer related Interface of the EDMA3 Driver
| enum EDMA3_DRV_IoctlCmd |
EDMA3 Driver IOCTL commands.
| enum EDMA3_DRV_PaRAMEntry |
PaRAM Set Entry type.
Use this enum to set or get any of the 8 DWords(unsigned int) within a Parameter RAM set
| enum EDMA3_DRV_PaRAMField |
PaRAM Set Field type.
Use this enum to set or get any of the PaRAM set fields
| EDMA3_DRV_Result EDMA3_DRV_checkAndClearTcc | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | tccNo, | |||
| unsigned short * | tccStatus | |||
| ) |
Returns the status of a previously initiated transfer.
This is a non-blocking function that returns the status of a previously initiated transfer, based on the IPR/IPRH bit. This bit corresponds to the tccNo specified by the user. It clears the corresponding bit, if SET, while returning also.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| tccNo | [IN] TCC, specific to which the function checks the status of the IPR/IPRH bit. | |
| tccStatus | [IN/OUT] Status of the transfer is returned here. Returns "TRUE" if the transfer has completed (IPR/IPRH bit SET), "FALSE" if the transfer has not completed successfully (IPR/IPRH bit NOT SET). |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numTccs, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Instance::regionId.
| EDMA3_DRV_Result EDMA3_DRV_getCCRegister | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | regOffset, | |||
| unsigned int * | regValue | |||
| ) |
Get the Channel Controller (CC) Register value.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| regOffset | [IN] CC Register offset whose value is needed | |
| regValue | [IN/OUT] CC Register Value |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, and EDMA3_DRV_Instance::pDrvObjectHandle.
| EDMA3_DRV_Handle EDMA3_DRV_getInstHandle | ( | unsigned int | phyCtrllerInstId, | |
| EDMA3_RM_RegionId | regionId, | |||
| EDMA3_DRV_Result * | errorCode | |||
| ) |
Return the previously opened EDMA3 Driver Instance handle.
This API is used to return the previously opened EDMA3 Driver's Instance Handle (region specific), which could be used to call other EDMA3 Driver APIs. Since EDMA3 Driver does not allow multiple instances, for a single shadow region, this API is provided. This API is meant for users who DO NOT want to / could not open a new Driver Instance and hence re-use the existing Driver Instance to allocate EDMA3 resources and use various other EDMA3 Driver APIs.
In case the Driver Instance is not yet opened, NULL is returned as the function return value whereas EDMA3_DRV_E_INST_NOT_OPENED is returned in the errorCode.
| phyCtrllerInstId | [IN] EDMA3 Controller Instance Id (Hardware instance id, starting from 0). | |
| regionId | [IN] Shadow Region id for which the previously opened driver's instance handle is required. | |
| errorCode | [OUT] Error code while returning Driver Instance Handle. |
References EDMA3_DRV_E_INST_NOT_OPENED, EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::numRegions, and EDMA3_DRV_Instance::pDrvObjectHandle.
| EDMA3_DRV_Result EDMA3_DRV_getMapChToEvtQ | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | channelId, | |||
| unsigned int * | mappedEvtQ | |||
| ) |
Get the Event Queue mapped to the specified DMA/QDMA channel.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| channelId | [IN] Logical Channel whose associated Event Queue is needed | |
| mappedEvtQ | [IN/OUT] The Event Queue which is mapped to the DMA/QDMA channel |
References EDMA3_DRV_DMA_CH_MAX_VAL, EDMA3_DRV_DMAQNUM_CLR_MASK, EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_QDMA_CH_MAX_VAL, EDMA3_DRV_QDMA_CH_MIN_VAL, EDMA3_DRV_QDMAQNUM_CLR_MASK, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, and EDMA3_DRV_Instance::pDrvObjectHandle.
| EDMA3_DRV_Result EDMA3_DRV_getPaRAM | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_DRV_PaRAMRegs * | currPaRAM | |||
| ) |
Retrieve existing PaRAM set associated with specified logical channel (DMA/QDMA/Link).
| hEdma | [IN] Handle to the EDMA Instance object | |
| lCh | [IN] Logical Channel whose PaRAM set is requested | |
| currPaRAM | [IN/OUT] User gets the existing PaRAM here |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_getPaRAMEntry | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_DRV_PaRAMEntry | paRAMEntry, | |||
| unsigned int * | paRAMEntryVal | |||
| ) |
Get a particular PaRAM set entry of the specified PaRAM set.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| lCh | [IN] Logical Channel bound to the Parameter RAM set whose specified field value is needed | |
| paRAMEntry | [IN] Specify the PaRAM set entry which needs to be obtained | |
| paRAMEntryVal | [IN/OUT] The value of the field is returned here |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_PARAM_ENTRY_CCNT, EDMA3_DRV_PARAM_ENTRY_OPT, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_getPaRAMField | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_DRV_PaRAMField | paRAMField, | |||
| unsigned int * | currPaRAMFieldVal | |||
| ) |
Get a particular PaRAM set field of the specified PaRAM set.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| lCh | [IN] Logical Channel bound to the PaRAM set whose specified field value is needed | |
| paRAMField | [IN] Specify the PaRAM set field which needs to be obtained | |
| currPaRAMFieldVal | [IN/OUT] The value of the field is returned here |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_PARAM_ENTRY_ACNT_BCNT, EDMA3_DRV_PARAM_ENTRY_CCNT, EDMA3_DRV_PARAM_ENTRY_DST, EDMA3_DRV_PARAM_ENTRY_LINK_BCNTRLD, EDMA3_DRV_PARAM_ENTRY_OPT, EDMA3_DRV_PARAM_ENTRY_SRC, EDMA3_DRV_PARAM_ENTRY_SRC_DST_BIDX, EDMA3_DRV_PARAM_ENTRY_SRC_DST_CIDX, EDMA3_DRV_PARAM_FIELD_ACNT, EDMA3_DRV_PARAM_FIELD_BCNT, EDMA3_DRV_PARAM_FIELD_BCNTRELOAD, EDMA3_DRV_PARAM_FIELD_CCNT, EDMA3_DRV_PARAM_FIELD_DESTADDR, EDMA3_DRV_PARAM_FIELD_DESTBIDX, EDMA3_DRV_PARAM_FIELD_DESTCIDX, EDMA3_DRV_PARAM_FIELD_LINKADDR, EDMA3_DRV_PARAM_FIELD_OPT, EDMA3_DRV_PARAM_FIELD_SRCADDR, EDMA3_DRV_PARAM_FIELD_SRCBIDX, EDMA3_DRV_PARAM_FIELD_SRCCIDX, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_getPaRAMPhyAddr | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| unsigned int * | paramPhyAddr | |||
| ) |
Get the PaRAM Set Physical Address associated with a logical channel.
This function returns the PaRAM Set Phy Address (unsigned 32 bits). The returned address could be used by the advanced users to program the PaRAM Set directly without using any APIs.
Least significant 16 bits of this address could be used to program the LINK field in the PaRAM Set. Users which program the LINK field directly SHOULD use this API to get the associated PaRAM Set address with the LINK channel.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| lCh | [IN] Logical Channel for which the PaRAM set physical address is required | |
| paramPhyAddr | [IN/OUT] PaRAM Set physical address is returned here. |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_Ioctl | ( | EDMA3_DRV_Handle | hEdma, | |
| EDMA3_DRV_IoctlCmd | cmd, | |||
| void * | cmdArg, | |||
| void * | param | |||
| ) |
EDMA3 Driver IOCTL.
This function provides IOCTL functionality for EDMA3 Driver.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| cmd | [IN] IOCTL command to be performed | |
| cmdArg | [IN/OUT] IOCTL command argument (if any) | |
| param | [IN/OUT] Device/Cmd specific argument |
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| cmd | [IN] IOCTL command to be performed | |
| cmdArg | [IN/OUT] IOCTL command argument (if any) | |
| param | [IN/OUT] Device/Cmd specific argument |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_IOCTL_GET_PARAM_CLEAR_OPTION, EDMA3_DRV_IOCTL_SET_PARAM_CLEAR_OPTION, and EDMA3_DRV_Instance::resMgrInstance.
| EDMA3_DRV_Result EDMA3_DRV_mapChToEvtQ | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | channelId, | |||
| EDMA3_RM_EventQueue | eventQ | |||
| ) |
Associate Channel to Event Queue.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| channelId | [IN] Logical Channel to which the Event Queue is to be mapped | |
| eventQ | [IN] The Event Queue which is to be mapped to the DMA channel |
References EDMA3_DRV_DMA_CH_MAX_VAL, EDMA3_DRV_DMAQNUM_CLR_MASK, EDMA3_DRV_DMAQNUM_SET_MASK, EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_QDMA_CH_MAX_VAL, EDMA3_DRV_QDMA_CH_MIN_VAL, EDMA3_DRV_QDMAQNUM_CLR_MASK, EDMA3_DRV_QDMAQNUM_SET_MASK, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numEvtQueue, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_setCCRegister | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | regOffset, | |||
| unsigned int | newRegValue | |||
| ) |
Set the Channel Controller (CC) Register value.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| regOffset | [IN] CC Register offset whose value needs to be set | |
| newRegValue | [IN] New CC Register Value |
Take the instance specific semaphore, to prevent simultaneous access to the shared resources.
References EDMA3_DRV_Instance::drvSemHandle, EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, and EDMA3_DRV_Instance::pDrvObjectHandle.
| EDMA3_DRV_Result EDMA3_DRV_setEvtQPriority | ( | EDMA3_DRV_Handle | hEdma, | |
| const EDMA3_DRV_EvtQuePriority * | evtQPriObj | |||
| ) |
Sets EDMA TC priority.
User can program the priority of the Event Queues at a system-wide level. This means that the user can set the priority of an IO initiated by either of the TCs (Transfer Ctrllers) relative to IO initiated by the other bus masters on the device (ARM, DSP, USB, etc)
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| evtQPriObj | [IN] Priority of the Event Queues |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_QPRIORITY_MAX_VAL, EDMA3_DRV_EvtQuePriority::evtQPri, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_setPaRAM | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| const EDMA3_DRV_PaRAMRegs * | newPaRAM | |||
| ) |
Copy the user specified PaRAM Set onto the PaRAM Set associated with the logical channel (DMA/QDMA/Link).
This API takes a PaRAM Set as input and copies it onto the actual PaRAM Set associated with the logical channel. OPT field of the PaRAM Set is written first and the CCNT field is written last.
Caution: It should be used carefully when programming the QDMA channels whose trigger words are not CCNT field.
| hEdma | [IN] Handle to the EDMA Instance object | |
| lCh | [IN] Logical Channel for which new PaRAM set is specified | |
| newPaRAM | [IN] Parameter RAM set to be copied onto existing PaRAM |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_setPaRAMEntry | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_DRV_PaRAMEntry | paRAMEntry, | |||
| unsigned int | newPaRAMEntryVal | |||
| ) |
Set a particular PaRAM set entry of the specified PaRAM set.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| lCh | [IN] Logical Channel bound to the Parameter RAM set whose specified field needs to be set | |
| paRAMEntry | [IN] Specify the PaRAM set entry which needs to be set | |
| newPaRAMEntryVal | [IN] The new field setting |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_PARAM_ENTRY_CCNT, EDMA3_DRV_PARAM_ENTRY_OPT, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_setPaRAMField | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_DRV_PaRAMField | paRAMField, | |||
| unsigned int | newPaRAMFieldVal | |||
| ) |
Set a particular PaRAM set field of the specified PaRAM set.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| lCh | [IN] Logical Channel bound to the PaRAM set whose specified field needs to be set | |
| paRAMField | [IN] Specify the PaRAM set field which needs to be set | |
| newPaRAMFieldVal | [IN] The new field setting |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_LOG_CH_MAX_VAL, EDMA3_DRV_PARAM_ENTRY_ACNT_BCNT, EDMA3_DRV_PARAM_ENTRY_CCNT, EDMA3_DRV_PARAM_ENTRY_DST, EDMA3_DRV_PARAM_ENTRY_LINK_BCNTRLD, EDMA3_DRV_PARAM_ENTRY_OPT, EDMA3_DRV_PARAM_ENTRY_SRC, EDMA3_DRV_PARAM_ENTRY_SRC_DST_BIDX, EDMA3_DRV_PARAM_ENTRY_SRC_DST_CIDX, EDMA3_DRV_PARAM_FIELD_ACNT, EDMA3_DRV_PARAM_FIELD_BCNT, EDMA3_DRV_PARAM_FIELD_BCNTRELOAD, EDMA3_DRV_PARAM_FIELD_CCNT, EDMA3_DRV_PARAM_FIELD_DESTADDR, EDMA3_DRV_PARAM_FIELD_DESTBIDX, EDMA3_DRV_PARAM_FIELD_DESTCIDX, EDMA3_DRV_PARAM_FIELD_LINKADDR, EDMA3_DRV_PARAM_FIELD_OPT, EDMA3_DRV_PARAM_FIELD_SRCADDR, EDMA3_DRV_PARAM_FIELD_SRCBIDX, EDMA3_DRV_PARAM_FIELD_SRCCIDX, EDMA3_DRV_QDMA_CHANNEL_0, EDMA3_DRV_QDMA_CHANNEL_7, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numPaRAMSets, EDMA3_DRV_ChBoundResources::paRAMId, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Object::phyCtrllerInstId.
| EDMA3_DRV_Result EDMA3_DRV_setQdmaTrigWord | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | lCh, | |||
| EDMA3_RM_QdmaTrigWord | trigWord | |||
| ) |
Assign a Trigger Word to the specified QDMA channel.
This API sets the Trigger word for the specific QDMA channel in the QCHMAP Register. Default QDMA trigger word is CCNT.
| hEdma | [IN] Handle to the EDMA Instance object | |
| lCh | [IN] QDMA Channel which needs to be assigned the Trigger Word | |
| trigWord | [IN] The Trigger Word for the QDMA channel. Trigger Word is the word in the PaRAM Register Set which, when written to by CPU, will start the QDMA transfer automatically. |
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_QCH_TRWORD_CLR_MASK, EDMA3_DRV_QCH_TRWORD_SET_MASK, EDMA3_DRV_QDMA_CH_MAX_VAL, EDMA3_DRV_QDMA_CH_MIN_VAL, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, and EDMA3_DRV_Instance::pDrvObjectHandle.
| EDMA3_DRV_Result EDMA3_DRV_waitAndClearTcc | ( | EDMA3_DRV_Handle | hEdma, | |
| unsigned int | tccNo | |||
| ) |
Wait for a transfer completion interrupt to occur and clear it.
This is a blocking function that returns when the IPR/IPRH bit corresponding to the tccNo specified, is SET. It clears the corresponding bit while returning also.
This function waits for the specific bit indefinitely in a tight loop, with out any delay in between. USE IT CAUTIOUSLY.
| hEdma | [IN] Handle to the EDMA Driver Instance | |
| tccNo | [IN] TCC, specific to which the function waits on a IPR/IPRH bit. |
Bit found SET, transfer is completed, clear the pending interrupt and return.
Bit found SET, transfer is completed, clear the pending interrupt and return.
References EDMA3_DRV_E_INVALID_PARAM, EDMA3_DRV_Object::gblCfgParams, EDMA3_DRV_GblConfigParams::globalRegs, EDMA3_DRV_GblConfigParams::numTccs, EDMA3_DRV_Instance::pDrvObjectHandle, and EDMA3_DRV_Instance::regionId.
1.5.9