Data Structures | |
| struct | EDMA3_RM_GblErrCallbackParams |
| Global Error Callback parameters. More... | |
Typedefs | |
| typedef void(* | EDMA3_RM_GblErrCallback )(EDMA3_RM_GlobalError deviceStatus, unsigned int instanceId, void *gblerrData) |
| Global Error callback - caters to module events like bus error etc which are not channel specific. Runs in ISR context. | |
Enumerations | |
| enum | EDMA3_RM_TccStatus { EDMA3_RM_XFER_COMPLETE = 1, EDMA3_RM_E_CC_DMA_EVT_MISS = 2, EDMA3_RM_E_CC_QDMA_EVT_MISS = 3 } |
| This enum defines the channel specific status codes of an EDMA3 transfer. It is returned while calling the channel specific callback function to tell the status. More... | |
| enum | EDMA3_RM_GlobalError { EDMA3_RM_E_CC_QUE_THRES_EXCEED = 1, EDMA3_RM_E_CC_TCC = 2, EDMA3_RM_E_TC_MEM_LOCATION_READ_ERROR = 3, EDMA3_RM_E_TC_MEM_LOCATION_WRITE_ERROR = 4, EDMA3_RM_E_TC_INVALID_ADDR = 5, EDMA3_RM_E_TC_TR_ERROR = 6 } |
| This enum defines the global (not specific to any channel) error codes of completion of an EDMA3 transfer. More... | |
| typedef void(* EDMA3_RM_GblErrCallback)(EDMA3_RM_GlobalError deviceStatus, unsigned int instanceId, void *gblerrData) |
Global Error callback - caters to module events like bus error etc which are not channel specific. Runs in ISR context.
gblerrData is application provided data when open'ing the Resource Manager.
| enum EDMA3_RM_GlobalError |
This enum defines the global (not specific to any channel) error codes of completion of an EDMA3 transfer.
| EDMA3_RM_E_CC_QUE_THRES_EXCEED | Threshold exceed:- for all event queues. These get latched in EDMA3CC error register (CCERR). This error has a direct relation with the setting of EDMA3_RM_GblConfigParams.evtQueueWaterMarkLvl |
| EDMA3_RM_E_CC_TCC | TCC error:- for outstanding transfer requests expected to return completion code (TCCHEN or TCINTEN bit in OPT is set to 1) exceeding the maximum limit of 63. This also gets latched in the CCERR. |
| EDMA3_RM_E_TC_MEM_LOCATION_READ_ERROR | Transfer Controller has reported an error Detection of a Read error signaled by the source or destination address |
| EDMA3_RM_E_TC_MEM_LOCATION_WRITE_ERROR | Detection of a Write error signaled by the source or destination address |
| EDMA3_RM_E_TC_INVALID_ADDR | Attempt to read or write to an invalid address in the configuration memory map. |
| EDMA3_RM_E_TC_TR_ERROR | Detection of a FIFO mode TR violating the FIFO mode transfer rules (the source/destination addresses and source/destination indexes must be aligned to 32 bytes). |
| enum EDMA3_RM_TccStatus |
This enum defines the channel specific status codes of an EDMA3 transfer. It is returned while calling the channel specific callback function to tell the status.
1.5.9