#include <edma3_rm.h>
Data Fields | |
| unsigned short | isSlave |
| unsigned short | param |
This configuration structure is used to specify some misc options while creating the RM Object. New options may also be added into this structure in future.
| unsigned short EDMA3_RM_MiscParam::isSlave |
In a multi-master system (for e.g. ARM + DSP), this option is used to distinguish between Master and Slave. Only the Master is allowed to program the global EDMA3 registers (like Queue priority, Queue water- mark level, error registers etc).
Referenced by EDMA3_RM_create().
| unsigned short EDMA3_RM_MiscParam::param |
For future use
1.5.9