Uncompressing Linux... done, booting the kernel. Linux version 2.6.37+ (sudhakar@linux-psp-server.india.ext.ti.com) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #3 PREEMPT Wed Jul 20 09:39:22 IST 2011 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177 CPU: VIVT data cache, VIVT instruction cache Machine: DaVinci DA850/OMAP-L138/AM18x EVM Memory policy: ECC disabled, Data cache writeback DaVinci da850/omap-l138 variant 0x0 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 24320 Kernel command line: console=ttyS2,115200n8 noinitrd rw ip=192.168.247.201 root=/dev/nfs nfsroot=192.168.247.76:/opt/filesystem/da8XX_fs,nolock mem=32M@0xc0000000 mem=64M@0xc4000000 PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 32MB 64MB = 96MB total Memory: 92928k/92928k available, 5376k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xff000000 - 0xffe00000 ( 14 MB) vmalloc : 0xc8800000 - 0xfea00000 ( 866 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .init : 0xc0008000 - 0xc002e000 ( 152 kB) .text : 0xc002e000 - 0xc0415000 (3996 kB) .data : 0xc0416000 - 0xc043cca0 ( 156 kB) SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptable hierarchical RCU implementation. RCU-based detection of stalled CPUs is disabled. Verbose stalled-CPUs detection is disabled. NR_IRQS:245 Console: colour dummy device 80x30 Calibrating delay loop... 185.54 BogoMIPS (lpj=927744) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok DaVinci: 144 gpio irqs regulator: core version 0.5 regulator: dummy: NET: Registered protocol family 16 WARNING: both McASP and McBSP are enabled, but they share pins. Only McASP will work. If you want McBSP support, disable McASP. da850_evm_init: eHRPWM module 0 cannot be used since it is being used by MII interface da850_evm_init: eHRPWM module1 outputA cannot be used since it is being used by LCD da850_evm_init: eHRPWM module1 outputB cannot be used since it is being used by spi1 bio: create slab at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb pca953x 1-0020: interrupt support not compiled in DA850/OMAP-L138 EVM UI card detected pca953x 1-0021: interrupt support not compiled in regulator: VDCDC1: 3200 <--> 3300 mV at 3300 mV regulator: VDCDC2: 1750 <--> 3300 mV at 3300 mV regulator: VDCDC3: 950 <--> 1350 mV at 1200 mV regulator: LDO1: 1800 mV regulator: LDO2: 1150 <--> 1300 mV at 1200 mV i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL) Advanced Linux Sound Architecture Driver Version 1.0.23. Switching to clocksource timer0_1 musb-hdrc: version 6.0, host, debug=0 musb-hdrc musb-hdrc: dma type: dma-cppi41 Waiting for USB PHY clock good... musb-hdrc musb-hdrc: MUSB HDRC host driver musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected musb-hdrc musb-hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58 NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 4096 (order: 3, 32768 bytes) TCP bind hash table entries: 4096 (order: 2, 16384 bytes) TCP: Hash tables configured (established 4096 bind 4096) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. EMAC: RMII PHY configured, MII PHY will not be functional McBSP:Probed McBSP1 JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc. msgmni has been set to 181 io scheduler noop registered (default) da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel Console: switching to colour frame buffer device 60x34 Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7 serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7 serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7 console [ttyS2] enabled brd: module loaded at24 1-0050: 32768 byte 24c256 EEPROM (writable) Read MAC addr from EEPROM: 00:0e:99:02:ff:ed ahci ahci: forcing PORTS_IMPL to 0x1 ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc scsi0 : ahci_platform ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67 spi_davinci spi_davinci.1: DMA: supported spi_davinci spi_davinci.1: DMA: RX channel: 18, TX channel: 19, event queue: 0 m25p80 spi1.0: w25x64 (8192 Kbytes) Creating 6 MTD partitions on "m25p80": 0x000000000000-0x000000010000 : "UBL" 0x000000010000-0x000000090000 : "U-Boot" 0x000000090000-0x0000000a0000 : "U-Boot-Env" 0x0000000a0000-0x000000320000 : "Kernel" 0x000000320000-0x000000720000 : "Filesystem" 0x0000007f0000-0x000000800000 : "MAC-Address" spi_davinci spi_davinci.1: Controller at 0xfef0e000 davinci_mdio davinci_mdio.0: davinci mdio revision 1.5 davinci_mdio davinci_mdio.0: detected phy mask fffffffe davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720 console [netcon0] enabled netconsole: network logging started ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver ohci ohci.0: DA8xx OHCI ohci ohci.0: new USB bus registered, assigned bus number 2 Waiting for USB PHY clock good... ohci ohci.0: irq 59, io mem 0x01e25000 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. input: gpio-keys-polled as /devices/platform/gpio-keys-polled.0/input/input0 input: gpio-keys-polled as /devices/platform/gpio-keys-polled.1/input/input1 input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/input2 omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 ata1: SATA link down (SStatus 0 SControl 300) omap_rtc: RTC power up reset detected i2c /dev entries driver watchdog watchdog: heartbeat 60 sec cpuidle: using governor ladder cpuidle: using governor menu davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode usbcore: registered new interface driver usbhid usbhid: USB HID core driver 1-0018 supply IOVDD not found, using dummy regulator 1-0018 supply DVDD not found, using dummy regulator 1-0018 supply AVDD not found, using dummy regulator 1-0018 supply DRVDD not found, using dummy regulator asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok ALSA device list: #0: DA850/OMAP-L138 EVM TCP cubic registered NET: Registered protocol family 17 regulator_init_complete: incomplete constraints, leaving LDO2 on regulator_init_complete: incomplete constraints, leaving LDO1 on regulator_init_complete: incomplete constraints, leaving VDCDC3 on regulator_init_complete: incomplete constraints, leaving VDCDC2 on regulator_init_complete: incomplete constraints, leaving VDCDC1 on omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) davinci_mdio davinci_mdio.0: resetting idled controller net eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=0:00, id=7c0f1) IP-Config: Guessing netmask 255.255.255.0 IP-Config: Complete: device=eth0, addr=192.168.247.201, mask=255.255.255.0, gw=255.255.255.255, host=192.168.247.201, domain=, nis-domain=(none), bootserver=255.255.255.255, rootserver=192.168.247.76, rootpath= PHY: 0:00 - Link is Up - 100/Full VFS: Mounted root (nfs filesystem) on device 0:13. Freeing init memory: 152K INIT: version 2.86 booting Please wait: booting... Starting udev udevd (552): /proc/552/oom_adj is deprecated, please use /proc/552/oom_score_adj instead. Populating dev cache Root filesystem already rw, not remounting WARNING: Couldn't open directory /lib/modules/2.6.37+: No such file or directory FATAL: Could not open /lib/modules/2.6.37+/modules.dep.temp for writing: No such file or directory modprobe: FATAL: Could not load /lib/modules/2.6.37+/modules.dep: No such file or directory modprobe: FATAL: Could not load /lib/modules/2.6.37+/modules.dep: No such file or directory root: mount: mounting rootfs on / failed: No such file or directory root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory Setting up IP spoofing protection: rp_filter. Configuring network interfaces... done. Thu Feb 3 11:36:00 UTC 2011 INIT: Entering runlevel: 5 Starting telnet daemon. modprobe: FATAL: Could not load /lib/modules/2.6.37+/modules.dep: No such file or directory Starting syslogd/klogd: done Starting thttpd. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org da850-omapl138-evm ttyS2 Arago 2009.11 da850-omapl138-evm ttyS2 da850-omapl138-evm login: