root@dm814x:/opt/dvr_rdk/ti814x# ./run.sh ========= Main Menu ========= 1: 4CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 2: 8CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 3: 16CH RT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 4: 16CH NRT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 5: VDEC + VDIS - SD/HD Decode ONLY e: Exit Enter Choice: 5 Sample ini files available in ./demo_ini folder. Enter the .ini filename with full path : demo ^H^Croot@dm814x:/opt/dvr_rdk/ti814x# ./run.sh ========= Main Menu ========= 1: 4CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 2: 8CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 3: 16CH RT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 4: 16CH NRT VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 5: VDEC + VDIS - SD/HD Decode ONLY e: Exit Enter Choice: 5 Sample ini files available in ./demo_ini folder. Enter the .ini filename with full path : demo_ini/dm816x_1080p_demo_1CH.ini *** a new param codec is needed for ini, if you not sure about this *** please reference demo_ini/704x576_02_32CH.ini *** H264: codec = h264 *** MPEG4: codec = mpeg4 *** MJPEG: codec = mjpeg *** MPEG2: codec = mpeg2 *** Four new params numbuf ,displaydelay,tilerEnable,fieldPicture has been added for ini, if not defaults are set *** Generate header files *** This will take very long time if the file is large. - For first time you MUST select YES. - If you already have the header file on disk, you can select NO. Do you want to generate header ? (YES - y, NO - n) : n 0: Opening file [/data/content/orig/TI/dm816x_1080p_demo.264] of 1920 x 10080 Codec: h264... gVdecVdis_config.numChannels : 1 gVdecVdis_config.chBufSize[0] : 19353600 File open ... DONE !!! --------------- CHANNEL DETAILS------------- Dec Channels => 1 Disp Channels => 1 ------------------------------------------- 0: SYSTEM: System Common Init in progress !!! 0: SYSTEM: IPC init in progress !!! 10: SYSTEM: CPU [DSP] syslink proc ID is [0] !!! 10: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!! 10: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!! 10: SYSTEM: CPU [HOST] syslink proc ID is [3] !!! 10: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ... 12: SYSTEM: Creating MsgQ [HOST_MSGQ] ... 14: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ... 15: SYSTEM: Opening MsgQ [DSP_MSGQ] ... 16: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ... 16: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ... 17: SYSTEM: Notify register to [DSP] line 0, event 15 ... 18: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ... 18: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ... 19: SYSTEM: IPC init DONE !!! 20: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ... 21: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ... 23: SYSTEM: ListElem Shared Addr = 0x40f8a680 23: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ... 25: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ... 26: SYSTEM: ListElem Shared Addr = 0x40fc1480 28: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ... 29: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ... 31: SYSTEM: ListElem Shared Addr = 0x40ff8280 32: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ... 33: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ... 35: SYSTEM: ListElem Shared Addr = 0x4103b580 35: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ... 37: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ... 39: SYSTEM: ListElem Shared Addr = 0x4107e880 57: SYSTEM: System Common Init Done !!! ch[0], h264 IOCTL_DEVICE_SII9022A_QUERY_HPD Failed!! This can happen because 1. enableConfigExtVideoEncoder is set to TRUE and Sii9022A is absent in the system OR ASSERT (ti_vdis.c|Vdis_init|404) 2. Loose connection between the board and the daugther card