Installation info to configure the Spectrum Digital XDS510PP_PLUS for SAM2 and the EVBC6747 (OMAPL-137) Click the link to the SpectrumDigital web site for the CodeComposer installation help. Run SDConfig V3.3 Configure the emulator to the correct IO port and EPP or other basic mode. Make sure you select the 510PP or 510PP_PLUS to match the emulator you have... run a diagnostic to be safe... Save the "SDOpts.cfg" file. Copy the folder "SAM2_v1" contents to C:\CCStudio_v3.3\boards\ Copy the 2".CCS" files: "evmc6747_xds510pp.ccs" and "SAM2_v1_xds510pp.ccs" to C:\CCStudio_v3.3\drivers\import\ Click on the desired shortcut, like "SAM2_v1 XDS10PP+ CCStudio v3.3" to setup the emulator for the desired board.