-----[Print the reset-command software log-file]-----------------------------

This utility has selected an XDS560 class product.
This utility will load the program 'bh560usbm.out'.
This utility will operate on port address '0'.
The controller does use a programmable FPGA.
The old VHDL code has a version number of '1544' (0x0608).
The new VHDL code has a version number of '1544' (0x0608).
The emulator program is named 'bh560usbm.out'.
The emulator program is version '35.34.0.2'.
The controller has a version number of '4' (0x0004).
The controller has an insertion length of '0' (0x0000).
The cable+pod has a version number of '6' (0x0006).
The cable+pod has a capability number of '8' (0x0008).
The local memory has a base address of '0' (0x000000).
The local memory has a word capacity of '32768' (0x008000).
This utility will now attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The software is configured to use all Nano-TBC VHDL features.
The controller type is the Nano-TBC VHDL.
The connection type is a 560-class revision-D multi-purpose cable.
The controller will be software reset via its configure register.
The controller will use rising-edge timing on output pins.
The controller may use rising edge timing on input pins.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The scan-path link-delay has been set to exactly '3' (0x0003).
The support logic has not previously detected a power-loss.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 512 32-bit words.

 || // -- \\  The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 4 bits.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.