########################################################################
#
#                           GettingStarted.eww
#
# $Revision: 46020 $
#
########################################################################

DESCRIPTION
===========
  This example project shows how to use the IAR Embedded Workbench for ARM
 to develop code for the TI TMS570LS3137 Argoboard. It shows basic use of the I/O,
 the timer and the interrupt controllers. It togble port B bit 7 ten times
 per second.

COMPATIBILITY
=============

   The example project is compatible with, on TI TMS570LS3137 Argoboard.
   By default, the project is configured to use the J-Link JTAG interface.

CONFIGURATION
=============

  The GettingStarted application is downloaded to the embeded Flash.

GETTING STARTED
===============

  1) Start the IAR Embedded Workbench for ARM.

  2) Select File->Open->Workspace...
     Open the following workspace:

      <installation-root>\arm\examples\TexasInstruments\
     TMS570LS3137\Argoboard\GettingStarted\GettingStarted.eww

  3) Run the program.