@REM ****************************************************************** @REM * FILE PURPOSE: Environment Setup @REM ****************************************************************** @REM * FILE NAME: mmwave_sdk_setupenv.bat @REM * @REM * DESCRIPTION: @REM * Configures and sets up the Build Environment for mmWave SDK. @REM * @REM ****************************************************************** @echo off set DOWNLOAD_FROM_CCS=yes set MMWAVE_SDK_DEVICE=iwr16xx set R4F_CODEGEN_INSTALL_PATH=C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS set MMWAVE_SDK_INSTALL_PATH=C:/ti/mmwave_sdk_01_00_00_05/packages set BIOS_INSTALL_PATH=c:/ti/bios_6_50_01_12/packages set XDC_INSTALL_PATH=c:/ti/xdctools_3_50_02_20_core set PERL_INSTALL_PATH=C:/StrawberryPerl/perl/bin set C674_CODEGEN_INSTALL_PATH=C:/ti/c6000_code_gen_tools/ti-cgt-c6000_8.2.0 set C64Px_DSPLIB_INSTALL_PATH=C:/ti/tmdemo/mmwave_demo_dev/lib/dsplib_c64Px_3_4_0_0 set C674x_MATHLIB_INSTALL_PATH=C:/ti/mathlib_c674x_3_1_2_1 set XWR16XX_RADARSS_IMAGE_BIN=C:/ti/mmwave_sdk_01_00_00_05/firmware/radarss/xwr16xx_radarss_rprc.bin set MMWAVE_DEMO_DEV_PATH=%CD%../../../../../.. set MMWAVE_DEMO_DEV_PATH=%MMWAVE_DEMO_DEV_PATH:\=/% REM ------------------------------------------------------------------- REM Sanity Check: Ensure that all the required variables are defined REM ------------------------------------------------------------------- if [%R4F_CODEGEN_INSTALL_PATH%] == [] ( @echo Error: R4F_CODEGEN_INSTALL_PATH [R4F Toochain] needs to be defined @echo For Example: @echo set R4F_CODEGEN_INSTALL_PATH=C:/ti/ccsv7/tools/compiler/arm_16.9.1.LTS goto fail ) if [%MMWAVE_SDK_INSTALL_PATH%] == [] ( @echo Error: MMWAVE_SDK_INSTALL_PATH [mmWave SDK Package Location] needs to be defined @echo For Example: @echo set MMWAVE_SDK_INSTALL_PATH=C:/ti/mmwave_sdk_01_00_00_03/packages goto fail ) if [%BIOS_INSTALL_PATH%] == [] ( @echo Error: BIOS_INSTALL_PATH [SYSBIOS] needs to be defined @echo For Example: @echo set BIOS_INSTALL_PATH=c:/ti/bios_6_50_01_12/packages goto fail ) if [%XDC_INSTALL_PATH%] == [] ( @echo Error: XDC_INSTALL_PATH [XDC Build Tools] needs to be defined @echo For Example: @echo set XDC_INSTALL_PATH=c:/ti/xdctools_3_50_00_10_core goto fail ) if [%PERL_INSTALL_PATH%] == [] ( @echo Error: PERL_INSTALL_PATH [Perl Install Path] needs to be defined @echo For Example: @echo set PERL_INSTALL_PATH=C:/Perl/Bin goto fail ) if [%DOWNLOAD_FROM_CCS%] == [] ( @echo Error: DOWNLOAD_FROM_CCS needs to be defined @echo For Example: @echo set DOWNLOAD_FROM_CCS=yes @echo OR @echo set DOWNLOAD_FROM_CCS=no goto fail ) if [%MMWAVE_SDK_DEVICE%] == [] ( @echo Error: MMWAVE_SDK_DEVICE needs to be defined @echo For Example: @echo set MMWAVE_SDK_DEVICE=awr14xx @echo OR @echo set MMWAVE_SDK_DEVICE=awr16xx @echo OR @echo set MMWAVE_SDK_DEVICE=iwr14xx @echo OR @echo set MMWAVE_SDK_DEVICE=iwr16xx goto fail ) set MMWAVE_SDK_DEVICE_TYPE=xwr14xx if [%MMWAVE_SDK_DEVICE%] == [awr16xx] ( set MMWAVE_SDK_DEVICE_TYPE=xwr16xx ) if [%MMWAVE_SDK_DEVICE%] == [iwr16xx] ( set MMWAVE_SDK_DEVICE_TYPE=xwr16xx ) if [%MMWAVE_SDK_DEVICE_TYPE%] == [xwr16xx] ( if [%C674_CODEGEN_INSTALL_PATH%] == [] ( @echo Error: C674_CODEGEN_INSTALL_PATH [DSP Toolchain] needs to be defined @echo For Example: @echo set C674_CODEGEN_INSTALL_PATH=C:/ti/ccsv7/tools/compiler/c6000_7.4.16 goto fail ) if [%C64Px_DSPLIB_INSTALL_PATH%] == [] ( @echo Error: C64Px_DSPLIB_INSTALL_PATH needs to be defined @echo For Example: @echo set C64Px_DSPLIB_INSTALL_PATH=C:/ti/dsplib_c64Px_3_4_0_0 goto fail ) if [%C674x_MATHLIB_INSTALL_PATH%] == [] ( @echo Error: C674x_MATHLIB_INSTALL_PATH needs to be defined @echo For Example: @echo set C674x_MATHLIB_INSTALL_PATH=C:/ti/mathlib_c674x_3_1_2_1 goto fail ) if [%XWR16XX_RADARSS_IMAGE_BIN%] == [] ( @echo Error: XWR16XX_RADARSS_IMAGE_BIN needs to be defined with the complete path and filename of the BSS binary @echo For Example: @echo set XWR16XX_RADARSS_IMAGE_BIN=%MMWAVE_SDK_INSTALL_PATH%/firmware/radarss/ar1xxx_bss_rprc.bin goto fail ) if NOT EXIST "%XWR16XX_RADARSS_IMAGE_BIN%" ( @echo Error: %XWR16XX_RADARSS_IMAGE_BIN% does not exist. Check the path goto fail ) ) REM ---------------------------------------------------------- REM Setup the PATH configuration: REM This can be modified if the tools are installed in a REM different directory. REM ---------------------------------------------------------- REM Clear all environment paths first. REM set PATH= set INCLUDE= set LIB= REM Test requirements REM set PATH=%PATH%;C:/Windows;C:/Windows/system32 REM ---------------------------------------------------------- REM Please do not change anything below this REM ---------------------------------------------------------- REM XDC Tools including gmake set PATH=%PERL_INSTALL_PATH%;%XDC_INSTALL_PATH%;%XDC_INSTALL_PATH%/bin;%PATH% REM Set XDC environment variables set XDCCGROOT=%C674_CODEGEN_INSTALL_PATH% set XDCBUILDCFG=%MMWAVE_SDK_INSTALL_PATH%/config.bld set XDCARGS= REM Clear all XDCPATH values first. set XDCPATH=%BIOS_INSTALL_PATH% set XDCPATH=%XDCPATH%;%MMWAVE_SDK_INSTALL_PATH% REM TI Code Generation Tools set PATH=%C674_CODEGEN_INSTALL_PATH%/bin;%PATH% set PATH=%R4F_CODEGEN_INSTALL_PATH%/bin;%PATH% REM Tools: REM - Doxygen REM These are only used by the release scripts. Customers can build without these defined. set PATH=%DOXYGEN_INSTALL_PATH%\bin;%GRAPHVIZ_INSTALL_PATH%\bin;%PATH% @echo ----------------------------------------------- @echo mmWave Build Environment Configured @echo ----------------------------------------------- REM Set the Title Window appropriately. Title mmWave Build Environment goto end :fail @echo Failed to setup mmWave Build Environment ! Title Failed to setup mmWave Build Environment :end