INFO: ParameterDMLParser: Found register map with name 'OPT9221' (vPG1P0) INFO: HardwareSerializer: Received 45190 bytes from hardware in 2.034 s INFO: Data2DCodec: Original number of 8-bit offsets = 2534 INFO: Data2DCodec: Number of invalid pixels in original data = 0 INFO: Data2DCodec: Current number of 8-bit offsets = 2534 INFO: DepthCamera: Setting parameter 'op_clk_freq' INFO: DepthCamera: Setting parameter 'unambiguous_range' INFO: DepthCamera: Setting parameter 'sub_frame_cnt_max' INFO: DepthCamera: Setting parameter 'quad_cnt_max' INFO: DepthCamera: Setting parameter 'intg_duty_cycle' INFO: DepthCamera: Setting parameter 'illum_power_percentage' INFO: DepthCamera: Setting parameter 'delay_fb_corr_mode' INFO: DepthCamera: Setting parameter 'delay_fb_dc_corr_mode' INFO: DepthCamera: Setting parameter 'sscg_en' INFO: DepthCamera: Setting parameter 'sscg_period' INFO: DepthCamera: Setting parameter 'sscg_modulation' INFO: DepthCamera: Setting parameter 'init_2' INFO: DepthCamera: Setting parameter 'init_3' INFO: DepthCamera: Setting parameter 'init_4' INFO: DepthCamera: Setting parameter 'init_5' ERROR: DepthCamera: Failed to update value for parameter 'mix_volt' ERROR: DepthCamera: Failed to update value for parameter 'pvdd' ERROR: CameraSystem: Could not refresh parameters for TintinCDKCamera(0::0451:9105::10979061099734). INFO: ToFCameraBase: Starting with 320x240@30.0001fps WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline. WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline. WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.Using rate factor = 0.1 WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.Using rate factor = 0.367879317995 Using rate factor = 0.147632532249 Using rate factor = 0.118288346978 C:\PROGRA~1\TEXASI~1\VOXELV~1.10\VOXELV~1\pyqtgraph\graphicsItems\ImageItem.py:354: VisibleDeprecationWarning: using a non-integer number instead of an integer will result in an error in the future ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535798530111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535799134111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535799738111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535800343111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535800947111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535801551111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535802156111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535802761111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535803365111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535803969111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535804573111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535805178111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535805782111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535806387111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535806991111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535807596111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535808200111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535808805111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535809410111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535810014111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535810618111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535811222111 ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes ERROR: USBIO: Could not transfer '0' bytes WARNING: USBBulkStreamer: Resetting bulk endpoint at 1533535811827111 ERROR: USBIO: Could not transfer '0' bytes INFO: DepthCamera: Streaming stopped.Deleting logger...