**** Build of configuration Debug for project viterbi_C55 **** C:\ti\ccsv5\utils\bin\gmake -k all 'Building file: J:/C55_Viterbi/Viterbi_t.c' 'Invoking: C5500 Compiler' "C:/ti/ccsv5/tools/compiler/c5500/bin/cl55" -g --include_path="C:/ti/ccsv5/tools/compiler/c5500/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="C:/CCSTUD~1.1/C5500/csl/include" --define="_DEBUG" --quiet --display_error_number --obj_directory="C:/temp_XP/C55_Viterbi/viterbi_C55/Debug" --preproc_with_compile --preproc_dependency="Viterbi_t.pp" "J:/C55_Viterbi/Viterbi_t.c" 'Finished building: J:/C55_Viterbi/Viterbi_t.c' ' ' 'Building file: J:/C55_Viterbi/viterbi_dec.asm' 'Invoking: C5500 Compiler' "C:/ti/ccsv5/tools/compiler/c5500/bin/cl55" -g --include_path="C:/ti/ccsv5/tools/compiler/c5500/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="C:/CCSTUD~1.1/C5500/csl/include" --define="_DEBUG" --quiet --display_error_number --obj_directory="C:/temp_XP/C55_Viterbi/viterbi_C55/Debug" --preproc_with_compile --preproc_dependency="viterbi_dec.pp" "J:/C55_Viterbi/viterbi_dec.asm" "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 118: [R5601] MMR writes to ST0 and ST2 are not pipeline protected against interrupts (see the C55x silicon exceptions errata; Advisory CPU_75) MOV #0, mmap(ST0_55) ;All fields cleared (OVx, C, TCx). "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 155: [R5601] MMR writes to ST0 and ST2 are not pipeline protected against interrupts (see the C55x silicon exceptions errata; Advisory CPU_75) OR #ST2mask, mmap(ST2_55) ;config circ/linear pointers) "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 357: [R5601] MMR writes to ST0 and ST2 are not pipeline protected against interrupts (see the C55x silicon exceptions errata; Advisory CPU_75) AND #0FF00h, mmap(ST2_55) "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 385: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) || RPTBLOCAL outer_loop; port of ||RPTBLOCAL outer_loop "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 388: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) RPTBLOCAL inner_loop; port of RPTBLOCAL inner_loop "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 411: [R5682] This outer loop contains a nested localrepeat that may cause execution to terminate if an iteration of the nested localrepeat is interrupted; (see the C55x silicon exceptions errata; Advisory CPU_116) } "J:\C55_Viterbi\viterbi_dec.asm", REMARK at line 419: [R5601] MMR writes to ST0 and ST2 are not pipeline protected against interrupts (see the C55x silicon exceptions errata; Advisory CPU_75) AND #0FE00h, mmap(ST2_55) ;clear CDPLC and AR[7-0]LC 'Finished building: J:/C55_Viterbi/viterbi_dec.asm' ' ' 'Building file: J:/C55_Viterbi/viterbi_enc.asm' 'Invoking: C5500 Compiler' "C:/ti/ccsv5/tools/compiler/c5500/bin/cl55" -g --include_path="C:/ti/ccsv5/tools/compiler/c5500/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="C:/CCSTUD~1.1/C5500/csl/include" --define="_DEBUG" --quiet --display_error_number --obj_directory="C:/temp_XP/C55_Viterbi/viterbi_C55/Debug" --preproc_with_compile --preproc_dependency="viterbi_enc.pp" "J:/C55_Viterbi/viterbi_enc.asm" "J:\C55_Viterbi\viterbi_enc.asm", REMARK at line 86: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) rptblocal encode_end ; port of rptblocal encode_end 'Finished building: J:/C55_Viterbi/viterbi_enc.asm' ' ' 'Building file: J:/C55_Viterbi/viterbi_upck.asm' 'Invoking: C5500 Compiler' "C:/ti/ccsv5/tools/compiler/c5500/bin/cl55" -g --include_path="C:/ti/ccsv5/tools/compiler/c5500/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="C:/CCSTUD~1.1/C5500/csl/include" --define="_DEBUG" --quiet --display_error_number --obj_directory="C:/temp_XP/C55_Viterbi/viterbi_C55/Debug" --preproc_with_compile --preproc_dependency="viterbi_upck.pp" "J:/C55_Viterbi/viterbi_upck.asm" "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 99: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) || rptblocal frame_loop; port of ||rptblocal frame_loop "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 103: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) || rptblocal wordg0_loop; port of || rptblocal wordg0_loop "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 111: [R5671] If an interrupt is asserted between this conditional execute instruction and the next instruction (to be executed based on the conditional's result), the next instruction may get executed regardless of the result of the conditional in this instruction; be sure that interrupts are not active or conditionalize in the AD_unit; (see the C55x silicon exceptions errata; Advisory CPU_93) XCCPART check2, ac1 != #0 "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 117: [R5573] Any BKxx and BSAxx updates are not pipline protected against MAR operations within 5 cycles (see line 112) (see the C55x silicon exceptions errata; Advisory CPU_43) ||amar *(g0_ptr+t0) "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 121: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) || rptblocal wordg1_loop; port of || rptblocal wordg1_loop "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 129: [R5671] If an interrupt is asserted between this conditional execute instruction and the next instruction (to be executed based on the conditional's result), the next instruction may get executed regardless of the result of the conditional in this instruction; be sure that interrupts are not active or conditionalize in the AD_unit; (see the C55x silicon exceptions errata; Advisory CPU_93) XCCPART check4, ac1!= #0 "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 133: [R5573] Any BKxx and BSAxx updates are not pipline protected against MAR operations within 5 cycles (see line 130) (see the C55x silicon exceptions errata; Advisory CPU_43) ||amar *(g1_ptr+t0) "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 134: [R5682] This outer loop contains a nested localrepeat that may cause execution to terminate if an iteration of the nested localrepeat is interrupted; (see the C55x silicon exceptions errata; Advisory CPU_116) } "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 143: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) rptblocal last_wordg0_loop; port of rptblocal last_wordg0_loop "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 151: [R5671] If an interrupt is asserted between this conditional execute instruction and the next instruction (to be executed based on the conditional's result), the next instruction may get executed regardless of the result of the conditional in this instruction; be sure that interrupts are not active or conditionalize in the AD_unit; (see the C55x silicon exceptions errata; Advisory CPU_93) XCCPART check6, ac1 != #0 "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 156: [R5573] Any BKxx and BSAxx updates are not pipline protected against MAR operations within 5 cycles (see line 153) (see the C55x silicon exceptions errata; Advisory CPU_43) ||amar *(g0_ptr+t0) "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 160: [R5688] A localrepeat may be corrupted when C54CM == 1 (see the C55x silicon exceptions errata; Advisory CPU_85) rptblocal last_wordg1_loop; port of rptblocal last_wordg1_loop "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 168: [R5671] If an interrupt is asserted between this conditional execute instruction and the next instruction (to be executed based on the conditional's result), the next instruction may get executed regardless of the result of the conditional in this instruction; be sure that interrupts are not active or conditionalize in the AD_unit; (see the C55x silicon exceptions errata; Advisory CPU_93) XCCPART check8, ac1 != #0 "J:\C55_Viterbi\viterbi_upck.asm", REMARK at line 173: [R5573] Any BKxx and BSAxx updates are not pipline protected against MAR operations within 5 cycles (see line 170) (see the C55x silicon exceptions errata; Advisory CPU_43) ||amar *(g1_ptr+t0) 'Finished building: J:/C55_Viterbi/viterbi_upck.asm' ' ' 'Building target: J:/C55_Viterbi/viterbi_C55/viterbi_C55/../../viterbi_C55/Debug/viterbi_C55.out' 'Invoking: C5500 Linker' "C:/ti/ccsv5/tools/compiler/c5500/bin/cl55" -g --define="_DEBUG" --quiet --display_error_number --obj_directory="C:/temp_XP/C55_Viterbi/viterbi_C55/Debug" -z -m"viterbi_C55.map" --stack_size=5000 -i"C:/ti/ccsv5/tools/compiler/c5500/lib" -i"C:/ti/ccsv5/tools/compiler/c5500/include" -i"J:/C55_Viterbi/viterbi_C55/viterbi_C55" -i"J:/C55_Viterbi/viterbi_C55/viterbi_C55/../../viterbi_C55" -i"C:/CCSTUD~1.1/C5500/csl/lib" --reread_libs --display_error_number --warn_sections --rom_model -o "J:/C55_Viterbi/viterbi_C55/viterbi_C55/../../viterbi_C55/Debug/viterbi_C55.out" "C:/temp_XP/C55_Viterbi/viterbi_C55/Debug/viterbi_upck.obj" "C:/temp_XP/C55_Viterbi/viterbi_C55/Debug/viterbi_enc.obj" "C:/temp_XP/C55_Viterbi/viterbi_C55/Debug/viterbi_dec.obj" "C:/temp_XP/C55_Viterbi/viterbi_C55/Debug/Viterbi_t.obj" -l"rts55.lib" "J:/C55_Viterbi/55x.cmd" warning #10210-D: creating ".sysstack" section with default size of 0x3e8; use the -sysstack option to change the default size 'Finished building target: J:/C55_Viterbi/viterbi_C55/viterbi_C55/../../viterbi_C55/Debug/viterbi_C55.out' ' ' **** Build Finished ****