for ref only - (800x480) DSI Clock= HVFPS = 928x525x60= 23.232MHz LVDS Clock= DSI Clock*24(bpp)/2(DDR)*4(Lanes)= 87.696MHz EN toggle 10ms delay 0x0A 0x01 0x0B 0x10 0x10 0x26 0x11 0x00 0x12 0x11 0x18 0x78 0x19 0x00 0x1A 0x03 0x1B 0x00 0x20 0x20 0x21 0x03 0x28 0x21 0x29 0x00 0x2C 0x30 0x2D 0x00 0x30 0x01 0x31 0x00 0x34 0x28 0xE0 0x01 0xE1 0xFE (ignore PLL unlock as it is sensitive, If all the time 0xE5=01 and display indeed goes blank we can write FF) 10ms delay 0x0D 0x01 // PLL enable 10ms delay 0x09 0x00 // Soft Reset wait for DSI source to start streaming(maybe give 750ms -900ms delay- this will not hinder in display coming up -rather monitoring error- if error happens during this period ignore) 0xE5 0xFF start observing INT gpio or 0xE5 for further errors here onwards