Test starts 0 = 0x36 1 = 0x38 2 = 0x49 3 = 0x53 4 = 0x44 5 = 0x20 6 = 0x20 7 = 0x20 8 = 0x02 9 = 0x00 10 = 0x86 11 = 0x00 12 = 0x00 13 = 0x01 14 = 0x00 15 = 0x00 16 = 0x20 17 = 0x00 18 = 0x7b 19 = 0x00 20 = 0x00 21 = 0x00 22 = 0x00 23 = 0x00 24 = 0x00 25 = 0x00 26 = 0x00 27 = 0x00 28 = 0x00 29 = 0x00 30 = 0x00 31 = 0x00 32 = 0x70 33 = 0x08 34 = 0x00 35 = 0x00 36 = 0xa0 37 = 0x05 38 = 0x00 39 = 0x00 40 = 0x00 41 = 0x00 42 = 0x00 43 = 0x00 44 = 0x20 45 = 0x00 46 = 0x00 47 = 0x00 48 = 0x0a 49 = 0x00 50 = 0x00 51 = 0x00 52 = 0x50 53 = 0x00 54 = 0x1b 55 = 0x00 56 = 0x30 57 = 0x00 58 = 0x03 59 = 0x00 60 = 0x00 61 = 0x00 62 = 0x00 63 = 0x00 64 = 0xaf 65 = 0x61 66 = 0x00 67 = 0x00 68 = 0x80 69 = 0x00 70 = 0x10 71 = 0x09 72 = 0xc8 73 = 0x05 74 = 0x70 75 = 0x00 76 = 0x25 77 = 0x00 78 = 0x20 79 = 0x00 80 = 0x0a 81 = 0x00 82 = 0x70 83 = 0x08 84 = 0xa0 85 = 0x05 86 = 0x20 87 = 0x00 88 = 0x40 89 = 0xe4 90 = 0x0d 91 = 0x00 92 = 0x10 93 = 0x00 94 = 0xb0 95 = 0x00 96 = 0xa0 97 = 0x60 98 = 0xa4 99 = 0x00 100 = 0x00 101 = 0x00 102 = 0x00 103 = 0x00 104 = 0x00 105 = 0x00 106 = 0x00 107 = 0x00 108 = 0x00 109 = 0x00 110 = 0x00 111 = 0x00 112 = 0x00 113 = 0x00 114 = 0x00 115 = 0x00 116 = 0x00 117 = 0x01 118 = 0x02 119 = 0x01 120 = 0x80 121 = 0x00 122 = 0x00 123 = 0x00 124 = 0x00 125 = 0x00 126 = 0x00 127 = 0x00 128 = 0x00 129 = 0x00 130 = 0x00 131 = 0x00 132 = 0x00 133 = 0x00 134 = 0x00 135 = 0x00 136 = 0x00 137 = 0x1f 138 = 0x7c 139 = 0xf0 140 = 0xc1 141 = 0x07 142 = 0x1f 143 = 0x7c 144 = 0xf0 145 = 0xc1 146 = 0x07 147 = 0x30 148 = 0x80 149 = 0x00 150 = 0x00 151 = 0x04 152 = 0x01 153 = 0x00 154 = 0x00 155 = 0x00 156 = 0x00 157 = 0x00 158 = 0x00 159 = 0x00 160 = 0x01 161 = 0xff 162 = 0xff 163 = 0x00 164 = 0x00 165 = 0x00 166 = 0x00 167 = 0x00 168 = 0x00 169 = 0x00 170 = 0x00 171 = 0x00 172 = 0x00 173 = 0x00 174 = 0x00 175 = 0x00 176 = 0x04 177 = 0x78 178 = 0xac 179 = 0xac 180 = 0x08 181 = 0x6c 182 = 0x9c 183 = 0x9c 184 = 0x0c 185 = 0x5c 186 = 0x5c 187 = 0x5c 188 = 0x0c 189 = 0x0c 190 = 0x0c 191 = 0x0c 192 = 0x3f 193 = 0x3f 194 = 0x0f 195 = 0x00 196 = 0x00 197 = 0x00 198 = 0x00 199 = 0x00 200 = 0x00 201 = 0x00 202 = 0x00 203 = 0x00 204 = 0x00 205 = 0x00 206 = 0x00 207 = 0x00 208 = 0x00 209 = 0x00 210 = 0x00 211 = 0x00 212 = 0x00 213 = 0x00 214 = 0x00 215 = 0x00 216 = 0x00 217 = 0x00 218 = 0x00 219 = 0x00 220 = 0x00 221 = 0x00 222 = 0x00 223 = 0x00 224 = 0x00 225 = 0x00 226 = 0x00 227 = 0x00 228 = 0x00 229 = 0x00 230 = 0x00 231 = 0x00 232 = 0x00 233 = 0x00 234 = 0x00 235 = 0x00 236 = 0x00 237 = 0x00 238 = 0x00 239 = 0x00 240 = 0x00 241 = 0x00 242 = 0x00 243 = 0x00 244 = 0x01 245 = 0x02 246 = 0x00 247 = 0x00 248 = 0x06 249 = 0x00 250 = 0x00 251 = 0x00 252 = 0x00 253 = 0x00 254 = 0x00 255 = 0x00