We dump the following registers: • 0x26 power path (8 bytes RO) • 0x27 global system config (14 bytes) • 0x28 port configuration (8 bytes) • 0x29 port control (4 bytes) • 0x2d boot flags (12 bytes RO) • 0x32 transmit source (64 bytes) • 0x33 transmit sink (57 bytes) 1. Startup configuration 3 Registers read-out after startup: 0x26 : 0x08 0x00 0x00 0x00 0x00 0x40 0x00 0x00 0x00 0x27 : 0x0e 0x00 0x00 0x02 0x00 0x00 0x00 0x00 0x00 0x10 0x10 0x00 0x00 0x30 0x76 0x28 : 0x08 0x08 0x00 0xb6 0x3f 0x00 0x00 0x00 0x00 0x29 : 0x04 0x02 0x10 0x01 0x40 0x2d : 0x0c 0x00 0x00 0x00 0x00 0xa2 0x06 0x00 0x00 0x30 0x00 0x00 0x00 0x32 : 0x40 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x33 : 0x39 0x02 0x5a 0x90 0x01 0x01 0x2c 0x41 0x06 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x2c 0x69 0x11 0x00 0x2c 0x69 0x11 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 2. Switch to DFP source mode Using RAW data from TPS65981 UI tool: 0x27 = 0x78000000141400800000000a0001 0x28 = 0x1dfb658c9 0x29 = 0x4011c4c2 0x32 = 0x190000000000000000000000000000000000000000000000000000501912c0000000100000001 0x33 = 0x4001692c4001692c00000000000000000000000000000000000000009901905a3601905a02 Registers read-out after switching to source mode: 0x26 : 0x08 0x00 0x00 0x00 0x00 0x40 0x00 0x00 0x00 0x27 : 0x0e 0x01 0x00 0x0a 0x00 0x00 0x00 0x80 0x00 0x14 0x14 0x00 0x00 0x00 0x78 0x28 : 0x08 0xc9 0x58 0xb6 0xdf 0x01 0x00 0x00 0x00 0x29 : 0x04 0xc2 0xc4 0x11 0x40 0x2d : 0x0c 0x00 0x00 0x00 0x00 0xa2 0x06 0x00 0x00 0x30 0x00 0x00 0x00 0x32 : 0x40 0x01 0x00 0x00 0x00 0x01 0x00 0x00 0x00 0x2c 0x91 0x01 0x05 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x90 0x01 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x33 : 0x39 0x02 0x5a 0x90 0x01 0x36 0x5a 0x90 0x01 0x99 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x2c 0x69 0x01 0x40 0x2c 0x69 0x01 0x40 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00