Configuration 1: Configuring Channel-A for Data Switch Transmit to use same channel LS and Data Switch Receive to use alternate channel HS where PRTAD0 pin control is disabled 1 0x18 0x1E 0x00 0x8630 1 0x18 0x1E 0x00 0x0610 1 0x18 0x1E 0x1D 0x0 1 0x18 0x1E 0x01 0x0B00 1 0x18 0x07 0x00 0x2000 1 0x18 0x01 0x96 0x0 1 0x18 0x1E 0x17 0x2020 1 0x18 0x1E 0x18 0x2C20 1 0x18 0x1E 0x19 0x2520 1 0x18 0x1E 0x1A 0xEC20 1 0x18 0x1E 0x0E 0x0008 1 0x18 0x01 0x9000 0x024D 1 0x18 0x1E 0x8101 0x0004 1 0x18 0x1E 0x8100 0x0004 1 0x18 0x1E 0x8100 0x0000 1 0x18 0x01 0x9001 0x0200 1 0x18 0x07 0x00 0x3000 1 0x18 0x01 0x96 0x2 1 0x18 0x01 0x9005 0x1C00 1 0x18 0x1E 0x0003 0xC888 1 0x18 0x1E 0x0004 0x3800 1 0x18 0x07 0x00 0x3200 0 0x18 0x07 0x00 Configuring Channel-B for Data Switch Transmit to use alternate channel LS and Data Switch Receive to use same channel HS where PRTAD0 pin control is disabled 1 0x19 0x1E 0x1D 0x0 1 0x19 0x1E 0x01 0x0B00 1 0x19 0x07 0x00 0x2000 1 0x19 0x01 0x96 0x0 1 0x19 0x1E 0x17 0x2020 1 0x19 0x1E 0x18 0xAC20 1 0x19 0x1E 0x19 0x2520 1 0x19 0x1E 0x1A 0x6C20 1 0x19 0x1E 0x0E 0x0008 1 0x19 0x01 0x9000 0x024D 1 0x19 0x1E 0x8101 0x0004 1 0x19 0x1E 0x8100 0x0004 1 0x19 0x1E 0x8100 0x0000 1 0x19 0x01 0x9001 0x0200 1 0x19 0x07 0x00 0x3000 1 0x19 0x01 0x96 0x2 1 0x19 0x01 0x9005 0x1C00 1 0x19 0x1E 0x0003 0xC888 1 0x19 0x1E 0x0004 0x3800 1 0x19 0x07 0x00 0x3200 0 0x19 0x07 0x00 Channel-A status registers 0x18 0x1E 0x0F --> 0x3803 (Second read value) 0x18 0x1E 0x1B --> 0x0 (Second read value) 0x18 0x07 0x01 --> 0x88 (Second read value) 0x18 0x01 0x97 --> 0x0 (Second read value) 0x18 0x07 0x30 --> 0x1 (Second read value) Channel-B status registers 0x19 0x1E 0x0F --> 0x1413 (Second read value) 0x19 0x1E 0x1B --> 0x1323 (First read value) 0x19 0x1E 0x1B --> 0x1023 (Second read value) 0x19 0x07 0x01 --> 0xbd (Second read value) 0x19 0x01 0x97 --> 0x1 (Second read value) 0x19 0x07 0x30 --> 0x9 (Second read value) With configuration 1, near end XAUI link at Device1 (LS-A) is showing UP and far end 10GKR link at Device3 (HS-B) is showing DOWN.