Configuration 2: Configuring Channel-A & B for Data Switch Transmit to use alternate channel LS and Data Switch Receive to use alternate channel HS with PRTAD0 pin to control Channel A Rx data switch 1 0x18 0x1E 0x00 0xBE30 1 0x18 0x1E 0x00 0x3E30 1 0x18 0x1E 0x1D 0x0 1 0x18 0x1E 0x1 0x0B00 1 0x18 0x7 0x00 0x2000 1 0x18 0x1 0x96 0x0 1 0x18 0x1E 0x0017 0x3220 1 0x18 0x1E 0x0019 0x3720 1 0x18 0x1E 0xE 0x0008 1 0x18 0x1 0x9000 0x024D 1 0x18 0x1E 0x8101 0x0004 1 0x18 0x1E 0x8100 0x0004 1 0x18 0x1E 0x8100 0x0000 1 0x18 0x1 0x9001 0x0200 1 0x18 0x7 0x00 0x3000 1 0x18 0x1 0x96 0x2 1 0x18 0x1 0x9005 0x1C00 1 0x18 0x1E 0x0003 0xC888 1 0x18 0x1E 0x0004 0x3800 1 0x18 0x7 0x00 0x3200 0 0x18 0x7 0x00 Channel-A status registers 0x18 0x1E 0x0F --> 0x3803 (Second read value) 0x18 0x07 0x01 --> 0x88 (Second read value) 0x18 0x01 0x97 --> 0x0 (Second read value) 0x18 0x07 0x30 --> 0x1 (Second read value) 0x18 0x1E 0x1B --> 0x0 (Second read value) 0x18 0x1E 0x11 --> 0xfffd (First read value) 0x18 0x1E 0x12 --> 0xfffd (First read value) 0x18 0x1E 0x13 --> 0xfffd (First read value) 0x18 0x1E 0x14 --> 0xfffd (First read value) 0x18 0x1E 0x15 --> 0x8147 (Second read value) 0x18 0x1E 0x16 --> 0xf000 Channel-B status registers 0x19 0x1E 0x0F --> 0x1403 (Second read value) 0x19 0x07 0x01 --> 0xbd (Second read value) 0x19 0x01 0x97 --> 0x1 (Second read value) 0x19 0x07 0x30 --> 0x9 (Second read value) 0x19 0x1E 0x1B --> 0x4787 (First read value) 0x19 0x1E 0x1B --> 0x4383 (Second read value) 0x19 0x1E 0x16 --> 0xf037 With configuration 2, near end XAUI link at Device1 (LS-A) is showing UP and far end 10GKR link at Device3(HS-B) is showing UP, but traffic is not flowing