# This uEnv.txt file can contain additional environment settings that you # want to set in U-Boot at boot time. This can be simple variables such # as the serverip or custom variables. The format of this file is: # variable=value # NOTE: This file will be evaluated after the bootcmd is run and the # bootcmd must be set to load this file if it exists (this is the # default on all newer U-Boot images. This also means that some # variables such as bootdelay cannot be changed by this file since # it is not evaluated until the bootcmd is run. optargs=vt.global_cursor_default=0