Texas Instruments, Inc. CC2540/41 Bluetooth Low Energy Software Development Kit Release Notes ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.2.1 Apr 13, 2012 Notices: - This version of the Texas Instruments BLE stack and software is a minor update to the v1.2 release. It contains some minor enhancements and bug fixes, with no API changes or major functional changes. Changes and Enhancements: - When advertising is enabled by calling GAP_MakeDiscoverable, the first advertisement event will now occur within a few milliseconds, rather than waiting for 10ms. Bug Fixes: - The HidEmuKbd project now properly implements the HID Service include of the Battery Service. This bug fix allows for proper interoperability between the CC254x HID Profile and host systems running Windows 8. - The source code file hal_board_cfg.h has been updated to better support the serial bootloader (SBL) and Universal Bootloader (UBL). - Scanning in BTool can now be cancelled at any time without hanging or freezing the system. Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. For technical support please visit the Texas Instruments Bluetooth low energy E2E Forum: http://e2e.ti.com/support/low_power_rf/f/538.aspx ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.2 Feb 13, 2012 Notices: - This version of the Texas Instruments BLE stack and software includes support for the CC2541, as well as some enhancements and bug fixes. Details of these can be found below. If you have not previously worked with the v1.1b release (which had limited distribution) it is recommend that you also read the notes detailing the changes and enhancements from v1.1a to v1.1b in addition to the notes for v1.2. Changes and Enhancements: - All projects have been migrated from IAR v7.60 to IAR v8.10.4. In order to build all projects, be sure to upgrade and have IAR v8.10.4. Also, be sure to download and install all of the latest patches from IAR for full CC2540 and CC2541 support. - Multi-role and combo-role support has been enhanced. The BLE stack can now support simultaneously advertising and/or scanning while in a connection as either a master or a slave. This allows for a central device to perform device discovery while in a connection. All previous rules for multiple simultaneous connections as a central device still apply (see v1.1a release notes below). - New sample projects "SimpleBLEBroadcaster" and "SimpleBLEObserver" have been added, as example projects for pure broadcaster and observer applications with very low code size. The projects make use of new GAP role profiles broacaster.c and observer.c that are included. - All projects have a modified architecture from the v1.1, v1.1a, and v1.1b releases. Each project contains a file "buildConfig.cfg" that can be found in the project directory and is included in the IAR project workspace as part of the "TOOLS" group. The settings in this file determine the role of the device in the application. Based on this configuration, different pieces of the BLE stack in object code are linked in, causing the code size to be larger or smaller depending on the roles supported. For example, HostTestRelease by default is now configured to support every single BLE GAP role in a single build, and therefore has a large code size (approx. 165kB). On the other hand, SimpleBLEBroadcaster is configured to only support the GAP broadcaster role, and therefore has a very small code size (approx. 39kB). - The function GAPRole_SendUpdateParam in peripheral.c has been made public to allow a peripheral application to send an L2CAP connection parameter update request at any time. - The names and configuration of the BLE stack libraries have changed. Different libraries are used depending on the GAP role (or combination of roles) used by the application. More information can be found in section 3.3.5the BLE Software Developer's Guide. - All library files now support power management. Power management must be enabled by the application by calling osal_pwrmgr_device( PWRMGR_BATTERY );. All sample applications that use power management make this call in the main function. - All GATT service source code has been cleaned up to make handling of client characteristic configuration descriptors (CCCDs) simpler. All CCCDs are now processing is now handled by GATTServApp and no longer must be handled by the service itself. Examples of this can be found in the included example services such as SimpleGATTprofile, Simple Keys service, Accelerometer service, etc... - The HostTestRelease network processor project now includes HCI Vendor Specific commands for each GATT client sub-procedure, matching the GATT client API. All GATT commands have been added to the "Adv. Commands" tab in BTool. The functions in the BTool GUI "Read / Write" tab now make use of the GATT commands as opposed to ATT commands. - The old "EmulatedKeyboard" project has been removed and replaced with the new "HIDEmuKbd" project. The new project performs the same functions as the old one, but is now based on the "HID over GATT Profile" v1.0 specification (HOGP_SPEC_V10) that has been adopted by the Bluetooth SIG. The HID profile functionality has been implemented in a OSAL task that runs separate from the application to allow for easy portability to other HID projects. More details on the new application can be found in the BLE Sample Application Guide included as part of the release. The following additional new services / profiles have been included to fully support the HOGP specification: - HID Service v1.0 (HIDS_SPEC_V10) - Scan Parameters Profile v1.0 (ScPP_SPEC_V10) - Scan Parameters Service v1.0 (ScPS_SPEC_V10) - Device Information Service v1.1 (DIS_SPEC_V11r00) - Battery Service v1.0 (BAS_SPEC_V10) - The KeyFobDemo project has been updated to use the adopted battery service. The custom battery service that was used in previous released has been removed. - The TimeApp project has been updated to include support for the Phone Alert Status Profile (PASP_SPEC_V10) in the Client role. - Support for "Production Test Mode" has been added, allowing a BLE application in a "single-chip" configuration to temporarily expose the HCI over the UART interface when triggered externally to do so (e.g. hold a GPIO pin low during power up). This allows the device to be connected to a Bluetooth tester in order to run direct test mode (DTM) commands on a production line using the final release firmware, while leaving the UART GPIO pins available for the application to use at all other times - A Universal Boot Loader (UBL) using the USB Mass Storage Device (USB-MSD) class has been added along with a Serial Boot Loader (SBL). The HostTestRelease project includes configurations with examples of both boot loaders. The SBL project is included with the installer. More information on the UBL can be found in the following document: C:\Texas Instruments\BLE-CC254x-1.2\Documents\ Universal Boot Loader for SOC-8051 by USB-MSD Developer's Guide.pdf - HCI extension command HCI_EXT_MapPmIoPortCmd added to support toggling of a GPIO line as CC254x device goes in and out of sleep. This command can be used to automatically control the bypass line of the TPS62730 DC/DC converter for reducing power consumption in an optimized manner. - A slave device will now dynamically widen it's Rx window when a previous connection event was missed. This improves connection stability by accounting for additional clock drift that may have occurred since the last successful connection event. - The application now has the capability to change the permissions of the device name in the GAP service by calling GGS_SetParameter and changing the value of the parameter GGS_W_PERMIT_DEVICE_NAME_ATT. The application can also receive a callback when a client device writes a new name to the device. The application registers the callback by calling GGS_RegisterAppCBs. The prototype for GGS_RegisterAppCBs can be found in gapgattserver.h. Bug Fixes: - Duplicate filtering now works with combination states. - Various minor application / profile bug fixes. Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. For technical support please visit the Texas Instruments Bluetooth low energy E2E Forum: http://e2e.ti.com/support/low_power_rf/f/538.aspx ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.1b Nov 30, 2011 Notices: - This version of the Texas Instruments BLE stack and software includes support for the CC2541, as well as some minor enhancements and bug fixes. Details of these can be found below. The general software architecture remains the same as in the v1.1 and v1.1a releases. Changes and Enhancements: - BLE stack libraries for the CC2541 are included. - All BLE libraries are renamed and now indicate whether they are used for CC2540 or CC2541. - For each project and configuration, new IAR projects are included for use with the CC2541. The only exception is that any project/configuration that uses the USB interface has not been replicated for the CC2541, as it does not have an on-chip hardware USB interface. - Link-layer processing has been optimized to provide for reduced power consumption during connection events and advertising events. - SimpleBLEPeripheral and SimpleBLECentral now use the HCI_EXT_ClkDivOnHaltCmd, which reduces the current level while the CC2540/41 radio is active. - The bond manager has been updated to allow peripheral devices to properly pair, bond, and resolve the address of central devices that use the private resolvable address type. - New command HCI_EXT_SetMaxDtmTxPowerCmd included, which allows the maximum Tx power level to be set. This is useful when using Direct Test Mode (DTM), in that the Tx power level will be set to the maximum value set by the HCI_EXT_SetMaxDtmTxPowerCmd command, which may be less than +4dBm for the CC2540 and less than 0dBm for the CC2541. The function prototype can be found in hci.h. Bug Fixes: - The command HCI_EXT_SetTxPowerCmd is now properly working. Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. - Duplicate filtering does not work when scan is used in combination with a connection. For technical support please visit the Texas Instruments Bluetooth low energy E2E Forum: http://e2e.ti.com/support/low_power_rf/f/538.aspx ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.1a Aug 10, 2011 Changes and Enhancements: - The thermometer profile sample application has been updated to support stored measurements. The TI_BLE_Sample_Applications_Guide has been updated to match these changes. Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. - Duplicate filtering does not work when scan is used in combination with a connection. For technical support please visit the Texas Instruments Bluetooth low energy E2E Forum: http://e2e.ti.com/support/low_power_rf/f/538.aspx ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.1 July 13, 2011 Notices: - This version of the Texas Instruments BLE stack and software features several changes, enhancements, and bug fixes from v1.0. Details of these can be found below. Changes and Enhancements: - All projects have been migrated from IAR v7.51A to IAR v.7.60. In order to build all projects, be sure to upgrade and have IAR v7.60. Also, be sure to download and install all of the latest patches from IAR for full CC2540 support. - The stack now supports up to 3 simultaneous connection as a central / master device, with a few constraints: - All connection intervals must be a multiple of the minimum connection interval (i.e. the minimum connection interval is the greatest common denominator of all connection intervals). - The minimum connection interval allowed is 25ms when using more than one connection. - When more than one connection is active, only one data packet per connection event will be allowed in each direction. - Scanning is not supported while in a connection. The consequences of this is that device discovery is not possible while in a connection. Therefore, to discover and connect to multiple devices, the device discovery must occur before the first connection is established. - Several new sample projects are included, with examples of many different BLE applications / profiles. Full details on the sample applications can be found in the BLE Sample Applications Guide, which can be accessed from the Windows Start Menu. These sample applications implement various functions. Some are based on adopted Bluetooth specifications, some are based on draft specifications, and others are custom designed by Texas Instruments. These projects should serve as good examples for various other BLE applications. - The following updates have been made to BTool (more information on these updates can be found in the CC2540DK-MINI User Guide which can be downloaded here: http://www.ti.com/lit/pdf/swru270): - Improved GUI and robustness. - All functions on the GUI been updated to handle multiple simultaneous connections. - A new "Pairing / Bonding" tab has been added, allowing link encryption and authentication, passkey entry, and saving / loading of long-term key data (from bonding) to file. - Ability to "Cancel" a link establishment while the dongle is initiating. - The following additional new controller stack features are included in this release: - Support for multiple simultaneous connections as a master (details above) - HCI Vendor Specific function HCI_EXT_SetSCACmd allows you to specify the exact sleep clock accuracy as any value from 0 to 500 PPM, in order to support any crystal accuracy with optimal power consumption. This feature is only available for slave / peripheral applications. - HCI Vendor Specific function HCI_EXT_SetMaxDtmTxPowerCmd allows you to set the maximum transmit output power for Direct Test Mode. This allows you to perform use the LE Transmitter Test command with power levels less than +4dBm. - A master device can now advertise while in a connection. - New production test mode (PTM) has been added allowing the CC2540 to run Direct Test Mode (DTM) while connected to a tester using a "single-chip" BLE library. - The controller now uses DMA to more efficiently encrypt and decrypt packets. All BLE projects must now define HAL_AES_DMA=TRUE in the preprocessor settings when using the v1.1 libraries. - The following additional new host stack features are included in this release: - A new GAP central role profile for single-chip embedded central applications is included, with functions similar to the GAP peripheral role profile. The SimpleBLECentral project serves as an example of an application making use of the central role profile. - The GAP peripheral role has been optimized to significantly improve power consumption while advertising with small amounts of data by no longer transmitting non-significant bytes from in the advertisement and scan response data. - The following additional new application / profile features are included in this release: - The GAP peripheral bond manager has been replaced with a general GAP bond manager, capable of managing bond data for both peripheral and central role devices. The gap peripheral bond manager has been included for legacy support; however it is recommend to switch to the general GAP bond manager (gapbondmgr.c/h). - The bond manager also now manages the storage of client characteristic configurations for each bond as per the Bluetooth 4.0 spec. - The simple GATT profile has a new fifth characteristic. This characteristic is 5 bytes long, and has readable permissions only while in an authenticated connection. It should serve as a reference for development of other profiles which require an encrypted link. - All GATT profiles have been updated to properly handle client characteristic configurations for both single and multiple connections. Characteristic configurations now get reset to zero (notifications / indications off) after a connection is terminated, and the bond manager now stores client characteristic configurations for bonded devices so that they are remembered for next time when the device reconnects. - Added linker configuration file for support of 128kB flash versions of the CC2540. An example is included in the SimpleBLEPeripheral project. - The SimpleBLEPeripheral project "CC2540 Slave" configuration has been updated to better support the SmartRF05EB + CC2540EM hardware platform, making use of the LCD display. Bug Fixes: - The following bugs have been fixed in the controller stack: - Scanning now working for master devices with power savings enabled. - RSSI reads no longer require a data packet to update. - Improved stability when using very high slave latency setting - HCI LE direct test modes now working properly. - HCI Read Local Supported Features now returns the proper value. - Use of two advertising channels now works. - When connecting to a device on the whitelist, the correct peer device address is returned to the host. - The following bugs have been fixed in the host stack: - Pairing no longer fails when either device is using a static, private resolvable, or private non-resolvable address. - The following bugs have been fixed in the profiles / applications: - Reading of RSSI with peripheral role profile now working. - Peripheral role profile now allows all legal whitelist modes. - Can now connect with short connection intervals (such as 7.5ms), since bond manager now reads data from NV memory upon initialization rather than immediately after a connection is established. Pairing still may not be stable when using the bond manager with very short connection intervals (for reason noted in "Known Issues" below) Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. - Duplicate filtering does not work when scan is used in combination with a connection. For technical support please visit the Texas Instruments Bluetooth low energy E2E Forum: http://e2e.ti.com/support/low_power_rf/f/538.aspx ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- Version 1.0 October 7, 2010 Notices: - The Texas Instruments Bluetooth® low energy (BLE) software development kit includes all necessary software to get started on the development of single-mode BLE applications using the CC2540 system-on-chip. It includes object code with the BLE protocol stack, a sample project and applications with source code, and BTool, a Windows PC application for testing BLE applications. In addition to the software, the kit contains documentation, including a developer’s guide and BLE API guide. - For complete information on the BLE software development kit, please read the developer's guide: BLE Software Developer's Guide: \Documents\TI_BLE_Software_Developer's_Guide.pdf (Also can be accessed through the Windows Start Menu) - The following additional documentation is included: BLE API Guide: \Documents\BLE_API_Guide_main.htm Vendor Specific HCI Guide: \Documents\TI_BLE_Vendor_Specific_HCI_Guide.pdf HAL Drive API Guide: \Documents\hal\HAL Driver API.pdf OSAL API Guide: \Documents\osal\OSAL API.pdf - The following software projects are included, all built using IAR Embedded Workbench v7.51A: SimpleBLEPeripheral: \Projects\ble\SimpleBLEPeripheral\CC2540DB\SimpleBLEPeripheral.eww HostTestRelease: \Projects\ble\HostTestApp\CC2540\HostTestRelease.eww - The following Windows PC application is included: BTool: \Projects\BTool\BTool.exe (Also can be accessed through the Windows Start Menu) Changes: - Initial Release Bug Fixes: - Initial Release Known Issues: - Use of the NV memory (to save application data or BLE Host bonding information) during a BLE connection may cause an unexpected disconnect. The likelihood of this happening increases with frequent usage, especially when using short connection intervals. The cause is related to the NV wear algorithm which at some point may cause an NV page erase which can disrupt system real-time processing. It is therefore recommended that the NV memory be used sparingly, or only when a connection is not active. ------------------------------------------------------------------------------- -------------------------------------------------------------------------------