/*
 * Copyright (c) 2015-2017, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== rfEasyLinkTx.c ========
 */
 /* Standard C Libraries */
#include <stdlib.h>

/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/Assert.h>
#include <xdc/runtime/Error.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/posix/unistd.h>

/* TI-RTOS Header files */
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>


#include DeviceFamily_constructPath(inc/hw_prcm.h)
#include DeviceFamily_constructPath(driverlib/sys_ctrl.h)

/* Board Header files */
#include "Board.h"

/* EasyLink API Header files */
#include "easylink/EasyLink.h"

/* Undefine to not use async mode */
#define RFEASYLINKTX_ASYNC

#define RFEASYLINKTX_TASK_STACK_SIZE    1024
#define RFEASYLINKTX_TASK_PRIORITY      2

#define RFEASYLINKTX_BURST_SIZE         10
#define RFEASYLINKTXPAYLOAD_LENGTH      30

Task_Struct txTask;    /* not static so you can see in ROV */
static Task_Params txTaskParams;
static uint8_t txTaskStack[RFEASYLINKTX_TASK_STACK_SIZE];

/* Pin driver handle */
static PIN_Handle pinHandle;
static PIN_State pinState;


PIN_Handle hButtons;

Semaphore_Struct but1_Sem;
Semaphore_Struct but2_Sem;

/* Clock used for debounce logic */
Clock_Struct buttonClock;
Clock_Handle hButtonClock;

PIN_Handle buttonHandle;

/* PIN_Id for active button (in debounce period) */
PIN_Id activeButtonPinId;

PIN_State buttonStateDetect;

/* Wake-up Button pin table */
PIN_Config ButtonTableWakeUp[] = {
    Board_PIN_BUTTON0     | PIN_INPUT_EN | PIN_PULLUP | PINCC26XX_WAKEUP_NEGEDGE,
    Board_PIN_BUTTON1     | PIN_INPUT_EN | PIN_PULLUP | PINCC26XX_WAKEUP_NEGEDGE,
    PIN_TERMINATE                                 /* Terminate list */
};


/*
 * Application LED pin configuration table:
 *   - All LEDs board LEDs are off.
 */
PIN_Config pinTable[] = {
    Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_PIN_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
#if defined __CC1352R1_LAUNCHXL_BOARD_H__
    Board_DIO30_RFSW | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
#endif    
	PIN_TERMINATE
};


static uint16_t seqNumber;

#ifdef RFEASYLINKTX_ASYNC
static Semaphore_Handle txDoneSem;
#endif //RFEASYLINKTX_ASYNC

#ifdef RFEASYLINKTX_ASYNC
void txDoneCb(EasyLink_Status status)
{
    if (status == EasyLink_Status_Success)
    {
        /* Toggle LED1 to indicate TX */
        //PIN_setOutputValue(pinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
    }
    else if(status == EasyLink_Status_Aborted)
    {
        /* Toggle LED2 to indicate command aborted */
        //PIN_setOutputValue(pinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
    }
    else
    {
        /* Toggle LED1 and LED2 to indicate error */
        //PIN_setOutputValue(pinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
        //PIN_setOutputValue(pinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
    }

    Semaphore_post(txDoneSem);
}
#endif //RFEASYLINKTX_ASYNC

static void rfEasyLinkTxFnx(UArg arg0, UArg arg1)
{
    uint8_t txBurstSize = 0;

#ifdef RFEASYLINKTX_ASYNC
    /* Create a semaphore for Async */
    Semaphore_Params params;
    Error_Block eb;

    /* Init params */
    Semaphore_Params_init(&params);
    Error_init(&eb);

    /* Create semaphore instance */
    txDoneSem = Semaphore_create(0, &params, &eb);
#endif //TX_ASYNC

    /* Pend on semaphore before going to shutdown */
    Semaphore_pend(Semaphore_handle(&but1_Sem), BIOS_WAIT_FOREVER);

    PIN_setOutputValue(pinHandle, Board_PIN_LED2, 1);
    EasyLink_init(EasyLink_Phy_Custom);

    /*
     * If you wish to use a frequency other than the default, use
     * the following API:
     * EasyLink_setFrequency(868000000);
     */

    /* Set output power to 12dBm */
    EasyLink_setRfPwr(12);


    EasyLink_TxPacket txPacket =  { {0}, 0, 0, {0} };
     /* Create packet with incrementing sequence number and random payload */
    txPacket.payload[0] = (uint8_t)(seqNumber >> 8);
    txPacket.payload[1] = (uint8_t)(seqNumber++);
    uint8_t i;
    for (i = 2; i < RFEASYLINKTXPAYLOAD_LENGTH; i++)
    {
      txPacket.payload[i] = rand();
    }

    txPacket.len = RFEASYLINKTXPAYLOAD_LENGTH;
    txPacket.dstAddr[0] = 0xaa;

    /* Add a Tx delay for > 500ms, so that the abort kicks in and brakes the burst */
    if(txBurstSize++ >= RFEASYLINKTX_BURST_SIZE)
    {
        /* Set Tx absolute time to current time + 1s */
        txPacket.absTime = EasyLink_getAbsTime() + EasyLink_ms_To_RadioTime(1000);
        txBurstSize = 0;
     }
     /* Else set the next packet in burst to Tx in 100ms */
     else
     {
        /* Set Tx absolute time to current time + 100ms */
        txPacket.absTime = EasyLink_getAbsTime() + EasyLink_ms_To_RadioTime(100);
     }

        EasyLink_transmitAsync(&txPacket, txDoneCb);
        /* Wait 300ms for Tx to complete */
        if(Semaphore_pend(txDoneSem, (300000 / Clock_tickPeriod)) == FALSE)
        {
            /* TX timed out, abort */
            if(EasyLink_abort() == EasyLink_Status_Success)
            {
                /*
                 * Abort will cause the txDoneCb to be called and the txDoneSem
                 * to be released, so we must consume the txDoneSem
                 */
               Semaphore_pend(txDoneSem, BIOS_WAIT_FOREVER);
            }
        }
        /* Go to shutdown */

        PIN_setOutputValue(pinHandle, Board_PIN_LED1, 0);
        PIN_setOutputValue(pinHandle, Board_PIN_LED2, 0);

        Power_shutdown(0, 0);
}

void txTask_init(PIN_Handle inPinHandle) {
    pinHandle = inPinHandle;

    Task_Params_init(&txTaskParams);
    txTaskParams.stackSize = RFEASYLINKTX_TASK_STACK_SIZE;
    txTaskParams.priority = RFEASYLINKTX_TASK_PRIORITY;
    txTaskParams.stack = &txTaskStack;
    txTaskParams.arg0 = (UInt)1000000;

    Task_construct(&txTask, rfEasyLinkTxFnx, &txTaskParams, NULL);
}

/*
 *  ======== main ========
 */
int main(void)
{
    Semaphore_Params semParams_1;
    Semaphore_Params semParams_2;

    /* Call driver init functions. */
    Board_initGeneral();

    PINCC26XX_setWakeup(ButtonTableWakeUp);

    /* Open LED pins */
    pinHandle = PIN_open(&pinState, pinTable);
    Assert_isTrue(pinHandle != NULL, NULL);

    PIN_setOutputValue(pinHandle, Board_PIN_LED1, 0);
    PIN_setOutputValue(pinHandle, Board_PIN_LED1, 0);

    /* Configure semaphore 1. */
    Semaphore_Params_init(&semParams_1);
    semParams_1.mode = Semaphore_Mode_BINARY;
    Semaphore_construct(&but1_Sem, 0, &semParams_1);

    /* Configure semaphore 1. */
    Semaphore_Params_init(&semParams_2);
    semParams_2.mode = Semaphore_Mode_BINARY;
    Semaphore_construct(&but2_Sem, 0, &semParams_2);

    uint32_t rSrc = SysCtrlResetSourceGet();

    /* Do pin init before starting BIOS */
    /* If coming from shutdown, use special gpio table.*/
    if(rSrc == RSTSRC_WAKEUP_FROM_SHUTDOWN) {
        uint8_t i = 0;
        uint32_t but0 = 0;
        uint32_t but1 = 0;
        for (i = 0; i < 10; i++)
        {
           but0 = but0 + PINCC26XX_getInputValue(Board_PIN_BUTTON0);
           but1 = but1 + PINCC26XX_getInputValue(Board_PIN_BUTTON1);
           CPUdelay(800*50);

        }
        if (but0 < 2) {
            Semaphore_post(Semaphore_handle(&but1_Sem));
            PIN_setOutputValue(pinHandle, Board_PIN_LED1, 1);
        }
        if (but1 < 2) {
            Semaphore_post(Semaphore_handle(&but2_Sem));
            PIN_setOutputValue(pinHandle, Board_PIN_LED2, 1);
        }
    }
    else
    {
        Power_shutdown(0, 0);
    }

    Board_shutDownExtFlash();

    txTask_init(pinHandle);

    /* Start BIOS */
    BIOS_start();

    return (0);
}