/*
 * Copyright (c) 2015-2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/***** Includes *****/
#include <stdlib.h>
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>

/* Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/crypto/CryptoCC26XX.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/UART.h>

/* Board Header files */
#include "Board.h"

//#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"

#include <stdlib.h>

/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;

/*
 * Application LED pin configuration table:
 *   - All LEDs board LEDs are off.
 */
PIN_Config pinTable[] =
{
    Board_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};



/***** Defines *****/

#define TX_TASK_STACK_SIZE 1024
#define TX_TASK_PRIORITY   3

#define AES_TASK_STACK_SIZE 1024
#define AES_TASK_PRIORITY   2


#define UART_TX_TASK_STACK_SIZE 1024
#define UART_TX_TASK_PRIORITY   1

/* ASCII values of some useful keys */
#define CHAR_LINEFEED                         0x0A
#define CHAR_LINE_END_1                       0x0D   // Enter
#define CHAR_LINE_END_2                       0x03   // Enter on numpad
#define CHAR_SPACE                            0x20
#define CHAR_ZERO                             0x30
#define CHAR_UPPERCASE_START                  0x40

/* Encryption Defines */

#define macLength           (4)
#define clearTextLength     (16)
#define cipherTextLength    (macLength + clearTextLength)
#define nonceLength         (12)
#define aadLength           (14)


/* TX Configuration */
#define PAYLOAD_LENGTH      20
#define PACKET_INTERVAL     (uint32_t)(4000000*0.5f) /* Set packet interval to 500ms */


// Holds the AES-CCM setup for this example
typedef struct
{
    uint8_t key[16];                                // A 128 Bit AES key
    CryptoCC26XX_KeyLocation keyLocation;           // One of 8 key locations in the hardware
    uint8_t clearAndCipherText[cipherTextLength];   // Holds the cleartext before, and the ciphertext
                                                    // after the encryption operation.
                                                    // Ciphertext = encrypted text + message authentication code (MAC).
    uint8_t nonce[nonceLength];  // A value that is used only once (cryptographic term 'nonce')
    uint8_t header[aadLength];   // A header that is not encrypted but is authenticated in the operation (AAD).
} AesCcmExample;

AesCcmExample ccmSetup =
{
    .key = { 0x2B, 0x7E, 0x15, 0x16, 0x28, 0xAE, 0xD2, 0xA6,
             0xAB, 0xF7, 0x15, 0x88, 0x09, 0xCF, 0x4F, 0x3C },
    .keyLocation = CRYPTOCC26XX_KEY_0,
    .clearAndCipherText = { 't','h','i','s','i','s','a','p','l','a','i','n','t','e','x','t','0','0','0','0' },
   // .clearAndCipherText = txPacket[0],
    .nonce  = { 't','h','i','s','i','s','a','n','o','n','c','e' },
    .header = { 't','h','i','s','i','s','a','h','e','a','d','e','r','1' }
};


/***** Prototypes *****/
static void txTaskFunction(UArg arg0, UArg arg1);
static void aesTaskFunction(UArg arg0, UArg arg1);
static void uartTxTaskFunction(UArg arg0, UArg arg1);

/***** Variable declarations *****/
static Task_Params txTaskParams;
Task_Struct txTask;    /* not static so you can see in ROV */
static uint8_t txTaskStack[TX_TASK_STACK_SIZE];

static Task_Params uartTxTaskParams;
Task_Struct uartTxTask;    /* not static so you can see in ROV */
static uint8_t uartTxTaskStack[UART_TX_TASK_STACK_SIZE];

static Task_Params aesTaskParams;
Task_Struct aesTask;
static uint8_t aesTxTaskStack[AES_TASK_STACK_SIZE];

Semaphore_Struct semTxStruct;
Semaphore_Handle semTxHandle;

Semaphore_Struct semAesStruct;
Semaphore_Handle semAesHandle;


static RF_Object rfObject;
static RF_Handle rfHandle;
static RF_CmdHandle rfTxCmd;

UART_Handle uart = NULL;
UART_Params uartParams;

uint32_t time;
static uint8_t txPacket[PAYLOAD_LENGTH];
static PIN_Handle pinHandle;

/***** Function Initailizations *****/

void UartTxTask_init(PIN_Handle ledPinHandle) {
    pinHandle = ledPinHandle;

    Task_Params_init(&uartTxTaskParams);
    uartTxTaskParams.stackSize = UART_TX_TASK_STACK_SIZE;
    uartTxTaskParams.priority = UART_TX_TASK_PRIORITY;
    uartTxTaskParams.stack = &uartTxTaskStack;
    uartTxTaskParams.arg0 = (UInt)1000000;

    Task_construct(&uartTxTask, uartTxTaskFunction, &uartTxTaskParams, NULL);
}

void AesTask_init(PIN_Handle inPinHandle)
{
    pinHandle = inPinHandle;

    Task_Params_init(&uartTxTaskParams);
    uartTxTaskParams.stackSize = AES_TASK_STACK_SIZE;
    uartTxTaskParams.priority = AES_TASK_PRIORITY;
    uartTxTaskParams.stack = &aesTxTaskStack;
    uartTxTaskParams.arg0 = (UInt)1000000;

    Task_construct(&aesTask, aesTaskFunction, &aesTaskParams, NULL);
}


void TxTask_init(PIN_Handle inPinHandle)
{
    pinHandle = inPinHandle;

    Task_Params_init(&txTaskParams);
    txTaskParams.stackSize = TX_TASK_STACK_SIZE;
    txTaskParams.priority = TX_TASK_PRIORITY;
    txTaskParams.stack = &txTaskStack;
    txTaskParams.arg0 = (UInt)1000000;

    Task_construct(&txTask, txTaskFunction, &txTaskParams, NULL);
}

/***** Function definitions *****/

#define UART_TX_BUFFER_SIZE 256
char uartTxBuffer[UART_TX_BUFFER_SIZE];

static void uartTxTaskFunction(UArg arg0, UArg arg1)
{
    char input;
    uint8_t charIndex = 0;

    /* Open UART if not already open */
    if (uart == NULL) {
        /* Create a UART with data processing off. */
        UART_Params_init(&uartParams);
        uartParams.writeDataMode = UART_DATA_BINARY;
        uartParams.readDataMode = UART_DATA_BINARY;
        uartParams.readReturnMode = UART_RETURN_FULL;
        uartParams.readEcho = UART_ECHO_OFF;
        uartParams.baudRate = 115200;
        uart = UART_open(Board_UART0, &uartParams);

        if (uart == NULL) {
            System_abort("Error opening the UART");
        }
    }

    while (1) {

        UART_read(uart, &input, sizeof(input));
        UART_write(uart, &input, sizeof(input));


        /* Skip the line feed that appears after an enter as the first character of new line */
//        if (input == (char)CHAR_LINEFEED)
  //          charIndex--;


        if ((input == (char)CHAR_LINE_END_1) | (input == (char)CHAR_LINE_END_2)) // (charIndex < UART_SERIAL_LINE_SIZE))
        {

            /* Cancel Rx */
        //    Semaphore_post(semTxHandle);
            Semaphore_post(semAesHandle);
            /* reset index to zero to point to begining of the line */
            charIndex = 0;
        }
        else
        {
            /* Store the input character */
            txPacket[charIndex++] = input;
        }

    }
}


static void aesTaskFunction(UArg arg0, UArg arg1)
{
	int i = 0;
	for(i=0; i<20; i++){

		ccmSetup.clearAndCipherText[i] = txPacket[i];

	}

	CryptoCC26XX_Handle             handle;
	int32_t                         keyIndex;
	CryptoCC26XX_AESCCM_Transaction trans;
	int32_t                         status;

	// Initialize Crypto driver structures
	CryptoCC26XX_init();

	// Open the crypto hardware with non-exclusive access and default parameters.
	handle = CryptoCC26XX_open(Board_CRYPTO, false, NULL);
	if (handle == NULL) {
	    System_abort("CryptoCC26XX did not open");
	}

	// Allocate a key storage location in the hardware
	keyIndex = CryptoCC26XX_allocateKey(handle, ccmSetup.keyLocation, (const uint32_t *) ccmSetup.key);
	if (keyIndex == CRYPTOCC26XX_STATUS_ERROR) {
	    System_abort("Key Location was not allocated.");
	}

    Semaphore_pend(semAesHandle, BIOS_WAIT_FOREVER);

	// Encrypt and authenticate the message
	CryptoCC26XX_Transac_init((CryptoCC26XX_Transaction *) &trans, CRYPTOCC26XX_OP_AES_CCM);
	trans.keyIndex   = keyIndex;
	trans.authLength = macLength;
	trans.nonce  = (char *) ccmSetup.nonce;
	trans.header = (char *) ccmSetup.header;
	trans.fieldLength  = 3;
	trans.msgInLength  = clearTextLength;
	trans.headerLength = aadLength;
	trans.msgIn  = (char *) &(ccmSetup.clearAndCipherText[0]);                // Message is encrypted in place
//	trans.msgIn  = (char *) &(ccmSetup.txPacket[0]);                // Message is encrypted in place
	trans.msgOut = (char *) &(ccmSetup.clearAndCipherText[clearTextLength]);  // MAC will be written to this position
	status = CryptoCC26XX_transact(handle, (CryptoCC26XX_Transaction *) &trans);

	// Do AES-CCM Encryption and authentication
	if (status != CRYPTOCC26XX_STATUS_SUCCESS) {
	    System_abort("Encryption and signing failed.");
	}
	// Decrypt and authenticate message
/*	CryptoCC26XX_Transac_init((CryptoCC26XX_Transaction *) &trans, CRYPTOCC26XX_OP_AES_CCMINV);
	trans.keyIndex   = keyIndex;
	trans.authLength = macLength;
	trans.nonce  = (char *) ccmSetup.nonce;
	trans.header = (char *) ccmSetup.header;
	trans.fieldLength  = 3;
	trans.msgInLength  = cipherTextLength;
	trans.headerLength = aadLength;
	trans.msgIn  = (char *) &(ccmSetup.clearAndCipherText[0]);                // Message is decrypted in place
	trans.msgOut = (char *) &(ccmSetup.clearAndCipherText[clearTextLength]);  // Points to the MAC, is used as input here

	// Do AES-CCM decryption and authentication
	status = CryptoCC26XX_transact(handle, (CryptoCC26XX_Transaction *) &trans);
	if(status != CRYPTOCC26XX_STATUS_SUCCESS){
	    System_abort("Decryption and authentication failed.");
	}*/

	Semaphore_post(semTxHandle);

	// Release the key location
	status = CryptoCC26XX_releaseKey(handle, &keyIndex);
	if (status != CRYPTOCC26XX_STATUS_SUCCESS) {
	    System_abort("Key release was not successful.");
	}

	//Semaphore_post(semTxHandle);
}


static void txTaskFunction(UArg arg0, UArg arg1)
{
    uint32_t time;
    RF_Params rfParams;
    RF_Params_init(&rfParams);

    RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
   // RF_cmdPropTx.pPkt = txPacket;
    RF_cmdPropTx.pPkt = ccmSetup.clearAndCipherText;
    RF_cmdPropTx.startTrigger.triggerType = TRIG_ABSTIME;
    RF_cmdPropTx.startTrigger.pastTrig = 1;
    RF_cmdPropTx.startTime = 0;

    while(1)
    {
        Semaphore_pend(semTxHandle, BIOS_WAIT_FOREVER);

        if (!rfHandle) {
            /* Request access to the radio */
            rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

            /* Set the frequency */
            RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
        }

        /* Get current time */
        time = RF_getCurrentTime();

        /* Set absolute TX time to utilize automatic power management */
        time += PACKET_INTERVAL;
        RF_cmdPropTx.startTime = time;

        /* Send packet */
        rfTxCmd = RF_postCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0);

        RF_EventMask result = RF_pendCmd(rfHandle, rfTxCmd, (RF_EventCmdDone | RF_EventCmdError | RF_EventLastCmdDone |
                RF_EventCmdAborted | RF_EventCmdCancelled | RF_EventCmdStopped));

        if (!(result & RF_EventLastCmdDone))
        {
            /* Error */
            while(1);
        }

        PIN_setOutputValue(pinHandle, Board_LED1,!PIN_getOutputValue(Board_LED1));

        /* clear txPacket buffer */
//        memset(txPacket, 0, sizeof(txPacket));
        memset(ccmSetup.clearAndCipherText, 0, sizeof(ccmSetup.clearAndCipherText));

    }
}

/*
 *  ======== main ========
 */
int main(void)
{
    Semaphore_Params semParams;

    /* Call board init functions. */
    Board_initGeneral();
    Board_initUART();

    /* Open LED pins */
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    if(!ledPinHandle)
    {
        System_abort("Error initializing board LED pins\n");
    }

    /* Construct a Semaphore object to be used as a resource lock, initial count 0 */
    Semaphore_Params_init(&semParams);
    Semaphore_construct(&semTxStruct, 0, &semParams);
    Semaphore_construct(&semAesStruct, 0, &semParams);


    /* Obtain instance handle */
    semTxHandle = Semaphore_handle(&semTxStruct);
    semAesHandle = Semaphore_handle(&semAesStruct);
    /* Initialize task */
    TxTask_init(ledPinHandle);

    UartTxTask_init(ledPinHandle);

    AesTask_init(ledPinHandle);

    /* Start BIOS */
    BIOS_start();

    return (0);
}